请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMS320F28388D 你好。
我使用处理器 TMS320F28388。
我在工作中使用 PWM。
它会生成所需的信号。
我有问题。
如何立即以编程方式禁用 PWM?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好。
我使用处理器 TMS320F28388。
我在工作中使用 PWM。
它会生成所需的信号。
我有问题。
如何立即以编程方式禁用 PWM?
我已经阅读了 tripZone 模块的相关内容。
但我找不到用于禁用 PWM 输出的函数。
//
// Trip Zone module related APIs
//
//*****************************************************************************
//
//! Enables Trip Zone signal.
//!
//! \param base is the base address of the EPWM module.
//! \param tzSignal is the Trip Zone signal.
//!
//! This function enables the Trip Zone signals specified by tzSignal as a
//! source for the Trip Zone module.
//! Valid values for tzSignal are:
//! - EPWM_TZ_SIGNAL_CBC1 - TZ1 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC2 - TZ2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC3 - TZ3 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC4 - TZ4 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC5 - TZ5 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC6 - TZ6 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_DCAEVT2 - DCAEVT2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_DCBEVT2 - DCBEVT2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_OSHT1 - One-shot TZ1
//! - EPWM_TZ_SIGNAL_OSHT2 - One-shot TZ2
//! - EPWM_TZ_SIGNAL_OSHT3 - One-shot TZ3
//! - EPWM_TZ_SIGNAL_OSHT4 - One-shot TZ4
//! - EPWM_TZ_SIGNAL_OSHT5 - One-shot TZ5
//! - EPWM_TZ_SIGNAL_OSHT6 - One-shot TZ6
//! - EPWM_TZ_SIGNAL_DCAEVT1 - One-shot DCAEVT1
//! - EPWM_TZ_SIGNAL_DCBEVT1 - One-shot DCBEVT1
//!
//! \b note: A logical OR of the valid values can be passed as the tzSignal
//! parameter.
//!
//! \return None.
//
//*****************************************************************************
static inline void
EPWM_enableTripZoneSignals(uint32_t base, uint16_t tzSignal)
{
//
// Check the arguments
//
ASSERT(EPWM_isBaseValid(base));
//
// Set the trip zone bits
//
EALLOW;
HWREGH(base + EPWM_O_TZSEL) |= tzSignal;
EDIS;
}
//*****************************************************************************
//
//! Disables Trip Zone signal.
//!
//! \param base is the base address of the EPWM module.
//! \param tzSignal is the Trip Zone signal.
//!
//! This function disables the Trip Zone signal specified by tzSignal as a
//! source for the Trip Zone module.
//! Valid values for tzSignal are:
//! - EPWM_TZ_SIGNAL_CBC1 - TZ1 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC2 - TZ2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC3 - TZ3 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC4 - TZ4 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC5 - TZ5 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC6 - TZ6 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_DCAEVT2 - DCAEVT2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_DCBEVT2 - DCBEVT2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_OSHT1 - One-shot TZ1
//! - EPWM_TZ_SIGNAL_OSHT2 - One-shot TZ2
//! - EPWM_TZ_SIGNAL_OSHT3 - One-shot TZ3
//! - EPWM_TZ_SIGNAL_OSHT4 - One-shot TZ4
//! - EPWM_TZ_SIGNAL_OSHT5 - One-shot TZ5
//! - EPWM_TZ_SIGNAL_OSHT6 - One-shot TZ6
//! - EPWM_TZ_SIGNAL_DCAEVT1 - One-shot DCAEVT1
//! - EPWM_TZ_SIGNAL_DCBEVT1 - One-shot DCBEVT1
//!
//! \b note: A logical OR of the valid values can be passed as the tzSignal
//! parameter.
//!
//! \return None.
//
//*****************************************************************************
static inline void
EPWM_disableTripZoneSignals(uint32_t base, uint16_t tzSignal)
{
//
// Check the arguments
//
ASSERT(EPWM_isBaseValid(base));
//
// Clear the trip zone bits
//
EALLOW;
HWREGH(base + EPWM_O_TZSEL) &= ~tzSignal;
EDIS;
}
//*****************************************************************************
我在这里看到仅由于外部信号而禁用 PWM 信号。
我希望以编程方式禁用和启用 PWM。
如何操作?
您说的 SW 是什么意思?

我配置了 PWM。 我希望以编程方式打开输出信号、然后将其关闭。