This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280025C:配置快速比较器(CMPSS)的问题=>触发非及时中断

Guru**** 2943400 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1116153/tms320f280025c-issue-to-configure-fast-comparator-cmpss-triggering-of-the-untimely-interruption

器件型号:TMS320F280025C

您好专家、

我的快速比较器有问题。 我将为您简要介绍我的架构:我使用 TZ1至 TZ3信号通过 INPUT_X_Bar 切断我的 EPWM (它们对应于驱动器返回)、并使用 TRIPIN4信号等用于过压信号等。
我在每个 ePWM 中使用触发区中断、这个中断允许我保留事件日志以及关闭 ePWM。
我已通过 EPWM_TZ_INTERRUPT_CBC 将 TZ1与中断中的 TZ3信号连接、并通过 EPWM_TZ_INTERRUPT_DCBEVT2事件将我的 CMPSS 连接在一起。
我有问题、系统打开时、我立即在 CMPSS 级别输入中断、而所有输入都为0。 我不认为这是硬件问题、我已经多次探索过该论坛、但我找不到答案。 我一定忘记了什么、能帮我吗?
如果我不想、我不会在 TZ1、TZ2或 TZ3上发生中断、因此我将问题瞄准 CMPSS。 初始化时、TZFLG、TZCBCFLG 和 TZEINT 寄存器为0、在我看来、在每个使用的 ePWM 上、这是一致的。 但是、在配置的比较器上、XBARFLT1寄存器设置为1、无法通过 XBARCLR1寄存器将其设置为0。 但这是一个标志、而不是源信号、我尝试进入这个链、但我的推理中阻止了我。

您可以看到屏幕截图:

#include "cmpss_module.h"
#include "device.h"
#include "adc_module.h"
#include "epwm_module.h"
#include "monitoring.h"

const uint16_t THRESHOLD_MU_FUEL_CELL_PCH = 700U;
const uint16_t THRESHOLD_MU_TRAC_BATT_PCH = 950U;
const uint16_t THRESHOLD_MI_L_U = 155U;
const uint16_t THRESHOLD_MI_L_V = 155U;
const uint16_t THRESHOLD_MI_L_W = 155U;
const uint16_t THRESHOLD_MI_TRAC_BATT = 230U;
const uint16_t THRESHOLD_MT_COLD_PLATE = 120U;

uint16_t THRESHOLD_MI_L_U_DIGITAL = 0;
uint16_t THRESHOLD_MI_L_V_DIGITAL = 0;
uint16_t THRESHOLD_MI_L_W_DIGITAL = 0;
uint16_t THRESHOLD_MI_TRAC_BATT_DIGITAL = 0;
uint16_t THRESHOLD_MU_FUEL_CELL_PCH_DIGITAL = 0;
uint16_t THRESHOLD_MU_TRAC_BATT_PCH_DIGITAL = 0;

/**Comparator subsystem module initialization
   See requirement REQ_SYST0030, REQ_SYST0031, REQ_SYST0035, REQ_SYST0036, REQ_SYST0037 and REQ_SYST0038*/
void cmpss_init()
{
    /**Enable CMPSS and configure the negative input signal to come from the DAC*/
    CMPSS_enableModule(CMPSS1_BASE);
    CMPSS_enableModule(CMPSS2_BASE);
    CMPSS_enableModule(CMPSS3_BASE);
    CMPSS_enableModule(CMPSS4_BASE);

    /**Use VDDA as the reference for the DAC and set DAC value to midpoint for arbitrary reference.*/
    CMPSS_configDAC(CMPSS1_BASE, CMPSS_DACREF_VDAC);
    CMPSS_configDAC(CMPSS2_BASE, CMPSS_DACREF_VDAC);
    CMPSS_configDAC(CMPSS3_BASE, CMPSS_DACREF_VDAC);
    CMPSS_configDAC(CMPSS4_BASE, CMPSS_DACREF_VDAC);

    /**To use CMP1_HP2 pin A6 for MU_TRAC_BATT_PCH*/
    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_1, 2);
    /**To use CMP1_LP3 pin A15/C7 for MU_FUEL_CELL_PCH*/
    ASysCtl_selectCMPLPMux(ASYSCTL_CMPLPMUX_SELECT_1, 3);
    /**To use CMP3_HP1 pin A5/C2 for MI_L_W*/
    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_3, 1);
    /**To use CMP2_HP1 pin A12/C1 for MI_L_U*/
    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_2, 1);
    /**To use CMP2_LP4 pin A8/C11 for MI_L_V*/
    ASysCtl_selectCMPLPMux(ASYSCTL_CMPLPMUX_SELECT_2, 4);
    /**To use CMP4_HP1 pin A7/C3 for MI_TRAC_BATT*/
    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_4, 1);

    /**Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.*/
    ///1
    THRESHOLD_MU_TRAC_BATT_PCH_DIGITAL = (((THRESHOLD_MU_TRAC_BATT_PCH * 8.2 * 0.00013796) + OFFSET_AMPLI) * ADC_RESOLUTION) / FULL_SCALE;
    CMPSS_configHighComparator(CMPSS1_BASE, CMPSS_INSRC_DAC);                   // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueHigh(CMPSS1_BASE, THRESHOLD_MU_TRAC_BATT_PCH_DIGITAL);     // Define threshold associated
    CMPSS_configOutputsHigh(CMPSS1_BASE, CMPSS_TRIP_SYNC_COMP);                 // Set output comparator (synchronous or asynchronous)
    ///2
    THRESHOLD_MU_FUEL_CELL_PCH_DIGITAL = (((THRESHOLD_MU_FUEL_CELL_PCH * 8.2 * 0.00013796) + OFFSET_AMPLI) * ADC_RESOLUTION) / FULL_SCALE;
    CMPSS_configLowComparator(CMPSS1_BASE, CMPSS_INSRC_DAC);                    // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueLow(CMPSS1_BASE, THRESHOLD_MU_FUEL_CELL_PCH_DIGITAL);      // Define threshold associated
    CMPSS_configOutputsLow(CMPSS1_BASE, CMPSS_TRIP_SYNC_COMP);                  // Set output comparator (synchronous or asynchronous)

    /**Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.*/
    ///1
    THRESHOLD_MI_L_U_DIGITAL = (((THRESHOLD_MI_L_U * 0.625 / 200) + REF_MI_H_2V5_AROUND) * ADC_RESOLUTION) / FULL_SCALE;
    CMPSS_configHighComparator(CMPSS2_BASE, CMPSS_INSRC_DAC);                   // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueHigh(CMPSS2_BASE, THRESHOLD_MI_L_U_DIGITAL);               // Define threshold associated
    CMPSS_configOutputsHigh(CMPSS2_BASE, CMPSS_TRIP_SYNC_COMP);                 // Set output comparator (synchronous or asynchronous)

    ///2
    THRESHOLD_MI_L_V_DIGITAL = (((THRESHOLD_MI_L_V * 0.625 / 200) + REF_MI_H_2V5_AROUND) * ADC_RESOLUTION) / FULL_SCALE;
    CMPSS_configLowComparator(CMPSS2_BASE, CMPSS_INSRC_DAC);                    // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueLow(CMPSS2_BASE, THRESHOLD_MI_L_V_DIGITAL);                // Define threshold associated
    CMPSS_configOutputsLow(CMPSS2_BASE, CMPSS_TRIP_SYNC_COMP);                  // Set output comparator (synchronous or asynchronous)

    /**Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.*/
    ///1
    THRESHOLD_MI_L_W_DIGITAL = (((THRESHOLD_MI_L_W * 0.625 / 200) + REF_MI_H_2V5_AROUND) * ADC_RESOLUTION) / FULL_SCALE;
    CMPSS_configHighComparator(CMPSS3_BASE, CMPSS_INSRC_DAC);                   // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueHigh(CMPSS3_BASE, THRESHOLD_MI_L_W_DIGITAL);               // Define threshold associated
    CMPSS_configOutputsHigh(CMPSS3_BASE, CMPSS_TRIP_SYNC_COMP);                 // Set output comparator (synchronous or asynchronous)

    /**Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.*/
    ///1
    THRESHOLD_MI_TRAC_BATT_DIGITAL = ((((THRESHOLD_MI_TRAC_BATT * 2 * 301) / 100000) + REF_MI_BT_1V5) * ADC_RESOLUTION) / FULL_SCALE;
    CMPSS_configHighComparator(CMPSS4_BASE, CMPSS_INSRC_DAC);                   // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueHigh(CMPSS4_BASE, THRESHOLD_MI_TRAC_BATT_DIGITAL);         // Define threshold associated
    CMPSS_configOutputsHigh(CMPSS4_BASE, CMPSS_TRIP_SYNC_COMP);                 // Set output comparator (synchronous or asynchronous)

    /**Configure TRIP4 to be CTRIP1H using the ePWM X-BAR. Attach CMPSS output to TRIPINx via EPWMXBAR module*/
    XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX00_CMPSS1_CTRIPH);
    XBAR_setEPWMMuxConfig(XBAR_TRIP5, XBAR_EPWM_MUX01_CMPSS1_CTRIPL);
    XBAR_setEPWMMuxConfig(XBAR_TRIP7, XBAR_EPWM_MUX04_CMPSS3_CTRIPH);
    XBAR_setEPWMMuxConfig(XBAR_TRIP8, XBAR_EPWM_MUX02_CMPSS2_CTRIPH);
    XBAR_setEPWMMuxConfig(XBAR_TRIP9, XBAR_EPWM_MUX03_CMPSS2_CTRIPL);
    XBAR_setEPWMMuxConfig(XBAR_TRIP10, XBAR_EPWM_MUX06_CMPSS4_CTRIPH);

    /**See the ePWM X-BAR Mux configuration table, see Crossbar(X-BAR) doc for more informations*/
    XBAR_enableEPWMMux(XBAR_TRIP4, XBAR_MUX00);
    XBAR_enableEPWMMux(XBAR_TRIP5, XBAR_MUX01);
    XBAR_enableEPWMMux(XBAR_TRIP7, XBAR_MUX04);
    XBAR_enableEPWMMux(XBAR_TRIP8, XBAR_MUX02);
    XBAR_enableEPWMMux(XBAR_TRIP9, XBAR_MUX03);
    XBAR_enableEPWMMux(XBAR_TRIP10, XBAR_MUX06);
}

/**Shutdown ePWM when DCBEVT2 is triggered*/
void cmpss_actions(uint32_t base)
{
    /**Configure ePWMx to output low on TZx TRIP*/
    EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW);
    EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZB, EPWM_TZ_ACTION_LOW);

    /**Trigger event when DCBH is high*/
    EPWM_setTripZoneDigitalCompareEventCondition(base, EPWM_TZ_DC_OUTPUT_B2, EPWM_TZ_EVENT_DCXH_HIGH);

    /**Configure DCBH to use TRIPINx as an input*/
    EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN4, EPWM_DC_TYPE_DCBH);
    EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN5, EPWM_DC_TYPE_DCBH);
    EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN7, EPWM_DC_TYPE_DCBH);
    EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN8, EPWM_DC_TYPE_DCBH);
    EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN9, EPWM_DC_TYPE_DCBH);
    EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN10, EPWM_DC_TYPE_DCBH);

    /**Enable DCB as DCBEVT2*/
    EPWM_enableTripZoneSignals(base, EPWM_TZ_SIGNAL_DCBEVT2);
    /**Enable interrupt*/
    EPWM_enableTripZoneInterrupt(base, EPWM_TZ_INTERRUPT_DCBEVT2);
}
#include "device.h"
#include "tripzone_module.h"
#include "epwm_module.h"
#include "monitoring.h"

/**Initialize trip zone concerned by DRV signals provided from InputXbar to shutdown ePWM when signals are to low level.
   See requirements REQ_SYST0022, REQ_SYST0023 and REQ_SYST0024*/
void trip_zone_config(void)
{
    /**DRV-U signals to trip zone*/
    GPIO_setPinConfig(GPIO_45_GPIO45);
    GPIO_setDirectionMode(45, GPIO_DIR_MODE_IN);
    GPIO_setPadConfig(45, GPIO_PIN_TYPE_STD);

    /**DRV-V signals to trip zone*/
    GPIO_setPinConfig(GPIO_5_GPIO5);
    GPIO_setDirectionMode(5, GPIO_DIR_MODE_IN);
    GPIO_setPadConfig(5, GPIO_PIN_TYPE_STD);

    /**DRV-W signals to trip zone*/
    GPIO_setPinConfig(GPIO_9_GPIO9);
    GPIO_setDirectionMode(9, GPIO_DIR_MODE_IN);
    GPIO_setPadConfig(9, GPIO_PIN_TYPE_STD);

    XBAR_setInputPin(INPUTXBAR_BASE, XBAR_INPUT1, 45);
    XBAR_setInputPin(INPUTXBAR_BASE, XBAR_INPUT2, 5);
    XBAR_setInputPin(INPUTXBAR_BASE, XBAR_INPUT3, 9);

    /**Enable TZx as cycle by cycle trip sources
       TZ1 for DRV_U*/
    EPWM_enableTripZoneSignals(SPWM_U, EPWM_TZ_SIGNAL_CBC1);
    EPWM_enableTripZoneSignals(SPWM_V, EPWM_TZ_SIGNAL_CBC1);
    EPWM_enableTripZoneSignals(SPWM_W, EPWM_TZ_SIGNAL_CBC1);

    /**TZ2 for DRV_V*/
    EPWM_enableTripZoneSignals(SPWM_U, EPWM_TZ_SIGNAL_CBC2);
    EPWM_enableTripZoneSignals(SPWM_V, EPWM_TZ_SIGNAL_CBC2);
    EPWM_enableTripZoneSignals(SPWM_W, EPWM_TZ_SIGNAL_CBC2);

    /**TZ3 for DRV_W*/
    EPWM_enableTripZoneSignals(SPWM_U, EPWM_TZ_SIGNAL_CBC3);
    EPWM_enableTripZoneSignals(SPWM_V, EPWM_TZ_SIGNAL_CBC3);
    EPWM_enableTripZoneSignals(SPWM_W, EPWM_TZ_SIGNAL_CBC3);

    /**Action on TZx*/
    EPWM_setTripZoneAction(SPWM_U, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW);
    EPWM_setTripZoneAction(SPWM_V, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW);
    EPWM_setTripZoneAction(SPWM_W, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW);

    EPWM_enableTripZoneInterrupt(SPWM_U, EPWM_TZ_INTERRUPT_CBC);
    EPWM_enableTripZoneInterrupt(SPWM_V, EPWM_TZ_INTERRUPT_CBC);
    EPWM_enableTripZoneInterrupt(SPWM_W, EPWM_TZ_INTERRUPT_CBC);
}

/**Interrupt is trigger if CMPSS (EpWMXbar signals) are set or if DRV (InputXbar signals TZ1 à TZ3) are set.
   If interrupt is trigger corresponding flag and variable state are set. And the processing of the variable is done in the state machine.*/
__interrupt void isr_trip_zone(void)
{
    // Priority interrupt

    // Save IER register on stack
    /*volatile uint16_t tempPIEIER = HWREGH(PIECTRL_BASE + PIE_O_IER2);

    // Set the global and group priority to allow CPU interrupts with higher priority
    IER |= M_INT2;
    IER &= MINT2;
    HWREGH(PIECTRL_BASE + PIE_O_IER2) &= MG1_1;

    // Enable Interrupts
    Interrupt_clearACKGroup(0xFFFFU);
    __asm("  NOP");
    EINT;*/

    /**Clear the flags, we will continue to take this interrupt until the TZ pin goes high.
       In TZFLG register when interrupt is due to EpWMXbar so DCxEVTx TZFLG.DCxEVTx.bit = 1 and TZFLG.CBC.bit = 1 it's normally*/
    EPWM_clearTripZoneFlag(SPWM_U, (EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_CBC | EPWM_TZ_FLAG_DCBEVT2));
    EPWM_clearTripZoneFlag(SPWM_V, (EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_CBC | EPWM_TZ_FLAG_DCBEVT2));
    EPWM_clearTripZoneFlag(SPWM_W, (EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_CBC | EPWM_TZ_FLAG_DCBEVT2));

    /**Clear corresponding bit of interrupt source
       Event log recording
       See requirement REQ_SYST0032*/
    if(EPWM_getCycleByCycleTripZoneFlagStatus(SPWM_U) == EPWM_TZ_CBC_FLAG_1)
    {
        drv_u_state = DRV_ERROR;
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_1);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_1);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_1);
        // Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }
    /**See requirement REQ_SYST0033*/
    else if(EPWM_getCycleByCycleTripZoneFlagStatus(SPWM_U) == EPWM_TZ_CBC_FLAG_2)
    {
        drv_v_state = DRV_ERROR;
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_2);
        // Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }
    /**See requirement REQ_SYST0034*/
    else if(EPWM_getCycleByCycleTripZoneFlagStatus(SPWM_U) == EPWM_TZ_CBC_FLAG_3)
    {
        drv_w_state = DRV_ERROR;
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_3);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_3);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_3);
        /// Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }
    /**See requirement REQ_SYST0031*/
    else if(XBAR_getInputFlagStatus(XBAR_INPUT_FLG_CMPSS1_CTRIPH) == PROTECTION_DETECTED)
    {
        mu_trac_batt_state = PROTECTION_DETECTED;
        XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS1_CTRIPH);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        /// Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }
    /**See requirement REQ_SYST0030*/
    else if(XBAR_getInputFlagStatus(XBAR_INPUT_FLG_CMPSS1_CTRIPL) == PROTECTION_DETECTED)
    {
        mu_fuel_cell_state = PROTECTION_DETECTED;
        XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS1_CTRIPL);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        /// Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }
    /**See requirement REQ_SYST0035*/
    else if(XBAR_getInputFlagStatus(XBAR_INPUT_FLG_CMPSS2_CTRIPH) == PROTECTION_DETECTED)
    {
        mi_l_u_state = PROTECTION_DETECTED;
        XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS2_CTRIPH);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        /// Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }
    /**See requirement REQ_SYST0036*/
    else if(XBAR_getInputFlagStatus(XBAR_INPUT_FLG_CMPSS2_CTRIPL) == PROTECTION_DETECTED)
    {
        mi_l_v_state = PROTECTION_DETECTED;
        XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS2_CTRIPL);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        /// Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }
    /**See requirement REQ_SYST0037*/
    else if(XBAR_getInputFlagStatus(XBAR_INPUT_FLG_CMPSS3_CTRIPH) == PROTECTION_DETECTED)
    {
        mi_l_w_state = PROTECTION_DETECTED;
        XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS3_CTRIPH);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        /// Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }
    /**See requirement REQ_SYST0038*/
    else if(XBAR_getInputFlagStatus(XBAR_INPUT_FLG_CMPSS4_CTRIPH) == PROTECTION_DETECTED)
    {
        mi_trac_batt_state = PROTECTION_DETECTED;
        XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS4_CTRIPH);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_DCBEVT2);
        /// Disable the interrupts to do the associated actions and not re-trigger the trip zone before the end of its processing. The interrupt will be reactivated at that time.
        Interrupt_disable(INT_EPWM1_TZ);
        Interrupt_disable(INT_EPWM2_TZ);
        Interrupt_disable(INT_EPWM4_TZ);
    }

    /**Acknowledge this interrupt to receive more interrupts from group 2*/
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP2);

    // Disable interrupts and restore registers saved:
    /*DINT;
    HWREGH(PIECTRL_BASE + PIE_O_IER2) = tempPIEIER;*/
}

谢谢、

Damien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在初始化位置

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    在启用触发区中断之前、清除标志以避免任何寄生事件。 PFB 供参考的代码片段。 请告诉我这是否解决了问题。

    //
    //在启用中断前清除所有寄生跳闸区域标志
    //
    ePWM_clearTripZoneFlag (epwmBase、ePWM_TZ_FLAG_DCAEVT1);

    ePWM_clearOneTripShotZoneFlag (epwmBase、ePWM_TZ_OST_FLAG_DCAEVT1);

     

    谢谢
    Vasudha

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Vasudha、您好!

    不能,它仍然不起作用,为什么在我使用 CBC 模式时重置主模式模块?  

    尽管我尝试复位为0、但在初始化后 XBARFLT1.CMPSSx_CTRIPx 寄存器仍保持在1级是否正常。 函数 XBAR_clearInputFlag (XBAR_INPUT_FLG_CMPSS1_CTRIPH)将在 XBARCLR 上执行操作、然后将 XBARFLG 重置为0、对吧? 对我来说不起作用、我在 XBARCLR 中看不到任何东西。 ISR 中用于确定触发哪个比较器的检测可通过 XBAR_getInputFlagStatus (XBAR_INPUT_FLG_CMPSS1_CTRIPH) NO 来完成。

    谢谢  

    Damien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [引用 userid="489604" URL"~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forume/1116153/tms320f280025c-issue-probleme-configure-fast-comparator-cmpss-trigging-of-unimitive-bc/4137717#4137717"cubost 模块,为什么它不使用复位模式?  [/报价]

    不、您只设置 CBC 模块、我刚才提供了一个参考代码。 通常、在启用中断之前、应清除标志以避免任何寄生中断。 PFB 参考片段。

    //
    //在启用中断前清除所有寄生跳闸区域标志
    //
    ePWM_clearTripZoneFlag (epwmBase、ePWM_TZ_FLAG_DCAEVT2);

    ePWM_clearCyclByCyclone TripZoneFlag (epwmBase、ePWM_TZ_CBC_FLAG_DCAEVT2);

    //
    //启用 TZ 中断
    //
    ePWM_enableTripZoneInterrupt (epwmBase、ePWM_TZ_INTERRUPT_CBC);

    谢谢
    Vasudha

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我能否使用 XBAR_getInputFlagStatus()函数在 ISR 中进行检测,以了解触发了哪个比较器?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    逐周期模式和单次触发模式之间的主要区别是什么?恐怕我无法区分这两种模式?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在哪里可以找到 PFB 基准? 请

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你(们)好  

    您能不能帮助我、为什么 XBARFLT1寄存器的值与初始化时使用的比较器有关?

    我想通过函数 XBAR_getInputFlagStatus (XBAR_INPUT_FLG_CMPSS1_CTRIPH)在该寄存器的中断中进行检测、这样做是否正确? 在我看来、它是这样的。 以下是我的代码的一部分:

    /**
     * Configure and actions CMPSS
     */
    cmpss_init();
    DEVICE_DELAY_US(10000);
    cmpss_actions(SPWM_U);
    DEVICE_DELAY_US(10000);
    cmpss_actions(SPWM_V);
    DEVICE_DELAY_US(10000);
    cmpss_actions(SPWM_W);
    DEVICE_DELAY_US(10000);
    /**
     * Clear XBARFLG1 register with CMPSS concerned (for detection => flag set 1 when comparator inputs is trigger).
     * Add delay after reset and then clear status flag (power up time).
     */
    EALLOW;
    XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS1_CTRIPH);
    DEVICE_DELAY_US(10000);
    XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS1_CTRIPL);
    DEVICE_DELAY_US(10000);
    EPWM_clearTripZoneFlag(SPWM_U, (EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_CBC | EPWM_TZ_FLAG_DCBEVT2));
    DEVICE_DELAY_US(10000);
    EPWM_clearTripZoneFlag(SPWM_V, (EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_CBC | EPWM_TZ_FLAG_DCBEVT2));
    DEVICE_DELAY_US(10000);
    EPWM_clearTripZoneFlag(SPWM_W, (EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_CBC | EPWM_TZ_FLAG_DCBEVT2));
    EPWM_clearCycleByCycleTripZoneFlag(SPWM_U ,EPWM_TZ_CBC_FLAG_DCBEVT2);
    DEVICE_DELAY_US(10000);
    EPWM_clearCycleByCycleTripZoneFlag(SPWM_V ,EPWM_TZ_CBC_FLAG_DCBEVT2);
    DEVICE_DELAY_US(10000);
    EPWM_clearCycleByCycleTripZoneFlag(SPWM_W ,EPWM_TZ_CBC_FLAG_DCBEVT2);
    EDIS;
    
    void cmpss_init()
    {
        /**Enable CMPSS and configure the negative input signal to come from the DAC*/
        CMPSS_enableModule(CMPSS1_BASE);
    
        /**Use VDDA as the reference for the DAC and set DAC value to midpoint for arbitrary reference.*/
        CMPSS_configDAC(CMPSS1_BASE, CMPSS_DACREF_VDDA | CMPSS_DACVAL_SYSCLK | CMPSS_DACSRC_SHDW);
    
    
        /**To use CMP1_HP2 pin A6 for MU_TRAC_BATT_PCH*/
        ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_1, 2);
    
        /**Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.*/
        ///1
        THRESHOLD_MU_TRAC_BATT_PCH_DIGITAL = (((THRESHOLD_MU_TRAC_BATT_PCH * 8.2 * 0.00013796) + OFFSET_AMPLI) * ADC_RESOLUTION) / FULL_SCALE;
        CMPSS_configHighComparator(CMPSS1_BASE, CMPSS_INSRC_DAC);                   // Threshold drive by GPIO or input DAC
        CMPSS_setDACValueHigh(CMPSS1_BASE, THRESHOLD_MU_TRAC_BATT_PCH_DIGITAL);     // Define threshold associated
        CMPSS_configOutputsHigh(CMPSS1_BASE, CMPSS_TRIP_SYNC_COMP);                // Set output comparator (synchronous or asynchronous)
        
        /**Configure TRIP4 to be CTRIP1H using the ePWM X-BAR. Attach CMPSS output to TRIPINx via EPWMXBAR module*/
        DEVICE_DELAY_US(10000);
        XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX00_CMPSS1_CTRIPH);
        DEVICE_DELAY_US(10000);
    
        /**See the ePWM X-BAR Mux configuration table, see Crossbar(X-BAR) doc for more informations*/
        XBAR_enableEPWMMux(XBAR_TRIP4, XBAR_MUX00);
    }
    
    /**Shutdown ePWM when DCBEVT2 is triggered*/
    void cmpss_actions(uint32_t base)
    {
        /**Configure ePWMx to output low on TZx TRIP*/
        EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW);
        EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZB, EPWM_TZ_ACTION_LOW);
    
        /**Trigger event when DCBH is high*/
        EPWM_setTripZoneDigitalCompareEventCondition(base, EPWM_TZ_DC_OUTPUT_B2, EPWM_TZ_EVENT_DCXH_HIGH);
    
        EPWM_clearTripZoneFlag(base, EPWM_TZ_FLAG_DCBEVT2);
    
        EPWM_clearCycleByCycleTripZoneFlag(base, EPWM_TZ_CBC_FLAG_DCBEVT2);
    
        /**Enable DCB as DCBEVT2*/
        EPWM_enableTripZoneSignals(base, EPWM_TZ_SIGNAL_DCBEVT2);
        /**Enable interrupt*/
        EPWM_enableTripZoneInterrupt(base, EPWM_TZ_INTERRUPT_DCBEVT2);
    }
    
    

    谢谢

    Damien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我正在研究这个问题、并返回给您。

    谢谢
    Vasudha

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    一切都很好、我发现了我的错误、就是 DAC 的配置在缩放中更加精确、以获得我在等式中参考了3V 的数值、而我的 PCB 上的 VDDA 为3.3V。 然后、我使用 DCAEVT1和 DCAH 重新配置。 一切都很好。

    谢谢

    Damien