This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28075:60MHz 配置是否正常?

Guru**** 2826855 points

Other Parts Discussed in Thread: TMS320F28075, C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1131456/tms320f28075-60mhz-configuration-worked

器件型号:TMS320F28075
主题中讨论的其他器件: C2000WARE

我使用 TMS320F28075制作了一个控制板。 借助 PLL、CPU 可实现80mH、100MHz、120MHz 的频率。 但奇怪的是、它不会在60MHz 设置中启动。

这是我的代码。

//*****************************************************************************
//
// Defines related to clock configuration
//
//*****************************************************************************
//
// 20MHz XTAL on controlCARD. For use with SysCtl_getClock().
//
#define DEVICE_OSCSRC_FREQ 20000000U

//
// Define to pass to SysCtl_setClock(). Will configure the clock as follows:
// PLLSYSCLK = 20MHz (XTAL_OSC) * 10 (IMULT) * 1 (FMULT) / 2 (PLLCLK_BY_2)
//
#if defined(SYSTEM_CLK_120MHz)
#define DEVICE_SETCLOCK_CFG (SYSCTL_OSCSRC_XTAL | SYSCTL_IMULT(12) | \
SYSCTL_FMULT_NONE | SYSCTL_SYSDIV(2) | \
SYSCTL_PLL_ENABLE)
#elif defined(SYSTEM_CLK_100MHz)
#define DEVICE_SETCLOCK_CFG (SYSCTL_OSCSRC_XTAL | SYSCTL_IMULT(10) | \
SYSCTL_FMULT_NONE | SYSCTL_SYSDIV(2) | \
SYSCTL_PLL_ENABLE)
#elif defined(SYSTEM_CLK_80MHz)
#define DEVICE_SETCLOCK_CFG (SYSCTL_OSCSRC_XTAL | SYSCTL_IMULT(8) | \
SYSCTL_FMULT_NONE | SYSCTL_SYSDIV(2) | \
SYSCTL_PLL_ENABLE)
#elif defined(SYSTEM_CLK_60MHz)
#define DEVICE_SETCLOCK_CFG (SYSCTL_OSCSRC_XTAL | SYSCTL_IMULT(6) | \
SYSCTL_FMULT_NONE | SYSCTL_SYSDIV(2) | \
SYSCTL_PLL_ENABLE)
#endif
//
// 100MHz SYSCLK frequency based on the above DEVICE_SETCLOCK_CFG. Update the
// code below if a different clock configuration is used!
//
#if defined(SYSTEM_CLK_120MHz)
#define DEVICE_SYSCLK_FREQ ((DEVICE_OSCSRC_FREQ * 12 * 1) / 2)
#elif defined(SYSTEM_CLK_100MHz)
#define DEVICE_SYSCLK_FREQ ((DEVICE_OSCSRC_FREQ * 10 * 1) / 2)
#elif defined(SYSTEM_CLK_80MHz)
#define DEVICE_SYSCLK_FREQ ((DEVICE_OSCSRC_FREQ * 8 * 1) / 2)
#elif defined(SYSTEM_CLK_60MHz)
#define DEVICE_SYSCLK_FREQ ((DEVICE_OSCSRC_FREQ * 6 * 1) / 2)
#endif
//
// 25MHz LSPCLK frequency based on the above DEVICE_SYSCLK_FREQ and a default
// low speed peripheral clock divider of 4. Update the code below if a
// different LSPCLK divider is used!
//
#define DEVICE_LSPCLK_FREQ (DEVICE_SYSCLK_FREQ / 4)
//*****************************************************************************
//
// Macro to call SysCtl_delay() to achieve a delay in microseconds. The macro
// will convert the desired delay in microseconds to the count value expected
// by the function. \b x is the number of microseconds to delay.
//
//*****************************************************************************
#define DEVICE_DELAY_US(x) SysCtl_delay(((((long double)(x)) / (1000000.0L / \
(long double)DEVICE_SYSCLK_FREQ)) - 9.0L) / 5.0L)

//*****************************************************************************
//
// Defines, Globals, and Header Includes related to Flash Support
//
//*****************************************************************************
#ifdef _FLASH
#include <stddef.h>

extern uint16_t RamfuncsLoadStart;
extern uint16_t RamfuncsLoadEnd;
extern uint16_t RamfuncsLoadSize;
extern uint16_t RamfuncsRunStart;
extern uint16_t RamfuncsRunEnd;
extern uint16_t RamfuncsRunSize;

#if defined(SYSTEM_CLK_120MHz)
#define DEVICE_FLASH_WAITSTATES 2
#elif defined(SYSTEM_CLK_100MHz)
#define DEVICE_FLASH_WAITSTATES 2
#elif defined(SYSTEM_CLK_80MHz)
#define DEVICE_FLASH_WAITSTATES 3
#elif defined(SYSTEM_CLK_60MHz)
#define DEVICE_FLASH_WAITSTATES 5
#endif


是否有人成功地使其工作?

谢谢你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    该器件在60MHz 下不工作绝对没有任何原因、尤其是在其他频率下工作正常时。 请检查写入寄存器的值。

    我注意到一件事(这可能与您的问题无关)。 您的等待状态配置不正确。 即使在120MHz 时、也只需要2个等待状态。 请参阅表7-4。 www.ti.com/lit/SPRS902J:第54页中的闪存等待状态


    #IF 定义(SYSTEM_CLK_120MHz)

    #define DEVICE_FLASH_WAITSTATES 2.

    定义的#elif (system_clk_100MHz)

    #define DEVICE_FLASH_WAITSTATES 2.

    #elif defined (system_clk_80MHz)

    #define DEVICE_FLASH_WAITSTATES 3.

    定义的#Elif (SYSTEM_CLK_60MHz)

    #define DEVICE_FLASH_WAITSTATES 5.

    #endif

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    正如您所说、我修改了 DEVICE_FLASH_WAITSTATES 的值。

    但问题仍然存在。

    我连接了 JTAG 调试器(XDS110 USB 探针)并找到了问题所在。

    问题出现在下面的函数 SYSCTL_setclock 中。

    当系统时钟设置为60MHz 时、变量'SysclkInvalidFreq'[line 425]设置为 true (1)、

    因此看门狗被处理并且 CPU 被复位。

    什么是时钟误差? 为什么会发生这种情况?

    这是一些实验结果。

    振荡器时钟 20. 20. 20. 20.
    系统时钟[MHz] 60 80 100 120
    6. 8. 10. 12.
    分频 4. 4. 4. 4.
    控制 6149 4120 5146. 6158
    TMR2INPCLKCTR 2048 2048 2048 2048
    乘法/除法 1.5 2. 2.5. 3.
    Ctrl/TMR2INPCLK 3.002441406 2.01171875 2.5127. 3.00684

    谢谢你。

    bool
    SysCtl_setClock(uint32_t config)
    {
        uint16_t divSel;
        uint16_t iMult = 0U, fMult = 0U, pllMult = 0U, div;
        bool status, sysclkInvalidFreq = true;
        uint16_t i, tempSCSR, tempWDCR, tempWDWCR, intStatus;
        uint16_t t1TCR, t1TPR, t1TPRH, t2TCR, t2TPR, t2TPRH, t2CLKCTL;
        uint32_t t1PRD, t2PRD, ctr1;
        float32_t sysclkToInClkError, mult;
    
        //
        // Check the arguments.
        //
        ASSERT((config & SYSCTL_OSCSRC_M) != SYSCTL_OSCSRC_M); // 3 is not valid
    
        //
        // Don't proceed to the PLL initialization if an MCD failure is detected.
        //
        if(SysCtl_isMCDClockFailureDetected())
        {
            //
            // OSCCLKSRC2 failure detected. Returning false. You'll need to clear
            // the MCD error.
            //
            status = false;
        }
        else
        {
            //
            // Configure oscillator source
            //
            SysCtl_selectOscSource(config & SYSCTL_OSCSRC_M);
    
            //
            // Bypass PLL
            //
            EALLOW;
            HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLCTL1) &=
                ~SYSCTL_SYSPLLCTL1_PLLCLKEN;
            EDIS;
    
            //
            // Delay of at least 120 OSCCLK cycles required post PLL bypass
            //
            SysCtl_delay(23U);
    
            //
            // Configure PLL if enabled
            //
            EALLOW;
            if((config & SYSCTL_PLL_ENABLE) == SYSCTL_PLL_ENABLE)
            {
                if((HWREGH(DEVCFG_BASE + SYSCTL_O_SYSDBGCTL) &
                    SYSCTL_SYSDBGCTL_BIT_0) != 0U)
                {
                    //
                    // The user can optionally insert handler code here. This will
                    // only be executed if a watchdog reset occurred after a failed
                    // system PLL initialization. See your device user's guide for
                    // more information.
                    //
                    // If the application has a watchdog reset handler, this bit
                    // should be checked to determine if the watchdog reset
                    // occurred because of the PLL.
                    //
                    // No action here will continue with retrying the PLL as
                    // normal.
                    //
                }
    
                //
                // Set dividers to /1
                //
                HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) = 0U;
    
                //
                // Get the PLL multiplier settings from config
                //
                iMult |= (uint16_t)(config & SYSCTL_IMULT_M);
                fMult |= (uint16_t)((config & SYSCTL_FMULT_M) >> SYSCTL_FMULT_S);
                pllMult |= (iMult << SYSCTL_SYSPLLMULT_IMULT_S) |
                           (fMult << SYSCTL_SYSPLLMULT_FMULT_S);
    
                //
                // Lock the PLL five times. This helps ensure a successful start.
                // Five is the minimum recommended number. The user can increase
                // this number according to allotted system initialization time.
                //
                for(i = 0U; i < 5U; i++)
                {
                    //
                    // Turn off PLL
                    //
                    HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLCTL1) &=
                        ~SYSCTL_SYSPLLCTL1_PLLEN;
    
                    asm(" RPT #60 || NOP");
    
                    //
                    // Write multiplier, which automatically turns on the PLL
                    //
                    HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLMULT) = pllMult;
    
                    //
                    // Wait for the SYSPLL lock counter
                    //
                    while((HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLSTS) &
                           SYSCTL_SYSPLLSTS_LOCKS) == 0U)
                    {
                        //
                        // Consider to servicing the watchdog using
                        // SysCtl_serviceWatchdog()
                        //
                    }
                }
            }
    
            //
            // Configure Dividers. Set divider to produce slower output frequency
            // to limit current increase.
            //
            divSel = (uint16_t)(config & SYSCTL_SYSDIV_M) >> SYSCTL_SYSDIV_S;
    
            if(divSel != (126U / 2U))
            {
                HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) =
                    (HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) &
                    ~(uint16_t)SYSCTL_SYSCLKDIVSEL_PLLSYSCLKDIV_M) | (divSel + 1U);
            }
            else
            {
                HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) =
                    (HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) &
                     ~(uint16_t)SYSCTL_SYSCLKDIVSEL_PLLSYSCLKDIV_M) | divSel;
            }
    
            //
            //      *CAUTION*
            // It is recommended to use the following watchdog code to monitor the
            // PLLstartup sequence. If your application has already cleared the
            // watchdog SCRS[WDOVERRIDE] bit this cannot be done. It is recommended
            // not to clear this bit until after the PLL has been initiated.
            //
    
            //
            // Backup User Watchdog
            //
            tempSCSR = HWREGH(WD_BASE + SYSCTL_O_SCSR);
            tempWDCR = HWREGH(WD_BASE + SYSCTL_O_WDCR);
            tempWDWCR = HWREGH(WD_BASE + SYSCTL_O_WDWCR);
    
            //
            // Disable windowed functionality, reset counter
            //
            HWREGH(WD_BASE + SYSCTL_O_WDWCR) = 0x0U;
            SysCtl_serviceWatchdog();
    
            //
            // Disable global interrupts
            //
            intStatus = __disable_interrupts();
    
            //
            // Configure for watchdog reset and to run at max frequency
            //
            EALLOW;
            HWREGH(WD_BASE + SYSCTL_O_SCSR) = 0x0U;
            HWREGH(WD_BASE + SYSCTL_O_WDCR) = SYSCTL_WD_CHKBITS;
    
            //
            // This bit is reset only by power-on-reset (POR) and will not be
            // cleared by a WD reset
            //
            HWREGH(DEVCFG_BASE + SYSCTL_O_SYSDBGCTL) |= SYSCTL_SYSDBGCTL_BIT_0;
    
            //
            // Enable PLLSYSCLK is fed from system PLL clock
            //
            HWREGH(CLKCFG_BASE +
                   SYSCTL_O_SYSPLLCTL1) |= SYSCTL_SYSPLLCTL1_PLLCLKEN;
    
            EDIS;
    
            //
            // Delay to ensure system is clocking from PLL prior to clearing
            // status bit
            //
            SysCtl_delay(3U);
    
            //
            // Slip Bit Monitor and SYSCLK Frequency Check using timers
            // Re-lock routine for SLIP condition or if SYSCLK and CLKSRC timer
            // counts are off by +/- 10%. At a minimum, SYSCLK check is performed.
            // Re-lock attempt is carried out if SLIPS bit is set.
            // This while loop is monitored by watchdog.
            // In the event that the PLL does not successfully lock, the loop will
            // be aborted by watchdog reset.
            //
            while(((config & SYSCTL_PLL_ENABLE) == SYSCTL_PLL_ENABLE) &&
                  (sysclkInvalidFreq == true))
            {
                EALLOW;
    
                //
                // Perform PLL re-lock only if SLIPS bit is set, otherwise monitor
                // SYSCLK frequency with timers
                //
                if((HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLSTS) &
                    SYSCTL_SYSPLLSTS_SLIPS) == 1U)
                {
                    //
                    // Bypass PLL
                    //
                    HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLCTL1) &=
                        ~SYSCTL_SYSPLLCTL1_PLLCLKEN;
    
                    //
                    // Delay of at least 120 OSCCLK cycles required post PLL bypass
                    //
                    SysCtl_delay(23U);
    
                    //
                    // Turn off PLL
                    //
                    HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLCTL1) &=
                        ~SYSCTL_SYSPLLCTL1_PLLEN;
    
                    SysCtl_delay(3U);
    
                    //
                    // Write multiplier, which automatically turns on the PLL
                    //
                    HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLMULT) |= pllMult;
    
                    //
                    // Wait for the SYSPLL lock counter
                    //
                    while((HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLSTS) &
                            SYSCTL_SYSPLLSTS_LOCKS) == 0U)
                    {
                        ;
                    }
    
                    //
                    // Enable PLLSYSCLK is fed from system PLL clock
                    //
                    HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLCTL1) |=
                        SYSCTL_SYSPLLCTL1_PLLCLKEN;
    
                    //
                    // Delay to ensure system is clocking from PLL prior to
                    // clearing status bit
                    //
                    SysCtl_delay(3U);
                }
    
                //
                // Backup timer1 and timer2 settings
                //
                t1TCR = HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR);
                t1PRD = HWREG(CPUTIMER1_BASE + CPUTIMER_O_PRD);
                t1TPR = HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TPR);
                t1TPRH = HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TPRH);
                t2CLKCTL = HWREGH(CPUSYS_BASE + SYSCTL_O_TMR2CLKCTL);
                t2TCR = HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR);
                t2PRD = HWREG(CPUTIMER2_BASE + CPUTIMER_O_PRD);
                t2TPR = HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TPR);
                t2TPRH = HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TPRH);
    
                //
                // Set up timers 1 and 2
                // Configure timer1 to count SYSCLK cycles
                //
    
                //
                // Stop timer 1
                // Seed timer1 counter
                // Set sysclock divider
                // Reload timer with value in PRD
                // Clear interrupt flag
                // Enable interrupt
                //
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TSS;
                HWREG(CPUTIMER1_BASE + CPUTIMER_O_PRD) = (uint32_t)TMR1SYSCLKCTR;
                HWREG(CPUTIMER1_BASE + CPUTIMER_O_TPR) = 0U;
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TRB;
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TIF;
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TIE;
    
                //
                // Configure timer2 to count Input clock cycles
                //
                switch (config & SYSCTL_OSCSRC_M)
                {
                    case SYSCTL_OSCSRC_OSC1:
                        //
                        // Clk Src = INT_OSC1
                        //
                        HWREGH(CPUSYS_BASE + SYSCTL_O_TMR2CLKCTL) &=
                            ~SYSCTL_TMR2CLKCTL_TMR2CLKSRCSEL_M;
                        HWREGH(CPUSYS_BASE + SYSCTL_O_TMR2CLKCTL) |= 1U;
                        break;
    
                    case SYSCTL_OSCSRC_OSC2:
                        //
                        // Clk Src = INT_OSC2
                        //
                        HWREGH(CPUSYS_BASE + SYSCTL_O_TMR2CLKCTL) &=
                            ~SYSCTL_TMR2CLKCTL_TMR2CLKSRCSEL_M;
                        HWREGH(CPUSYS_BASE + SYSCTL_O_TMR2CLKCTL) |= 2U;
                        break;
    
                    case SYSCTL_OSCSRC_XTAL:
                        //
                        // Clk Src = XTAL
                        //
                        HWREGH(CPUSYS_BASE + SYSCTL_O_TMR2CLKCTL) &=
                            ~SYSCTL_TMR2CLKCTL_TMR2CLKSRCSEL_M;
                        HWREGH(CPUSYS_BASE + SYSCTL_O_TMR2CLKCTL) |= 3U;
                        break;
    
                    default:
                        //
                        // Do nothing. Not a valid clock source value.
                        //
                        break;
                }
    
                //
                // Clear interrupt flag
                // Enable interrupt
                // Stop timer 2
                // Seed timer2 counter
                // Set sysclock divider
                // Reload timer with value in PRD
                //
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TIF;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TIE;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TSS;
                HWREG(CPUTIMER2_BASE + CPUTIMER_O_PRD) = (uint32_t)TMR2INPCLKCTR;
                HWREG(CPUTIMER2_BASE + CPUTIMER_O_TPR) = 0U;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TRB;
    
                //
                // Stop/Start timer counters
                //
    
                //
                // Stop timer 1
                // Stop timer 2
                // Reload timer1 with value in PRD
                // Reload timer2 with value in PRD
                // Clear timer2 interrupt flag
                // Start timer2
                // Start timer1
                //
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TSS;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TSS;
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TRB;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TRB;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TIF;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) &= ~CPUTIMER_TCR_TSS;
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) &= ~CPUTIMER_TCR_TSS;
    
                //
                // Wait for Timers - Stop if either timer overflows
                //
                while(((HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) &
                       CPUTIMER_TCR_TIF) == 0U)  &&
                      ((HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) &
                       CPUTIMER_TCR_TIF) == 0U))
                {
                    ;
                }
    
                //
                // Stop timer 1 and 2
                //
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TSS;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) |= CPUTIMER_TCR_TSS;
    
                //
                // Calculate elapsed counts on timer1
                //
                ctr1 = (uint32_t)TMR1SYSCLKCTR - HWREG(CPUTIMER1_BASE +
                                                       CPUTIMER_O_TIM);
    
                //
                // Restore timer settings
                //
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TCR) = t1TCR;
                HWREG(CPUTIMER1_BASE + CPUTIMER_O_PRD) = t1PRD;
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TPR) = t1TPR;
                HWREGH(CPUTIMER1_BASE + CPUTIMER_O_TPRH) = t1TPRH;
                HWREGH(CPUSYS_BASE + SYSCTL_O_TMR2CLKCTL) = t2CLKCTL;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TCR) = t2TCR;
                HWREG(CPUTIMER2_BASE + CPUTIMER_O_PRD) = t2PRD;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TPR) = t2TPR;
                HWREGH(CPUTIMER2_BASE + CPUTIMER_O_TPRH) = t2TPRH;
    
                //
                // Calculate Clock Error:
                // Error = (mult/div) - (timer1 count/timer2 count)
                //
                mult = (float32_t)iMult + ((float32_t)fMult / 4.0F);
    
                if((HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) & 0x3FU) == 0U)
                {
                    div = 1U;
                }
                else
                {
                    div = (HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) &
                           0x3FU) << 1;
                }
    
                sysclkToInClkError = (mult / (float32_t)div) -
                                     ((float32_t)ctr1 / (float32_t)TMR2INPCLKCTR);
    
                //
                // sysclkInvalidFreq will be set to true if sysclkToInClkError is
                // off by 10%
                //
                sysclkInvalidFreq = ((sysclkToInClkError > 0.10F) ||
                                     (sysclkToInClkError < -0.10F));
    
                EDIS;
            }
    
            //
            // Clear bit
            //
            EALLOW;
            HWREGH(DEVCFG_BASE + SYSCTL_O_SYSDBGCTL) &= ~SYSCTL_SYSDBGCTL_BIT_0;
            EDIS;
    
            //
            // Restore user watchdog, first resetting counter
            //
            SysCtl_serviceWatchdog();
    
            //
            // Set the KEY bits and make sure not to set the WDOVERRIDE bit
            //
            EALLOW;
            HWREGH(WD_BASE + SYSCTL_O_WDCR) = tempWDCR | SYSCTL_WD_CHKBITS;
            HWREGH(WD_BASE + SYSCTL_O_WDWCR) = tempWDWCR;
            HWREGH(WD_BASE + SYSCTL_O_SCSR) = tempSCSR & ~SYSCTL_SCSR_WDOVERRIDE;
            EDIS;
    
            //
            // Restore state of ST1[INTM]. This was set by the
            // __disable_interrupts() intrinsic previously.
            //
            if((intStatus & 0x1U) == 0U)
            {
                EINT;
            }
    
            //
            // Restore state of ST1[DBGM]. This was set by the
            // __disable_interrupts() intrinsic previously.
            //
            if((intStatus & 0x2U) == 0U)
            {
                SYSCTL_CLRC_DBGM;
            }
    
            //
            // ~200 PLLSYSCLK delay to allow voltage regulator to stabilize prior
            // to increasing entire system clock frequency.
            //
            SysCtl_delay(40U);
    
            //
            // Set the divider to user value
            //
            EALLOW;
            HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) =
                (HWREGH(CLKCFG_BASE + SYSCTL_O_SYSCLKDIVSEL) &
                 ~SYSCTL_SYSCLKDIVSEL_PLLSYSCLKDIV_M) | divSel;
            EDIS;
    
            status = true;
        }
    
        return(status);
    }

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这可能需要软件团队中的某个人来解决。 您使用的是什么版本的 C2000ware? 如果您未使用最新版本(4.01)、请下载并安装。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我使用的 C2000Ware 版本从一开始就是4.01。  

    当时钟设置为60MHz 时、sysclkToInClkError 超出允许的范围。 我针对各种频率进行了测试。

    测试通过至72MHz、在60MHz 和70MHz 时失败。

    我还测试了28075 100引脚和176引脚。 结果是一样的。

                sysclkToInClkError = (mult / (float32_t)div) -
                                     ((float32_t)ctr1 / (float32_t)TMR2INPCLKCTR);
    
                //
                // sysclkInvalidFreq will be set to true if sysclkToInClkError is
                // off by 10%
                //
                sysclkInvalidFreq = ((sysclkToInClkError > 0.10F) ||
                                     (sysclkToInClkError < -0.10F));

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    [引用 userid="265787" URL"~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forume/1131456/tms320f28075-60MHz-configuring-wed/4199105#4199105"]
    分频 4. 4. 4. 4.
    [/报价]

    我认为您的意思是在所有情况下都使用 div = 2

    根据该规范、PLLRAWCK 应介于120-400之间

    在本例中、PLLRAWCLK 为20*6 = 120。 您能否尝试使用不同的乘法器和除法器(例如:20 * 12 /4)来确保内部频率不在允许范围的边界?

    此致、

    Veena

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    表中的"DIL"不是寄存器设置、而是代码中的变量、如下所示。

    DIV =(HWREGH (CLKCFG_base + SYSCTL_O_SYSCLKDIVSEL)&
    0x3FU)<< 1;

    div 的值为4。

    我更改了 device.h 中的代码、如下所示。

    [ASIS]

    #define DEVICE_SETCLOCK_CFG (SYSCTL_OSCSRC_XTAL | SYSCTL_IMULT (6)|\
    SYSCTL_FMULT_NONE | SYSCTL_SYSDIV (2)|\
    SYSCTL_PLL_ENABLE)

    [待定]

    #define DEVICE_SETCLOCK_CFG (SYSCTL_OSCSRC_XTAL | SYSCTL_IMULT (12)|\
    SYSCTL_FMULT_NONE | SYSCTL_SYSDIV (4)|\
    SYSCTL_PLL_ENABLE)

    之后、错误消失。

    谢谢你。