This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280025:CMPSS 错误触发问题

Guru**** 2524460 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1049212/tms320f280025-problem-of-cmpss-false-triggering

器件型号:TMS320F280025

尊敬的团队:

在测试 cmpss 模块时、我的客户发现、当实际电压仅为1.9V 时、保护功能会被错误触发。 将相应的引脚(引脚8)接地后、仍将触发保护。

可能的原因是什么? 以下是客户代码:

void InitComp(void)
{
/* set up the GPIO and X-BAR input configurations before enabling the TZ*/
EPwm1Regs.TZSEL.all = 0x0;
EPwm2Regs.TZSEL.all = 0x0;

/* Initialize Analog Subsystem */
EALLOW;
AnalogSubsysRegs.CMPHPMXSEL.bit.CMP1HPMXSEL = 1; // Bits to select one of the many sources on CopmHP inputs. Refer to Pimux diagram for details.
EDIS;

/* Initialize Comparators */
EALLOW;
//Cmpss1Regs.COMPCTL.all = 0x9414;
Cmpss1Regs.COMPCTL.bit.COMPHSOURCE = 0; // 0 High Comparator Source Select
Cmpss1Regs.COMPCTL.bit.COMPHINV = 0; // 1 High Comparator Invert Select
Cmpss1Regs.COMPCTL.bit.CTRIPHSEL = 1; // 3:2 High Comparator Trip Select
Cmpss1Regs.COMPCTL.bit.CTRIPOUTHSEL = 1; // 5:4 High Comparator Trip Output Select
Cmpss1Regs.COMPCTL.bit.ASYNCHEN = 0; // 6 High Comparator Asynchronous Path Enable
Cmpss1Regs.COMPCTL.bit.COMPLSOURCE = 0; // 8 Low Comparator Source Select
Cmpss1Regs.COMPCTL.bit.COMPLINV = 0; // 9 Low Comparator Invert Select
Cmpss1Regs.COMPCTL.bit.CTRIPLSEL = 1; // 11:10 Low Comparator Trip Select
Cmpss1Regs.COMPCTL.bit.CTRIPOUTLSEL = 1; // 13:12 Low Comparator Trip Output Select
Cmpss1Regs.COMPCTL.bit.ASYNCLEN = 0; // 14 Low Comparator Asynchronous Path Enable
Cmpss1Regs.COMPCTL.bit.COMPDACE = 1; // 15 Comparator/DAC Enable


Cmpss1Regs.DACHVALS.bit.DACVAL = 3723; // 20A / #define ADC_CURRENT_BUSIN_OC_FIXED_COEFF (0.0052882)
Cmpss1Regs.DACLVALS.bit.DACVAL = 3723; // 20A / #define ADC_CURRENT_BUSIN_OC_FIXED_COEFF (0.0052882)

//Cmpss1Regs.COMPLOCK.all = 0x000F;
Cmpss1Regs.COMPLOCK.bit.COMPCTL = 1; // 0 COMPCTL Lock
Cmpss1Regs.COMPLOCK.bit.COMPHYSCTL = 1; // 1 COMPHYSCTL Lock
Cmpss1Regs.COMPLOCK.bit.DACCTL = 1; // 2 DACCTL Lock
Cmpss1Regs.COMPLOCK.bit.CTRIP = 1; // 3 CTRIP Lock
EDIS;

/* Initialize EPwmXbarRegs */
EALLOW;
EPwmXbarRegs.TRIP4MUX0TO15CFG.bit.MUX0 = 0; // 1:0 Mux0 Configuration for TRIP4 of EPWM-XBAR
EPwmXbarRegs.TRIP4MUXENABLE.bit.MUX0 = 1; // ePWM XBAR Mux Enable for TRIP4
EPwmXbarRegs.TRIPOUTINV.bit.TRIP4 = 0; // ePWM XBAR Output Inversion Register
EDIS;

/* Initialize DC */
EALLOW;
EPwm1Regs.DCTRIPSEL.bit.DCAHCOMPSEL = DC_TRIPIN4; // 3:0 Digital Compare A High COMP Input Select
EPwm1Regs.DCTRIPSEL.bit.DCBHCOMPSEL = DC_TRIPIN4; // 11:8 Digital Compare B High COMP Input Select
EPwm1Regs.DCACTL.bit.EVT2SRCSEL = DC_EVT2; // 8 DCAEVT2 Source Signal
EPwm1Regs.DCACTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC; // 9 DCAEVT2 Force Sync Signal

EPwm2Regs.DCTRIPSEL.bit.DCAHCOMPSEL = DC_TRIPIN4; // 3:0 Digital Compare A High COMP Input Select
EPwm2Regs.DCTRIPSEL.bit.DCBHCOMPSEL = DC_TRIPIN4; // 11:8 Digital Compare B High COMP Input Select
EPwm2Regs.DCACTL.bit.EVT2SRCSEL = DC_EVT2; // 8 DCAEVT2 Source Signal
EPwm2Regs.DCACTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC; // 9 DCAEVT2 Force Sync Signal
EDIS;

/* Initialize TZ */
EALLOW;
EPwm1Regs.TZDCSEL.bit.DCAEVT2 = TZ_DCAH_HI; // 5:3 Digital Compare Output A Event 2
EPwm1Regs.TZSEL.bit.DCAEVT2 = 1; // 6 DCAEVT2 CBC select
EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // 1:0 TZ1 to TZ6 Trip Action On EPWMxA
EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // 3:2 TZ1 to TZ6 Trip Action On EPWMxB
EPwm1Regs.TZCLR.all = 0xFFFF; // Trip Zone Clear Register

EPwm2Regs.TZDCSEL.bit.DCAEVT2 = TZ_DCAH_HI; // 5:3 Digital Compare Output A Event 2
EPwm2Regs.TZSEL.bit.DCAEVT2 = 1; // 6 DCAEVT2 CBC select
EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // 1:0 TZ1 to TZ6 Trip Action On EPWMxA
EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // 3:2 TZ1 to TZ6 Trip Action On EPWMxB
EPwm2Regs.TZCLR.all = 0xFFFF; // Trip Zone Clear Register
EDIS;

此致

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    绿色环保、

    查看您的配置代码、您只进行配置

    EALLOW;
    AnalogSubsysRegs.CMPHPMXSEL.bit.CMP1HPMXSEL = 1; // Bits to select one of the many sources on CopmHP inputs. Refer to Pimux diagram for details.
    EDIS;

    未配置 CMP1LPMXSEL。 压实是随机跳变吗?