This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] McbspB 至 SPI 模式:在时钟停止模式中、接收器始终为0xFF、无延迟

Guru**** 2526700 points
Other Parts Discussed in Thread: C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1045892/mcbspb-to-spi-mode-the-receiver-is-always-0xff-in-clock-stop-mode-without-delay

器件型号:TMS320F28335
主题中讨论的其他器件:C2000WARE

您好:

   我使用的演示代码为"F:\c2000_sdk\C2000Ware_1_00_03_00\device_support\F2833x\examples\McBSP_loopback_DMA"。 我将 McBSP_SPI 模式从 DLB 更改为时钟停止模式。 SPI 的 CLK 为400kHz。

   我想使用 MCBSPB 作为 SPI 模式来与 SD 卡通信。 下面是我的配置。

void InitMcbspbGpio(void)
{
    EALLOW;

    // Configure McBSP-A pins using GPIO regs
    // This specifies which of the possible GPIO pins will be McBSP functional
    // pins.
    // Comment out other unwanted lines.
    GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 3;	    // GPIO12 is MDXB pin MOSI
    GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 3;	    // GPIO13 is MDRB pin MISO
    GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 3;	    // GPIO14 is MCLKXB pin CLK
    GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 3;	    // GPIO15 is MFSXB pin

    // Enable internal pull-up for the selected pins
    // Pull-ups can be enabled or disabled by the user.
    // This will enable the pullups for the specified pins.
    // Comment out other unwanted lines.
    GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0;	        //Enable pull-up on GPIO12 (MDXB)
    GpioCtrlRegs.GPAPUD.bit.GPIO13 = 0;	        //Enable pull-up on GPIO13 (MDRB)
    GpioCtrlRegs.GPAPUD.bit.GPIO14 = 0;	        //Enable pull-up on GPIO14 (MCLKXB)
    GpioCtrlRegs.GPAPUD.bit.GPIO15 = 0;	        //Enable pull-up on GPIO15 (MFSXB)

    // Set qualification for selected input pins to asynch only
    // This will select asynch (no qualification) for the selected pins.
    // Comment out other unwanted lines.
    GpioCtrlRegs.GPAQSEL1.bit.GPIO13 = 3; // Asynch input GPIO13 (MDRB)
    GpioCtrlRegs.GPAQSEL1.bit.GPIO14 = 3; // Asynch input GPIO14 (MCLKXB)
    GpioCtrlRegs.GPAQSEL1.bit.GPIO15 = 3; // Asynch input GPIO15 (MFSXB)

    EDIS;
}

void McbspB_init(void)
{

    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.MCBSPAENCLK = 1;      // enable low speed clock to McBSP-A
    SysCtrlRegs.PCLKCR0.bit.MCBSPBENCLK = 1;      // enable low speed clock to McBSP-B
    EDIS;

    // Reset FS generator, sample rate generator & transmitter
    McbspbRegs.SPCR2.all=0x0000;
    McbspbRegs.SPCR1.all=0x0000;                 // Reset Receiver, Right justify word
    McbspbRegs.PCR.all = 0xF08;                  // CLKXM = CLKRM = FSXM = FSRM = 1, FSXP = 1

    // clocking scheme:
    //McbspbRegs.MFFINT.all=0x0;                 // Disable all interrupts
    McbspbRegs.SPCR1.bit.CLKSTP = 2;             // clock stop mode, without clock delay
    McbspbRegs.PCR.bit.CLKXP = 1;                // transmit data are sampled on the rising edge of clock signal
    McbspbRegs.PCR.bit.CLKRP = 0;                // receive data are sampled on the falling edge of clock signal

    McbspbRegs.RCR2.bit.RDATDLY = 1;             // 1 for master mode, 0 for slave mode (?)
    McbspbRegs.XCR2.bit.XDATDLY = 1;             // 1 for master mode, 0 for slave mode (?)

    McbspbRegs.RCR1.bit.RWDLEN1 = 0;             // 8-bit word
    McbspbRegs.XCR1.bit.XWDLEN1 = 0;             // 8-bit word


    McbspbRegs.SRGR2.all = 0x2000;               // CLKSM = 1, FPER = 1 CLKG period
     //               LSPCLK
     // CLKG_freq = ----------
     //             CLKGDV + 1
    //McbspbRegs.SRGR1.all = 0x000F;             // frame width = 1 CLKG period, CLKGDV = 15 (2.34 MHz)
    McbspbRegs.SRGR1.all = 95;               // frame width = 1 CLKG period, CLKGDV = 5 (6.25 MHz)
    //
    // Enable Sample rate generator
    //
    McbspbRegs.SPCR2.bit.GRST=1;    // Enable the sample rate generator
    delay_loop();                   // Wait at least 2 SRG clock cycles
    McbspbRegs.SPCR2.bit.XRST=1;    // Release TX from Reset
    McbspbRegs.SPCR1.bit.RRST=1;    // Release RX from Reset
    McbspbRegs.SPCR2.bit.FRST=1;    // Frame Sync Generator reset
}

我需要使用400kHz CLK 来发送 cmd 来初始化 SD 卡。 但是、不管我在"DXR1"中发送什么、接收寄存器"DRR1"将始终为0xFF。  

我的 McBSP 配置是否有任何问题?

顺便说一下、由于硬接线电路是固定的、我无法执行回路测试。 此外、我已禁用 TX 和 Rx 中断、这很重要吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    到目前为止、我没有发现您的配置有任何问题。 它似乎与 TRM 中记录的 SPI 模式所需的所有寄存器值相匹配。 您是否完全能够探测 SPI 引脚、以便使用逻辑分析仪或示波器来显示它们、以查看实际发送的内容?

    惠特尼