This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28035:基于 TMS320FF28035的 PSFB 峰值电流控制的相移全桥问题

Guru**** 657500 points
Other Parts Discussed in Thread: CONTROLSUITE, TIDM-02000
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1043467/tms320f28035-the-phase-shifted-full-bridge-problem-of-psfb-peak-current-control-based-on-tms320ff28035

器件型号:TMS320F28035
Thread 中讨论的其他器件:controlSUITETIDM-02000

尊敬的团队:

我的客户有以下问题、希望您能帮助回答:

我正在调试基于 F28035芯片的相移全桥降压电路、并通过峰值电流控制实现相移。 我使用 EPWM2作为 ARM 的驱动器、使用 EPWM1作为迟滞 ARM、使用 EPWM3作为侧同步整流的驱动器、使用 EPWM4作为触发 ADC 采样、使用 COMP3A 作为峰值电流检测。同时同步 EPWM2时钟以实现相移。

但是、在低电流时不能触发 COMP3A 比较器事件、因此无法实现 EPWM2的相移。

EPWM2模块配置如下:

#define HSFB_PERIOD       205   //146kHz

void PWM_Config(void)
{

EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // Disable TBCLK within the EPWM
EDIS;
//Time Base SubModule Register
EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE; // Set Immediate load
EPwm1Regs.TBPRD = HSFB_PERIOD;
EPwm1Regs.TBPHS.half.TBPHS = 0;
EPwm1Regs.TBCTR = 0;

EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_CMPB; // Used to sync EPWM(n+1) "down-stream"
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;

// Counter compare submodule registers
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;
EPwm1Regs.CMPA.half.CMPA = HSFB_PERIOD-68;//trig_up;ynj
EPwm1Regs.CMPB = HSFB_PERIOD;

// Action Qualifier SubModule Registers
EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET;
EPwm1Regs.AQCTLA.bit.PRD = AQ_CLEAR;

// DeadBand Control Register
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi Complimentary
EPwm1Regs.DBRED = 6; // Initial value
EPwm1Regs.DBFED = 6; // Initial value

// ePWM(n+1) init. EPWM(n+1) is a slave

EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm2Regs.TBPRD = HSFB_PERIOD-1;
EPwm2Regs.TBPHS.half.TBPHS = 0;
EPwm2Regs.TBCTR = 0;

EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Sync "flow through" mode
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;

// Counter compare submodule registers
EPwm2Regs.CMPA.half.CMPA = HSFB_PERIOD + 10; // Initial valueynj
EPwm2Regs.CMPB = 20; // Initial value ynj
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;

// Action Qualifier SubModule Registers
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET;//AQ_CLEAR;ynj
EPwm2Regs.AQCTLA.bit.ZRO = AQ_CLEAR;
EPwm2Regs.AQCTLA.bit.CBU = AQ_CLEAR;//AQ_SET;
EPwm2Regs.AQCTLA.bit.PRD = AQ_CLEAR;

EPwm2Regs.AQCTLB.bit.CBU = AQ_SET;
EPwm2Regs.AQCTLB.bit.ZRO = AQ_CLEAR;//AQ_CLEAR;
EPwm2Regs.AQCTLB.bit.CAU = AQ_CLEAR;
EPwm2Regs.AQCTLB.bit.PRD = AQ_CLEAR;

// Peak current control configure.
EALLOW;
//===========================================================================
// Define an event (DCAEVT1) based on Comparator 1 Output
EPwm2Regs.DCTRIPSEL.bit.DCAHCOMPSEL = DC_COMP3OUT; // DCAH = Comparator 1 output
EPwm2Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCAH_HI; // DCAEVT1 = DCAH high(will become active
// as Comparator output goes high)
EPwm2Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT1;//DC_EVT_FLT; // DCAEVT1 = DC_EVT_FLT (filtered)
EPwm2Regs.DCACTL.bit.EVT1FRCSYNCSEL = DC_EVT_ASYNC; // Take async path
// EPwm2Regs.TBCTL.bit.SWFSYNC =1;
// EPwm2Regs.TBCTL.bit.PRDLD=1;
// Enable DCAEVT1 as a one-shot sourceEPwm2Regs.TZFLG.bit.DCAEVT1
EPwm2Regs.TZSEL.bit.DCAEVT1 = 1; // Enable One-Shot Trip

// Following code for the sync mechanism based on the same trigger event - COMPxOUT
EPwm2Regs.DCACTL.bit.EVT1SYNCE = 1; // Sync enabled

// What do we want the DCAEVT1 event to do? - Initial Configuration
EPwm2Regs.TZCTL.bit.TZA = TZ_NO_CHANGE; // EPWMxA - no change
EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO;//TZ_NO_CHANGE; // EPWMxB - go low
// EPwm2Regs.TZCTL.bit.DCAEVT1 = TZ_NO_CHANGE;//YNJ
//===========================================================================
// Event Filtering Configuration
EPwm2Regs.DCFCTL.bit.SRCSEL = DC_SRC_DCAEVT1;
EPwm2Regs.DCFCTL.bit.BLANKE = DC_BLANK_ENABLE;
EPwm2Regs.DCFCTL.bit.PULSESEL = DC_PULSESEL_ZERO;

// EPwm2Regs.DCFOFFSET = 2; // Blanking Window Offset = CMPA(n+1)
// EPwm2Regs.DCFWINDOW = 4; // Blanking window length - initial value
//===========================================================================
EDIS;


//Time Base SubModule Register
EPwm3Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;
EPwm3Regs.TBPRD = HSFB_PERIOD-35;
EPwm3Regs.TBPHS.half.TBPHS = 0;
EPwm3Regs.TBCTR = 0;

EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE;
EPwm3Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;

EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass the Sync signal through to ePWM4

EPwm3Regs.CMPA.half.CMPA = HSFB_PERIOD/2 - 10; // Initial value

// Action Qualifier SubModule Registers
EPwm3Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm3Regs.AQCTLA.bit.ZRO = AQ_SET;

EPwm3Regs.AQCTLB.bit.CAU = AQ_CLEAR;
EPwm3Regs.AQCTLB.bit.ZRO = AQ_SET;

//Configure EPWM4 time base for ADC SOC generation and syncing the DAC

//Configure EPWM(n+2) time base for ADC SOC generation and syncing the DAC

//Time Base SubModule Register
EPwm4Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;
EPwm4Regs.TBPRD = HSFB_PERIOD-1;
EPwm4Regs.TBPHS.half.TBPHS = HSFB_PERIOD-35;
EPwm4Regs.TBCTR = 0;

EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm4Regs.TBCTL.bit.PHSEN = TB_ENABLE;
EPwm4Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm4Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm4Regs.TBCTL.bit.CLKDIV = TB_DIV1;

EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass the Sync signal through to ePWM4


// ADC SOC generation
//===========================================================================
// SOC generation using PWM(n) - 1st of 4 Vout conversions in one half cycle
EPwm1Regs.ETSEL.bit.SOCAEN = 1;
EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_PRDZERO; // Use ZRO and PRD events as trigger
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event

// SOC generation using PWM(n+1) - Iout conversion
EPwm2Regs.ETSEL.bit.SOCAEN = 1;
EPwm2Regs.ETSEL.bit.SOCASEL = ET_CTR_ZERO; // Use ZRO event as trigger
EPwm2Regs.ETPS.bit.SOCAPRD = ET_2ND; // Generate pulse on 1st event

// SOC generation using PWM(n+2) - 2nd, 3rd and 4th Vout conversions in one half cycle; Vin and Ipri conversions
EPwm4Regs.ETSEL.bit.SOCAEN = 1;
EPwm4Regs.ETSEL.bit.SOCASEL = ET_CTRU_CMPA; // Use CAU event as trigger
EPwm4Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm4Regs.CMPA.half.CMPA = 40; // Note: This value is based on 100 KHz switching frequency

EPwm4Regs.ETSEL.bit.SOCBEN = 1;
EPwm4Regs.ETSEL.bit.SOCBSEL = ET_CTRU_CMPB; // Use CBU event as trigger
EPwm4Regs.ETPS.bit.SOCBPRD = 1; // Generate pulse on 1st event
EPwm4Regs.CMPB = 165; // Note: This value is based on 100 KHz switching frequency

EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
/*-----------------------------------------*/

}

COMP3A 配置如下:

EALLOW;
AdcRegs.COMPHYSTCTL.bit.COMP3_HYST_DISABLE=0;
EDIS;

EALLOW;
GpioCtrlRegs.AIOMUX1.bit.AIO6 = 2;
EDIS;

EALLOW;

Comp3Regs.COMPCTL.bit.COMPDACEN = 1; // Power up Comparator locally
Comp3Regs.COMPCTL.bit.COMPSOURCE = 0; // Connect the inverting input to internal DAC
Comp3Regs.DACVAL.bit.DACVAL = 500; // Set DAC output - Input is Q15 - Convert to Q10
Comp3Regs.DACCTL.bit.DACSOURCE = 1; // 0 - DACVAL; 1 - Internal ramp for slope compensation

// Following lines of code are used when internal slope compensation is used

Comp3Regs.COMPCTL.bit.QUALSEL =5; // Comparator output must be active for 4 consecutive clocks before resetting the RAMP
Comp3Regs.DACCTL.bit.RAMPSOURCE = 3; // 0 - PMW1; 1 - PWM2, 2-PWM3, 3-PWM4
Comp3Regs.RAMPDECVAL_SHDW = 40;
EPwm4Regs.HRPCTL.bit.PWMSYNCSEL = 1; // PWM SYNC generated at CTR = ZRO for synchronizing internal ramp
Comp3Regs.COMPCTL.bit.CMPINV = 0; // Comparator Output passed


EDIS;

中断功能如下:

#define DACDRV_RAMP_In    38400  //环路计算值

if(TB_DIR_UP == EPwm1Regs.TBSTS.bit.CTRDIR) //PWM counter direction is UP
{

EPwm2Regs.TZCLR.all |= 0x0C;

EPwm2Regs.TZCTL.all = 0x0FFF;//0x0FFB; //Force EPWMxB to a low state

EPwm2Regs.AQCTLB.all = 0x0215; //CBU=HIGH, CAU=LOW, PRD=LOW, ZERO=LOW
EPwm2Regs.AQCTLA.all = 0x0124; //CBU=LOW, CAU=HIGH, PRD=LOW, ZERO=Nothing
EPwm2Regs.CMPA.half.CMPA = DB_AtoP;
EPwm2Regs.CMPB = (HSFB_PERIOD);

EPwm2Regs.DCFWINDOW = DB_PtoA+3;

EPwm1Regs.CMPA.half.CMPA = trig_up;
EPwm1Regs.CMPB = (HSFB_PERIOD+10); //set to 0, avoid CMPB to force EPWM2 sync event. Use DCAEVT1.sync to sync EPwm2 module.
EPwm1Regs.ETSEL.all=0x0B0D;

//Update RAMP value.
Comp3Regs.RAMPMAXREF_SHDW = DACDRV_RAMP_In; //Q16 type, max value is 0xFFFF;
Comp3Regs.DACVAL.all = (DACDRV_RAMP_In>>6); //Q10 type

}
else //PWM counter direction is DOWN
{

EPwm2Regs.TZCLR.all |= 0x0C;
EPwm2Regs.TZCTL.all = 0x0FFF;//0x0FFE; //Force EPWMxA to a low state

EPwm2Regs.AQCTLA.all = 0x0125; //CBU=LOW, CAU=HIGH,PRD=LOW, ZERO=LOW
EPwm2Regs.AQCTLB.all = 0x0214; //CBU=HIGH,CAU=LOW, PRD=LOW, ZER0=Nothing

EPwm2Regs.CMPB = DB_AtoP;
EPwm2Regs.CMPA.half.CMPA = (HSFB_PERIOD);

EPwm2Regs.DCFWINDOW = DB_PtoA+3; //Need confirm


EPwm1Regs.CMPA.half.CMPA = trig_dwn;
EPwm1Regs.CMPB = HSFB_PERIOD+10; //set to period, avoid CMPB to force EPWM2 sync event. Use DCAEVT1.sync to sync EPwm2 module.
EPwm1Regs.ETSEL.all = 0x0B0C;


}

上述配置是否通过更改 DACDRV_RAMP_IN 的值来更改相移角?

此致

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    绿色环保、

    您是否查看过 controlSUITE 中的参考设计代码? 它包含一个峰值电流模式控制相移全桥解决方案。  

    C:\ti\controlSUITE\development_kits\HVPSFB_v1.1

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、我们参考了此例程。我想知道:

    (1) TI 例程具有 F28027、但内部中断是用汇编语言编写的、看起来更困难、是否有纯 C 语言例程?

    (2)同时、我发现如果我减小 DACDRV_RAMP_IN 的值、相移角确实会减小、但如果低于1700、相移角将增大。(RAMPDECVAL_Shdw=15)、如何设置斜率和基准尺寸。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Feng:

    [引用 userid="402909" URL"~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1043467/tms320f28035-the-phase-shifted-full-bridge-problem-of-psfb-peak-current-control-based-on-tms320ff28035/3860520 #3860520"](1) TI 例程具有 F28027、但内部中断是用汇编语言编写的、看起来更困难、是否有纯 C 语言例程?

    我们没有用于 F28027器件的 C 代码 ISR。 我们还有另一个基于全新 F28004x 器件的 TIDM-02000设计。 这也是一个峰值电流模式控制相移全桥、它使用 C 代码 ISR 和一些新器件功能。

    [引用 userid="402909" URL"~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1043467/tms320f28035-the-phase-shifted-full-bridge-problem-of-psfb-peak-current-control-based-on-tms320ff28035/3860520 #3860520"](2)同时、我发现如果我减小 DACDRV_RAMP_IN 的值、相移角度确实会减小、但如果低于1700、相移角度将增大。(RAMPDECVAL_Shdw=15)、如何设置斜率[和引用]。

    我不知道为什么相位角开始增加。 但您可以参阅 TIDM-02000用户指南的第3.3.4节、了解斜坡补偿。

    此致、

    陈  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Chen、

    我想问一个问题、即如何实现 SR 驱动器的打开和关闭。 我们知道、它使用比较器事件来打开 SR 驱动器、但如何关闭驱动器。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    似乎您在另一个主题中询问了问题、因此我将关闭这个主题。

    此致、