This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMDSCNCD28388D:为实现无限回送而需要做的更改

Guru**** 2763585 points

Other Parts Discussed in Thread: C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1018605/tmdscncd28388d-what-changes-to-make-to-achieve-loopback-infinitely

器件型号:TMDSCNCD28388D
主题中讨论的其他器件:C2000WARE

大家好、  

我可以寻求帮助吗? 以下是我的客户问题:

"我想从 c2000ware 无限运行以太网环回示例。 为了实现这一点、我必须对 C2000ware 的现有代码(ethernet_ex1_basic_tx_rx_loopback)进行哪些更改?"

我们希望收到您的建议。 非常感谢您的参与。

此致、

Gerald

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我附加了一个更新的环回示例、该示例持续发送更新的数据并将其接收到 Rx 缓冲器中。

    pData 是发送缓冲区。 接收到的数据存储在 EtherNet_rxBuffer 中。 I 是环路计数。

    请注意 、您需要在示例中使用 ethernet_no_f_RX_packets = 2、否则会出现故障 ISR、因为在 ethernet.c 中、ethernet_no_fo_fo_RX_packets 定义为2、因此下一个接收缓冲区地址在默认 ex1中变为无效地址。

    //#############################################################################
    //
    // FILE:   ethernet_ex1_basic_tx_rx_loopback.c
    //
    // TITLE:  Ethernet Basic Transmit and Receive MAC Loopback Example
    //
    //! \addtogroup driver_example_cm_list
    //! <h1> Ethernet MAC Internal Loopback </h1>
    //!
    //! This example demonstrates the steps to be followed in using the
    //! Ethernet of the Communication Manager Subsystem to initialize
    //! the Ethernet module and Configure the module in MAC Loop back mode
    //! Prepares a packet to be sent, Sends the packet and reads the statistics
    //! to check if the packet is received by the module
    //! Before running this Communication Manager code the C28x cpu1 code has to be run
    //! to configure the clocks to Communication manager
    //! and required IO pads for Ethernet module
    //!
    //! \b External \b Connections \n
    //!  This example programs the Ethernet module in Internal Loop back mode
    //! and hence needs no external connection on the MII Data lines.
    //! But it needs the MII Tx and Rx clocks to be input on those pins
    //! Refer to the C28x CPU1 code of ethernet_config_c28x project
    //! for which GPIOs are used for connecting to the PHY
    //!
    //! \b Watch \b Variables \n
    //!  - None
    //!
    //
    //#############################################################################
    //
    //
    // $Copyright: $
    //#############################################################################
    
    //
    // Included Files
    //
    #include "driverlib_cm.h"
    #include "cm.h"
    
    //
    // Defines
    //
    #define PACKET_LENGTH 132
    
    
    #define ETHERNET_NO_OF_RX_PACKETS   2U
    //
    //Change this define for changing Packet buffer length
    //
    #define ETHERNET_MAX_PACKET_LENGTH 1538U
    
    
    
    //
    // Globals
    //
    uint8_t pData[PACKET_LENGTH];
    //
    // Globals
    //
    uint8_t Ethernet_rxBuffer[ETHERNET_NO_OF_RX_PACKETS *
                              ETHERNET_MAX_PACKET_LENGTH];
    
    //
    // Main
    //
    void main(void)
    {
        Ethernet_InitInterfaceConfig initInterfaceConfig;
        Ethernet_InitConfig *pInitCfg;
        Ethernet_Pkt_Desc pktDesc;
        uint32_t i;
        Ethernet_Statistics stats;
        Ethernet_Handle emac_handle;
    
        //
        // Initialize device clock and peripherals
        //
        CM_init();
    
        //
        //Form the unicast Packet in Memory
        //
        for(i=0;i<PACKET_LENGTH/4;i++)
        {
            //
            //First 6 bytes of the packet are the MAC Destination Address
            //Bytes, the Destination and CRC shall be inserted by the hardware
            //
            if(i == 0)
                *((uint32_t *)pData + i) = 0x01020304;
            else if(i == 1)
                *((uint32_t *)pData + i)  = 0xFFFF0506;
            else
                HWREG((uint32_t *)pData +i) = 0xFFFFFFFF;
        }
    
        //
        //Select the MII interface of the module
        //
        initInterfaceConfig.ssbase = EMAC_SS_BASE;
        initInterfaceConfig.enet_base = EMAC_BASE;
        initInterfaceConfig.phyMode = ETHERNET_SS_PHY_INTF_SEL_MII;
        //
        //Assign SoC specific functions for Enabling,Disabling interrupts
        //and for enabling the Peripheral at system level
        //
        initInterfaceConfig.ptrPlatformInterruptDisable = &Platform_disableInterrupt;
        initInterfaceConfig.ptrPlatformInterruptEnable = &Platform_enableInterrupt;
        initInterfaceConfig.ptrPlatformPeripheralEnable = &Platform_enablePeripheral;
        initInterfaceConfig.ptrPlatformPeripheralReset = &Platform_resetPeripheral;
        //
        //Assign the peripheral number at the SoC
        //
        initInterfaceConfig.peripheralNum = SYSCTL_PERIPH_CLK_ENET;
        //
        //Assign the default SoC specific interrupt numbers of Ethernet interrupts
        //
        initInterfaceConfig.interruptNum[0] = INT_EMAC;
        initInterfaceConfig.interruptNum[1] = INT_EMAC_TX0;
        initInterfaceConfig.interruptNum[2] = INT_EMAC_TX1;
        initInterfaceConfig.interruptNum[3] = INT_EMAC_RX0;
        initInterfaceConfig.interruptNum[4] = INT_EMAC_RX1;
    
        pInitCfg = Ethernet_initInterface(initInterfaceConfig);
    
        //
        // Get an initial configuration of known good parameters
        //
        Ethernet_getInitConfig(pInitCfg);
        pInitCfg->dmaMode.InterruptMode = ETHERNET_DMA_MODE_INTM_MODE2;
        //
        //Configure the Loopback mode
        //
        pInitCfg->loopbackMode = ETHERNET_MAC_CONFIGURATION_LM_LOOPBACK_ENABLED;
        
        //
        //Assign the callbacks for Getting packet buffer when needed
        //Releasing the TxPacketBuffer on Transmit interrupt callbacks
        //Receive packet callback on Receive packet completion interrupt
        //
        pInitCfg->pfcbGetPacket = &Ethernet_getPacketBuffer;
        pInitCfg->pfcbFreePacket = &Ethernet_releaseTxPacketBuffer;
        pInitCfg->pfcbRxPacket = &Ethernet_receivePacketCallback;
        //
        //Assign the Buffer to be used by the Low level driver for receiving
        //Packets. This should be accessible by the Ethernet DMA
        //
        pInitCfg->rxBuffer = Ethernet_rxBuffer;
    
        //
        //The Application handle is not used by this application
        //Hence using a dummy value of 1
        //
        Ethernet_getHandle((Ethernet_Handle)1,pInitCfg , &emac_handle);
        //
        //Do global Interrupt Enable
        //
        (void)Interrupt_enableInProcessor();
        //
        //Assign default ISRs
        //
        Interrupt_registerHandler(INT_EMAC_TX0, Ethernet_transmitISR);
        Interrupt_registerHandler(INT_EMAC_RX0, Ethernet_receiveISR);
        //
        //Enable the default interrupt handlers
        //
        Interrupt_enable(INT_EMAC_TX0);
        Interrupt_enable(INT_EMAC_RX0);
                pktDesc.bufferLength = PACKET_LENGTH;
                pktDesc.dataOffset = 0;
                pktDesc.dataBuffer = pData;
                pktDesc.nextPacketDesc = 0;
                pktDesc.flags = ETHERNET_PKT_FLAG_SOP |ETHERNET_PKT_FLAG_EOP|ETHERNET_PKT_FLAG_SA_INS;
                pktDesc.pktChannel = ETHERNET_DMA_CHANNEL_NUM_0;
                pktDesc.pktLength = PACKET_LENGTH;
                pktDesc.validLength = PACKET_LENGTH;
                pktDesc.numPktFrags = 1;
    
        //
        //Send the packet prepared
        //
        i=0;
        while(1)
        {
            //
            //Prepare a Packet Descriptor structure to send a packet
            //This contains a single buffer packet
            //The Source address shall be inserted by the MAC
            //Packet CRC is auto computed by the module and appended in the packet
            //
            pktDesc.bufferLength = PACKET_LENGTH;
            pktDesc.dataOffset = 0;
            pktDesc.dataBuffer = pData;
            pktDesc.nextPacketDesc = 0;
            pktDesc.flags = ETHERNET_PKT_FLAG_SOP |ETHERNET_PKT_FLAG_EOP;
            pktDesc.pktChannel = ETHERNET_DMA_CHANNEL_NUM_0;
            pktDesc.pktLength = PACKET_LENGTH;
            pktDesc.validLength = PACKET_LENGTH;
            pktDesc.numPktFrags = 1;
    
            Ethernet_sendPacket(emac_handle,&pktDesc);
    
            //
            //Delay for the MAC to send the packet on the wire and receive it
            //
            SysCtl_delay(3000000);
    
            //
            //Read the statistics of the Module
            //
            Ethernet_getStatistics(emac_handle, &stats);
            i++;
            pData[7] = i;
        }
    
    
        //
        //Check if a packet has been received
        //
        if(!stats.rxUnicastPacketsGood)
             __asm("   bkpt #0");
    
    }
    
    
    

    此致、

    Yashwant