This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28388D:闪存–预取队列字的深度

Guru**** 2609285 points
Other Parts Discussed in Thread: C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1027589/tms320f28388d-flash-the-prefetch-queue-words-depth

器件型号:TMS320F28388D
主题中讨论的其他器件:C2000WARE

勘误表 TMS320F2838x 实时 MCU 器件勘误表 器件修订版本 A、0  

通报存储器:有效存储器之外的预取

闪存中提到了它–预取队列深度为16个 x16字。

但在 表3-1中。 受通报影响的存储器-闪存(0x000B FFF8-0x000B FFFF)为8字深度。

请澄清。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Tarun、

    这意味着、如果该段用于程序代码、则在链接器.cmd 文件中、对于闪存存储器、您应该从分配中排除地址0xBFFF8-0xBFFFF (在闪存扇区13中)。  如果存储器用于数据存储、则没有此类限制。

    在任何使用闪存存储程序代码的示例中、我们都在 C2000Ware 示例中的.cmd 文件中处理了上述内容

    我用 C/P 来显示2838x_flash_lnk_cpu1.cmd 以下内容(在目录路径 C:\ti\c2000\C2000Ware_3_04_00_00\device_support\f2838x\con\cmd):

    MEMORY
    {
       /* BEGIN is used for the "boot to Flash" bootloader mode   */
       BEGIN            : origin = 0x080000, length = 0x000002
       BOOT_RSVD        : origin = 0x000002, length = 0x0001AF     /* Part of M0, BOOT rom will use this for stack */
       RAMM0            : origin = 0x0001B1, length = 0x00024F
       RAMM1            : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD       : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
       RAMD0            : origin = 0x00C000, length = 0x000800
       RAMD1            : origin = 0x00C800, length = 0x000800
       RAMLS0           : origin = 0x008000, length = 0x000800
       RAMLS1           : origin = 0x008800, length = 0x000800
       RAMLS2           : origin = 0x009000, length = 0x000800
       RAMLS3           : origin = 0x009800, length = 0x000800
       RAMLS4           : origin = 0x00A000, length = 0x000800
       RAMLS5           : origin = 0x00A800, length = 0x000800
       RAMLS6           : origin = 0x00B000, length = 0x000800
       RAMLS7           : origin = 0x00B800, length = 0x000800
       RAMGS0           : origin = 0x00D000, length = 0x001000
       RAMGS1           : origin = 0x00E000, length = 0x001000
       RAMGS2           : origin = 0x00F000, length = 0x001000
       RAMGS3           : origin = 0x010000, length = 0x001000
       RAMGS4           : origin = 0x011000, length = 0x001000
       RAMGS5           : origin = 0x012000, length = 0x001000
       RAMGS6           : origin = 0x013000, length = 0x001000
       RAMGS7           : origin = 0x014000, length = 0x001000
       RAMGS8           : origin = 0x015000, length = 0x001000
       RAMGS9           : origin = 0x016000, length = 0x001000
       RAMGS10          : origin = 0x017000, length = 0x001000
       RAMGS11          : origin = 0x018000, length = 0x001000
       RAMGS12          : origin = 0x019000, length = 0x001000
       RAMGS13          : origin = 0x01A000, length = 0x001000
       RAMGS14          : origin = 0x01B000, length = 0x001000
       RAMGS15          : origin = 0x01C000, length = 0x000FF8
    //   RAMGS15_RSVD     : origin = 0x01CFF8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       /* Flash sectors */
       FLASH0           : origin = 0x080002, length = 0x001FFE  /* on-chip Flash */
       FLASH1           : origin = 0x082000, length = 0x002000  /* on-chip Flash */
       FLASH2           : origin = 0x084000, length = 0x002000  /* on-chip Flash */
       FLASH3           : origin = 0x086000, length = 0x002000  /* on-chip Flash */
       FLASH4           : origin = 0x088000, length = 0x008000  /* on-chip Flash */
       FLASH5           : origin = 0x090000, length = 0x008000  /* on-chip Flash */
       FLASH6           : origin = 0x098000, length = 0x008000  /* on-chip Flash */
       FLASH7           : origin = 0x0A0000, length = 0x008000  /* on-chip Flash */
       FLASH8           : origin = 0x0A8000, length = 0x008000  /* on-chip Flash */
       FLASH9           : origin = 0x0B0000, length = 0x008000  /* on-chip Flash */
       FLASH10          : origin = 0x0B8000, length = 0x002000  /* on-chip Flash */
       FLASH11          : origin = 0x0BA000, length = 0x002000  /* on-chip Flash */
       FLASH12          : origin = 0x0BC000, length = 0x002000  /* on-chip Flash */
       FLASH13          : origin = 0x0BE000, length = 0x001FF0  /* on-chip Flash */
    //   FLASH13_RSVD     : origin = 0x0BFFF0, length = 0x000010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       CPU1TOCPU2RAM   : origin = 0x03A000, length = 0x000800
       CPU2TOCPU1RAM   : origin = 0x03B000, length = 0x000800
       CPUTOCMRAM      : origin = 0x039000, length = 0x000800
       CMTOCPURAM      : origin = 0x038000, length = 0x000800
    
       CANA_MSG_RAM     : origin = 0x049000, length = 0x000800
       CANB_MSG_RAM     : origin = 0x04B000, length = 0x000800
    
       RESET            : origin = 0x3FFFC0, length = 0x000002
    }
    
    SECTIONS
    {
       codestart           : > BEGIN, ALIGN(8)
       .text               : >> FLASH1 | FLASH2 | FLASH3 | FLASH4, ALIGN(8)
       .cinit              : > FLASH4, ALIGN(8)
       .switch             : > FLASH1, ALIGN(8)
       .reset              : > RESET, TYPE = DSECT /* not used, */
       .stack              : > RAMM1
    
    #if defined(__TI_EABI__)
       .init_array      : > FLASH1, ALIGN(8)
       .bss             : > RAMLS5
       .bss:output      : > RAMLS3
       .bss:cio         : > RAMLS5
       .data            : > RAMLS5
       .sysmem          : > RAMLS5
       /* Initalized sections go in Flash */
       .const           : > FLASH5, ALIGN(8)
    #else
       .pinit           : > FLASH1, ALIGN(8)
       .ebss            : > RAMLS5
       .esysmem         : > RAMLS5
       .cio             : > RAMLS5
       /* Initalized sections go in Flash */
       .econst          : >> FLASH4 | FLASH5, ALIGN(8)
    #endif
    
       ramgs0 : > RAMGS0, type=NOINIT
       ramgs1 : > RAMGS1, type=NOINIT
       
       MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT
       MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, type=NOINIT
       MSGRAM_CPU_TO_CM    : > CPUTOCMRAM, type=NOINIT
       MSGRAM_CM_TO_CPU    : > CMTOCPURAM, type=NOINIT
    
       /* The following section definition are for SDFM examples */
       Filter_RegsFile  : > RAMGS0
       Filter1_RegsFile : > RAMGS1, fill=0x1111
       Filter2_RegsFile : > RAMGS2, fill=0x2222
       Filter3_RegsFile : > RAMGS3, fill=0x3333
       Filter4_RegsFile : > RAMGS4, fill=0x4444
       Difference_RegsFile : >RAMGS5, fill=0x3333
    
       #if defined(__TI_EABI__)
           .TI.ramfunc : {} LOAD = FLASH3,
                            RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                            LOAD_START(RamfuncsLoadStart),
                            LOAD_SIZE(RamfuncsLoadSize),
                            LOAD_END(RamfuncsLoadEnd),
                            RUN_START(RamfuncsRunStart),
                            RUN_SIZE(RamfuncsRunSize),
                            RUN_END(RamfuncsRunEnd),
                            ALIGN(8)
       #else
           .TI.ramfunc : {} LOAD = FLASH3,
                            RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                            LOAD_START(_RamfuncsLoadStart),
                            LOAD_SIZE(_RamfuncsLoadSize),
                            LOAD_END(_RamfuncsLoadEnd),
                            RUN_START(_RamfuncsRunStart),
                            RUN_SIZE(_RamfuncsRunSize),
                            RUN_END(_RamfuncsRunEnd),
                            ALIGN(8)
       #endif
    
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

    最棒的

    Matthew