This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280049C:F280049 SDFM 程序

Guru**** 2847400 points

Other Parts Discussed in Thread: AMC1306EVM, C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1006872/tms320f280049c-f280049-sdfm-program

器件型号:TMS320F280049C
主题中讨论的其他器件:AMC1306EVMC2000WARE

你(们)好

我尝试使用 AMC1306EVM 来测试 SDFM 程序。 我对文件 sdfm_ex4_pwm_sync_cpuread.c 进行了一些更改

在文件夹//ti/c2000/C2000Ware_3_02_00_00/drivelib/f28004x/examples/sdfm.下

//###########################################################################
//
// FILE:   sdfm_ex4_pwm_sync_cpuread.c
//
// TITLE:  SDFM PWM Sync Example
//
//! \addtogroup driver_example_list
//! <h1> SDFM PWM Sync </h1>
//!
//! In this example, SDFM filter data is read by CPU in SDFM ISR routine. The
//! SDFM configuration is shown below:
//!     - SDFM1 is used in this example.
//!     - MODE0 Input control mode selected
//!     - Comparator settings
//!         - Sinc3 filter selected
//!         - OSR = 32
//!         - hlt = 0x7FFF (Higher threshold setting)
//!         - llt  = 0x0000(Lower threshold setting)
//!  -  Data filter settings
//!      - All the 4 filter modules enabled
//!      - Sinc3 filter selected
//!      - OSR = 256
//!      - All the 4 filters are synchronized by using PWM
//!       (Master Filter enable bit)
//!      - Filter output represented in 16 bit format
//!      - In order to convert 25 bit Data filter
//!        into 16 bit format user needs to right shift by 10 bits for
//!        Sinc3 filter with OSR = 256
//!  - Interrupt module settings for SDFM filter
//!      - All the 4 higher threshold comparator interrupts disabled
//!      - All the 4 lower threshold comparator interrupts disabled
//!      - All the 4 modulator failure interrupts disabled
//!      - All the 4 filter will generate interrupt when a new filter data
//!        is available
//!
//! \b External \b Connections \n
//!    Connect Sigma-Delta streams to (SD-D1, SD-C1 to SD-D4,SD-C4)
//!    on GPIO24-GPIO31
//!
//! \b Watch \b Variables \n
//! -  \b filter1Result - Output of filter 1
//! -  \b filter2Result - Output of filter 2
//! -  \b filter3Result - Output of filter 3
//! -  \b filter4Result - Output of filter 4
//!
//
//###########################################################################
// $TI Release: F28004x Support Library v1.10.00.00 $
// $Release Date: Tue May 26 17:06:03 IST 2020 $
// $Copyright:
// Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include <stdio.h>

//
// Defines
//
#define MAX_SAMPLES               1024
#define EPWM_TIMER_TBPRD          65535  // ePWM Period register

#define JIAKAI
//
// Globals
//
uint32_t sdfmInstance;
uint32_t pwmInstance = EPWM8_BASE; // ePWM 8 for synchronizing SDFM1 filters
int16_t  filter1Result[MAX_SAMPLES];
int16_t  filter2Result[MAX_SAMPLES];
int16_t  filter3Result[MAX_SAMPLES];
int16_t  filter4Result[MAX_SAMPLES];
#pragma DATA_SECTION(filter1Result, "Filter1_RegsFile");
#pragma DATA_SECTION(filter2Result, "Filter2_RegsFile");
#pragma DATA_SECTION(filter3Result, "Filter3_RegsFile");
#pragma DATA_SECTION(filter4Result, "Filter4_RegsFile");

//
// Function Prototypes
//
void configureSDFMPins(void);
void initEPWM(uint32_t epwmInstance);
__interrupt void sdfm1ErrorISR(void);
__interrupt void sdfmDR1ISR(void);

//
// Main
//
void main(void)
{
   uint16_t  hlt, llt;

   //
   // Initialize device clock and peripherals
   //
   Device_init();

   //
   // Setup GPIO by disabling pin locks and enabling pullups
   //
   Device_initGPIO();

   //
   // Initialize PIE and clear PIE registers. Disables CPU interrupts.
   //
   Interrupt_initModule();

   //
   // Initialize the PIE vector table with pointers to the shell Interrupt
   // Service Routines (ISR).
   //
   Interrupt_initVectorTable();

   //
   // Interrupts that are used in this example are re-mapped to
   // ISR functions found within this file.
   //
   Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP5);
   Interrupt_register(INT_SDFM1DR1, sdfmDR1ISR);
   Interrupt_register(INT_SDFM1, sdfm1ErrorISR);

   //
   // Enable SDFM1 Error and DR interrupts
   //
   Interrupt_enable(INT_SDFM1);
   Interrupt_enable(INT_SDFM1DR1);

   //
   // Configure GPIO pins as SDFM pins
   //
   configureSDFMPins();

    //
    // Select SDFM1
    //
    sdfmInstance = SDFM1_BASE;

    //
    // Input Control Module:
    // Configure Modulator Clock rate = Modulator data rate
    //
    SDFM_setupModulatorClock(sdfmInstance, SDFM_FILTER_1,
                             SDFM_MODULATOR_CLK_EQUAL_DATA_RATE);
#ifndef JIAKAI
    SDFM_setupModulatorClock(sdfmInstance, SDFM_FILTER_2,
                             SDFM_MODULATOR_CLK_EQUAL_DATA_RATE);

    SDFM_setupModulatorClock(sdfmInstance, SDFM_FILTER_3,
                             SDFM_MODULATOR_CLK_EQUAL_DATA_RATE);

    SDFM_setupModulatorClock(sdfmInstance, SDFM_FILTER_4,
                             SDFM_MODULATOR_CLK_EQUAL_DATA_RATE);
#endif
    //
    // Comparator Module
    //
    hlt = 0x7FFF;    //Over value threshold settings
    llt = 0x0000;    //Under value threshold settings

    //
    // Configure Comparator module's comparator filter type and comparator's OSR
    // value, higher threshold, lower threshold
    //
    SDFM_configComparator(sdfmInstance,
        (SDFM_FILTER_1 | SDFM_FILTER_SINC_3 | SDFM_SET_OSR(32)),
        (SDFM_GET_LOW_THRESHOLD(llt) | SDFM_GET_HIGH_THRESHOLD(hlt)), 0);
#ifndef JIAKAI
    SDFM_configComparator(sdfmInstance,
        (SDFM_FILTER_2 | SDFM_FILTER_SINC_3 | SDFM_SET_OSR(32)),
        (SDFM_GET_LOW_THRESHOLD(llt) | SDFM_GET_HIGH_THRESHOLD(hlt)), 0);
    SDFM_configComparator(sdfmInstance,
        (SDFM_FILTER_3 | SDFM_FILTER_SINC_3 | SDFM_SET_OSR(32)),
        (SDFM_GET_LOW_THRESHOLD(llt) | SDFM_GET_HIGH_THRESHOLD(hlt)), 0);
    SDFM_configComparator(sdfmInstance,
        (SDFM_FILTER_4 | SDFM_FILTER_SINC_3 | SDFM_SET_OSR(32)),
        (SDFM_GET_LOW_THRESHOLD(llt) | SDFM_GET_HIGH_THRESHOLD(hlt)), 0);
#endif
    //
    // Data filter Module
    //
    // Configure Data filter modules filter type, OSR value and
    // enable / disable data filter
    //
    SDFM_configDataFilter(sdfmInstance, (SDFM_FILTER_1 | SDFM_FILTER_SINC_3 |
           SDFM_SET_OSR(256)), (SDFM_DATA_FORMAT_16_BIT | SDFM_FILTER_ENABLE |
           SDFM_SHIFT_VALUE(0x000A)));
#ifndef JIAKAI
    SDFM_configDataFilter(sdfmInstance, (SDFM_FILTER_2 | SDFM_FILTER_SINC_3 |
           SDFM_SET_OSR(256)), (SDFM_DATA_FORMAT_16_BIT | SDFM_FILTER_ENABLE |
           SDFM_SHIFT_VALUE(0x000A)));

    SDFM_configDataFilter(sdfmInstance, (SDFM_FILTER_3 | SDFM_FILTER_SINC_3 |
           SDFM_SET_OSR(256)), (SDFM_DATA_FORMAT_16_BIT | SDFM_FILTER_ENABLE |
           SDFM_SHIFT_VALUE(0x000A)));

    SDFM_configDataFilter(sdfmInstance, (SDFM_FILTER_4 | SDFM_FILTER_SINC_3 |
           SDFM_SET_OSR(256)), (SDFM_DATA_FORMAT_16_BIT | SDFM_FILTER_ENABLE |
           SDFM_SHIFT_VALUE(0x000A)));
#endif
    //
    // Enable Master filter bit: Unless this bit is set none of the filter modules
    // can be enabled. All the filter modules are synchronized when master filter
    // bit is enabled after individual filter modules are enabled.
    //
    SDFM_enableMasterFilter(sdfmInstance);

    //
    // PWM signals can synchronize SDFM1 filters. Enabling PWM sync for SDFM
    // filters.
    //
    SDFM_enableExternalReset(sdfmInstance, SDFM_FILTER_1);
#ifndef JIAKAI
    SDFM_enableExternalReset(sdfmInstance, SDFM_FILTER_2);
    SDFM_enableExternalReset(sdfmInstance, SDFM_FILTER_3);
    SDFM_enableExternalReset(sdfmInstance, SDFM_FILTER_4);
#endif
    SDFM_setPWMSyncSource(sdfmInstance, SDFM_FILTER_1, SDFM_SYNC_PWM8_SOCA);
#ifndef JIAKAI
    SDFM_setPWMSyncSource(sdfmInstance, SDFM_FILTER_2, SDFM_SYNC_PWM8_SOCA);
    SDFM_setPWMSyncSource(sdfmInstance, SDFM_FILTER_3, SDFM_SYNC_PWM8_SOCA);
    SDFM_setPWMSyncSource(sdfmInstance, SDFM_FILTER_4, SDFM_SYNC_PWM8_SOCA);
#endif
    //
    // Init EPWMs
    //
    initEPWM(pwmInstance);

    //
    // Enable interrupts
    //
    // Following SDFM interrupts can be enabled / disabled using this function.
    //  Enable / disable comparator high threshold
    //  Enable / disable comparator low threshold
    //  Enable / disable modulator clock failure
    //  Enable / disable filter acknowledge
    //
    SDFM_enableInterrupt(sdfmInstance, SDFM_FILTER_1,
            (SDFM_MODULATOR_FAILURE_INTERRUPT |
             SDFM_DATA_FILTER_ACKNOWLEDGE_INTERRUPT));
#ifndef JIAKAI
    SDFM_enableInterrupt(sdfmInstance, SDFM_FILTER_2,
            (SDFM_MODULATOR_FAILURE_INTERRUPT |
             SDFM_DATA_FILTER_ACKNOWLEDGE_INTERRUPT));

    SDFM_enableInterrupt(sdfmInstance, SDFM_FILTER_3,
            (SDFM_MODULATOR_FAILURE_INTERRUPT |
             SDFM_DATA_FILTER_ACKNOWLEDGE_INTERRUPT));

    SDFM_enableInterrupt(sdfmInstance, SDFM_FILTER_4,
            (SDFM_MODULATOR_FAILURE_INTERRUPT |
             SDFM_DATA_FILTER_ACKNOWLEDGE_INTERRUPT));
#endif
    SDFM_disableInterrupt(sdfmInstance, SDFM_FILTER_1,
            (SDFM_HIGH_LEVEL_THRESHOLD_INTERRUPT |
             SDFM_LOW_LEVEL_THRESHOLD_INTERRUPT));
#ifndef JIAKAI
    SDFM_disableInterrupt(sdfmInstance, SDFM_FILTER_2,
            (SDFM_HIGH_LEVEL_THRESHOLD_INTERRUPT |
             SDFM_LOW_LEVEL_THRESHOLD_INTERRUPT));

    SDFM_disableInterrupt(sdfmInstance, SDFM_FILTER_3,
            (SDFM_HIGH_LEVEL_THRESHOLD_INTERRUPT |
             SDFM_LOW_LEVEL_THRESHOLD_INTERRUPT));

    SDFM_disableInterrupt(sdfmInstance, SDFM_FILTER_4,
            (SDFM_HIGH_LEVEL_THRESHOLD_INTERRUPT |
             SDFM_LOW_LEVEL_THRESHOLD_INTERRUPT));
#endif
    while((HWREGH(pwmInstance + EPWM_O_TBCTR)) < 550);

    //
    // Enable master interrupt so that any of the filter interrupts can trigger
    // by SDFM interrupt to CPU
    //
    SDFM_enableMasterInterrupt(sdfmInstance);

    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

    while(1);
}

//
// sdfm1ErrorISR - SDFM1 Error ISR
//
__interrupt void sdfm1ErrorISR(void)
{
    //
    // Clear SDFM flag register (SDIFLG)
    //
    SDFM_clearInterruptFlag(SDFM1_BASE, SDFM_MASTER_INTERRUPT_FLAG |
                            0xFFFF);

    //
    // Acknowledge this interrupt to receive more interrupts from group 5
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP5);
}

//
// sdfmDR1ISR - SDFM DR1 ISR
//
__interrupt void sdfmDR1ISR(void)
{
    static uint16_t loopCounter1 = 0;

    SDFM_setOutputDataFormat(SDFM1_BASE, SDFM_FILTER_1,
                             SDFM_DATA_FORMAT_16_BIT);

    //
    // Read SDFM flag register (SDIFLG)
    //
    if(loopCounter1 >= MAX_SAMPLES)
    {
        loopCounter1 = 0;
    }

    while((HWREG(SDFM1_BASE + SDFM_O_SDIFLG) & 0xF000U) != 0xF000U)
    {
    }

#ifdef JIAKAI
    filter1Result[loopCounter1++] =
           (int16_t)(SDFM_getFilterData(SDFM1_BASE, SDFM_FILTER_1) >> 16U);
#else
    filter1Result[loopCounter1] =
           (int16_t)(SDFM_getFilterData(SDFM1_BASE, SDFM_FILTER_1) >> 16U);
    filter2Result[loopCounter1] =
           (int16_t)(SDFM_getFilterData(SDFM1_BASE, SDFM_FILTER_2) >> 16U);
    filter3Result[loopCounter1] =
           (int16_t)(SDFM_getFilterData(SDFM1_BASE, SDFM_FILTER_3) >> 16U);
    filter4Result[loopCounter1++] =
           (int16_t)(SDFM_getFilterData(SDFM1_BASE, SDFM_FILTER_4) >> 16U);
#endif

    //
    // Clear SDFM flag register (SDIFLG)
    //
    SDFM_clearInterruptFlag(SDFM1_BASE, SDFM_MASTER_INTERRUPT_FLAG |
                            SDFM_FILTER_1_NEW_DATA_FLAG            |
                            SDFM_FILTER_2_NEW_DATA_FLAG            |
                            SDFM_FILTER_3_NEW_DATA_FLAG            |
                            SDFM_FILTER_4_NEW_DATA_FLAG);

    //
    // Acknowledge this interrupt to receive more interrupts from group 5
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP5);
}

//
// configureSDFMPins - Configure SDFM GPIOs
//
void configureSDFMPins(void)
{
    uint16_t pin;

    //
    // Configure GPIO16-GPIO31 as SDFM pins
    //
#ifdef JIAKAI
    for(pin = 16; pin <= 17; pin++)
    {
        GPIO_setDirectionMode(pin, GPIO_DIR_MODE_IN);
        GPIO_setMasterCore(pin, GPIO_CORE_CPU1);
        GPIO_setPadConfig(pin, GPIO_PIN_TYPE_STD);
        GPIO_setQualificationMode(pin, GPIO_QUAL_ASYNC);
    }
    GPIO_setPinConfig(GPIO_16_SD_D1);
    GPIO_setPinConfig(GPIO_17_SD_C1);
#else
    for(pin = 24; pin <= 31; pin++)
    {
        GPIO_setDirectionMode(pin, GPIO_DIR_MODE_IN);
        GPIO_setMasterCore(pin, GPIO_CORE_CPU1);
        GPIO_setPadConfig(pin, GPIO_PIN_TYPE_STD);
        GPIO_setQualificationMode(pin, GPIO_QUAL_ASYNC);
    }
    GPIO_setPinConfig(GPIO_24_SD_D1);
    GPIO_setPinConfig(GPIO_25_SD_C1);
    GPIO_setPinConfig(GPIO_26_SD_D2);
    GPIO_setPinConfig(GPIO_27_SD_C2);
    GPIO_setPinConfig(GPIO_28_SD_D3);
    GPIO_setPinConfig(GPIO_29_SD_C3);
    GPIO_setPinConfig(GPIO_30_SD_D4);
    GPIO_setPinConfig(GPIO_31_SD_C4);
#endif
}

//
// done - Function to halt debugger and stop application
//
void done(void)
{
    asm(" ESTOP0");
    for(;;);
}

//
// initEPWM - Initialize specified EPWM settings
//
void initEPWM(uint32_t epwmInstance)
{
    //
    // Disable sync(Freeze clock to PWM as well)
    //
    SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);

    //
    // Setup TBCLK: Configure timer period = 801 TBCLKs, phase = 0 &
    // clear counter
    //
    EPWM_setTimeBasePeriod(epwmInstance, EPWM_TIMER_TBPRD);
    EPWM_setPhaseShift(epwmInstance, 0U);
    EPWM_setTimeBaseCounter(epwmInstance, 0U);

    //
    // Set CMPA value
    //
    EPWM_setCounterCompareValue(epwmInstance, EPWM_COUNTER_COMPARE_A, 200U);

    //
    // Setup counter mode
    //
    EPWM_setTimeBaseCounterMode(epwmInstance, EPWM_COUNTER_MODE_UP);
    EPWM_setClockPrescaler(epwmInstance,
                           EPWM_CLOCK_DIVIDER_1,
                           EPWM_HSCLOCK_DIVIDER_1);

    //
    // Set actions:
    // Toggle PWMxA on event A, up-count
    // Toggle PWMxB on event A, up-count
    //
    GPIO_setPadConfig(0, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_0_EPWM1A);
    GPIO_setPadConfig(1, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_1_EPWM1B);
    EPWM_setTimeBasePeriod(EPWM1_BASE, 24);     // PWM1 period: 0.5us
    EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP);
    EPWM_setClockPrescaler(EPWM1_BASE,
                           EPWM_CLOCK_DIVIDER_1,
                           EPWM_HSCLOCK_DIVIDER_1);
    EPWM_setActionQualifierAction(EPWM1_BASE,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_TOGGLE,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);
//                                EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
    EPWM_setActionQualifierAction(EPWM1_BASE,
                                  EPWM_AQ_OUTPUT_B,
                                  EPWM_AQ_OUTPUT_TOGGLE,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);
//                                EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);

#ifndef JIAKAI
    //
    // Configure SOCA signal
    //
    //
    EPWM_setADCTriggerSource(EPWM1_BASE, EPWM_SOC_A, EPWM_SOC_TBCTR_U_CMPA);
    EPWM_setADCTriggerEventPrescale(EPWM1_BASE, EPWM_SOC_A, 1);
#endif

    //
    // Enable sync and clock to PWM
    //
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
}

//
// End of file
//

主要更改如下(代码中标记为"JAIKAI"):

1、 将 Sdfm1.CH1 GPIO 更改为 GPIO16和 GPIO17。

2.更改 PWM1以生成2MHz 50/50占空比(PWM1A 为 Sdfm1.CH1和 AMC1306EVM 提供时钟)。

我运行代码、但程序永远不会进入中断例程 sdfmDR1ISR 和 sdfm1ErrorISR。

如果 PWM1未连接到 GPIO17、程序进入 sdfmErrorISR、但仍然不进入  sdfmDR1ISR。

谢谢、

Jiakai

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Jaikai、

    您设置的 PWM 周期小于寄存器中的计数器比较值、因为该值导致器件未正确计时。 请您在使用为 SDFM 模块计时时检查 ePWM 输出。

    此外、如果值未发生更改、我建议不要再次调用函数、例如。 设置预分频器被调用两次是您的代码。

    谢谢、

    Aditya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Aditya、

    我再次检查代码、发现 CPU 不会在中断例程 sdfmDR1ISR 中的断点处中断、

    程序进入下面的循环、无法从循环中退出。

      while ((HWREG (SDFM1_base + SDFM_O_SDIFLG)& 0xF000U)!= 0xF000U)
      {
      }

    我已按如下方式更改程序、现在代码正常工作:

    while ((HWREG (SDFM1_base + SDFM_O_SDIFLG)& 0xF000U)!= 0x1000U)

    您能告诉我如何在此代码中添加 FIFO 操作吗?

    谢谢、

    Jiakai

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Jaikai、

    很高兴您找到了该问题。 不过、您能否说明您是否更新了 PWM 配置? 我想知道。

    有关启用 FIFO 的信息、请参阅 。  您可以在代码中直接使用一段代码。

    Aditya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Aditya、

    我更改了 PWM 配置、因为我需要 PWM1为 AMC1306EVM 和 SDFM1.C1提供时钟。

    我已经合并了 ex4和 ex5、因此该程序现在可以在按下后使用 PWM8.SOCA 来启动 SDFM 数据转换

    足够的数据进入 FIFO、SDFM 会引起中断。

    非常感谢你的帮助。

    Jiakai