This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMDSSOLARUINVKIT:SolarMicroInv-Main.c 初始化过程

Guru**** 2587365 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/995652/tmdssolaruinvkit-solarmicroinv-main-c-initialization-procedure

器件型号:TMDSSOLARUINVKIT

大家好、下午好、

我有一个有关 TI 太阳能微型逆变器开发套件的超级问题。  我的嵌入式编程技能扩展到一个大学课程、实现非常基本的功能。  我 不是100%确定如何执行第6.1.3.1节第5和6号、内容如下:5.运行偏移校准例程以计算 PV 电流和电网的 ADC 输入通道上的模拟偏移。  6.为控制循环使用的50KHz ISR 配置中断,为后台任务配置1KHz ISR。 选择1KHz ISR 时、50Hz ISR 可中断1KHz ISR。   

是否有一个演示或一个如何解释我需要对给定代码执行的确切操作? 我使用过 MPLAB IDE、但从未使用过 Code Composer。  我担心、通过添加或更改代码、如果文件实际编译和编译、我可能会损坏电路板或其中一个组件。 非常感谢您的帮助。  下面是.c 文件和开发套件用户指南的链接。   

www.ti.com/.../tidu405b.pdf

//----------------------------------------------------------------------------------
//	FILE:			SolarMicroInv_F2803x-Main.C
//
//	Description:	Solar MicroInverter Project
//
//	Version: 		1.0
//
//  Target:  		TMS320F2803x(PiccoloB), 
//
//----------------------------------------------------------------------------------
//  Copyright Texas Instruments Copyright 2004-2013
//----------------------------------------------------------------------------------
//  Revision History:
//----------------------------------------------------------------------------------
//  Date	  | Description / Status
//----------------------------------------------------------------------------------
// June 26 2013 :  (Manish Bhardwaj, Shamim Choudhury)
//----------------------------------------------------------------------------------
//
// PLEASE READ - Useful notes about this Project
// Although this project is made up of several files, the most important ones are:
//	 "{ProjectName}-Main.C"	- this file
//		- Application Initialization, Peripheral config,
//		- Application management
//		- Slower background code loops and Task scheduling
//	 "{ProjectName}-DevInit_F28xxx.C
//		- Device Initialization, e.g. Clock, PLL, WD, GPIO mapping
//		- Peripheral clock enables
//		- DevInit file will differ per each F28xxx device series, e.g. F280x, F2833x,
//	 "{ProjectName}-Settings.h"
//		- Global defines (settings) project selections are found here
//		- This file is referenced by both C and ASM files.
//	 "{ProjectName}-Includes.h"
//		- Include file used by project are defined in this file
//
// Code is made up of sections, e.g. "FUNCTION PROTOTYPES", "VARIABLE DECLARATIONS" ,..etc
//	each section has FRAMEWORK and USER areas.
//  FRAMEWORK areas provide useful ready made "infrastructure" code which for the most part
//	does not need modification, e.g. Task scheduling, ISR call, GUI interface support,...etc
//  USER areas have functional example code which can be modified by USER to fit their appl.
//
// Code can be compiled with various build options (Incremental Builds IBx), these
//  options are selected in file "{ProjectName}-Settings.h".  Note: "Rebuild All" compile
//  tool bar button must be used if this file is modified.
//----------------------------------------------------------------------------------

#include "SolarMicroInv-Includes.h"

//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// FUNCTION PROTOTYPES
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// Add prototypes of functions being used in the project here

void DeviceInit(void);
#ifdef FLASH		
void InitFlash();
#endif
void MemCopy();

#ifdef FLASH
#pragma CODE_SECTION(Inv_ISR,"ramfuncs");
#pragma CODE_SECTION(OneKhzISR,"ramfuncs");
#endif
//This is the control loop ISR run at 50Khz
interrupt void Inv_ISR(void);
//This is 1 Khz ISR slaved off CPU timer 2,
interrupt void OneKhzISR();

void InitECapture();

void ADC_SOC_CNF(int ChSel[], int Trigsel[], int ACQPS[], int IntChSel, int mode);

void PWM_1ch_UpDwnCnt_CNF(int16 n, Uint16 period, int16 mode, int16 phase);
void PWM_MicroInvLineClamp_CNF(int n,int period,int deadband_rising,int deadband_falling);

// -------------------------------- FRAMEWORK --------------------------------------
// State Machine function prototypes
//----------------------------------------------------------------------------------
// Alpha states
void A0(void);	//state A0
void B0(void);	//state B0

// A branch states
void A1(void);	//state A1
void A2(void);	//state A2
void A3(void);	//state A3
void A4(void);	//state A4

// B branch states
void B1(void);	//state B1
void B2(void);	//state B2
void B3(void);	//state B3

// Variable declarations
void (*Alpha_State_Ptr)(void);	// Base States pointer
void (*A_Task_Ptr)(void);		// State pointer A branch
void (*B_Task_Ptr)(void);		// State pointer B branch
//----------------------------------------------------------------------------------

//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// VARIABLE DECLARATIONS - GENERAL
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// -------------------------------- FRAMEWORK --------------------------------------

int16 VTimer0[4];					// Virtual Timers slaved off CPU Timer 0
int16 VTimer1[4];					// Virtual Timers slaved off CPU Timer 1

// Used for running BackGround in flash, and ISR in RAM
extern Uint32 *RamfuncsLoadStart, *RamfuncsLoadEnd, *RamfuncsRunStart;
extern Uint32 *IQfuncsLoadStart, *IQfuncsLoadEnd, *IQfuncsRunStart;

// Used for ADC Configuration 
int ChSel[16] = { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 };
int TrigSel[16] = { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 };
int ACQPS[16] = { 8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8 };

//---------------------------------------------------------------------------
// Used to indirectly access all EPWM modules
volatile struct EPWM_REGS *ePWM[] = {
		&EPwm1Regs,			//intentional: (ePWM[0] not used)
		&EPwm1Regs, &EPwm2Regs, &EPwm3Regs, &EPwm4Regs, &EPwm5Regs, &EPwm6Regs,
		&EPwm7Regs, };

// Used to indirectly access all Comparator modules
volatile struct COMP_REGS *Comp[] = { &Comp1Regs,//intentional: (Comp[0] not used)
		&Comp1Regs, &Comp2Regs, &Comp3Regs };
// ---------------------------------- USER -----------------------------------------

//-----------------------------Inverter & DC-DC Control Loop Variables -------------
// String to describe the state of the PV Inverter
char cPV_State[40];

// Solar Library Objects

// RAMP to generate forced angle when grid is not present
RAMPGEN_IQ rgen1;

// CNTL 3p3z for inverter current control
#pragma DATA_SECTION(cntl3p3z_InvI_vars,"cntl_var_RAM")
#pragma DATA_SECTION(cntl3p3z_InvI_coeff,"cntl_coeff_RAM")
CNTL_3P3Z_IQ_VARS cntl3p3z_InvI_vars;
CNTL_3P3Z_IQ_COEFFS cntl3p3z_InvI_coeff;

// CNTL 2p2z for flyback current control
#pragma DATA_SECTION(cntl2p2z_DCDCI_vars,"cntl_var_RAM")
#pragma DATA_SECTION(cntl2p2z_DCDCI_coeff,"cntl_coeff_RAM")
CNTL_2P2Z_IQ_VARS cntl2p2z_DCDCI_vars;
CNTL_2P2Z_IQ_COEFFS cntl2p2z_DCDCI_coeff;

// CNTL PI for bus control
CNTL_PI_IQ cntlPI_BusInv;
int16 UpdateCoef;
long Pgain_BusInv, Dgain_BusInv, Igain_BusInv, Dmax_BusInv;

// SPLL Objects of two types for grid angle lock
SPLL_1ph_IQ spll1;
SPLL_1ph_SOGI_IQ spll2;
float c2, c1;
long Phase_Jump, Phase_Jump_Trig;

// Sine analyzer block for RMS Volt, Curr and Power measurements
SINEANALYZER_DIFF_wPWR_IQ sine_mains;

// notch filter objects for filtering bus voltage, pv current and voltage sense signals
#pragma DATA_SECTION(Bus_Volt_notch,"cntl_var_RAM")
#pragma DATA_SECTION(PV_volt_notch,"cntl_var_RAM")
#pragma DATA_SECTION(PV_cur_notch,"cntl_var_RAM")
#pragma DATA_SECTION( notch_TwiceGridFreq,"cntl_coeff_RAM")
NOTCH_COEFF_IQ notch_TwiceGridFreq;
NOTCH_VARS_IQ Bus_Volt_notch,PV_volt_notch,PV_cur_notch;

// MPPT object for flyback current reference selection
MPPT_INCC_I_IQ mppt_incc_I1;
int16 MPPT_slew;
int16 Run_MPPT;
int16 MPPT_ENABLE;

// Datalogger to plot variables
#if INCR_BUILD==1 || INCR_BUILD==2
DLOG_4CH_IQ dlog1;
int16 DBUFF1[100], DBUFF2[100], DBUFF3[100], DBUFF4[100];
int16 D_val1, D_val2, D_val3, D_val4;
#endif

//TODO
// Inverter and Flyback Variables
_iq24 inv_meas_cur_inst, inv_meas_vol_inst, vbus_meas_inst, vbus_meas_avg ;
// reference variable Inverter
_iq24 InvModIndex, inv_Iset, inv_ref_cur_inst, inv_bus_ref;
// Measure Values DC-DC Stage
long pv_meas_cur_inst,pv_meas_vol_inst,pv_meas_cur_avg, pv_meas_vol_avg;
// Reference Values DC-DC Stage
long pv_ref_cur_inst, pv_ref_cur_mppt, pv_ref_cur_fixed;
// Measurement Offsets
_iq24 offset_165, offset_GridCurrent, PV_SenseVolt_Offset, PV_SenseCurr_Offset,DC_Bus_Offset;
//Offset filter coefficient K1: 0.05/(T+0.05);
_iq K1 = _IQ(0.998);
//Offset filter coefficient K2: T/(T+0.05)
_iq K2 = _IQ(0.001999);
int16 OffsetCalCounter;
// Duty variables for flyback and inverter (per unit and compare register values)
_iq24 duty_flyback_pu, duty_inv_pu;
long duty_inv, duty_flyback;
// Duty for which the inverter is not switched around zero
int16 DontSwitchZeroLimit;
// Flags for clearing trips and closing the loops and the Relay
int16 CloseIloopInv, ClearInvTrip,CloseFlybackLoop, ClearFlyBackTrip, RlyConnect;
// Flags for detecting ZCD
_iq24 InvSine, InvSine_prev;
int16 ZCDDetect;
// State Machine Variable
enum PVInverterStates {
	Idle = 0,
	CheckGrid = 1,
	CheckPV = 2,
	MonitorDCBus = 3,
	EnableMPPT = 4,
	PVInverterActive = 5,
	ResetState1 = 6,
	ResetState2 = 7,
	FaultState=8
};
enum PVInverterStates PVInverterState = Idle;
enum PVInverterStates PVInverterState_Old= Idle;
int16 SlewState4;
int32 SlewClrInvTrip;
// Value that is emperically tested to make sure the relay connect happens at ZCD
// This accounts for any delay in the relay connection from the time the GPIO is triggered high
long RlyConnectVal;
// DC Bus voltage values where the state machine is triggered to connect relay,
// start the invetrter and flag faults
volatile long inv_bus_rly_connect, inv_bus_start_volt, inv_bus_UV, inv_bus_OV;
//detecting faults
enum Faults {
	NoFault = 0,
	OverVoltageDCBus = 1,
	UnderVoltageDCBus = 2,
	OverVoltageGrid = 3,
	UnderVoltageGrid = 4,
	OverCurrentFlag = 5
};
enum Faults FaultFlag = NoFault;
int16 BusOverVoltageTrip, BusUnderVoltageTrip,OverCurrent;
Uint16 Gui_InvStart;
Uint16 Gui_InvStop;
// Measuring AC signal
long ACFreq_SysTicks;
volatile float AC_Freq;
volatile _iq24 ACFreq;
_iq24 ACFreq2;
volatile int UF_Flag, OF_Flag, UV_Flag, OV_Flag;
volatile long GRID_MAX_VRMS, GRID_MIN_VRMS;
volatile long GRID_MIN_FREQ, GRID_MAX_FREQ;
int Grid_Freq = GRID_FREQ;
long ECAP_TimerMaxVal;
volatile long inv_emavg_vol;

// Stand Alone Flash Image Instrumentation
// GPIO toggles for different states
int16 LedBlinkCnt1, LedBlinkCnt2;
int16 timer1;

// Display Values 

// Monitor ("Get")						// Display as:
int32 Gui_Vbus;							//Q20
int32 Gui_Vpv;							//Q20
int32 Gui_Ipv;                          //Q20
int32 Gui_GridFreq;						//Q20
int32 Gui_Prms;							//Q6
int32 Gui_Irms;							//Q12
long Gui_Vrms;							//Q6
int32 Gui_Vavg;
int Gui_MPPTEnable;
long IRMS, VRMS, PRMS;
long K_Irms, K_Vrms, K_Prms, K_Vpv, K_Ipv;

// The following declarations are required in order to use the SFO
// library functions:
int MEP_ScaleFactor; // Global variable used by the SFO library
// Result can be used for all HRPWM channels
// This variable is also copied to HRMSTEP
// register by SFO() function.
int status;

//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// MAIN CODE - starts here
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
void main(void) {
//=================================================================================
//	INITIALISATION - General
//=================================================================================

	// The DeviceInit() configures the clocks and pin mux registers 
	// The function is declared in {ProjectName}-DevInit_F2803/2x.c,
	// Please ensure/edit that all the desired components pin muxes 
	// are configured properly that clocks for the peripherals used
	// are enabled, for example the individual PWM clock must be enabled 
	// along with the Time Base Clock 

	DeviceInit();	// Device Life support & GPIO

//-------------------------------- FRAMEWORK --------------------------------------

// Only used if running from FLASH
// Note that the variable FLASH is defined by the compiler with -d FLASH

#ifdef FLASH		
// Copy time critical code and Flash setup code to RAM
// The  RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart
// symbols are created by the linker. Refer to the linker files. 
	MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
	MemCopy(&IQfuncsLoadStart, &IQfuncsLoadEnd, &IQfuncsRunStart);

// Call Flash Initialization to setup flash waitstates
// This function must reside in RAM
	InitFlash();	// Call the flash wrapper init function
#endif //(FLASH)

// Timing sync for background loops
// Timer period definitions found in PeripheralHeaderIncludes.h
	CpuTimer0Regs.PRD.all = mSec5;		// A tasks
	CpuTimer1Regs.PRD.all = mSec50;	// B tasks
// Configure CPU-Timer 2 to interrupt every second:
// 60MHz CPU Freq, Period (in uSeconds)
// Configure CPU Timer interrupt for 1KHz interrupt
	ConfigCpuTimer(&CpuTimer2, 60, 1000);
	CpuTimer2Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0

// Tasks State-machine init
	Alpha_State_Ptr = &A0;
	A_Task_Ptr = &A1;
	B_Task_Ptr = &B1;

	VTimer0[0] = 0;
	VTimer1[0] = 0;

	LedBlinkCnt1 = 5;
	LedBlinkCnt2 = 5;

//==================================================================================
//	INCREMENTAL BUILD OPTIONS - NOTE: selected via {ProjectName-Settings.h
//==================================================================================
// ---------------------------------- USER -----------------------------------------

	//TODO PWM Configuration
	/*************  PWM Configuration **************************/
	SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;   // Disable clocks for EPWM

	// 50Khz at 60Mhz device = > 60*1000/50 =1200,
	PWM_MicroInvLineClamp_CNF(1, (CPU_FREQ/(INV_FREQ)), INV_DEADBAND,
			INV_DEADBAND);

	// Put DC-DC PWM configuration here
	PWM_1ch_UpDwnCnt_CNF(3, (CPU_FREQ / (FLYBACK_FREQ)), 0,
			(CPU_FREQ / (FLYBACK_FREQ * 2)) - 2);

	// PWM 4 configured only to verify the blanking pulse for over current trips
//	PWM_1ch_UpDwnCnt_CNF(4, (CPU_FREQ / (FLYBACK_FREQ)), 0,
//				(CPU_FREQ / (FLYBACK_FREQ * 2)) - 2);
//
//	EPwm4Regs.TBPHS.half.TBPHS=EPwm4Regs.TBPHS.half.TBPHS-2;
//
//	EPwm4Regs.AQCTLA.bit.CAD=AQ_SET;
//	EPwm4Regs.AQCTLA.bit.CBU=AQ_CLEAR;
//	EPwm4Regs.AQCTLA.bit.CAU=AQ_NO_ACTION;
//
//	EPwm4Regs.CMPA.half.CMPA=0;
//	EPwm4Regs.CMPB=0;

	// Add the dead band configuration for PWM3
	EALLOW;
	EPwm3Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; /* Rising Delay on 1A & Falling Delay on 1B*/
	EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; /* Active high complementary mode (EPWMxA is inverted)*/
	EPwm3Regs.DBCTL.bit.IN_MODE = DBA_ALL; /* 1A for Rising& Falling*/
	EPwm3Regs.DBRED = FLYBACK_DEADBAND_RED; /* Delay at Rising edge*/
	EPwm3Regs.DBFED = FLYBACK_DEADBAND_FED; /* Delay at Falling edge*/
	EDIS;

	SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;   // Enable TBCLK

	// Calling SFO() updates the HRMSTEP register with calibrated MEP_ScaleFactor.
	// MEP_ScaleFactor/HRMSTEP must be filled with calibrated value in order // for the module to work
	status = SFO_INCOMPLETE;
	while (status == SFO_INCOMPLETE) { // Call until complete
		status = SFO();
	}
	if (status != SFO_ERROR) { // IF SFO() is complete with no errors
		EALLOW;
		EPwm1Regs.HRMSTEP = MEP_ScaleFactor;
		EDIS;
	}
	if (status == SFO_ERROR) {
		while (1)
			; // SFO function returns 2 if an error occurs
		// The code would loop here for infinity if it // returns an error
	}

	/************ PWM Configuration END **********************/

	/****************** ADC  Configuration *******************/
	//TODO ADC Configuration
#define IPV_FB		AdcResult.ADCRESULT1
#define VPV_FB      AdcResult.ADCRESULT2
#define VBUS_FB		AdcResult.ADCRESULT3

#define IINV_FB		AdcResult.ADCRESULT5
#define VAC_FB		AdcResult.ADCRESULT6
#define VREF165_FB	AdcResult.ADCRESULT7
#define V0_5_REF	AdcResult.ADCRESULT8

	//Map channel to ADC Pin
	// the dummy reads are to account for first sample issue in Rev 0 silicon
	// Please refer to the Errata and the datasheet, this would be fixed in later versions of the silicon

	// EPWM 3 SOC Signals
	ChSel[0] = 6;		// Dummy read for first
	ChSel[1] = 6;		// A6 - IPV, A2 - IP1 Sen - CT
	ChSel[2] = 11;		// B3 - VPV
	//ChSel[3] = 14;		// B6 - VBOOST in Rev 1 PCB
	ChSel[3] = 4;		// A4 - VBOOST in Rev 2 PCB

	// EPWM 1 SOC Signals
	ChSel[4] = 1;		// A1 - IGRID
	ChSel[5] = 1;		// A1 - IGRID
	ChSel[6] = 9;		// B1 - VGRID
	ChSel[7] = 7;		// A7 - Ref_1.65V
	ChSel[8] = 5;		// A5 - Ref_0.5V
	ChSel[9] = 8;		// B0 - LEM Current Reference Output
	//ChSel[10] = 0;		// A0 - PLC

	// Select Trigger Event 
	TrigSel[0] = ADCTRIG_EPWM3_SOCA;
	TrigSel[1] = ADCTRIG_EPWM3_SOCA;
	TrigSel[2] = ADCTRIG_EPWM3_SOCA;

	TrigSel[3] = ADCTRIG_EPWM2_SOCA;
	TrigSel[4] = ADCTRIG_EPWM2_SOCA;
	TrigSel[5] = ADCTRIG_EPWM2_SOCA;
	TrigSel[6] = ADCTRIG_EPWM2_SOCA;
	TrigSel[7] = ADCTRIG_EPWM2_SOCA;
	TrigSel[8] = ADCTRIG_EPWM2_SOCA;
	//TrigSel[9]= ADCTRIG_EPWM2_SOCA;
	//TrigSel[10]= ADCTRIG_EPWM2_SOCA;

	// use auto clr ADC int flag mode=2
	// end of conversion of inverter current triggers ADC INT 1
	ADC_SOC_CNF(ChSel, TrigSel, ACQPS, 5, 2);

	// Configure the PWM to issue appropriate Start of Conversion for the ADC
	// DC-DC Flyback
	EPwm3Regs.ETSEL.bit.SOCAEN = 1; /* Enable SOC on A group*/
	EPwm3Regs.ETSEL.bit.SOCASEL = ET_CTRD_CMPB; /* Select SOC from counter at ctr = 0*/
	EPwm3Regs.ETPS.bit.SOCAPRD = ET_1ST; /* Generate pulse on 1st even*/
	EPwm3Regs.ETSEL.bit.SOCAEN = 1; /* Enable SOC on A group*/
	EPwm3Regs.CMPB = 12;

	// DC-AC Inverter
	// Note: SOCA is configured by the PWM CNF macro
	// but we ovewirte it to make the adc sampling centered
	EPwm2Regs.ETSEL.bit.SOCAEN = 1;
	EPwm2Regs.ETSEL.bit.SOCASEL = ET_CTRD_CMPB;
	EPwm2Regs.ETPS.bit.SOCAPRD = ET_1ST;
	EPwm2Regs.ETSEL.bit.SOCAEN = 1;
	EPwm2Regs.CMPB = 70; // EPWM 2 is phase shifter by 50 i.e. when EPWM1 Ctr is zero then EPWM2 Ctr is 52
						 // The we take 8 cycles to sample + 6 cycles to covert the first dummy
						 // and add half the ADC sample width =? 52+8+6+4

	/************ ADC Configuration END **********************/

	/************ ECAP Init **********************************/
	InitECapture();
	/************ ECAP Init END ******************************/

	/************ Control Variable Initialization ************/
	//TODO Solar Library Module Initialization
	// Initialize the net variables
	//RAMPGEN
	RAMPGEN_IQ_init(&rgen1);
	rgen1.Freq = _IQ24(GRID_FREQ);
	rgen1.StepAngleMax = _IQ24(1.0/INV_FREQ);

	//CNTL3P3Z Inverter Current Loop
	CNTL_3P3Z_IQ_VARS_init(&cntl3p3z_InvI_vars);
	CNTL_3P3Z_IQ_COEFFS_init(&cntl3p3z_InvI_coeff);

	cntl3p3z_InvI_coeff.Coeff_A1 = _IQ24(1.584);
	cntl3p3z_InvI_coeff.Coeff_A2 = _IQ24(-0.6978);
	cntl3p3z_InvI_coeff.Coeff_A3 = _IQ24(0.1137);
	cntl3p3z_InvI_coeff.Coeff_B0 = _IQ24(0.2866);
	cntl3p3z_InvI_coeff.Coeff_B1 = _IQ24(-0.3173);
	cntl3p3z_InvI_coeff.Coeff_B2 = _IQ24(0.3338);
	cntl3p3z_InvI_coeff.Coeff_B3 = _IQ24(-0.2616);

	cntl3p3z_InvI_coeff.Max = _IQ24(0.95);
	cntl3p3z_InvI_coeff.Min = _IQ24(-0.95);

	//CNTL2P2Z Flyback DCDC Current Loop
	CNTL_2P2Z_IQ_VARS_init(&cntl2p2z_DCDCI_vars);
	CNTL_2P2Z_IQ_COEFFS_init(&cntl2p2z_DCDCI_coeff);

	cntl2p2z_DCDCI_coeff.Coeff_A1 = _IQ24(1.0);                       // A1 = 1
	cntl2p2z_DCDCI_coeff.Coeff_A2 = 0.0;                              // A2 = 0
	cntl2p2z_DCDCI_coeff.Coeff_B0 = _IQ24(0.0917);      			  // B0
	cntl2p2z_DCDCI_coeff.Coeff_B1 = _IQ24(-0.07138);                  // B1
	cntl2p2z_DCDCI_coeff.Coeff_B2 = _IQ24(0.0);                       // B2
	cntl2p2z_DCDCI_coeff.Max = _IQ24(0.8);
	cntl2p2z_DCDCI_coeff.Min = _IQ24(0.0);
	cntl2p2z_DCDCI_coeff.IMin = _IQ24(-0.05);

	//CNTL PI Inverter Bus Voltage Regulation Loop
	Dmax_BusInv = _IQ24(0.80);
	Pgain_BusInv = _IQ24(1.0);
	Igain_BusInv = _IQ24(0.001);

	CNTL_PI_IQ_init(&cntlPI_BusInv);
	cntlPI_BusInv.Kp = Pgain_BusInv;
	cntlPI_BusInv.Ki = Igain_BusInv;
	cntlPI_BusInv.Umax = Dmax_BusInv;
	cntlPI_BusInv.Umin = _IQ(0.025);

	// MPPT
	MPPT_INCC_I_IQ_init(&mppt_incc_I1);
	mppt_incc_I1.IpvH = _IQ24(0.000);
	mppt_incc_I1.IpvL = _IQ24(0.000);
	mppt_incc_I1.VpvH = _IQ24(0.000);
	mppt_incc_I1.VpvL = _IQ24(0.000);
	mppt_incc_I1.MaxI = _IQ24(0.5);
	mppt_incc_I1.MinI = _IQ24(0.0);
	mppt_incc_I1.Stepsize = _IQ24(0.005);
	mppt_incc_I1.mppt_first = 1;
	mppt_incc_I1.mppt_enable = 1;
	mppt_incc_I1.StepFirst = _IQ24(0.01);

	// SPLL 1ph Notch Filter Method intialization
	SPLL_1ph_IQ_init(GRID_FREQ, _IQ21((float)(1.0/ISR_FREQUENCY)), &spll1);

	spll1.lpf_coeff.B0_lf = _IQ21(B0_LPF);
	spll1.lpf_coeff.B1_lf = _IQ21(B1_LPF);
	spll1.lpf_coeff.A1_lf = _IQ21(A1_LPF);

	c1 = 0.1;
	c2 = 0.00001;

	SPLL_1ph_IQ_notch_coeff_update(((float) (1.0 / ISR_FREQUENCY)),
			(float) (2 * PI * GRID_FREQ * 2), (float) c2, (float) c1, &spll1);

	//SPLL 1ph SOGI Method initialization

	SPLL_1ph_SOGI_IQ_init(GRID_FREQ, _IQ23((float)(1.0/ISR_FREQUENCY)), &spll2);
	spll2.lpf_coeff.B0_lf = _IQ23(B0_LPF);
	spll2.lpf_coeff.B1_lf = _IQ23(B1_LPF);
	spll2.lpf_coeff.A1_lf = _IQ23(A1_LPF);
	SPLL_1ph_SOGI_IQ_coeff_update(((float) (1.0 / ISR_FREQUENCY)),
			(float) (2 * PI * GRID_FREQ), &spll2);

	// NOTCH COEFF update for measurement filtering
	NOTCH_FLTR_IQ_VARS_init(&Bus_Volt_notch);
	NOTCH_FLTR_IQ_VARS_init(&PV_volt_notch);
	NOTCH_FLTR_IQ_VARS_init(&PV_cur_notch);
	NOTCH_FLTR_IQ_COEFF_Update(((float)(1.0/ISR_FREQUENCY)), (float)(2*PI*GRID_FREQ*2),(float)c2,(float)c1, &notch_TwiceGridFreq);

	//sine analyzer initialization
	SINEANALYZER_DIFF_wPWR_IQ_init(&sine_mains);
	sine_mains.Vin = 0;
	sine_mains.Iin = 0;
	sine_mains.SampleFreq = _IQ15(1000.0);
	sine_mains.Threshold = _IQ15(0.1);
	sine_mains.nsamplesMax=1000/UNIVERSAL_GRID_MIN_FREQ;
	sine_mains.nsamplesMin=1000/UNIVERSAL_GRID_MAX_FREQ;

	// Initialize DATALOG module
#if INCR_BUILD==1 || INCR_BUILD==2
	dlog1.input_ptr1 = &D_val1;
	dlog1.input_ptr2 = &D_val2;
	dlog1.input_ptr3 = &D_val3;  // spll.Out logged in buff3
	dlog1.input_ptr4 = &D_val4;  // ramp_sin logged in buff4
	dlog1.output_ptr1 = DBUFF1;
	dlog1.output_ptr2 = DBUFF2;
	dlog1.output_ptr3 = DBUFF3;
	dlog1.output_ptr4 = DBUFF4;
	dlog1.prev_value = 0;
	dlog1.trig_value = _IQ15(0.1);
	dlog1.status = 0;
	dlog1.pre_scalar = 10;
	dlog1.skip_count = 0;
	dlog1.size = 100;
	dlog1.count = 0;
#endif

	//Variable initialization
	// inverter measurement
	inv_meas_cur_inst=0;
	inv_meas_vol_inst=0;
	vbus_meas_inst=0;
	vbus_meas_avg=0;
	// reference variable Inverter
	InvModIndex=0;
	inv_Iset=0;
	inv_ref_cur_inst=0;
	inv_bus_ref = DC_BUS_REF_60HZ;
	// Measure Values DC-DC Stage
	pv_meas_cur_inst=0;
	pv_meas_vol_inst=0;
	pv_meas_cur_avg=0;
	pv_meas_vol_avg=0;
	// Reference Values DC-DC Stage
	pv_ref_cur_inst=0;
	pv_ref_cur_mppt=0;
	pv_ref_cur_fixed = _IQ24(0.15);
	// Measurement Offsets
	offset_GridCurrent = OFFSET_GRIDCURRENT_MEAS;
	PV_SenseVolt_Offset = OFFSET_PV_SENSEVOLT_MEAS;
	PV_SenseCurr_Offset = OFFSET_PV_SENSECURR_MEAS;
	DC_Bus_Offset=OFFSET_DC_BUS_MEAS;
	offset_165=0;
	// Duty variables for flyback and inverter (per unit and compare register values)
	duty_flyback_pu=0;
	duty_inv_pu=0;;
	duty_inv=0;
	duty_flyback=0;
	// Duty for which the inverter is not switched around zero
	DontSwitchZeroLimit = 15;
	// Flags for clearing trips and closing the loops and the Relay
	CloseIloopInv=0;
	ClearInvTrip=0;
	CloseFlybackLoop=0;
	ClearFlyBackTrip=0;
	RlyConnect=0;
	// Flags for detecting ZCD
	InvSine=0;
	InvSine_prev=0;
	ZCDDetect=0;
	PVInverterState = Idle;
	PVInverterState_Old= Idle;
	SlewState4=0;
	SlewClrInvTrip=0;
	// Value that is emperically tested to make sure the relay connect happens at ZCD
	// This accounts for any delay in the relay connection from the time the GPIO is triggered high
	RlyConnectVal = _IQ24(0.55);
	// DC Bus voltage values where the state machine is triggered to connect relay,
	// start the invetrter and flag faults
	inv_bus_rly_connect = DC_BUS_RELAY_CONNECT_VOLT_60HZ;
	inv_bus_start_volt = DC_BUS_INV_START_VOLT_60HZ;
	inv_bus_UV = DC_BUS_UNDERVOLTAGE_LIMIT_60HZ;
	inv_bus_OV = DC_BUS_OVERVOLTAGE_LIMIT_60HZ;
	FaultFlag = NoFault;
	BusOverVoltageTrip = 0;
	BusUnderVoltageTrip = 0;
	OverCurrent=0;
	Gui_InvStart=0;
	Gui_InvStop=0;
	// Measuring AC signal
	ACFreq_SysTicks=0;
	AC_Freq=0;
	ACFreq=0;
	ACFreq2=0;
	UF_Flag=0;
	OF_Flag=0;
	UV_Flag=0;
	OV_Flag=0;
	GRID_MIN_FREQ = UNIVERSAL_GRID_MIN_FREQ;
	GRID_MAX_FREQ = UNIVERSAL_GRID_MAX_FREQ;
	GRID_MIN_VRMS = UNIVERSAL_GRID_MIN_VRMS;
	GRID_MAX_VRMS = UNIVERSAL_GRID_MAX_VRMS;
	Grid_Freq = GRID_FREQ;
	ECAP_TimerMaxVal = (CPU_FREQ / CAP_MIN_FREQ_MEAS) >> 1; // Where 40 is the lowest frequency measured by ECAP module
	inv_emavg_vol=0;
	// Gui Variables
	Gui_Vbus=0;
	Gui_Vpv=0;
	Gui_Ipv=0;
	Gui_GridFreq=0;						//Q20
	Gui_Prms=0;							//Q6
	Gui_Irms=0;							//Q12
	Gui_Vrms=0;							//Q6
	Gui_MPPTEnable=1;
	Gui_Vavg=0;

	K_Vrms = 26803;	//K_Vrms=(418/511)*32767 = 26803, //RMS voltage is viewed as a Q6 number
	K_Irms = 28671;	//K_Irms=(7/8)*32767 = 28671, //Current is viewed as a Q12 number
	K_Prms = 187624;//K_Prms=(7*418/511)*32767 = 187624, //Power is viewed as a Q6 number
	K_Vpv = 17732; //K_Vpv=(138/255)*32767= 17732, // Panel Voltage is viewed as Q8
	K_Ipv = 30719;//K_Ipv=(15/16)*32767=30719 // Panel Current is viewed in Q11 number

	UpdateCoef = 0;
	MPPT_ENABLE = 0;
	Run_MPPT = 0;
	MPPT_slew = 0;

	strcpy(cPV_State,"Idle");

	/************ Control Variable Initialization END *********/

	/*********  Protection Mechanisms *****************/
	//TODO Protection Code
	EALLOW;
	// Cycle by cycle interrupt for CPU halt trip
	EPwm1Regs.TZSEL.bit.CBC6 = 0x1;
	EPwm2Regs.TZSEL.bit.CBC6 = 0x1;
	EPwm3Regs.TZSEL.bit.CBC6 = 0x1;

	// Adding one shot trip for over-current protection on the inverter TZ2
	EPwm1Regs.TZSEL.bit.OSHT2 = 0x1;
	EPwm2Regs.TZSEL.bit.OSHT2 = 0x1;

	// Adding one shot trip for over current of the flyback stage but avoid the <1% duty condition using blanking

	// First enable the COMP3
	Comp3Regs.COMPCTL.bit.COMPDACEN  =0x1;
	Comp3Regs.COMPCTL.bit.SYNCSEL    =0x0;	// asynchronous version of the COMP signal is passed to the EPWM/GPIO module
	Comp3Regs.COMPCTL.bit.CMPINV     =0x0;	// Output of the comparator is passed directly
	Comp3Regs.COMPCTL.bit.COMPSOURCE =0x0;	// inverting input of the comparator is connected to the internal DAC
	Comp3Regs.DACVAL.bit.DACVAL		 =700;	// set DAC input to peak trip point ~10 Amps, full scale is 15Amps
	AdcRegs.COMPHYSTCTL.bit.COMP1_HYST_DISABLE = 0x1;

	//Select COMP3 as one shot trip
	EPwm3Regs.DCTRIPSEL.bit.DCAHCOMPSEL=DC_COMP3OUT ;
	EPwm3Regs.TZDCSEL.bit.DCAEVT1=TZ_DCAH_HI;
	EPwm3Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT_FLT ;
	EPwm3Regs.DCACTL.bit.EVT1FRCSYNCSEL=DC_EVT_ASYNC;
	EPwm3Regs.TZSEL.bit.DCAEVT1=0x1;

	//Add blanking to avoid conditions where the over current trip generates <1% duty cycle

	EPwm3Regs.DCFCTL.bit.BLANKE=DC_BLANK_ENABLE; // Blanking window is enabled
	EPwm3Regs.DCFCTL.bit.BLANKINV=DC_BLANK_NOTINV; // Blanking window is not inverted
	EPwm3Regs.DCFCTL.bit.SRCSEL=DC_SRC_DCAEVT1; //DCAEVT1
	EPwm3Regs.DCFCTL.bit.PULSESEL=DC_PULSESEL_PRD; // apply offset from TBCTR=TBPRD
	EPwm3Regs.DCFOFFSET=59;
	EPwm3Regs.DCFWINDOW=255;

	// What do we want the OST/CBC events to do?
	// TZA events can force EPWMxA
	// TZB events can force EPWMxB

	EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // EPWMxA will go low
	EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low

	EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // EPWMxA will go low
	EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low

	EPwm3Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // EPWMxA will go low
	EPwm3Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low

	//clear any spurious trips
	EPwm1Regs.TZCLR.bit.OST = 1;
	EPwm2Regs.TZCLR.bit.OST = 1;
	EPwm3Regs.TZCLR.bit.OST = 1;

	// Force a trip event on all the PWM modules for safety
	EPwm1Regs.TZFRC.bit.OST = 0x1;
	EPwm2Regs.TZFRC.bit.OST = 0x1;
	EPwm3Regs.TZFRC.bit.OST = 0x1;
	EDIS;

	/*********  Protection Mechanism END *****************/

	/********* Run Calibration for offset in grid and panel current ******/
//TODO Run Calibration Task
	OffsetCalCounter=0;
	offset_GridCurrent=0;
	PV_SenseCurr_Offset=0;

	while(OffsetCalCounter<5000)
		{
			if(AdcRegs.ADCINTFLG.bit.ADCINT1==1)
			{
			PV_SenseCurr_Offset= _IQmpy(K1,PV_SenseCurr_Offset)+_IQmpy(K2,_IQ12toIQ(IPV_FB));
			offset_GridCurrent=_IQmpy(K1,offset_GridCurrent)+_IQmpy(K2,_IQ12toIQ(IINV_FB));
			OffsetCalCounter++;
			AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;		// Clear ADCINT1 flag
			}
		}

	/*********  INTERRUPTS & ISR INITIALIZATION ***********/
	// (best to run this section after other initialization)
	// Set up C28x Interrupt
	EALLOW;
	PieVectTable.ADCINT1 = &Inv_ISR;		// Inverter Control Interrupt
	PieVectTable.TINT2 = &OneKhzISR;		// 1kHz interrupt from CPU timer 2
	PieCtrlRegs.PIEIER1.bit.INTx1 = 1;	// Enable ADCINT1 in PIE group 1

	//ADC interrupt already enabled by ADC SOC Cnf
	IER |= M_INT1;		// Enable CPU INT1 for ADCINT1,ADCINT2,ADCINT9,TripZone
	IER |= M_INT14;					// CPU timer 2 is connected to CPU INT 14
	EINT;
	// Enable Global interrupt INTM
	ERTM;
	// Enable Global realtime interrupt DBGM
	EDIS;

	/************** BACKGROUND ********************/

//--------------------------------- FRAMEWORK -------------------------------------
	for (;;)  //infinite loop
			{
		// State machine entry & exit point
		//===========================================================
		(*Alpha_State_Ptr)();	// jump to an Alpha state (A0,B0,...)
		//===========================================================
	}
} //END MAIN CODE

//=================================================================================
//	STATE-MACHINE SEQUENCING AND SYNCRONIZATION
//=================================================================================

//--------------------------------- FRAMEWORK -------------------------------------
void A0(void) {
	// loop rate synchronizer for A-tasks
	if (CpuTimer0Regs.TCR.bit.TIF == 1) {
		CpuTimer0Regs.TCR.bit.TIF = 1;	// clear flag

		//-----------------------------------------------------------
		(*A_Task_Ptr)();		// jump to an A Task (A1,A2,A3,...)
		//-----------------------------------------------------------

		VTimer0[0]++;			// virtual timer 0, instance 0 (spare)
	}

	Alpha_State_Ptr = &B0;		// Comment out to allow only A tasks
}

void B0(void) {
	// loop rate synchronizer for B-tasks
	if (CpuTimer1Regs.TCR.bit.TIF == 1) {
		CpuTimer1Regs.TCR.bit.TIF = 1;				// clear flag

		//-----------------------------------------------------------
		(*B_Task_Ptr)();		// jump to a B Task (B1,B2,B3,...)
		//-----------------------------------------------------------
		VTimer1[0]++;			// virtual timer 1, instance 0 (spare)
	}

	Alpha_State_Ptr = &A0;		// Allow C state tasks
}

//=================================================================================
//	A - TASKS
//=================================================================================
//--------------------------------------------------------
void A1(void)
//--------------------------------------------------------
{
	if(PVInverterState_Old!=PVInverterState)
	{
		switch(PVInverterState)
		{
		case Idle:	strcpy(cPV_State,"Idle");
				break;
		case CheckGrid:	strcpy(cPV_State,"CheckGrid");
					break;
		case CheckPV:	strcpy(cPV_State,"CheckPV");
					break;
		case MonitorDCBus:	strcpy(cPV_State,"MonitorDCBus");
					break;
		case EnableMPPT:	strcpy(cPV_State,"EnableMPPT");
					break;
		case PVInverterActive:	strcpy(cPV_State,"PVInverterActive");
					break;
		case ResetState1:	strcpy(cPV_State,"ResetState1");
					break;
		case ResetState2:	strcpy(cPV_State,"ResetState2");
					break;
		case FaultState:if(FaultFlag==OverVoltageDCBus)
							strcpy(cPV_State,"FaultState: DC Bus Over Voltage");
						else if (FaultFlag==UnderVoltageDCBus)
							strcpy(cPV_State,"FaultState: DC Bus Under Voltage");
						else if (FaultFlag==OverVoltageGrid)
							strcpy(cPV_State,"FaultState: Over Voltage Grid");
						else if (FaultFlag==UnderVoltageGrid)
							strcpy(cPV_State,"FaultState: Under Voltage Grid");
						else if (FaultFlag==OverCurrentFlag)
							strcpy(cPV_State,"FaultState: Grid Current Over");
						else
							strcpy(cPV_State,"FaultState");
					break;
		}
	}

	PVInverterState_Old=PVInverterState;

	if(PVInverterState==Idle)
		Gui_GridFreq=ACFreq<<16;
	else
		Gui_GridFreq=(long)(spll2.fo)>>3;

	//-------------------
	//the next time CpuTimer0 'counter' reaches Period value go to A2
	A_Task_Ptr = &A2;
	//-------------------
}

//--------------------------------------------------------
void A2(void)  // Connect Disconnect
//-----------------------------------------------------------------
{
#if(INCR_BUILD==1)||(INCR_BUILD==2)
	if(RlyConnect==1)
	{
		GpioDataRegs.GPASET.bit.GPIO22=1;
	}
	else
	{
		GpioDataRegs.GPACLEAR.bit.GPIO22=1;
	}
#endif
	//-------------------
	//the next time CpuTimer0 'counter' reaches Period value go to A1
	A_Task_Ptr = &A3;
	//-------------------
}

//--------------------------------------------------------
void A3(void)
//-----------------------------------------
{

	//-----------------
	//the next time CpuTimer0 'counter' reaches Period value go to A1
	A_Task_Ptr = &A4;
	//-----------------
}

//--------------------------------------------------------
void A4(void)  // Spare
//--------------------------------------------------------
{
	//-----------------
	//the next time CpuTimer0 'counter' reaches Period value go to A1
	A_Task_Ptr = &A1;
	//-----------------
}

//=================================================================================
//	B - TASKS
//=================================================================================
//----------------------------------------
void B1(void)
//----------------------------------------
{
	if (UpdateCoef == 1) {

		UpdateCoef = 0;

		//SPLL_1ph_IQ_notch_coeff_update(((float)(1.0/ISR_FREQUENCY)), (float)(2*PI*GRID_FREQ*2),c2,c1, &spll1);
	}

	//-----------------
	//the next time CpuTimer1 'counter' reaches Period value go to B2
	B_Task_Ptr = &B2;
	//-----------------
}

//----------------------------------------
void B2(void) // Blink LED on the control CArd
//----------------------------------------
{
	// Toggle LD3 on control card to show execution of code
	if (LedBlinkCnt1 == 0) {
		GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1;//turn on/off LD3 on the controlCARD
		LedBlinkCnt1 = 4;
	} else
		LedBlinkCnt1--;

	//-----------------
	//the next time CpuTimer1 'counter' reaches Period value go to B3
	B_Task_Ptr = &B3;
	//-----------------
}

//----------------------------------------
void B3(void) // State Machine, Enable Disable Loops, User Controls  
//----------------------------------------
{

#if ((INCR_BUILD == 1))
	if (ClearInvTrip==1)
	{
		EALLOW;
		EPwm1Regs.TZCLR.bit.OST=0x1;
		EPwm2Regs.TZCLR.bit.OST=0x1;
		EDIS;
		ClearInvTrip=0;
	}
#endif

#if ((INCR_BUILD==1)||(INCR_BUILD==2))
	if (ClearFlyBackTrip==1)
	{
		EALLOW;
		EPwm3Regs.TZCLR.bit.OST=0x1;
		EDIS;
		ClearFlyBackTrip=0;
	}
#endif

	//-----------------
	//the next time CpuTimer1 'counter' reaches Period value go to B4
	B_Task_Ptr = &B1;
	//-----------------
}

// ISR for inverter 
interrupt void Inv_ISR() {

/*************************************************/
/************  Inverter Code *********************/
/*************************************************/

//-------------------------------------------------------------------
// Inverter Current and Voltage Measurements
//-------------------------------------------------------------------
	// TODO Inverter ISR
	offset_165 = ((int32) VREF165_FB) << 12;
	vbus_meas_inst = (((long)VBUS_FB<<12)-DC_Bus_Offset);
	inv_meas_vol_inst = ((long) (((long) VAC_FB << 12) - offset_165)) << 1;
	inv_meas_cur_inst = (((int32) IINV_FB << 12) - offset_GridCurrent) << 1;

//-----------------------------------------------------------------------------------------
#if (INCR_BUILD == 1 ) // Open Loop Check
//-----------------------------------------------------------------------------------------
	// Run the ramp ctl to generate the forced sine angle for open loop test of the inverter
	RAMPGEN_IQ_MACRO(rgen1);

	if(Phase_Jump==1)
	{
		rgen1.Angle+=_IQ24(0.25);
		if(rgen1.Angle>_IQ24(1.0))
		rgen1.Angle=rgen1.Angle-_IQ24(1.0);
		rgen1.Out=rgen1.Angle;
		Phase_Jump=0;
		if(Phase_Jump_Trig==0)
		Phase_Jump_Trig=_IQ24(1.0);
		else
		Phase_Jump_Trig=0;
	}
	// Use the angle value to compute the sine value
	InvSine = _IQsinPU(rgen1.Out);

	//NOTCH PLL
	/*spll1.AC_input=(long)InvSine>>3; // Q24 to Q21
	 SPLL_1ph_IQ_MACRO(spll1);*/
	//SOGI PLL
	spll2.u[0]=(long)InvSine>>1;
	SPLL_1ph_SOGI_IQ_MACRO(spll2);

	// inverter duty value
	duty_inv_pu=_IQ24mpy(InvSine,InvModIndex);

#endif // (INCR_BUILD == 1)
//-----------------------------------------------------------------------------------------
#if (INCR_BUILD == 2) 	//Closed Current Loop Inverter with forced/internal sine angle
//-----------------------------------------------------------------------------------------
#if (GRID_CONNECT==1)
	// Run the SPLL and compute the inverter sine value
	spll2.u[0]=(long)inv_meas_vol_inst>>1;// shift from Q24 to Q23
	SPLL_1ph_SOGI_IQ_MACRO(spll2);

	InvSine=spll2.sin<<1;// shift from Q23 to Q24
#else
	// Run the ramp ctl to generate the forced sine angle for open loop test of the inverter
	RAMPGEN_IQ_MACRO(rgen1);

	// Use the angle value to compute the sine value
	InvSine = _IQsinPU(rgen1.Out);
#endif

	if((InvSine_prev<=_IQ24(0.00))&&(InvSine>_IQ24(0.00)))
	ZCDDetect=1;
	else
	ZCDDetect=0;

	if (ClearInvTrip==1 && ZCDDetect==1)
	{
		EALLOW;
		EPwm1Regs.TZCLR.bit.OST=0x1;
		EPwm2Regs.TZCLR.bit.OST=0x1;
		EDIS;
		ClearInvTrip=0;
		CloseIloopInv=1;
	}

	inv_ref_cur_inst = _IQ24mpy(inv_Iset, InvSine);

	if(CloseIloopInv==1)
	{
		cntl3p3z_InvI_vars.Ref=inv_ref_cur_inst;
		cntl3p3z_InvI_vars.Fdbk=inv_meas_cur_inst;
		CNTL_3P3Z_IQ_ASM(&cntl3p3z_InvI_coeff,&cntl3p3z_InvI_vars);
		duty_inv_pu=_IQ24div((cntl3p3z_InvI_vars.Out+inv_meas_vol_inst),vbus_meas_inst);

		duty_inv_pu= (duty_inv_pu>_IQ24(1.0))?_IQ24(1.0):duty_inv_pu;
		duty_inv_pu= (duty_inv_pu<_IQ24(-1.0))?_IQ24(-1.0):duty_inv_pu;
	}
	else
	{
		duty_inv_pu=0;
	}

#endif

//-----------------------------------------------------------------------------------------
#if (INCR_BUILD == 3 ) //Grid Connected Test
//-----------------------------------------------------------------------------------------

#if (GRID_CONNECT==1)
	// Run the SPLL and compute the inverter sine value
	spll2.u[0]=(long)inv_meas_vol_inst>>1;// shift from Q24 to Q23
	SPLL_1ph_SOGI_IQ_MACRO(spll2);

	InvSine=spll2.sin<<1;// shift from Q23 to Q24
#else
	// Run the ramp ctl to generate the forced sine angle for open loop test of the inverter
	RAMPGEN_IQ_MACRO(rgen1);

	// Use the angle value to compute the sine value
	InvSine = _IQsinPU(rgen1.Out);
#endif

	if((InvSine_prev<=_IQ24(0.00))&&(InvSine>_IQ24(0.00)))
	{
		ZCDDetect=1;

		if(MPPT_slew==0)
		{
			if(MPPT_ENABLE==1)
			{
				Run_MPPT=1;
			}
			MPPT_slew=10;
		}
		else
		MPPT_slew--;
	}
	else
	{
		ZCDDetect=0;
	}

	if((InvSine_prev<=RlyConnectVal)&&(InvSine>RlyConnectVal))
	{
		if(RlyConnect==1)
		{
			RlyConnect=0;
			GpioDataRegs.GPASET.bit.GPIO22=1;
		}
	}
	InvSine_prev=InvSine;

	if ( ClearInvTrip==1 && ZCDDetect==1 )
	{
		EALLOW;
		EPwm1Regs.TZCLR.bit.OST=0x1;
		EPwm2Regs.TZCLR.bit.OST=0x1;
		EDIS;
		ClearInvTrip=0;
		CloseIloopInv=1;
	}

	if(CloseIloopInv==1)
	{
		cntlPI_BusInv.Ref   =Bus_Volt_notch.Out;
		cntlPI_BusInv.Fbk	=inv_bus_ref;
		CNTL_PI_IQ_MACRO(cntlPI_BusInv)
		inv_Iset=cntlPI_BusInv.Out;

		inv_ref_cur_inst = _IQ24mpy(inv_Iset, InvSine);
		cntl3p3z_InvI_vars.Ref=inv_ref_cur_inst;
		cntl3p3z_InvI_vars.Fdbk=inv_meas_cur_inst;
		CNTL_3P3Z_IQ_ASM(&cntl3p3z_InvI_coeff,&cntl3p3z_InvI_vars);
		duty_inv_pu=_IQ24div((cntl3p3z_InvI_vars.Out+inv_meas_vol_inst),vbus_meas_inst);
		duty_inv_pu= (duty_inv_pu>_IQ24(1.0))?_IQ24(1.0):duty_inv_pu;
		duty_inv_pu= (duty_inv_pu<_IQ24(-1.0))?_IQ24(-1.0):duty_inv_pu;
	}
#endif // (INCR_BUILD == 3)
//--------------------------------------------------------------------------------
// PWM Driver for the inverter
//--------------------------------------------------------------------------------
	duty_inv = _IQ24mpy((long)(INV_PWM_PERIOD),_IQ24abs(duty_inv_pu));

	if (duty_inv < DontSwitchZeroLimit) {
		if (duty_inv_pu > 0) {
			EPwm1Regs.CMPA.half.CMPA = 0;
			EPwm1Regs.CMPB = 0;
			EPwm2Regs.CMPA.half.CMPA = INV_PWM_PERIOD;
		} else {
			EPwm1Regs.CMPB = 0;
			EPwm1Regs.CMPA.half.CMPA = 0;
			EPwm2Regs.CMPA.half.CMPA = 0;
		}
	} else {
		if (duty_inv_pu > 0) {
			EPwm1Regs.CMPA.half.CMPA = duty_inv;
			EPwm1Regs.CMPB = 0;
			EPwm2Regs.CMPA.half.CMPA = EPwm2Regs.TBPRD;

		} else {
			EPwm1Regs.CMPA.half.CMPA = 0;
			EPwm1Regs.CMPB = duty_inv;
			EPwm2Regs.CMPA.half.CMPA = 0;

		}
	}


/*************************************************/
/************  fly back Code **********************/
/*************************************************/
//TODO Fly Back ISR
//-------------------------------------------------------------------
// PV Current and Voltage
//-------------------------------------------------------------------
	pv_meas_cur_inst = _IQsat((((long)IPV_FB<<12)- PV_SenseCurr_Offset),_IQ24(1.0),_IQ24(0.0));
	//pv_meas_cur_inst=_IQsat((((long)IPV_FB<<12)- ((long)V0_5_REF<<12)),_IQ24(1.0),_IQ24(0.0)); // use this when using CT
	pv_meas_vol_inst = _IQsat((((long)VPV_FB<<12)-PV_SenseVolt_Offset),_IQ24(1.0),_IQ24(0.0));
	pv_meas_cur_inst=(pv_meas_cur_inst>0)?pv_meas_cur_inst:0;

//-----------------------------------------------------------------------------------------
#if (INCR_BUILD == 1 ) // Open Loop Check
//-----------------------------------------------------------------------------------------
	// flyback duty value

#endif // (INCR_BUILD == 1)

//-----------------------------------------------------------------------------------------
#if (INCR_BUILD == 2) 	//Closed Current Loop Flyback
//-----------------------------------------------------------------------------------------
	cntl2p2z_DCDCI_vars.Ref=pv_ref_cur_inst;
	cntl2p2z_DCDCI_vars.Fdbk=pv_meas_cur_inst;
	CNTL_2P2Z_IQ_ASM(&cntl2p2z_DCDCI_coeff,&cntl2p2z_DCDCI_vars);
	duty_flyback_pu=cntl2p2z_DCDCI_vars.Out;

#endif // (INCR_BUILD == 2)
//-----------------------------------------------------------------------------------------
#if (INCR_BUILD == 3) 	//Closed Current Loop Fly back
//-----------------------------------------------------------------------------------------

	if(CloseFlybackLoop==1)
	{
		cntl2p2z_DCDCI_vars.Ref=pv_ref_cur_inst; //cntl2p2z_DCDCV_vars.Out;
		cntl2p2z_DCDCI_vars.Fdbk=pv_meas_cur_inst;
		CNTL_2P2Z_IQ_ASM(&cntl2p2z_DCDCI_coeff,&cntl2p2z_DCDCI_vars);
		// fly back duty value
		duty_flyback_pu=cntl2p2z_DCDCI_vars.Out;
	}

#endif // (INCR_BUILD == 2)

//--------------------------------------------------------------------------------
// PWM Driver for fly back DC-DC
//--------------------------------------------------------------------------------

	duty_flyback =(_IQ22mpy((int32)(FLYBACK_PWM_PERIOD)<<22,(int32)duty_flyback_pu>>2))>> 6;

	if (duty_flyback > _IQ16(25))
		EPwm3Regs.CMPA.all = duty_flyback;
	else
		EPwm3Regs.CMPA.all = 0;

//--------------------------------------------------------------------------------
// Moving Average for MPPT and Notch Filters
//--------------------------------------------------------------------------------
	Bus_Volt_notch.In=vbus_meas_inst;
	NOTCH_FLTR_IQ_ASM(&Bus_Volt_notch,&notch_TwiceGridFreq);

	PV_volt_notch.In=pv_meas_vol_inst;
	NOTCH_FLTR_IQ_ASM(&PV_volt_notch,&notch_TwiceGridFreq);

	PV_cur_notch.In=pv_meas_cur_inst;
	NOTCH_FLTR_IQ_ASM(&PV_cur_notch,&notch_TwiceGridFreq);

	MATH_EMAVG2_IQ_MACRO(Bus_Volt_notch.Out, vbus_meas_avg, _IQ(0.0005));
	MATH_EMAVG2_IQ_MACRO(PV_cur_notch.Out, pv_meas_cur_avg, _IQ(0.0005));
	pv_meas_cur_avg=(pv_meas_cur_avg>0)?pv_meas_cur_avg:0;
	MATH_EMAVG2_IQ_MACRO(PV_volt_notch.Out, pv_meas_vol_avg, _IQ(0.0005));
	pv_meas_vol_avg=(pv_meas_vol_avg>0)?pv_meas_vol_avg:0;

// ------------------------------------------------------------------------------
//    Connect inputs of the Datalogger module
// ------------------------------------------------------------------------------
#if INCR_BUILD==1
	// First two DBUFF check SPLL operations
	D_val1 = (int16)_IQtoIQ15(InvSine);
	D_val2 = (int16)_IQtoIQ15(spll2.sin<<1);
	// Next two check Vac and Iac measurement
	D_val3 = (int16)_IQtoIQ15(inv_meas_cur_inst);
	D_val4 = (int16)_IQtoIQ15(inv_meas_vol_inst);
	DLOG_4CH_IQ_MACRO(dlog1);
#endif

#if INCR_BUILD==2
#if GRID_CONNECT==1
	D_val1 = (int16)_IQtoIQ15(inv_meas_vol_inst);
	D_val2 = (int16)_IQtoIQ15(InvSine);
#else
	D_val1 = (int16)_IQtoIQ15(InvSine);
	D_val2 = (int16)_IQtoIQ15(inv_meas_vol_inst);
#endif
	D_val3 = (int16)_IQtoIQ15(inv_meas_cur_inst);
	D_val4 = (int16)_IQtoIQ15(inv_ref_cur_inst);
	DLOG_4CH_IQ_MACRO(dlog1);
#endif

//-------------------------------------------------------------------
//	Acknowledge interrupt
//-------------------------------------------------------------------
	PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;	// Must acknowledge the PIE group
	AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;		// Clear ADCINT1 flag
//-------------------------------------------------------------------

	return;

}



// One KHz ISR
interrupt void OneKhzISR() {

	// Let the inv_ISR interrupt this routine
	EINT;

	//TODO State Machine
#if (INCR_BUILD == 3)
	// Inverter State ==0 , Idle state, wait for the inverter start command
	// Inverter State ==1 , Check if grid is present
	// Inverter State ==2 , Check if sufficient panel voltage is available
	// Inverter State ==3 , Check if dc bus is enough to feed power into the grid
	// Inverter State ==4 , wait for stop command, Check if dc bus goes into under volatage condition
	// Inverter State ==5 , if stop, trip all PWM's, shut down MPPT and return to state 0, reset all values
	switch(PVInverterState)
	{
		case Idle:
			// Wait for the command to start the inverter
		    if(Gui_InvStart==1)
		    {
		    	PVInverterState=CheckGrid;
		    	Gui_InvStart=0;
		    }
		    break;
		case CheckGrid:
			// once the inverter command is issued check if the grid is present
			// once identified re -initailize the VRMS and FREQ limit for that grid range
			// also modify the PLL coefficients for the grid frequency
			#if(GRID_CONNECT==1)
			if(OV_Flag==0&&UV_Flag==0&&UF_Flag==0&&OF_Flag==0)
			{
				if(_IQ4abs((ACFreq-_IQ4(50.0)))<_IQ4(GRID_OVER_UNDER_FREQ_LIMIT))
				{
					PVInverterState=CheckPV;
					Grid_Freq=50;
					GRID_MIN_FREQ=Grid_Freq-GRID_OVER_UNDER_FREQ_LIMIT;
					GRID_MAX_FREQ=Grid_Freq+GRID_OVER_UNDER_FREQ_LIMIT;
					GRID_MIN_VRMS=220-GRID_OVER_UNDER_VRMS_LIMIT;
					GRID_MAX_VRMS=220+GRID_OVER_UNDER_VRMS_LIMIT;

					// SPLL 1ph Notch Filter Method intialization
					SPLL_1ph_IQ_init(Grid_Freq,_IQ21((float)(1.0/ISR_FREQUENCY)),&spll1);

					spll1.lpf_coeff.B0_lf=B0_LPF;
					spll1.lpf_coeff.B1_lf=B1_LPF;
					spll1.lpf_coeff.A1_lf=A1_LPF;

					c1=0.1;
					c2=0.00001;

					SPLL_1ph_IQ_notch_coeff_update(((float)(1.0/ISR_FREQUENCY)), (float)(2*PI*Grid_Freq*2),(float)c2,(float)c1, &spll1);

					NOTCH_FLTR_IQ_COEFF_Update(((float)(1.0/ISR_FREQUENCY)), (float)(2*PI*Grid_Freq*2),(float)c2,(float)c1, &notch_TwiceGridFreq);

					//SPLL 1ph SOGI Method initialization

					SPLL_1ph_SOGI_IQ_init(Grid_Freq,_IQ23((float)(1.0/ISR_FREQUENCY)),&spll2);
					spll2.lpf_coeff.B0_lf=_IQ23(166.877556);
					spll2.lpf_coeff.B1_lf=_IQ23(-166.322444);
					spll2.lpf_coeff.A1_lf=_IQ23(-1.0);
					SPLL_1ph_SOGI_IQ_coeff_update(((float)(1.0/ISR_FREQUENCY)),(float)(2*PI*Grid_Freq),&spll2);

					inv_bus_ref=DC_BUS_REF_50HZ;
					inv_bus_rly_connect= DC_BUS_RELAY_CONNECT_VOLT_50HZ;
					inv_bus_start_volt=DC_BUS_INV_START_VOLT_50HZ;
					inv_bus_UV=DC_BUS_UNDERVOLTAGE_LIMIT_50HZ;
					inv_bus_OV=DC_BUS_OVERVOLTAGE_LIMIT_50HZ;
					cntlPI_BusInv.Umin =_IQ(0.015);
					SlewClrInvTrip=10;
				}
				else if(_IQ4abs((ACFreq-_IQ4(60.0)))<_IQ4(GRID_OVER_UNDER_FREQ_LIMIT))
				{
					PVInverterState=CheckPV;
					Grid_Freq=60;
					GRID_MIN_FREQ=Grid_Freq-GRID_OVER_UNDER_FREQ_LIMIT;
					GRID_MAX_FREQ=Grid_Freq+GRID_OVER_UNDER_FREQ_LIMIT;
					GRID_MIN_VRMS=110-GRID_OVER_UNDER_VRMS_LIMIT;
					GRID_MAX_VRMS=110+GRID_OVER_UNDER_VRMS_LIMIT;
					// SPLL 1ph Notch Filter Method intialization
					SPLL_1ph_IQ_init(Grid_Freq,_IQ21((float)(1.0/ISR_FREQUENCY)),&spll1);

					spll1.lpf_coeff.B0_lf=B0_LPF;
					spll1.lpf_coeff.B1_lf=B1_LPF;
					spll1.lpf_coeff.A1_lf=A1_LPF;

					c1=0.1;
					c2=0.00001;

					SPLL_1ph_IQ_notch_coeff_update(((float)(1.0/ISR_FREQUENCY)), (float)(2*PI*Grid_Freq*2),(float)c2,(float)c1, &spll1);
					NOTCH_FLTR_IQ_COEFF_Update(((float)(1.0/ISR_FREQUENCY)), (float)(2*PI*Grid_Freq*2),(float)c2,(float)c1, &notch_TwiceGridFreq);

					//SPLL 1ph SOGI Method initialization

					SPLL_1ph_SOGI_IQ_init(Grid_Freq,_IQ23((float)(1.0/ISR_FREQUENCY)),&spll2);
					spll2.lpf_coeff.B0_lf=_IQ23(166.877556);
					spll2.lpf_coeff.B1_lf=_IQ23(-166.322444);
					spll2.lpf_coeff.A1_lf=_IQ23(-1.0);
					SPLL_1ph_SOGI_IQ_coeff_update(((float)(1.0/ISR_FREQUENCY)),(float)(2*PI*Grid_Freq),&spll2);

					inv_bus_ref=DC_BUS_REF_60HZ;
					inv_bus_rly_connect= DC_BUS_RELAY_CONNECT_VOLT_60HZ;
					inv_bus_start_volt=DC_BUS_INV_START_VOLT_60HZ;
					inv_bus_UV=DC_BUS_UNDERVOLTAGE_LIMIT_60HZ;
					inv_bus_OV=DC_BUS_OVERVOLTAGE_LIMIT_60HZ;
					cntlPI_BusInv.Umin =_IQ(0.025);
					SlewClrInvTrip=10;
				}
			}
		    #else
			PVInverterState=CheckPV;
			#endif
			if(Gui_InvStop==1)
			{
				PVInverterState=Idle;
				Gui_InvStop=0;
			}
			break;
		case CheckPV:
			// AC is present, check if PV is present
			if(Gui_InvStop==1)
			{
				PVInverterState=ResetState1; // go to the re-initalization state, this logs any fault conditions as well
				Gui_InvStop=0;
			}
			if(Gui_Vpv>VPV_MIN)
			{
				// sufficient PV voltage is present
				// Clear Fly Back Trip and monitor DC BUs
				PVInverterState=MonitorDCBus;
				EALLOW;
				EPwm3Regs.TZCLR.bit.OST=0x1;
				CloseFlybackLoop=1;
				EDIS;
				pv_ref_cur_inst=_IQ24(0.1);
				pv_ref_cur_fixed=_IQ24(0.15);
			}
		break;
		case MonitorDCBus:
			// Flyback is pumping current into the DC Bus
			// Monitor the DC Bus Value
			#if(GRID_CONNECT==1)
			if(UV_Flag==1||OV_Flag==1) //UF_Flag==1||||OF_Flag==1
			{
				Gui_InvStop=1;
			}
			#endif
			if(vbus_meas_inst>inv_bus_OV) // Check for Over Voltage Condition
			{
				BusOverVoltageTrip=1;
				Gui_InvStop=1;
			}
			if(Gui_InvStop==1)
			{
				PVInverterState=ResetState1; // go to the re-initalization state
				Gui_InvStop=0;
			}
			if(vbus_meas_inst>inv_bus_rly_connect)
			{
				RlyConnect=1;
			}

			// Check if DC Bus is greater than DC_BUS_INV_START_VOLT
			// Also Check if the Relay has been connected
			// As currently the inverter is off this will happen quickly
			if(vbus_meas_inst>inv_bus_start_volt && GpioDataRegs.GPADAT.bit.GPIO22==1)
			{
				SlewClrInvTrip--;
				if(SlewClrInvTrip==0)
				{
					PVInverterState=EnableMPPT;
					// Take inverter out of reset
					ClearInvTrip=1;
				}
			}
			SlewState4=250;
			break;
		case EnableMPPT:
			// Wait Before enabling MPPT
			SlewState4--;
			if(SlewState4==0)
			{
				PVInverterState=PVInverterActive;
				//Enable MPPT
				MPPT_ENABLE=1;
				mppt_incc_I1.mppt_first=1;
				mppt_incc_I1.mppt_enable=1;
			}
			// check for under voltage
			if(vbus_meas_inst<inv_bus_UV)
			{
				BusUnderVoltageTrip=1;
				Gui_InvStop=1;
			}
			// Check for Over Voltage Condition
			if(vbus_meas_inst>inv_bus_OV)
			{
				BusOverVoltageTrip=1;
				Gui_InvStop=1;
			}
			#if(GRID_CONNECT==1)
			if(UV_Flag==1||OV_Flag==1) //UF_Flag==1||||OF_Flag==1
			{
				Gui_InvStop=1;
			}
			#endif
			if(Gui_InvStop==1)
			{
				PVInverterState=ResetState1; // go to the re-initalization state
				Gui_InvStop=0;
			}
			break;
		case PVInverterActive:
			//Inverter is Fully Active Now
			// Check for Faults or Stop Command
			#if(GRID_CONNECT==1)
			if(UV_Flag==1||OV_Flag==1) //||OF_Flag==1UF_Flag==1||
			{
				Gui_InvStop=1;
			}
			#endif
			// check for under voltage
			if(vbus_meas_inst<inv_bus_UV)
			{
				BusUnderVoltageTrip=1;
				Gui_InvStop=1;
			}
			// Check for Over Voltage Condition
			if(vbus_meas_inst>inv_bus_OV)
			{
				BusOverVoltageTrip=1;
				Gui_InvStop=1;
			}
			if(Gui_InvStop==1)
			{
				PVInverterState=ResetState1; // go to the re-initalization state
				Gui_InvStop=0;
			}
			break;
		case ResetState1:
			#if(GRID_CONNECT==1)
			/*if(UF_Flag==1)
			 {
			 FaultFlag=1;
			 Gui_InvStop=1;
			 }
			 else if (OF_Flag==1)
			 {
			 FaultFlag=2;
			 Gui_InvStop=1;
			 }
			 */
			if(UV_Flag==1)
			{
				FaultFlag=UnderVoltageGrid;
			}
			else if(OV_Flag==1)
			{
				FaultFlag=OverVoltageGrid;
			}
			else if(BusUnderVoltageTrip==1)
			{
				FaultFlag=UnderVoltageDCBus;
			}
			else if(BusOverVoltageTrip==1)
			{
				FaultFlag=OverVoltageDCBus;
			}
			#endif
			// Run the reset sequence
			// Fist disable MPPT and set the ref current command to zero
			// This is done to make sure the flyback does not see <10% duty when tripping
			MPPT_ENABLE=0;
			mppt_incc_I1.mppt_first=1;
			mppt_incc_I1.mppt_enable=0;
			pv_ref_cur_inst=_IQ24(0.0);
			// zero the buffer values, this makes sure the DC-DC Flyback stage shuts down fast
			//DINT;
			//	CNTL_2P2Z_IQ_C_VAR_INIT(cntl2p2z_DCDCI_vars);
			//EINT;
			duty_flyback=0;
			duty_flyback_pu=0;
			CloseFlybackLoop=0;
			PVInverterState=ResetState2;
			break;
		case ResetState2:
			//Disconnect relay
			GpioDataRegs.GPACLEAR.bit.GPIO22=1;
			// by now the CMPA value should be zero
			if(EPwm3Regs.CMPA.half.CMPA==0)
			{
				// Trip the PWM for the inverter
				// software force the trip of inverter and flyback
				EALLOW;
				EPwm1Regs.TZFRC.bit.OST=0x1;
				EPwm2Regs.TZFRC.bit.OST=0x1;
				EPwm3Regs.TZFRC.bit.OST=0x1;
				EPwm1Regs.CMPA.half.CMPA=0;
				EPwm1Regs.CMPB=0;
				EPwm2Regs.CMPA.half.CMPA=0;
				EPwm3Regs.CMPA.half.CMPA=0;
				EDIS;
				duty_inv_pu=0;
				duty_inv=0;
				inv_Iset=0;
				CloseIloopInv=0;
				#if (GRID_CONNECT==1)
					if(FaultFlag==0)
						PVInverterState=Idle;
					else
						PVInverterState=FaultState;
				#else
					PVInverterState=Idle;
				#endif
				CNTL_2P2Z_IQ_VARS_init(&cntl2p2z_DCDCI_vars);
				CNTL_3P3Z_IQ_VARS_init(&cntl3p3z_InvI_vars);
				cntlPI_BusInv.up=0;
				cntlPI_BusInv.ui=0;
				cntlPI_BusInv.v1=0;
				cntlPI_BusInv.i1=0;
				cntlPI_BusInv.up=0;
				cntlPI_BusInv.w1=0;
			}
		break;
		default:
		break;
	}
#endif

	//TODO AC Measurements
	//---------------------------------------------------------------------
	// Grid Frequency Measurements
	//---------------------------------------------------------------------
	ACFreq_SysTicks = (ECap1Regs.CAP1 + ECap1Regs.CAP2 + ECap1Regs.CAP3
			+ ECap1Regs.CAP4) << 3;
	ACFreq = _IQ4div(_IQ4(CPU_FREQ), ACFreq_SysTicks);

	if (ECap1Regs.TSCTR > ECAP_TimerMaxVal
			|| (ECap1Regs.CAP1 > ECAP_TimerMaxVal)
			|| (ECap1Regs.CAP2 > ECAP_TimerMaxVal)
			|| (ECap1Regs.CAP3 > ECAP_TimerMaxVal)) {
		ACFreq_SysTicks = 0;
		ACFreq = 0;
	}

	if (ACFreq < _IQ4(GRID_MIN_FREQ))
		UF_Flag = 1;
	else
		UF_Flag = 0;

	if (ACFreq > _IQ4(GRID_MAX_FREQ))
		OF_Flag = 1;
	else
		OF_Flag = 0;

	MATH_EMAVG2_IQ_MACRO((_IQ24abs(inv_meas_vol_inst)), inv_emavg_vol,
			_IQ24(0.0003));
	Gui_Vavg = _IQ16mpy((int32)inv_emavg_vol>>8,_IQ16(AC_PEAK_SENSE));

	if (Gui_Vavg < _IQ16(GRID_MIN_VRMS))
		UV_Flag = 1;
	else
		UV_Flag = 0;

	if (Gui_Vavg > _IQ16(GRID_MAX_VRMS))
		OV_Flag = 1;
	else
		OV_Flag = 0;

	if (UF_Flag == 0 && Gui_Vavg > _IQ16(40.0)) {
		//Calculate RMS input voltage and input frequency
		sine_mains.Iin = inv_meas_cur_inst >> 9;
		sine_mains.Vin = inv_meas_vol_inst >> 9;
		SINEANALYZER_DIFF_wPWR_IQ_MACRO(sine_mains);

		VRMS = (sine_mains.Vrms) << 9;//    Convert sine_mainsV.Vrms from Q15 to Q24 and save as VrectRMS
		IRMS = (sine_mains.Irms) << 9;//    Convert sine_mainsV.Irms from Q15 to Q24 and save as IrectRMS
		PRMS = (sine_mains.Prms) << 9;//    Convert sine_mainsV.Prms from Q15 to Q24 and save as PinRMS

		Gui_Prms = (sine_mains.Prms * K_Prms) >> 15;
		Gui_Irms = (sine_mains.Irms * K_Irms) >> 15;
		Gui_Vrms = (sine_mains.Vrms * K_Vrms) >> 15;

		/*if(Gui_Vrms<_IQ6(GRID_MIN_VRMS))
		 UV_Flag=1;
		 else
		 UV_Flag=0;

		 if(Gui_Vrms>_IQ6(GRID_MAX_VRMS))
		 OV_Flag=1;
		 else
		 OV_Flag=0;
		 */
	} else {
		VRMS = 0;//    Convert sine_mainsV.Vrms from Q15 to Q24 and save as VrectRMS
		IRMS = 0;//    Convert sine_mainsV.Irms from Q15 to Q24 and save as IrectRMS
		PRMS = 0;//    Convert sine_mainsV.Prms from Q15 to Q24 and save as PinRMS

		Gui_Prms = 0;
		Gui_Irms = 0;
		Gui_Vrms = 0;

		SINEANALYZER_DIFF_wPWR_IQ_init(&sine_mains);
		sine_mains.Vin = 0;
		sine_mains.Iin = 0;
		sine_mains.SampleFreq = _IQ15(1000.0);
		sine_mains.Threshold = _IQ15(0.1);
		sine_mains.nsamplesMax=1000/UNIVERSAL_GRID_MIN_FREQ;
		sine_mains.nsamplesMin=1000/UNIVERSAL_GRID_MAX_FREQ;

	}

	Gui_Vpv = _IQ20mpy(pv_meas_vol_avg>>4,_IQ20(PV_VOL_SENSE_MAX));
	Gui_Ipv = _IQ20mpy(pv_meas_cur_avg>>4,_IQ20(PV_CURR_SENSE_MAX));
	Gui_Vbus = _IQ20mpy(vbus_meas_avg>>4,_IQ20(VBUS_VOL_SENSE_MAX));

	//Freq_Vin = sine_mainsV.SigFreq;// Q15
	//VrmsReal = _IQ15mpy (KvInv, sine_mainsV.Vrms);

	//Gui_PinRMS = (sine_mainsV.Prms*K_Prms) >> 15;//Q15*Q15 >> 15 = Q15, When no calibration is used

//	if((sine_mainsV.Prms>123)&&(sine_mainsV.Prms <= 858)){	//Max Power used for normalization is 19.8*405.2=8022.96W.//
//										//So 210W = 210/8022.96 *32767 = 858 in Q15 format//
//										// 30W = 30/8022.96 *32767 = 123 in Q15 format//
//			Gui_PinRMS = (((sine_mainsV.Prms*slope_Pcorr) >> 15)- offset_Pcorr);//Q15*Q15 >> 15 = Q15,
//			//apply calibration between 30W and 210W
//		}
//		else{
//			Gui_PinRMS = (sine_mainsV.Prms*K_Prms) >> 15;//Q15*Q15 >> 15 = Q15, apply zero calibration
//		}
//
//
//	Gui_PinRMS_16 = (int16)(Gui_PinRMS);





	//TODO MPPT Task
#if INCR_BUILD==2
	if(MPPT_ENABLE==1)
	{
		if(MPPT_slew==0)
		{
			Run_MPPT=1;
			MPPT_slew=100;
		}
		else
		MPPT_slew--;
	}
#endif
	if (Run_MPPT == 1) {
		Run_MPPT = 0;

		// MPPT routine
		mppt_incc_I1.Ipv =pv_meas_cur_avg; //IpvRead;
		mppt_incc_I1.Vpv =pv_meas_vol_avg; //VpvRead;

		MPPT_INCC_I_IQ_MACRO(mppt_incc_I1);

		pv_ref_cur_mppt = mppt_incc_I1.ImppOut;

#if(MPPT==1)
		if(Gui_MPPTEnable==1)
			pv_ref_cur_inst=pv_ref_cur_mppt;
		else
			pv_ref_cur_inst=pv_ref_cur_fixed;
#else
		pv_ref_cur_inst = pv_ref_cur_fixed;
#endif

	}

	if (EPwm1Regs.TZFLG.bit.OST == 1 && RlyConnect == 1
			&& PVInverterState >= 4) {
		OverCurrent = 1;
	} else if (EPwm1Regs.TZFLG.bit.OST == 0) {
		OverCurrent = 0;
	}

}

/**********************************************************/
/********************** ECAP INIT *************************/
/**********************************************************/
void InitECapture() {

	ECap1Regs.ECEINT.all = 0x0000;             // Disable all capture interrupts
	ECap1Regs.ECCLR.all = 0xFFFF;              // Clear all CAP interrupt flags
	ECap1Regs.ECCTL1.bit.CAPLDEN = 0;        // Disable CAP1-CAP4 register loads
	ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0;      // Make sure the counter is stopped

	// Configure peripheral registers
	ECap1Regs.ECCTL2.bit.CONT_ONESHT = 0;      // Operation in Continuous Mode
	ECap1Regs.ECCTL2.bit.STOP_WRAP = 3;        // Wrap after 4 events
	ECap1Regs.ECCTL1.bit.CAP1POL = 1;          // Falling edge
	ECap1Regs.ECCTL1.bit.CAP2POL = 0;          // Rising edge
	ECap1Regs.ECCTL1.bit.CAP3POL = 1;          // Falling edge
	ECap1Regs.ECCTL1.bit.CAP4POL = 0;          // Rising edge
	ECap1Regs.ECCTL1.bit.CTRRST1 = 1;          // Difference operation
	ECap1Regs.ECCTL1.bit.CTRRST2 = 1;          // Difference operation
	ECap1Regs.ECCTL1.bit.CTRRST3 = 1;          // Difference operation
	ECap1Regs.ECCTL1.bit.CTRRST4 = 1;          // Difference operation
	ECap1Regs.ECCTL2.bit.SYNCI_EN = 0;         // Enable sync in
	ECap1Regs.ECCTL2.bit.SYNCO_SEL = 0;        // Pass through
	ECap1Regs.ECCTL1.bit.CAPLDEN = 1;          // Enable capture units

	ECap1Regs.ECCTL2.bit.TSCTRSTOP = 1;        // Start Counter
	//ECap1Regs.ECCTL2.bit.REARM = 1;            // arm one-shot
	ECap1Regs.ECCTL1.bit.CAPLDEN = 1;         // Enable CAP1-CAP4 register loads
	// ECap1Regs.ECEINT.bit.CEVT4 = 1;            // 4 events = interrupt

}



  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我们将就此向您回复。

    Shamim

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Chris、

    我认为这里的措辞有点令人困惑。  "程序"部分中的所有步骤已在代码中执行。  目的是指出每个构建步骤中涉及的一些关键功能、以控制系统。

    对于构建级别1、请注意:

    -2 ISR:

      Inv_ISR()以50kHz 的频率运行,是逆变器的主 ISR

      OneKhzISR()是1kHz ISR,负责网格检测和后台任务

    如果您在 main.c 中搜索上述内容、您将看到它们的声明位置、它们所连接的饼图中断(即触发它们运行的原因)以及 main.c 底部的 ISR 函数

    偏移校正例程位于第761行、再次供您按照自己的认为合适的方式进行检查。

    您只需确保.h 文件中的构建设置符合建议并进行编译和加载/运行即可。   

    最棒的

    Matthew