This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28027F:闪存编程不能与 XDS110调试探针一起使用

Guru**** 2931100 points

Other Parts Discussed in Thread: TMS320F28027, LAUNCHXL-F28027F

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1004147/tms320f28027f-flash-programming-not-working-with-xds110-debug-probe

器件型号:TMS320F28027F
主题中讨论的其他器件:TMS320F28027LAUNCHXL-F28027F

我无法使用 XDS 110调试探针将代码"刷写"到 PCB 上的微控制器(TMS320F28027)。 PCB 上的微控制器已成功编程为 RAM 配置。 我已进行了必要的更改(更改.cmd 文件)。

在使用 XDS 100V2调试探针的 Launchpad (Launchxl-f28027F)上使用时、相同的代码在"闪存"模式下工作。  

我已包含必要的.cmd 文件。

我包括以下行:

memcpy (&RamfuncsRunStart、&RamfuncsLoadStart、(size_t)&RamfuncsLoadSize);
InitFlash();

编译设置设置设置为:

以下是 PCB 上电路板的调试连接原理图:

代码是  对'Example_2802xEPwmDeadBand'的简单修改。

//###########################################################################
//
// FILE:    Example_2802xEpwmDeadBand.c
//
// TITLE:   Check PWM deadband generation
//
// ASSUMPTIONS:
//
//    This program requires the f2802x header files.
//
//    Monitor ePWM1 - ePWM3 on an Oscilloscope as described
//    below.
//
//       EPWM1A is on GPIO0
//       EPWM1B is on GPIO1
//
//       EPWM2A is on GPIO2
//       EPWM2B is on GPIO3
//
//       EPWM3A is on GPIO4
//       EPWM3B is on GPIO5
//
//    As supplied, this project is configured for "boot to SARAM"
//    operation.  The 2802x Boot Mode table is shown below.
//    For information on configuring the boot mode of an eZdsp,
//    please refer to the documentation included with the eZdsp,
//
//    $Boot_Table
//    While an emulator is connected to your device, the TRSTn pin = 1,
//    which sets the device into EMU_BOOT boot mode. In this mode, the
//    peripheral boot modes are as follows:
//
//      Boot Mode:   EMU_KEY        EMU_BMODE
//                   (0xD00)	     (0xD01)
//      ---------------------------------------
//      Wait		 !=0x55AA        X
//      I/O		     0x55AA	         0x0000
//      SCI		     0x55AA	         0x0001
//      Wait 	     0x55AA	         0x0002
//      Get_Mode	 0x55AA	         0x0003
//      SPI		     0x55AA	         0x0004
//      I2C		     0x55AA	         0x0005
//      OTP		     0x55AA	         0x0006
//      Wait		 0x55AA	         0x0007
//      Wait		 0x55AA	         0x0008
//      SARAM		 0x55AA	         0x000A	  <-- "Boot to SARAM"
//      Flash		 0x55AA	         0x000B
//	    Wait		 0x55AA          Other
//
//   Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger
//   according to the Boot Mode Table above. Build/Load project,
//   Reset the device, and Run example
//
//   $End_Boot_Table
//
//
//
// DESCRIPTION:
//
//    This example configures ePWM1, ePWM2 and ePWM3 for:
//    - Count up/down
//    - Deadband
//
//    3 Examples are included:
//    * ePWM1: Active low PWMs
//    * ePWM2: Active low complementary PWMs
//    * ePWM3: Active high complementary PWMs
//
//    Each ePWM is configured to interrupt on the 3rd zero event
//    when this happens the deadband is modified such that
//    0 <= DB <= DB_MAX.  That is, the deadband will move up and
//    down between 0 and the maximum value.
//
//
//    View the EPWM1A/B, EPWM2A/B and EPWM3A/B waveforms
//    via an oscilloscope
//
//
//###########################################################################
// $TI Release: F2802x Support Library v230 $
// $Release Date: Fri May  8 07:43:05 CDT 2015 $
// $Copyright: Copyright (C) 2008-2015 Texas Instruments Incorporated -
//             http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

// Prototype statements for functions found within this file.
void InitEPwm1Example(void);
void InitEPwm2Example(void);
void InitEPwm3Example(void);
__interrupt void epwm1_isr(void);
__interrupt void epwm2_isr(void);
__interrupt void epwm3_isr(void);

// Global variables used in this example
uint32_t  EPwm1TimerIntCount;
uint32_t  EPwm2TimerIntCount;
uint32_t  EPwm3TimerIntCount;
uint16_t  EPwm1_DB_Direction;
uint16_t  EPwm2_DB_Direction;
uint16_t  EPwm3_DB_Direction;

// Maximum Dead Band values
#define EPWM1_MAX_DB   0x000A
#define EPWM2_MAX_DB   0x03FF
#define EPWM3_MAX_DB   0x000F

//#define    0
#define EPWM1_MIN_DB   0x000A
#define EPWM2_MIN_DB   0
#define EPWM3_MIN_DB   0x000F

// To keep track of which way the Dead Band is moving
#define DB_UP   1
#define DB_DOWN 0
#define phase 150
#define D 90

// The following pointer to a function call calibrates the ADC and internal oscillators

#define Device_cal (void   (*)(void))0x3D7C80
//#pragma CODE_SECTION(InitFlash, "ramfuncs");
//#pragma CODE_SECTION(&epwm1_isr, "ramfuncs");
//#pragma CODE_SECTION(&epwm2_isr, "ramfuncs");
//#pragma CODE_SECTION(&epwm3_isr, "ramfuncs");

/******************************************************************************/
// These are defined by the linker
extern uint16_t RamfuncsLoadStart;
extern uint16_t RamfuncsLoadSize;
extern uint16_t RamfuncsRunStart;

void main(void)
{
// WARNING: Always ensure you call memcpy before running any functions from RAM
// InitSysCtrl includes a call to a RAM based function and without a call to
// memcpy first, the processor will go "into the weeds"
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t) &RamfuncsLoadSize);
    InitFlash();
 //  #ifdef _FLASH
//	memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
  // #endif

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the f2802x_SysCtrl.c file.
   InitSysCtrl();

// Step 2. Initialize GPIO:
// This example function is found in the f2802x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();  // Skipped for this example

// For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
// These functions are in the f2802x_EPwm.c file
   InitEPwm1Gpio();
   InitEPwm2Gpio();
   InitEPwm3Gpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the f2802x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in f2802x_DefaultIsr.c.
// This function is found in f2802x_PieVect.c.
   InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
   EALLOW;  // This is needed to write to EALLOW protected registers
   PieVectTable.EPWM1_INT = &epwm1_isr;
   PieVectTable.EPWM2_INT = &epwm2_isr;
   PieVectTable.EPWM3_INT = &epwm3_isr;
   EDIS;    // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize all the Device Peripherals:
// Not required for this example

   EALLOW;
   SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
   EDIS;

   InitEPwm1Example();
   InitEPwm2Example();
   InitEPwm3Example();

   EALLOW;
   SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
   EDIS;

// Step 5. User specific code, enable interrupts
// Initialize counters:
   EPwm1TimerIntCount = 0;
   EPwm2TimerIntCount = 0;
   EPwm3TimerIntCount = 0;

// Enable CPU INT3 which is connected to EPWM1-3 INT:
   IER |= M_INT3;

// Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
   PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
   PieCtrlRegs.PIEIER3.bit.INTx2 = 1;
   PieCtrlRegs.PIEIER3.bit.INTx3 = 1;

// Enable global Interrupts and higher priority real-time debug events:
   EINT;   // Enable Global interrupt INTM
   ERTM;   // Enable Global realtime interrupt DBGM


// Step 6. IDLE loop. Just sit and loop forever (optional):
   for(;;)
   {
       __asm("          NOP");
   }
}

__interrupt void epwm1_isr(void)
{
   if(EPwm1_DB_Direction == DB_UP)
   {
       if(EPwm1Regs.DBFED < EPWM1_MAX_DB)
       {
          EPwm1Regs.DBFED++;
          EPwm1Regs.DBRED++;
       }
       else
       {
          EPwm1_DB_Direction = DB_DOWN;
          EPwm1Regs.DBFED--;
          EPwm1Regs.DBRED--;
       }
   }
   else
   {
       if(EPwm1Regs.DBFED == EPWM1_MIN_DB)
       {
          EPwm1_DB_Direction = DB_UP;
          EPwm1Regs.DBFED++;
          EPwm1Regs.DBRED++;
       }
       else
       {
          EPwm1Regs.DBFED--;
          EPwm1Regs.DBRED--;
       }
   }
   EPwm1TimerIntCount++;

   // Clear INT flag for this timer
   EPwm1Regs.ETCLR.bit.INT = 1;

   // Acknowledge this interrupt to receive more interrupts from group 3
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}

__interrupt void epwm2_isr(void)
{
   if(EPwm2_DB_Direction == DB_UP)
   {
       if(EPwm2Regs.DBFED < EPWM2_MAX_DB)
       {
          EPwm2Regs.DBFED++;
          EPwm2Regs.DBRED++;
       }
       else
       {
          EPwm2_DB_Direction = DB_DOWN;
          EPwm2Regs.DBFED--;
          EPwm2Regs.DBRED--;
       }
   }
   else
   {
       if(EPwm2Regs.DBFED == EPWM2_MIN_DB)
       {
          EPwm2_DB_Direction = DB_UP;
          EPwm2Regs.DBFED++;
          EPwm2Regs.DBRED++;
       }
       else
       {
          EPwm2Regs.DBFED--;
          EPwm2Regs.DBRED--;
       }
   }

   EPwm2TimerIntCount++;

   // Clear INT flag for this timer
   EPwm2Regs.ETCLR.bit.INT = 1;

   // Acknowledge this interrupt to receive more interrupts from group 3
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}

__interrupt void epwm3_isr(void)
{
   if(EPwm3_DB_Direction == DB_UP)
   {
       if(EPwm3Regs.DBFED < EPWM3_MAX_DB)
       {
          EPwm3Regs.DBFED++;
          EPwm3Regs.DBRED++;
       }
       else
       {
          EPwm3_DB_Direction = DB_DOWN;
          EPwm3Regs.DBFED--;
          EPwm3Regs.DBRED--;
       }
   }
   else
   {
       if(EPwm3Regs.DBFED == EPWM3_MIN_DB)
       {
          EPwm3_DB_Direction = DB_UP;
          EPwm3Regs.DBFED++;
          EPwm3Regs.DBRED++;
       }
       else
       {
          EPwm3Regs.DBFED--;
          EPwm3Regs.DBRED--;
       }
   }

   EPwm3TimerIntCount++;

   // Clear INT flag for this timer
   EPwm3Regs.ETCLR.bit.INT = 1;

   // Acknowledge this interrupt to receive more interrupts from group 3
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}

void InitEPwm1Example()
{
   EPwm1Regs.TBPRD = 200;                        // Set timer period 300 IS 100KHZ
   EPwm1Regs.TBPHS.half.TBPHS = 0x0000;           //  is 0
   EPwm1Regs.TBCTR = 0x0000;                      // Clear counter

   // Setup TBCLK
   EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
   EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;        // Disable  loading
   EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;       // Clock ratio to SYSCLKOUT
   EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
   EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;

   EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;    // Load registers every ZERO
   EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
   EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
   EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

   // Setup compare
   EPwm1Regs.CMPA.half.CMPA = 100; //CHANGE DUTY

   // Set actions
   EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;             // Set PWM1A on Zero
   EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;

   EPwm1Regs.AQCTLB.bit.CAU = AQ_CLEAR;          // Set PWM1A on Zero
   EPwm1Regs.AQCTLB.bit.CAD = AQ_SET;

   // Active Low PWMs - Setup Deadband
   EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
   EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
   EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL;
   EPwm1Regs.DBRED = EPWM1_MAX_DB ;
   EPwm1Regs.DBFED = EPWM1_MIN_DB ;
   EPwm1_DB_Direction = DB_UP;


   // Interrupt where we will change the band
   EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;     // Select INT on Zero event
   EPwm1Regs.ETSEL.bit.INTEN = 1;                // Enable INT
   EPwm1Regs.ETPS.bit.INTPRD = ET_DISABLE  ;           // Generate INT on 3rd event ET_DISABLE  ET_3RD
}

void InitEPwm2Example()
{
   /*EPwm2Regs.TBPRD = 300;                        // Set timer period
   EPwm2Regs.TBPHS.half.TBPHS = 150;           //  is 0
   EPwm2Regs.TBCTR = 0x0000;                      // Clear counter

   // Setup TBCLK
   EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
   EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;        // Disable  loading
   EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV4;       // Clock ratio to SYSCLKOUT
   EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV4;          // Slow just to observe on the scope

   // Setup compare
   EPwm2Regs.CMPA.half.CMPA = 3000;

   // Set actions
   EPwm2Regs.AQCTLA.bit.CAU = AQ_SET;             // Set PWM2A on Zero
   EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;

   EPwm2Regs.AQCTLB.bit.CAU = AQ_CLEAR;           // Set PWM2A on Zero
   EPwm2Regs.AQCTLB.bit.CAD = AQ_SET;

   // Active Low complementary PWMs - setup the band
   EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
   EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_LOC;
   EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;
   EPwm2Regs.DBRED = EPWM2_MIN_DB;
   EPwm2Regs.DBFED = EPWM2_MIN_DB;
   EPwm2_DB_Direction = DB_UP;

   // Interrupt where we will modify the band
   EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;      // Select INT on Zero event
   EPwm2Regs.ETSEL.bit.INTEN = 1;                 // Enable INT
   EPwm2Regs.ETPS.bit.INTPRD = ET_3RD;            // Generate INT on 3rd event
   */
    EPwm2Regs.TBPRD = 300;                         // Set timer period
    EPwm2Regs.TBPHS.half.TBPHS = 0x0000;            //  is 0
    EPwm2Regs.TBCTR = 0x0000;                       // Clear counter

    // Setup TBCLK
    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
    EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;        // Disable  loading
    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;       // Clock ratio to SYSCLKOUT
    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;          // Slow so we can observe on the scope

    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;

    // Setup compare
    EPwm2Regs.CMPA.half.CMPA = D;

    // Set actions
    EPwm2Regs.AQCTLA.bit.CAU = AQ_SET;              // Set PWM3A on Zero
    EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;

    EPwm2Regs.AQCTLB.bit.CAU = AQ_CLEAR;            // Set PWM3A on Zero
    EPwm2Regs.AQCTLB.bit.CAD = AQ_SET;

    // Active high complementary PWMs - Setup the band
    EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
    EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
    EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;
    EPwm2Regs.DBRED = 0;
    EPwm2Regs.DBFED = 0;
    EPwm2_DB_Direction = DB_UP;

    // Interrupt where we will change the deadband
    EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;       // Select INT on Zero event
    EPwm2Regs.ETSEL.bit.INTEN = 1;                  // Enable INT
    //EPwm3Regs.ETPS.bit.INTPRD = ET_3RD;             // Generate INT on 3rd event
    EPwm2Regs.ETPS.bit.INTPRD = ET_DISABLE;             // Generate INT on 3rd event

    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;        //TBCLK = SYSCLKOUT
    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;           //set 1
}

void InitEPwm3Example()
{
   EPwm3Regs.TBCTL.bit.PHSDIR = TB_DOWN;         //Count DOWN on sync
   EPwm3Regs.TBCTL.bit.PRDLD = TB_SHADOW;
   EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
   EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;        //Clock ratio to SYSCLKOUT
   EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;
   EPwm3Regs.TBPRD = 300;                         // Set timer period
   EPwm3Regs.TBPHS.half.TBPHS = 300;            // phase is 0
   EPwm3Regs.TBCTR = 0x0000;                       // Clear counter

   // Setup TBCLK
   EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
   EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE;        // Disable  loading
   EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;       // Clock ratio to SYSCLKOUT
   EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;          // Slow so we can observe on the scope

   // Setup compare
   EPwm3Regs.CMPA.half.CMPA = D;

   // Set actions
   EPwm3Regs.AQCTLA.bit.CAU = AQ_SET;              // Set PWM3A on Zero
   EPwm3Regs.AQCTLA.bit.CAD = AQ_CLEAR;

   EPwm3Regs.AQCTLB.bit.CAU = AQ_CLEAR;            // Set PWM3A on Zero
   EPwm3Regs.AQCTLB.bit.CAD = AQ_SET;

   // Active high complementary PWMs - Setup the deadband
   EPwm3Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
   EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
   EPwm3Regs.DBCTL.bit.IN_MODE = DBA_ALL;
   EPwm3Regs.DBRED = 0;
   EPwm3Regs.DBFED = 0;
   EPwm3_DB_Direction = DB_UP;

   // Interrupt where we will change the deadband
   EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;       // Select INT on Zero event
   EPwm3Regs.ETSEL.bit.INTEN = 1;                  // Enable INT
   //EPwm3Regs.ETPS.bit.INTPRD = ET_3RD;             // Generate INT on 3rd event
   EPwm3Regs.ETPS.bit.INTPRD = ET_DISABLE;             // Generate INT on 3rd event

}
==========================================================================

请告诉我如何解决此问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ujjwal、

    当您从 CCS 将"闪存"应用程序加载到定制板时、故障看起来是什么:CCS 是否显示错误? 如果不是、一旦您从 CCS 加载应用并从 CCS 发出运行命令、应用程序会执行、但在您发出复位命令时不会执行? 请提供其他详细信息、因为这会有所帮助。

    对于从闪存独立执行、请检查引导模式选择引脚是否配置正确。 请参阅 https://www.ti.com/lit/ug/sprui09/sprui09.pdf TRM 的第2.2.9节

    谢谢、
    Ashwini

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ashwini、

    感谢您的快速响应。

     当我 从 CCS 将"flash"应用程序加载到定制板时:CCS 不显示错误。 一旦 我从 CCS 加载应用程序并从 CCS 发出运行命令-是的、应用程序会在我 发出复位命令时执行、但不会执行。

    引导模式选择引脚配置为独立引导模式- GetMode:

    引导模式选择引脚在硬件中配置:

    我无法在调试窗口中读取0x3D7FF 处的值以确认它是否闪烁 (错误:存储器映射阻止读取)。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ujjwal、

    我将与您提供的引导模式配置团队同步、然后返回给您。

    谢谢、

    Ashwini

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    [引用 userid="471735" URL"~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1004147/tms320f28027f-flash-programming-not-working-with-xds110-debug-probe/3710881 #3710881"]

     当我 从 CCS 将"flash"应用程序加载到定制板时:CCS 不显示错误。 一旦 我从 CCS 加载应用程序并从 CCS 发出运行命令-是的、应用程序会在我 发出复位命令时执行、但不会执行。

    引导模式选择引脚配置为独立引导模式- GetMode:

    [/报价]

    您好 Ujjwal、

    在尝试从复位状态运行时、CCS 是否已连接或 XDS100是否已连接?  如果是、则器件将查看设置的 EMU 引导选项。  (使用示波器仔细检查 TRSTn 的状态)。   在 CCS 中、您可以通过脚本-> emu 引导模式选择-> FLASH 来设置 emu 引导模式

    此致

    Lori

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Lori、

    1) 1)连接 CCS (XDS 110)时、我尝试了脚本-> emu 引导模式选择->闪存

    CPU 被重新设置后。  在我单击"re继续"后、代码成功运行。

    一旦我断开 CCS 并为 PCB 上的微控制器上电、代码就不会运行。  

    当我使用相同的代码和 XDS 100v2对另一个 LaunchPad-F28027F 进行编程时。  一旦我断开 CCS 并为 Launchpad 加电、代码就会运行。  

    2) 2)我检查了示波器上 TRSTn 引脚的状态:  

    • 它通常为"低电平" 、并在 "编程/调试"期间变为高电平(3.3V)。 我认为这是好的。
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的详细信息。  您能否检查下面突出显示的存储器位置中的值?  在您之前的屏幕截图中、地址不正确(0x3d7FF 与0x3d7BFE)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Lori、

    感谢您指出我的错误、以下是我观察到的情况:

    0x3d7BFF:0xFFFF

    0x3d7BFE:0xFFFF

    我也选中了

    0x0D00:0x55AA

    0x0D01:0x000B

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Lori 和 Ashwini、

    我已经解决了我的问题。 这是我的错。  它之所以不工作、是因为我在 GPIO 34处有一个下拉电阻器、而不是上拉电阻器(未显示在上面发布的原理图中)。

    感谢 您的快速有效响应。