This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/TMS320F28034:引脚功能故障

Guru**** 2962970 points

Other Parts Discussed in Thread: TMS320F28034

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/965858/ccs-tms320f28034-pin-function-failure

器件型号:TMS320F28034

工具/软件:Code Composer Studio

设计

Tms320f28034执行功能测试来点亮 LED 半克线管、LED 半克线管不会显示。 失败的引脚测试为 PIN33

对接地故障通道的 PIN33进行电阻测试

正常芯片接地电阻为11-15m Ω、故障芯片电阻为1.2-1.5k Ω。

普通芯片的电路板、即数字管可以正常显示的电路板。 在33引脚对地短路、然后通电后、如果数字管未显示、则可能会重复这种现象

TMS320F28034 SCH 的故障是否相同、请执行 以下步骤

THS F28034引脚 SCH   

 VCC=3.3V

RS485 SCH:

LED SCH