This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28377S:DCAEVT1强制同步信号选择- TI 文献中此位的定义不同

Guru**** 2478765 points
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/846787/tms320f28377s-dcaevt1-force-synchronization-signal-select---this-bit-is-defined-differently-in-ti-literature

器件型号:TMS320F28377S
Thread 中讨论的其他器件:controlSUITEC2000WARE

引用 TI TRMS、SPRUHX5E 第1753页:

"DCAEVT1强制同步信号选择
0:源被异步传递
1:源与 EPWMCLK 同步"

而 SPRUHX5D 第1619页:

"DCAEVT1强制同步信号选择
0:源是同步信号
1:源是异步信号"

此外、请注意 、controlSUITE 和 C2000Ware/driverlib 使用0=SYNC、1=异 步。

哪一项是正确的?