This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好。
我使用 TMS320F28377D 来控制/驱动定制的直流/直流转换器。 现在我必须尝试控制2个转换器、我想问您是否可以从 CPU1单独控制一个转换器、从 CPU2单独控制第二个转换器。
这是因为我的转换器开关频率为200kHz、而且我的控制/PWM 更新等以200kHz 的频率运行(我使用一个 ADC 中断、每5us 发生一次、即200kHz)、 我认为、如果我尝试以这个频率从同一 CPU 驱动/控制两个转换器、中断代码的执行时间将远远超过5us (200kHz)、因此、如果可能、我希望从 CPU1驱动一个转换器、从 CPU2驱动另一个转换器。
如果您对此有任何意见/建议、那将会很好、
非常感谢您、
Leo