This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-F28379D:使用 cos 函数生成波形可降低 ISR 的频率

Guru**** 2589245 points
Other Parts Discussed in Thread: C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1179096/launchxl-f28379d-using-cos-functions-for-wave-generation-decreases-the-frequency-of-isr

器件型号:LAUNCHXL-F28379D
主题中讨论的其他器件:C2000WARE

//#############################################################################
//
// FILE:   epwm_ex2_updown_aq.c
//
// TITLE:  ePWM Action Qualifier Module - Using up/down count.
//
//! \addtogroup driver_example_list
//! <h1> ePWM Up Down Count Action Qualifier</h1>
//!
//! This example configures ePWM1, ePWM2, ePWM3 to produce a waveform with
//! independent modulation on ePWMxA and ePWMxB.
//!
//! The compare values CMPA and CMPB are modified within the ePWM's ISR.
//!
//! The TB counter is in up/down count mode for this example.
//!
//! View the ePWM1A/B(GPIO0 & GPIO1), ePWM2A/B(GPIO2 &GPIO3)
//! and ePWM3A/B(GPIO4 & GPIO5) waveforms on oscilloscope.
//
//#############################################################################
// $TI Release: F2837xD Support Library v3.11.00.00 $
// $Release Date: Sun Oct  4 15:55:24 IST 2020 $
// $Copyright:
// Copyright (C) 2013-2020 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
//   Redistributions of source code must retain the above copyright
//   notice, this list of conditions and the following disclaimer.
//
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the
//   documentation and/or other materials provided with the
//   distribution.
//
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################

//
// Included Files
//
#include "driverlib.h"
#include "device.h"


static double angle_gen=0,m1=1,Vrefa=0,Vrefb=0,Vrefc=0;
static double Vrefx=0,Vrefy=0,Vrefz=0;
double PI = 3.14159265359;
static double CLK_count=0;
//
// Defines
//
#define EPWM1_TIMER_TBPRD  2500U
#define EPWM1_MAX_CMPA     1950U
#define EPWM1_MIN_CMPA       50U
#define EPWM1_MAX_CMPB     1950U
#define EPWM1_MIN_CMPB       50U

#define EPWM2_TIMER_TBPRD  2000U
#define EPWM2_MAX_CMPA     1950U
#define EPWM2_MIN_CMPA       50U
#define EPWM2_MAX_CMPB     1950U
#define EPWM2_MIN_CMPB       50U

#define EPWM3_TIMER_TBPRD  2000U
#define EPWM3_MAX_CMPA      950U
#define EPWM3_MIN_CMPA       50U
#define EPWM3_MAX_CMPB     1950U
#define EPWM3_MIN_CMPB     1050U

#define EPWM_CMP_UP           1U
#define EPWM_CMP_DOWN         0U

//
// Globals
//
typedef struct
{
    uint32_t epwmModule;
    uint16_t epwmCompADirection;
    uint16_t epwmCompBDirection;
    uint16_t epwmTimerIntCount;
    uint16_t epwmMaxCompA;
    uint16_t epwmMinCompA;
    uint16_t epwmMaxCompB;
    uint16_t epwmMinCompB;
}epwmInformation;

//
// Globals to hold the ePWM information used in this example
//
epwmInformation epwm1Info;
epwmInformation epwm2Info;
epwmInformation epwm3Info;

//
// Function Prototypes
//
void initEPWM1(void);
void initEPWM2(void);
void initEPWM3(void);
__interrupt void epwm1ISR(void);
__interrupt void epwm2ISR(void);
__interrupt void epwm3ISR(void);
void updateCompare(epwmInformation *epwmInfo);

//
// Main
//
void main(void)
{
    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Disable pin locks and enable internal pull ups.
    //
    Device_initGPIO();

    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts.
    //
    Interrupt_initModule();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    Interrupt_initVectorTable();

    //
    // Assign the interrupt service routines to ePWM interrupts
    //
    Interrupt_register(INT_EPWM1, &epwm1ISR);
    Interrupt_register(INT_EPWM2, &epwm2ISR);
    Interrupt_register(INT_EPWM3, &epwm3ISR);

    //
    // Configure GPIO0/1 , GPIO2/3 and GPIO4/5 as ePWM1A/1B, ePWM2A/2B and
    // ePWM3A/3B pins respectively
    //
    GPIO_setPadConfig(0, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_0_EPWM1A);
    GPIO_setPadConfig(1, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_1_EPWM1B);

    GPIO_setPadConfig(2, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_2_EPWM2A);
    GPIO_setPadConfig(3, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_3_EPWM2B);

    GPIO_setPadConfig(4, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_4_EPWM3A);
    GPIO_setPadConfig(5, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_5_EPWM3B);


    GPIO_setPadConfig(29, GPIO_PIN_TYPE_STD);   // Enable pullup on GPIO6
    GPIO_setDirectionMode(29, GPIO_DIR_MODE_OUT);  // GPIO6 = output

    //
    // Disable sync(Freeze clock to PWM as well)
    //
    SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);

    initEPWM1();
    initEPWM2();
    initEPWM3();

    //
    // Enable sync and clock to PWM
    //
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);

    //
    // Enable ePWM interrupts
    //
    Interrupt_enable(INT_EPWM1);
    Interrupt_enable(INT_EPWM2);
    Interrupt_enable(INT_EPWM3);

    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

    //
    // IDLE loop. Just sit and loop forever (optional):
    //
    for(;;)
    {
        NOP;
    }
}

//
// epwm1ISR - ePWM 1 ISR
//
__interrupt void epwm1ISR(void)
{
    GPIO_togglePin(29);
    CLK_count++;
    if (CLK_count==10000)
    {
        CLK_count=0;
    }
    angle_gen = 2*PI*m1*50*(CLK_count*0.0001); //50Hz

        Vrefa   =   m1*1*cos(angle_gen);
        Vrefb   =   m1*1*cos(angle_gen - 2*PI/3);
        Vrefc   =   m1*1*cos(angle_gen + 2*PI/3);

        Vrefx   =   m1*1*cos(angle_gen - PI/6);
        Vrefy   =   m1*1*cos(angle_gen - 5*PI/6);
        Vrefz   =   m1*1*cos(angle_gen + PI/2);

    //
    // Update the CMPA and CMPB values
    //
    updateCompare(&epwm1Info);

    //
    // Clear INT flag for this timer
    //
    EPWM_clearEventTriggerInterruptFlag(EPWM1_BASE);

    //
    // Acknowledge interrupt group
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}

//
// epwm2ISR - ePWM 2 ISR
//
__interrupt void epwm2ISR(void)
{
    //
    // Update the CMPA and CMPB values
    //
    updateCompare(&epwm2Info);

    //
    // Clear INT flag for this timer
    //
    EPWM_clearEventTriggerInterruptFlag(EPWM2_BASE);

    //
    // Acknowledge interrupt group
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}

//
// epwm3ISR - ePWM 3 ISR
//
__interrupt void epwm3ISR(void)
{
    //
    // Update the CMPA and CMPB values
    //
    updateCompare(&epwm3Info);

    //
    // Clear INT flag for this timer
    //
    EPWM_clearEventTriggerInterruptFlag(EPWM3_BASE);

    //
    // Acknowledge interrupt group
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}

//
// initEPWM1 - Configure ePWM1
//
void initEPWM1()
{
    //
    // Set-up TBCLK
    //
    EPWM_setTimeBasePeriod(EPWM1_BASE, EPWM1_TIMER_TBPRD);
    EPWM_setPhaseShift(EPWM1_BASE, 0U);
    EPWM_setTimeBaseCounter(EPWM1_BASE, 0U);

    //
    // Set Compare values
    //
    EPWM_setCounterCompareValue(EPWM1_BASE,
                                EPWM_COUNTER_COMPARE_A,
                                EPWM1_MIN_CMPA);
    EPWM_setCounterCompareValue(EPWM1_BASE,
                                EPWM_COUNTER_COMPARE_B,
                                EPWM1_MAX_CMPB);

    //
    // Set up counter mode
    //
    EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP_DOWN);
    EPWM_disablePhaseShiftLoad(EPWM1_BASE);
    EPWM_setClockPrescaler(EPWM1_BASE,
                           EPWM_CLOCK_DIVIDER_1,
                           EPWM_HSCLOCK_DIVIDER_1);

    //
    // Set up shadowing
    //
    EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE,
                                         EPWM_COUNTER_COMPARE_A,
                                         EPWM_COMP_LOAD_ON_CNTR_ZERO);
    EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE,
                                         EPWM_COUNTER_COMPARE_B,
                                         EPWM_COMP_LOAD_ON_CNTR_ZERO);

    //
    // Set actions
    //
    EPWM_setActionQualifierAction(EPWM1_BASE,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_HIGH,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
    EPWM_setActionQualifierAction(EPWM1_BASE,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_LOW,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
    EPWM_setActionQualifierAction(EPWM1_BASE,
                                  EPWM_AQ_OUTPUT_B,
                                  EPWM_AQ_OUTPUT_HIGH,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
    EPWM_setActionQualifierAction(EPWM1_BASE,
                                  EPWM_AQ_OUTPUT_B,
                                  EPWM_AQ_OUTPUT_LOW,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB);

    //
    // Interrupt where we will change the Compare Values
    // Select INT on Time base counter zero event,
    // Enable INT, generate INT on 3rd event
    //
    EPWM_setInterruptSource(EPWM1_BASE, EPWM_INT_TBCTR_ZERO);
    EPWM_enableInterrupt(EPWM1_BASE);
    EPWM_setInterruptEventCount(EPWM1_BASE, 1U);

    //
    // Information this example uses to keep track of the direction the
    // CMPA/CMPB values are moving, the min and max allowed values and
    // a pointer to the correct ePWM registers
    //
    epwm1Info.epwmCompADirection = EPWM_CMP_UP;
    epwm1Info.epwmCompBDirection = EPWM_CMP_DOWN;
    epwm1Info.epwmTimerIntCount = 0U;
    epwm1Info.epwmModule = EPWM1_BASE;
    epwm1Info.epwmMaxCompA = EPWM1_MAX_CMPA;
    epwm1Info.epwmMinCompA = EPWM1_MIN_CMPA;
    epwm1Info.epwmMaxCompB = EPWM1_MAX_CMPB;
    epwm1Info.epwmMinCompB = EPWM1_MIN_CMPB;
}

//
// initEPWM2 - Configure ePWM2
//
void initEPWM2()
{
    //
    // Set-up TBCLK
    //
    EPWM_setTimeBasePeriod(EPWM2_BASE, EPWM2_TIMER_TBPRD);
    EPWM_setPhaseShift(EPWM2_BASE, 0U);
    EPWM_setTimeBaseCounter(EPWM2_BASE, 0U);

    //
    // Set Compare values
    //
    EPWM_setCounterCompareValue(EPWM2_BASE,
                                EPWM_COUNTER_COMPARE_A,
                                EPWM2_MIN_CMPA);
    EPWM_setCounterCompareValue(EPWM2_BASE,
                                EPWM_COUNTER_COMPARE_B,
                                EPWM2_MIN_CMPB);

    //
    // Set-up counter mode
    //
    EPWM_setTimeBaseCounterMode(EPWM2_BASE, EPWM_COUNTER_MODE_UP_DOWN);
    EPWM_disablePhaseShiftLoad(EPWM2_BASE);
    EPWM_setClockPrescaler(EPWM2_BASE,
                           EPWM_CLOCK_DIVIDER_1,
                           EPWM_HSCLOCK_DIVIDER_1);

    //
    // Set-up shadowing
    //
    EPWM_setCounterCompareShadowLoadMode(EPWM2_BASE,
                                         EPWM_COUNTER_COMPARE_A,
                                         EPWM_COMP_LOAD_ON_CNTR_ZERO);
    EPWM_setCounterCompareShadowLoadMode(EPWM2_BASE,
                                         EPWM_COUNTER_COMPARE_B,
                                         EPWM_COMP_LOAD_ON_CNTR_ZERO);

    //
    // Set Action qualifier
    //
    EPWM_setActionQualifierAction(EPWM2_BASE,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_HIGH,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
    EPWM_setActionQualifierAction(EPWM2_BASE,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_LOW,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB);
    EPWM_setActionQualifierAction(EPWM2_BASE,
                                  EPWM_AQ_OUTPUT_B,
                                  EPWM_AQ_OUTPUT_LOW,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
    EPWM_setActionQualifierAction(EPWM2_BASE,
                                  EPWM_AQ_OUTPUT_B,
                                  EPWM_AQ_OUTPUT_HIGH,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);

    //
    // Interrupt where we will change the Compare Values
    // Select INT on Time base counter zero event,
    // Enable INT, generate INT on 3rd event
    //
    EPWM_setInterruptSource(EPWM2_BASE, EPWM_INT_TBCTR_ZERO);
    EPWM_enableInterrupt(EPWM2_BASE);
    EPWM_setInterruptEventCount(EPWM2_BASE, 3U);

    //
    // Information this example uses to keep track of the direction the
    // CMPA/CMPB values are moving, the min and max allowed values and
    // a pointer to the correct ePWM registers
    //
    epwm2Info.epwmCompADirection = EPWM_CMP_UP;
    epwm2Info.epwmCompBDirection = EPWM_CMP_UP;
    epwm2Info.epwmTimerIntCount = 0U;
    epwm2Info.epwmModule = EPWM2_BASE;
    epwm2Info.epwmMaxCompA = EPWM2_MAX_CMPA;
    epwm2Info.epwmMinCompA = EPWM2_MIN_CMPA;
    epwm2Info.epwmMaxCompB = EPWM2_MAX_CMPB;
    epwm2Info.epwmMinCompB = EPWM2_MIN_CMPB;
}

//
// initEPWM3 - Configure ePWM3
//
void initEPWM3(void)
{
    //
    // Set-up TBCLK
    //
    EPWM_setTimeBaseCounterMode(EPWM3_BASE, EPWM_COUNTER_MODE_UP_DOWN);
    EPWM_setTimeBasePeriod(EPWM3_BASE, EPWM3_TIMER_TBPRD);
    EPWM_disablePhaseShiftLoad(EPWM3_BASE);
    EPWM_setPhaseShift(EPWM3_BASE, 0U);
    EPWM_setTimeBaseCounter(EPWM3_BASE, 0U);
    EPWM_setClockPrescaler(EPWM3_BASE,
                           EPWM_CLOCK_DIVIDER_1,
                           EPWM_HSCLOCK_DIVIDER_1);

    //
    // Set up shadowing
    //
    EPWM_setCounterCompareShadowLoadMode(EPWM3_BASE,
                                         EPWM_COUNTER_COMPARE_A,
                                         EPWM_COMP_LOAD_ON_CNTR_ZERO);

    EPWM_setCounterCompareShadowLoadMode(EPWM3_BASE,
                                         EPWM_COUNTER_COMPARE_B,
                                         EPWM_COMP_LOAD_ON_CNTR_ZERO);

    //
    // Set Compare values
    //
    EPWM_setCounterCompareValue(EPWM3_BASE,
                                EPWM_COUNTER_COMPARE_A,
                                EPWM3_MIN_CMPA);

    EPWM_setCounterCompareValue(EPWM3_BASE,
                                EPWM_COUNTER_COMPARE_B,
                                EPWM3_MAX_CMPB);

    //
    // Set actions
    //
    EPWM_setActionQualifierAction(EPWM3_BASE,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_HIGH,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);
    EPWM_setActionQualifierAction(EPWM3_BASE,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_LOW,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB);
    EPWM_setActionQualifierAction(EPWM3_BASE,
                                  EPWM_AQ_OUTPUT_B,
                                  EPWM_AQ_OUTPUT_LOW,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);
    EPWM_setActionQualifierAction(EPWM3_BASE,
                                  EPWM_AQ_OUTPUT_B,
                                  EPWM_AQ_OUTPUT_HIGH,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);

    //
    // Interrupt where we will change the Compare Values
    // Select INT on Time base counter zero event,
    // Enable INT, generate INT on 3rd event
    //
    EPWM_setInterruptSource(EPWM3_BASE, EPWM_INT_TBCTR_ZERO);
    EPWM_enableInterrupt(EPWM3_BASE);
    EPWM_setInterruptEventCount(EPWM3_BASE, 3U);

    //
    // Information this example uses to keep track of the direction the
    // CMPA/CMPB values are moving, the min and max allowed values and
    // a pointer to the correct ePWM registers
    //
    epwm3Info.epwmCompADirection = EPWM_CMP_UP;
    epwm3Info.epwmCompBDirection = EPWM_CMP_DOWN;
    epwm3Info.epwmTimerIntCount = 0U;
    epwm3Info.epwmModule = EPWM3_BASE;
    epwm3Info.epwmMaxCompA = EPWM3_MAX_CMPA;
    epwm3Info.epwmMinCompA = EPWM3_MIN_CMPA;
    epwm3Info.epwmMaxCompB = EPWM3_MAX_CMPB;
    epwm3Info.epwmMinCompB = EPWM3_MIN_CMPB;
}

//
// updateCompare - Function to update the frequency
//
void updateCompare(epwmInformation *epwmInfo)
{
    uint16_t compAValue;
    uint16_t compBValue;

    compAValue = EPWM_getCounterCompareValue(epwmInfo->epwmModule,
                                             EPWM_COUNTER_COMPARE_A);

    compBValue = EPWM_getCounterCompareValue(epwmInfo->epwmModule,
                                             EPWM_COUNTER_COMPARE_B);

    //
    //  Change the CMPA/CMPB values every 10th interrupt.
    //
    if(epwmInfo->epwmTimerIntCount == 10U)
    {
        epwmInfo->epwmTimerIntCount = 0U;

        //
        // If we were increasing CMPA, check to see if we reached the max
        // value. If not, increase CMPA else, change directions and decrease
        // CMPA
        //
        if(epwmInfo->epwmCompADirection == EPWM_CMP_UP)
        {
            if(compAValue < (epwmInfo->epwmMaxCompA))
            {
                EPWM_setCounterCompareValue(epwmInfo->epwmModule,
                                            EPWM_COUNTER_COMPARE_A,
                                            ++compAValue);
            }
            else
            {
                epwmInfo->epwmCompADirection = EPWM_CMP_DOWN;
                EPWM_setCounterCompareValue(epwmInfo->epwmModule,
                                            EPWM_COUNTER_COMPARE_A,
                                            --compAValue);
            }
        }
        //
        // If we were decreasing CMPA, check to see if we reached the min
        // value. If not, decrease CMPA else, change directions and increase
        // CMPA
        //
        else
        {
            if( compAValue == (epwmInfo->epwmMinCompA))
            {
                epwmInfo->epwmCompADirection = EPWM_CMP_UP;
                EPWM_setCounterCompareValue(epwmInfo->epwmModule,
                                            EPWM_COUNTER_COMPARE_A,
                                            ++compAValue);
            }
            else
            {
                EPWM_setCounterCompareValue(epwmInfo->epwmModule,
                                            EPWM_COUNTER_COMPARE_A,
                                            --compAValue);
            }
        }

        //
        // If we were increasing CMPB, check to see if we reached the max
        // value. If not, increase CMPB else, change directions and decrease
        // CMPB
        //
        if(epwmInfo->epwmCompBDirection == EPWM_CMP_UP)
        {
            if(compBValue < (epwmInfo->epwmMaxCompB))
            {
                EPWM_setCounterCompareValue(epwmInfo->epwmModule,
                                            EPWM_COUNTER_COMPARE_B,
                                            ++compBValue);
            }
            else
            {
                epwmInfo->epwmCompBDirection = EPWM_CMP_DOWN;
                EPWM_setCounterCompareValue(epwmInfo->epwmModule,
                                            EPWM_COUNTER_COMPARE_B,
                                            --compBValue);
            }
        }
        //
        // If we were decreasing CMPB, check to see if we reached the min
        // value. If not, decrease CMPB else, change directions and increase
        // CMPB
        //
        else
        {
            if(compBValue == (epwmInfo->epwmMinCompB))
            {
                epwmInfo->epwmCompBDirection = EPWM_CMP_UP;
                EPWM_setCounterCompareValue(epwmInfo->epwmModule,
                                            EPWM_COUNTER_COMPARE_B,
                                            ++compBValue);
            }
            else
            {
                EPWM_setCounterCompareValue(epwmInfo->epwmModule,
                                            EPWM_COUNTER_COMPARE_B,
                                            --compBValue);
            }
        }
    }
    else
    {
        epwmInfo->epwmTimerIntCount++;
    }
}

这是使用库的"ti\c2000\C2000Ware_3_03_00_00\driverlib\f2837xd\examples\CPU1\ePWM"的示例代码。

唯一完成的更改是在 EPWM1ISR 中:

__interrupt void epwm1ISR(void)
{
    GPIO_togglePin(29);
    CLK_count++;
    if (CLK_count==10000)
    {
        CLK_count=0;
    }
    angle_gen = 2*PI*m1*50*(CLK_count*0.0001); //50Hz

        Vrefa   =   m1*1*cos(angle_gen);
        Vrefb   =   m1*1*cos(angle_gen - 2*PI/3);
        Vrefc   =   m1*1*cos(angle_gen + 2*PI/3);

        Vrefx   =   m1*1*cos(angle_gen - PI/6);
        Vrefy   =   m1*1*cos(angle_gen - 5*PI/6);
        Vrefz   =   m1*1*cos(angle_gen + PI/2);

    //
    // Update the CMPA and CMPB values
    //
    updateCompare(&epwm1Info);

    //
    // Clear INT flag for this timer
    //
    EPWM_clearEventTriggerInterruptFlag(EPWM1_BASE);

    //
    // Acknowledge interrupt group
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}

移除 cos 函数会将 GPIO 切换频率恢复为10kHz、而通过添加 cos 函数、切换频率会降至1.94Khz。

我尝试了相同的代码、进行了逐位操作、而不是函数、这是正常的。

我使用 launchpad 2806x 尝试了同样的东西、也可以正常工作。

但是、一旦我使用函数、就会出现此问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Syed、

    首先、我想当您说"降低 ISR 的频率"时、您是指"降低 ISR 生成的波形的频率"。

    接下来、当您说"函数"时、我假设您是指对 RTS 库的 cos()函数调用。 是否在项目处理器选项中启用了 TMU、FP_MODE=relaxed? 这将允许编译器使用 TMU 支持的三角运算的硬件指令替换对 RTS 库中三角函数的计算密集型调用。 ISR 可能以特定速率发生(具体取决于您配置 EPWM 中断的发生方式)、并且您没有足够的处理能力来运行对 RTS 库的6个 cos 函数调用。

    话虽如此、我不清楚您的"使用 launchpad 2806x 也能正常工作"语句是指使用 cos 函数还是位操作。 在 F2806x 上、没有 TMU、因此唯一的可能性是 RTS 库、或者作为替代方法、C2000Ware 中的 FPUFastRTS 库。

    谢谢、

    Sira

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    据我所知、"F28x_project"支持逐位操作
    "driver.h"提供了操作 DSP 的函数。

    按函数、我指的是 device.h 函数、而不是逐位操作。 实际上、ePWM 代码是逐位形式的、可以从"driverlib/ca.h"中获取  
    TMU 已启用、FP 模式已放宽。

    使用 device.h ePWM 函数和 cos 函数时、问题仍然存在。  
    因此、我将所有内容都移到了"F28x_project.h"、而不是使用"driver.h"。
    正如我之前提到过的、如果我使用按位操作、它可以正常工作

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Syed、我不理解您的解决方案说明。 为了其他人的利益、您是否可以粘贴您在此处提到的代码:"我尝试了相同的代码、进行逐位操作、而不是函数 "。

    此外、在上面、当您说"driver.h"时、您是指"driverlib.h"吗?

    谢谢、

    Sira