您好!
我修改了原始示例 ADC_Ex5_SoC_Continuous、该示例将2个连续转换为1个转换。
代码如下:
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
//
// Function Prototypes
//
void configureADC(uint32_t adcBase);
void setupADCContinuous(uint32_t adcBase, uint32_t channel);
//
// Defines
//
#define RESULTS_BUFFER_SIZE 1024 //buffer for storing conversion results
//(size must be multiple of 16)
#define EX_ADC_RESOLUTION 12
// 12 for 12-bit conversion resolution, which supports (ADC_MODE_SINGLE_ENDED)
// Sample on single pin (VREFLO is the low reference)
// Or 16 for 16-bit conversion resolution, which supports (ADC_MODE_DIFFERENTIAL)
// Sample on pair of pins (difference between pins is converted, subject to
// common mode voltage requirements; see the device data manual)
//
// Globals
//
uint16_t adcAResults[RESULTS_BUFFER_SIZE];
uint16_t resultsIndex;
void main(void)
{
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
Device_initGPIO();
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Configure the ADC and power it up
//
configureADC(ADCA_BASE);
//
// Setup the ADC for continuous conversions on channel 0
//
setupADCContinuous(ADCA_BASE, 0U);
//
// Initialize results buffer
//
for(resultsIndex = 0; resultsIndex < RESULTS_BUFFER_SIZE; resultsIndex++)
{
adcAResults[resultsIndex] = 0;
}
resultsIndex = 0;
//
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//
// Take conversions indefinitely in loop
//
do
{
//
// Enable ADC interrupts
//
ADC_enableInterrupt(ADCA_BASE, ADC_INT_NUMBER1);
// ADC_enableInterrupt(ADCA_BASE, ADC_INT_NUMBER2);
// ADC_enableInterrupt(ADCA_BASE, ADC_INT_NUMBER3);
// ADC_enableInterrupt(ADCA_BASE, ADC_INT_NUMBER4);
//
// Clear all interrupts flags(INT1-4)
//
HWREGH(ADCA_BASE + ADC_O_INTFLGCLR) = 0x000F;
//
// Initialize results index
//
resultsIndex = 0;
//
// Software force start SOC0 to SOC7
//
// HWREGH(ADCA_BASE + ADC_O_SOCFRC1) = 0x00FF;
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER0 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER1 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER2 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER3 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER4 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER5 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER6 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER7 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER8 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER9 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER10 );
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER11);
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER12);
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER13);
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER14);
ADC_forceSOC(ADCA_BASE, ADC_SOC_NUMBER15);
//
// Keep taking samples until the results buffer is full
//
while(resultsIndex < RESULTS_BUFFER_SIZE)
{
//
// Wait for first set of 8 conversions to complete
//
while(false == ADC_getInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1));
//
// Clear the interrupt flag
//
ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1);
//
// Save results for first 8 conversions
//
// Note that during this time, the second 8 conversions have
// already been triggered by EOC6->ADCIN1 and will be actively
// converting while first 8 results are being saved
//
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER0);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER1);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER2);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER3);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER4);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER5);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER6);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER7);
//
// Wait for the second set of 8 conversions to complete
//
// while(false == ADC_getInterruptStatus(ADCA_BASE, ADC_INT_NUMBER4));
//
// Clear the interrupt flag
//
// ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER4);
//
// Save results for second 8 conversions
//
// Note that during this time, the first 8 conversions have
// already been triggered by EOC14->ADCIN2 and will be actively
// converting while second 8 results are being saved
//
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER8);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER9);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER10);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER11);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER12);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER13);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER14);
adcAResults[resultsIndex++] = ADC_readResult(ADCARESULT_BASE,
ADC_SOC_NUMBER15);
}
//
// Disable all ADCINT flags to stop sampling
//
ADC_disableInterrupt(ADCA_BASE, ADC_INT_NUMBER1);
// ADC_disableInterrupt(ADCA_BASE, ADC_INT_NUMBER2);
// ADC_disableInterrupt(ADCA_BASE, ADC_INT_NUMBER3);
// ADC_disableInterrupt(ADCA_BASE, ADC_INT_NUMBER4);
//
// At this point, adcAResults[] contains a sequence of conversions
// from the selected channel
//
//
// Software breakpoint, hit run again to get updated conversions
//
asm(" ESTOP0");
}
while(1); // Loop forever
}
//
// configureADC - Write ADC configurations and power up the ADC for both
// ADC A and ADC B
//
void configureADC(uint32_t adcBase)
{
//
// Set ADCDLK divider to /4
//
ADC_setPrescaler(adcBase, ADC_CLK_DIV_4_0);
//
// Set resolution and signal mode (see #defines above) and load
// corresponding trims.
//
#if(EX_ADC_RESOLUTION == 12)
ADC_setMode(adcBase, ADC_RESOLUTION_12BIT, ADC_MODE_SINGLE_ENDED);
#elif(EX_ADC_RESOLUTION == 16)
ADC_setMode(adcBase, ADC_RESOLUTION_16BIT, ADC_MODE_DIFFERENTIAL);
#endif
//
// Set pulse positions to late
//
ADC_setInterruptPulseMode(adcBase, ADC_PULSE_END_OF_CONV);
//
// Power up the ADCs and then delay for 1 ms
//
ADC_enableConverter(adcBase);
//
// Delay for 1ms to allow ADC time to power up
//
DEVICE_DELAY_US(1000);
}
//
// setupADCContinuous - setup the ADC to continuously convert on one channel
//
void setupADCContinuous(uint32_t adcBase, uint32_t channel)
{
uint16_t acqps;
//
// Determine acquisition window (in SYSCLKS) based on resolution
//
if(EX_ADC_RESOLUTION == 12)
{
acqps = 30; // 150ns
}
else //resolution is 16-bit
{
acqps = 64; // 320ns
}
//
// - NOTE: A longer sampling window will be required if the ADC driving
// source is less than ideal (an ideal source would be a high bandwidth
// op-amp with a small series resistance). See TI application report
// SPRACT6 for guidance on ADC driver design.
// - NOTE: A slightly longer S+H window is used with 12-bit resolution to
// ensure the data collection loop can keep up with the ADC
//
//
// Configure SOCs channel no. & acquisition window.
//
ADC_setupSOC(adcBase, ADC_SOC_NUMBER0, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER1, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER2, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER3, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER4, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER5, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER6, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER7, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER8, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER9, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER10, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER11, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER12, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER13, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER14, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
ADC_setupSOC(adcBase, ADC_SOC_NUMBER15, ADC_TRIGGER_SW_ONLY,
(ADC_Channel)channel, acqps);
//
// Setup interrupt trigger for SOCs. ADCINT2 will trigger first 8 SOCs.
// ADCINT1 will trigger next 8 SOCs
//
//
// ADCINT2 trigger for SOC0-SOC7
//
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER0,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER1,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER2,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER3,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER4,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER5,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER6,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER7,
ADC_INT_SOC_TRIGGER_ADCINT1);
//
// ADCINT1 trigger for SOC8-SOC15
//
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER8,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER9,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER10,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER11,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER12,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER13,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER14,
ADC_INT_SOC_TRIGGER_ADCINT1);
ADC_setInterruptSOCTrigger(adcBase, ADC_SOC_NUMBER15,
ADC_INT_SOC_TRIGGER_ADCINT1);
//
// Disable Interrupt flags
//
ADC_disableInterrupt(adcBase, ADC_INT_NUMBER1);
// ADC_disableInterrupt(adcBase, ADC_INT_NUMBER2);
// ADC_disableInterrupt(adcBase, ADC_INT_NUMBER3);
// ADC_disableInterrupt(adcBase, ADC_INT_NUMBER4);
//
// Enable continuous mode
//
ADC_enableContinuousMode(adcBase, ADC_INT_NUMBER1);
// ADC_enableContinuousMode(adcBase, ADC_INT_NUMBER2);
// ADC_enableContinuousMode(adcBase, ADC_INT_NUMBER3);
// ADC_enableContinuousMode(adcBase, ADC_INT_NUMBER4);
//
// Configure interrupt triggers
//
ADC_setInterruptSource(adcBase, ADC_INT_NUMBER1, ADC_SOC_NUMBER15);
// ADC_setInterruptSource(adcBase, ADC_INT_NUMBER1, ADC_SOC_NUMBER14);
// ADC_setInterruptSource(adcBase, ADC_INT_NUMBER1, ADC_SOC_NUMBER13); // good results
// ADC_setInterruptSource(adcBase, ADC_INT_NUMBER1, ADC_SOC_NUMBER5);
}
//
// End of file
//
当我输入5kHz 正弦波并使用不同的中断源时、我看到有干扰。 我希望 ADC_setInterruptSource (adcBase、ADC_INT_number1、ADC_SOC_NUMBER15); 不应出现任何干扰、因为它会确保所有转换完成。 这是图形的屏幕截图

谢谢 Vadim