This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280049C:使用 HRPWM 周期控制时的抖动

Guru**** 2966250 points

Other Parts Discussed in Thread: TMDSCNCD280049C, TMS320F280049C, C2000WARE, SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1191674/tms320f280049c-jitter-when-using-hrpwm-period-control

器件型号:TMS320F280049C
主题中讨论的其他器件:TMDSCNCD280049C、 C2000WARE、 SysConfig

大家好、
我正在尝试使用 C2000微控制器生成 PWM 信号。 但是、当我使用 HRPWM 时、我看到输出抖动。 对于配置、我在 CCS 中使用了.syscfg、我不知道我做了什么错误。

我使用的是集成在控制卡(TMDSCNCD280049C)中的 TMS320F280049C。 我使用 Code Composer Studio 版本12.1.0.00007进行编程。

我想实现高达10MHz 的 PWM 频率、恒定占空比为50%、死区时间可配置。 频率需要设置为高分辨率。 当我启用 HRPWM 周期控制(在.syscfg 中或通过 driverlib 函数 HRPWM_enablePeriodControl (PWM_base))时、我会获得抖动。
我知道、当存在同步事件或时基周期发生变化时、可能会发生抖动、但在我的情况下、两者都不会发生。 (至少我认为我已禁用所有同步事件)。

请在下面找到一个最小示例、其中我尝试实现2.10MHz 的 HRPWM。 我使用向上向下计数模式、并在计数器的值等于 CMPA 时设置输出引脚。 为了生成精确的 PWM 信号、启用了 CMPA 的高分辨率(MEP 控制上升沿和下降沿)以及具有自动 HRMSTEP 缩放功能的高分辨率周期。 我用示波器显示抖动的屏幕截图。

测量抖动的时间偏差会得到10ns 的增量 t、这正是所用 C2000的时钟。 因此、在我看来、HRPWM 根本不起作用。

此外、我注意到仅在启用 HR 周期控制时才会发生抖动-与 CMPAHR 无关。

非常感谢!

###代码:###

main.c:

// main.c

#include "board.h"

void main(void)
{
    // Device Initialization
    Device_init();
    Board_init();

    while(1)
    {

    }
}

自动生成 board.h:

/*
 * Copyright (c) 2020 Texas Instruments Incorporated - http://www.ti.com
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 */

#ifndef BOARD_H
#define BOARD_H

//
// Included Files
//

#include "driverlib.h"
#include "device.h"

#define GPIO_PIN_EPWM1_A 0
#define GPIO_PIN_EPWM1_B 1

#define PWM_BASE EPWM1_BASE

void	Board_init();
void	EPWM_init();
void	SYNC_init();
void	PinMux_init();

#endif  // end of BOARD_H definition

自动生成 board.c:

/*
 * Copyright (c) 2020 Texas Instruments Incorporated - http://www.ti.com
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 */

#include "board.h"

void Board_init()
{
	EALLOW;

	PinMux_init();
	SYNC_init();
	EPWM_init();

	EDIS;
}

void PinMux_init()
{
	//
	// EPWM1 -> PWM Pinmux
	//
	GPIO_setPinConfig(GPIO_0_EPWM1_A);
	GPIO_setPinConfig(GPIO_1_EPWM1_B);

}

void EPWM_init(){
    HRPWM_setEmulationMode(PWM_BASE, EPWM_EMULATION_FREE_RUN);	
    HRPWM_setClockPrescaler(PWM_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1);	
    EPWM_setTimeBasePeriod(PWM_BASE, 23);	
    HRPWM_setTimeBaseCounter(PWM_BASE, 0);	
    HRPWM_setTimeBaseCounterMode(PWM_BASE, EPWM_COUNTER_MODE_UP_DOWN);	
    HRPWM_disablePhaseShiftLoad(PWM_BASE);	
    HRPWM_setPhaseShift(PWM_BASE, 0);	
    HRPWM_setSyncOutPulseMode(PWM_BASE, EPWM_SYNC_OUT_PULSE_DISABLED);	
    EPWM_setCounterCompareValue(PWM_BASE, EPWM_COUNTER_COMPARE_A, 11);	
    HRPWM_setCounterCompareShadowLoadMode(PWM_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO_PERIOD);	
    EPWM_setCounterCompareValue(PWM_BASE, EPWM_COUNTER_COMPARE_B, 0);	
    HRPWM_setCounterCompareShadowLoadMode(PWM_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);	
    HRPWM_setActionQualifierAction(PWM_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB);	
    HRPWM_setDeadBandDelayPolarity(PWM_BASE, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_LOW);	
    HRPWM_setDeadBandDelayMode(PWM_BASE, EPWM_DB_RED, true);	
    HRPWM_setRisingEdgeDelayCount(PWM_BASE, 10);	
    HRPWM_setDeadBandDelayMode(PWM_BASE, EPWM_DB_FED, true);	
    HRPWM_setFallingEdgeDelayCount(PWM_BASE, 10);	
    HRPWM_setDeadBandCounterClock(PWM_BASE, EPWM_DB_COUNTER_CLOCK_HALF_CYCLE);	
    HRPWM_enableAutoConversion(PWM_BASE);	
    HRPWM_setMEPEdgeSelect(PWM_BASE, HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_RISING_AND_FALLING_EDGE);	
    HRPWM_setHiResCounterCompareValueOnly(PWM_BASE, HRPWM_COUNTER_COMPARE_A, 230);	
    HRPWM_setCounterCompareShadowLoadEvent(PWM_BASE, HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_ZERO_PERIOD);	
    HRPWM_enablePeriodControl(PWM_BASE);	
    HRPWM_setHiResTimeBasePeriodOnly(PWM_BASE, 205);	
}

void SYNC_init(){
	SysCtl_setSyncOutputConfig(SYSCTL_SYNC_OUT_SRC_EPWM1SYNCOUT);
	// For EPWM1, the sync input is: SYSCTL_SYNC_IN_SRC_EXTSYNCIN1
	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_EPWM4, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_EPWM7, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_ECAP1, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_ECAP4, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_ECAP6, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
	// SOCA
	SysCtl_enableExtADCSOCSource(0);
	// SOCB
	SysCtl_enableExtADCSOCSource(0);
}

SYSCFG-文件:

/**
 * These arguments were used when this file was generated. They will be automatically applied on subsequent loads
 * via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
 * @cliArgs --device "F28004x" --package "F28004x_100PZ" --part "F28004x_100PZ" --product "C2000WARE@4.01.00.00"
 * @versions {"tool":"1.14.0+2667"}
 */

/**
 * Import the modules used in this configuration.
 */
const epwm  = scripting.addModule("/driverlib/epwm.js");
const epwm1 = epwm.addInstance();
const sync  = scripting.addModule("/driverlib/sync.js");

/**
 * Write custom configuration values to the imported modules.
 */
epwm1.epwmTimebase_hsClockDiv                                    = "EPWM_HSCLOCK_DIVIDER_1";
epwm1.epwmTimebase_counterMode                                   = "EPWM_COUNTER_MODE_UP_DOWN";
epwm1.epwmTimebase_syncOutPulseMode                              = "EPWM_SYNC_OUT_PULSE_DISABLED";
epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_A_shadowMode            = true;
epwm1.epwmDeadband_polarityFED                                   = "EPWM_DB_POLARITY_ACTIVE_LOW";
epwm1.epwmDeadband_controlShadowMode                             = true;
epwm1.epwmDeadband_deadbandCounterClockRate                      = "EPWM_DB_COUNTER_CLOCK_HALF_CYCLE";
epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_A_ON_TIMEBASE_UP_CMPA   = "EPWM_AQ_OUTPUT_HIGH";
epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_A_ON_TIMEBASE_DOWN_CMPA = "EPWM_AQ_OUTPUT_LOW";
epwm1.hrpwm_HRLoadA                                              = "HRPWM_LOAD_ON_CNTR_ZERO_PERIOD";
epwm1.epwmCounterCompare_shadowLoadModeCMPA                      = "EPWM_COMP_LOAD_ON_CNTR_ZERO_PERIOD";
epwm1.epwmTimebase_emulationMode                                 = "EPWM_EMULATION_FREE_RUN";
epwm1.epwmDeadband_enableRED                                     = true;
epwm1.$name                                                      = "PWM";
epwm1.epwmDeadband_enableFED                                     = true;
epwm1.epwmDeadband_delayRED                                      = 10;
epwm1.epwmDeadband_delayFED                                      = 10;
epwm1.hrpwm_enable                                               = true;
epwm1.hrpwm_autoConv                                             = true;
epwm1.useInterfacePins                                           = ["EPWM#_A","EPWM#_B"];
epwm1.hrpwm_edgeModeA                                            = "HRPWM_MEP_CTRL_RISING_AND_FALLING_EDGE";
epwm1.hrpwm_periodEnable                                         = true;
epwm1.epwmTimebase_period                                        = 23;
epwm1.hrpwm_tbprdHR                                              = 205;
epwm1.epwmCounterCompare_cmpA                                    = 11;
epwm1.hrpwm_cmpaHR                                               = 230;
epwm1.epwm.$assign                                               = "EPWM1";

/**
 * Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
 * version of the tool will not impact the pinmux you originally saw.  These lines can be completely deleted in order to
 * re-solve from scratch.
 */
epwm1.epwm.epwm_aPin.$suggestSolution = "GPIO0";
epwm1.epwm.epwm_bPin.$suggestSolution = "GPIO1";

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Jonathan、

    感谢您发表您的问题。 我需要一些时间来查看您的配置。 我将在明天答复。

    此致、

    Marlyn

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Jonathan、

    我看到您的 main.c 中没有使用 SFO 库。 请尝试以下示例吗?

    C:\ti\c2000Ware_version\driverlib\f28004x\examples\HRPWM\HRPWM_ex3_prd_updown_SFS.c

    此致、

    Marlyn

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Marlyn、

    感谢您的回复。 我能够使用 SFO 库来部分抑制抖动(如 HRPWM_ex3_prd_updown_SFS.c 中所示):ePWM1A 的输出(屏幕截图中的黄色信号)不再抖动。 然而、ePWM1B (蓝色信号)仍然抖动、但与上次时略有不同。

    我使用死区配置生成 ePWM1B 信号。 因此、我将 epwmDeadband _polarityFED 设置为 ePWM_DB_POLICAL_ACTIVE_LOW。

    如果我将 CMPB 与操作限定符结合使用、我就不再遇到抖动问题了。 但实际上、CMPB 方法会在我的项目中花费更多的运行时计算时间、因此它不是一个替代方案。

    我更改了一些选项、发现更改 epwmDeadband _polarityFED 参数对抖动没有影响(请参阅以下屏幕截图)。 仅当我完全禁用死区时、抖动才会消失。

    我还想将 HRPWM_edgeModeDB 设置为 HRPWM_DB_MEP_CTRL_RED_FED、但这也没有积极的影响。

    此致、
    Jonathan

    main.c:

    // Includes
    #include "board.h"
    #include "SFO_V8.h"
    
    
    // Globals
    uint16_t status = SFO_INCOMPLETE;
    int MEP_ScaleFactor; // Global variable used by the SFO library
    volatile uint32_t ePWM[] = {0, PWM_BASE}; // only using one PWM instance
    
    // Function Prototypes
    void error(void);
    
    
    void main(void)
    {
        // autogenerated init functions
        Device_init();
        Device_initGPIO();
        Interrupt_initModule();
        Interrupt_initVectorTable();
    
        while(status == SFO_INCOMPLETE)
        {
            status = SFO(); // Calling SFO() updates the HRMSTEP register with calibrated MEP_ScaleFactor.
            if(status == SFO_ERROR)
            {
                error();
            }
        }
    
        // autogenerated init functions
        SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
        Board_init();
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
        EINT; // Enable Global Interrupt (INTM)
        ERTM; // Enable realtime interrupt (DBGM)
    
    
        while(1)
        {
            DEVICE_DELAY_US(1000);
    
            status = SFO(); // Calling SFO() updates the HRMSTEP register with calibrated MEP_ScaleFactor.
            if(status == SFO_ERROR)
            {
                error();
            }
        }
    }
    
    // error - Halt debugger when called
    void error (void)
    {
        ESTOP0; // Stop here and handle error
    }

    .syscfg-file:

    /**
     * These arguments were used when this file was generated. They will be automatically applied on subsequent loads
     * via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
     * @cliArgs --device "F28004x" --package "F28004x_100PZ" --part "F28004x_100PZ" --context "system" --product "C2000WARE@4.02.00.00"
     * @versions {"tool":"1.14.0+2667"}
     */
    
    /**
     * Import the modules used in this configuration.
     */
    const epwm             = scripting.addModule("/driverlib/epwm.js", {}, false);
    const epwm1            = epwm.addInstance();
    const inputxbar        = scripting.addModule("/driverlib/inputxbar.js", {}, false);
    const inputxbar1       = inputxbar.addInstance();
    const inputxbar_input  = scripting.addModule("/driverlib/inputxbar_input.js");
    const inputxbar_input1 = inputxbar_input.addInstance();
    const inputxbar_input2 = inputxbar_input.addInstance();
    
    /**
     * Write custom configuration values to the imported modules.
     */
    epwm1.epwmTimebase_hsClockDiv                                    = "EPWM_HSCLOCK_DIVIDER_1";
    epwm1.epwmTimebase_counterMode                                   = "EPWM_COUNTER_MODE_UP_DOWN";
    epwm1.epwmTimebase_syncOutPulseMode                              = "EPWM_SYNC_OUT_PULSE_DISABLED";
    epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_A_ON_TIMEBASE_DOWN_CMPA = "EPWM_AQ_OUTPUT_LOW";
    epwm1.hrpwm_enable                                               = true;
    epwm1.hrpwm_autoConv                                             = true;
    epwm1.hrpwm_edgeModeA                                            = "HRPWM_MEP_CTRL_RISING_AND_FALLING_EDGE";
    epwm1.hrpwm_HRLoadB                                              = "HRPWM_LOAD_ON_CNTR_ZERO_PERIOD";
    epwm1.hrpwm_HRLoadA                                              = "HRPWM_LOAD_ON_CNTR_ZERO_PERIOD";
    epwm1.hrpwm_periodEnable                                         = true;
    epwm1.epwmCounterCompare_shadowLoadModeCMPB                      = "EPWM_COMP_LOAD_ON_CNTR_ZERO_PERIOD";
    epwm1.epwmCounterCompare_shadowLoadModeCMPA                      = "EPWM_COMP_LOAD_ON_CNTR_ZERO_PERIOD";
    epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_A_ON_TIMEBASE_UP_CMPA   = "EPWM_AQ_OUTPUT_HIGH";
    epwm1.epwmTimebase_forceSyncPulse                                = true;
    epwm1.$name                                                      = "PWM";
    epwm1.epwmTimebase_period                                        = 23;
    epwm1.epwmCounterCompare_cmpA                                    = 11;
    epwm1.hrpwm_cmpaHR                                               = 230;
    epwm1.hrpwm_tbprdHR                                              = 205;
    epwm1.epwmDeadband_enableRED                                     = true;
    epwm1.epwmDeadband_enableFED                                     = true;
    epwm1.epwmDeadband_deadbandCounterClockRate                      = "EPWM_DB_COUNTER_CLOCK_HALF_CYCLE";
    epwm1.epwmDeadband_delayRED                                      = 8;
    epwm1.epwmDeadband_delayFED                                      = 8;
    epwm1.epwmDeadband_polarityFED                                   = "EPWM_DB_POLARITY_ACTIVE_LOW";
    epwm1.epwm.$assign                                               = "EPWM1";
    epwm1.epwm.epwm_aPin.$assign                                     = "GPIO0";
    epwm1.epwm.epwm_bPin.$assign                                     = "GPIO1";
    
    inputxbar1.$name = "myINPUTXBAR5";
    
    inputxbar_input1.$name          = "myINPUTXBARINPUT0";
    inputxbar_input1.inputxbarInput = "XBAR_INPUT5";
    inputxbar_input1.inputxbarGpio  = "GPIO40";
    
    inputxbar_input2.$name          = "myINPUTXBARINPUT1";
    inputxbar_input2.inputxbarInput = "XBAR_INPUT6";
    inputxbar_input2.inputxbarGpio  = "GPIO40";

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Jonathan、

    我将文件加载到 SysConfig 中、并看到设置 HRPWM 的方式会出现警告。 您能否纠正此问题并查看这是否有助于消除 B 通道上的抖动?

    您可以通过 ePWM 模块顶部的"全局参数"启用警告:

    此致、

    Marlyn

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Marlyn、

    感谢你的答复。 我已按照警告中的说明更改了配置。 同样、现在抖动看起来不同、但我不会在通道 B 上消除它

    如何配置 PWM 以将 HR 周期控制与死区模块结合使用? 我是否必须以特殊方式配置 SFO 库?

    我的 main.c 文件这次保持不变、请参阅下面的.syscfg 文件。

    此致、
    Jonathan

    /**
     * These arguments were used when this file was generated. They will be automatically applied on subsequent loads
     * via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
     * @cliArgs --device "F28004x" --package "F28004x_100PZ" --part "F28004x_100PZ" --context "system" --product "C2000WARE@4.02.00.00"
     * @versions {"tool":"1.14.0+2667"}
     */
    
    /**
     * Import the modules used in this configuration.
     */
    const epwm       = scripting.addModule("/driverlib/epwm.js");
    const epwm1      = epwm.addInstance();
    const inputxbar  = scripting.addModule("/driverlib/inputxbar.js", {}, false);
    const inputxbar1 = inputxbar.addInstance();
    
    /**
     * Write custom configuration values to the imported modules.
     */
    epwm.enableWarning = true;
    epwm.enableInfo    = true;
    
    epwm1.epwmDeadband_polarityFED                                   = "EPWM_DB_POLARITY_ACTIVE_LOW";
    epwm1.epwmDeadband_enableRED                                     = true;
    epwm1.epwmTimebase_hsClockDiv                                    = "EPWM_HSCLOCK_DIVIDER_1";
    epwm1.epwmTimebase_counterMode                                   = "EPWM_COUNTER_MODE_UP_DOWN";
    epwm1.epwmTimebase_syncOutPulseMode                              = "EPWM_SYNC_OUT_PULSE_DISABLED";
    epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_A_ON_TIMEBASE_DOWN_CMPA = "EPWM_AQ_OUTPUT_LOW";
    epwm1.hrpwm_enable                                               = true;
    epwm1.hrpwm_autoConv                                             = true;
    epwm1.hrpwm_edgeModeA                                            = "HRPWM_MEP_CTRL_RISING_AND_FALLING_EDGE";
    epwm1.hrpwm_HRLoadB                                              = "HRPWM_LOAD_ON_CNTR_ZERO_PERIOD";
    epwm1.hrpwm_HRLoadA                                              = "HRPWM_LOAD_ON_CNTR_ZERO_PERIOD";
    epwm1.hrpwm_periodEnable                                         = true;
    epwm1.epwmCounterCompare_shadowLoadModeCMPB                      = "EPWM_COMP_LOAD_ON_CNTR_ZERO_PERIOD";
    epwm1.epwmCounterCompare_shadowLoadModeCMPA                      = "EPWM_COMP_LOAD_ON_CNTR_ZERO_PERIOD";
    epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_A_ON_TIMEBASE_UP_CMPA   = "EPWM_AQ_OUTPUT_HIGH";
    epwm1.epwmTimebase_forceSyncPulse                                = true;
    epwm1.$name                                                      = "PWM";
    epwm1.epwmTimebase_period                                        = 23;
    epwm1.epwmCounterCompare_cmpA                                    = 11;
    epwm1.hrpwm_cmpaHR                                               = 230;
    epwm1.hrpwm_tbprdHR                                              = 205;
    epwm1.epwmDeadband_deadbandCounterClockRate                      = "EPWM_DB_COUNTER_CLOCK_HALF_CYCLE";
    epwm1.epwmDeadband_delayRED                                      = 8;
    epwm1.epwmDeadband_delayFED                                      = 8;
    epwm1.hrpwm_edgeModeB                                            = "HRPWM_MEP_CTRL_RISING_AND_FALLING_EDGE";
    epwm1.epwmTimebase_emulationMode                                 = "EPWM_EMULATION_FREE_RUN";
    epwm1.epwmDeadband_enableFED                                     = true;
    epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_B_ON_TIMEBASE_UP_CMPB   = "EPWM_AQ_OUTPUT_HIGH";
    epwm1.epwmActionQualifier_EPWM_AQ_OUTPUT_B_ON_TIMEBASE_DOWN_CMPB = "EPWM_AQ_OUTPUT_LOW";
    epwm1.epwm.$assign                                               = "EPWM1";
    epwm1.epwm.epwm_aPin.$assign                                     = "GPIO0";
    epwm1.epwm.epwm_bPin.$assign                                     = "GPIO1";
    
    inputxbar1.$name = "myINPUTXBAR5";
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Jonathan、

    [引用 userid="551268" URL"~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1191674/tms320f280049c-jitter-when-using-hrpwm-period-control/4495688 #4495688"]如何配置 PWM 以将 HR 周期控制与死区模块结合使用? 我是否必须以特殊方式配置 SFO 库?[/QUERP]

    感谢您解决警告问题。 不、您不必这么做。

    我看到您正在为 CMPAHR 写入一个值、您是否也可以为 CMPBHR 写入该值:
    epwm1.HRPWM_cmpbHR = 230;

    下面是一个相关主题、对 其进行了更详细的解释:https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1002939/c2000ware-do-you-need-to-program-cmpb-and-cmpbhr-if-using-active-high-complimentary-mode 

    此致、

    Marlyn

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Marlyn、
    这起作用了。 现在抖动已完全消失。 (说实话、最后一个程序对我来说似乎不太直观)。
    总之、感谢您的支持!
    此致
    Jonathan