This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28069M:设置 HRPWM 占空比

Guru**** 2517950 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1196526/tms320f28069m-setting-hrpwm-duty-cycle

器件型号:TMS320F28069M

您好!  

我正在使用 dev.ti.com 上的2806xHRPWM 示例代码。 我尝试理解示例代码、以便通过 while 环路中的变量设置占空比、而不是移位位。

代码包含在底部、并随附示例代码的链接。


谢谢你。

https://dev.ti.com/tirex/explore/node?devices=F28069M&devtools=F28069M&node=A__AC9UwFyMyNzT.8M6MowG1A__c2000ware_software_package__gYkahfz__LATEST

 

//###########################################################################
//
// FILE:   Example_2806xHRPWM.c
//
// TITLE:  High Resolution PWM Example
//
//!  \addtogroup f2806x_example_list
//!  <h1>High Resolution PWM (hrpwm)</h1>
//!
//!  This example modifies the MEP control registers to show edge displacement
//!  due to the HRPWM control extension of the respective EPwm module
//!  All EPwm1A,2A,3A,4A channels (GPIO0, GPIO2, GPIO4, GPIO6) will have fine
//!  edge movement due to HRPWM logic
//!
//! -# \f$ PWM\ Freq = \frac{SYSCLK}{period=10} \f$,
//!   - ePWM1A toggle low/high with MEP control on rising edge
//!   - ePWM1B toggle low/high with NO HRPWM control
//!
//! -# \f$ PWM\ Freq = \frac{SYSCLK}{period=20} \f$,
//!   - ePWM2A toggle low/high with MEP control on rising edge
//!   - ePWM2B toggle low/high with NO HRPWM control
//!
//! -# \f$ PWM\ Freq = \frac{SYSCLK}{period=10} \f$,
//!   - ePWM3A toggle as high/low with MEP control on falling edge
//!   - ePWM3B toggle low/high with NO HRPWM control
//!
//! -# \f$ PWM\ Freq = \frac{SYSCLK}{period=20} \f$,
//!   - ePWM4A toggle as high/low with MEP control on falling edge
//!   - ePWM4B toggle low/high with NO HRPWM control
//!
//!
//!  \b External \b Connections \n
//!  Monitor ePWM1-ePWM4 pins on an oscilloscope as described
//!  below:
//!  - ePWM1A is on GPIO0
//!  - ePWM1B is on GPIO1
//!
//!  - ePWM2A is on GPIO2
//!  - ePWM2B is on GPIO3
//!
//!  - ePWM3A is on GPIO4
//!  - ePWM3B is on GPIO5
//!
//!  - ePWM4A is on GPIO6
//!  - ePWM4B is on GPIO7
//
//###########################################################################
// $TI Release:  $
// $Release Date:  $
// $Copyright:
// Copyright (C) 2009-2022 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "F2806x_Device.h"     	   // F2806x Headerfile
#include "F2806x_Examples.h"       // F2806x Examples Headerfile
#include "F2806x_EPwm_defines.h"   // useful defines for initialization

//
// Function prototypes
//
void HRPWM1_Config(Uint16);
void HRPWM2_Config(Uint16);
void HRPWM3_Config(Uint16);
void HRPWM4_Config(Uint16);

//
// Globals
//
Uint16 i,j,	DutyFine, n,update;

Uint32 temp;

//
// Main
//
void main(void)
{
    //
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the F2806x_SysCtrl.c file.
    //
    InitSysCtrl();

    //
    // Step 2. Initalize GPIO:
    // This example function is found in the F2806x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    // For this case, just init GPIO for EPwm1-EPwm4
    //
    //InitGpio();  // Skipped for this example

    //
    // For this case just init GPIO pins for EPwm1, EPwm2, EPwm3, EPwm4
    // These functions are in the F2806x_EPwm.c file
    //
    InitEPwm1Gpio();
    InitEPwm2Gpio();
    InitEPwm3Gpio();
    InitEPwm4Gpio();

    //
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    //
    DINT;

    //
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the F2806x_PieCtrl.c file.
    //
    InitPieCtrl();

    //
    // Disable CPU interrupts and clear all CPU interrupt flags
    //
    IER = 0x0000;
    IFR = 0x0000;

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in F2806x_DefaultIsr.c.
    // This function is found in F2806x_PieVect.c.
    //
    InitPieVectTable();

    //
    // Step 4. Initialize all the Device Peripherals:
    // This function is found in F2806x_InitPeripherals.c
    //
    // InitPeripherals();  // Not required for this example

    //
    // For this example, only initialize the EPwm
    // Step 5. User specific code, enable interrupts:
    //
    update =1;
    DutyFine =0;

    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
    EDIS;

    //
    // Some useful Period vs Frequency values
    //  SYSCLKOUT =     80 MHz
    //  ---------------------------
    //	Period	        Frequency
    //	1000	        80 kHz
    //	800		        100 kHz
    //	600		        133 kHz
    //	500		        160 kHz
    //	250		        320 kHz
    //	200		        400 kHz
    //	100		        800 kHz
    //	50		        1.6 Mhz
    //	25		        3.2 Mhz
    //	20		        4.0 Mhz
    //	12		        6.7 MHz
    //	10		        8.0 MHz
    //	9		        8.9 MHz
    //	8		        10.0 MHz
    //	7		        11.4 MHz
    //	6		        13.3 MHz
    //	5		        16.0 MHz
    //

    //
    // ePWM and HRPWM register initializaition
    //
    HRPWM1_Config(45);	    // ePWM1 target, Period = 10
    HRPWM2_Config(45);	    // ePWM2 target, Period = 20
    HRPWM3_Config(10);	    // ePWM3 target, Period = 10
    HRPWM4_Config(20);	    // ePWM4 target, Period = 20

    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
    EDIS;

    while (update ==1)
    {
//        DutyFine = 16;
        for(DutyFine =1; DutyFine <256 ;DutyFine ++)
        {
            //
            // Example, write to the HRPWM extension of CMPA
            //

            //
            // Left shift by 8 to write into MSB bits
            //
//            EPwm1Regs.CMPA.half.CMPAHR = DutyFine << 8;
            EPwm1Regs.CMPA.half.CMPAHR = 0.3;
//                        EPwm1Regs.CMPA.all = ((Uint32)EPwm1Regs.CMPA.half.CMPA << 16) +
//                                              (DutyFine << 8);

//            //
//            // Left shift by 8 to write into MSB bits
//            //
//            EPwm2Regs.CMPA.half.CMPAHR = DutyFine << 8;
//
//            //
//            // Example, 32-bit write to CMPA:CMPAHR
//            //
//            EPwm3Regs.CMPA.all = ((Uint32)EPwm3Regs.CMPA.half.CMPA << 16) +
//                                  (DutyFine << 8);
//            EPwm4Regs.CMPA.all = ((Uint32)EPwm4Regs.CMPA.half.CMPA << 16) +
//                                  (DutyFine << 8);

            //
            // Dummy delay between MEP changes
            //
            for (i=0;i<10000;i++)
            {

            }
        }
//        EPwm1Regs.CMPA.half.CMPAHR =
    }
}

//
// HRPWM1_Config - 
//
void
HRPWM1_Config(Uint16 period)
{
    //
    // ePWM1 register configuration with HRPWM
    // ePWM1A toggle low/high with MEP control on Rising edge
    //
    EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;	 // set Immediate load
//    EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
    EPwm1Regs.TBPRD = period-1;		             // PWM frequency = 1 / period
    EPwm1Regs.CMPA.half.CMPA = period / 1.1;       // set duty 50% initially
    EPwm1Regs.CMPA.half.CMPAHR = (1 << 8);       // initialize HRPWM extension
    EPwm1Regs.CMPB = period / 2;	             // set duty 50% initially
    EPwm1Regs.TBPHS.all = 0;
    EPwm1Regs.TBCTR = 0;

    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;		 // EPwm1 is the Master
    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;

    EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR;        // PWM toggle low/high
    EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;
    EPwm1Regs.AQCTLB.bit.ZRO = AQ_CLEAR;
    EPwm1Regs.AQCTLB.bit.CBU = AQ_SET;

    EALLOW;
    EPwm1Regs.HRCNFG.all = 0x0;
    EPwm1Regs.HRCNFG.bit.EDGMODE = HR_REP;		// MEP control on Rising edge
    EPwm1Regs.HRCNFG.bit.CTLMODE = HR_CMP;
    EPwm1Regs.HRCNFG.bit.HRLOAD  = HR_CTR_ZERO;
    EDIS;
}

//
// HRPWM2_Config - 
//
void
HRPWM2_Config(Uint16 period)
{
    //
    // ePWM2 register configuration with HRPWM
    // ePWM2A toggle low/high with MEP control on Rising edge
    //
    EPwm2Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;	 // set Immediate load
    EPwm2Regs.TBPRD = period-1;		             // PWM frequency = 1 / period
    EPwm2Regs.CMPA.half.CMPA = period / 2;       // set duty 50% initially
    EPwm1Regs.CMPA.half.CMPAHR = (1 << 8);       // initialize HRPWM extension
    EPwm2Regs.CMPB = period / 2;	             // set duty 50% initially
    EPwm2Regs.TBPHS.all = 0;
    EPwm2Regs.TBCTR = 0;

    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
    EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;		 // EPwm2 is the Master
    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
    EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;

    EPwm2Regs.AQCTLA.bit.ZRO = AQ_CLEAR;         // PWM toggle low/high
    EPwm2Regs.AQCTLA.bit.CAU = AQ_SET;
    EPwm2Regs.AQCTLB.bit.ZRO = AQ_CLEAR;
    EPwm2Regs.AQCTLB.bit.CBU = AQ_SET;

    EALLOW;
    EPwm2Regs.HRCNFG.all = 0x0;
    EPwm2Regs.HRCNFG.bit.EDGMODE = HR_REP;       // MEP control on Rising edge
    EPwm2Regs.HRCNFG.bit.CTLMODE = HR_CMP;
    EPwm2Regs.HRCNFG.bit.HRLOAD  = HR_CTR_ZERO;

    EDIS;
}

//
// HRPWM3_Config - 
//
void
HRPWM3_Config(Uint16 period)
{
    //
    // ePWM3 register configuration with HRPWM
    // ePWM3A toggle high/low with MEP control on falling edge
    //
    EPwm3Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;	 // set Immediate load
    EPwm3Regs.TBPRD = period-1;		             // PWM frequency = 1 / period
    EPwm3Regs.CMPA.half.CMPA = period / 2;       // set duty 50% initially
    EPwm3Regs.CMPA.half.CMPAHR = (1 << 8);       // initialize HRPWM extension
    EPwm3Regs.TBPHS.all = 0;
    EPwm3Regs.TBCTR = 0;

    EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
    EPwm3Regs.TBCTL.bit.PHSEN = TB_DISABLE;		 // EPwm3 is the Master
    EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
    EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
    EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;

    EPwm3Regs.AQCTLA.bit.ZRO = AQ_SET;           // PWM toggle high/low
    EPwm3Regs.AQCTLA.bit.CAU = AQ_CLEAR;
    EPwm3Regs.AQCTLB.bit.ZRO = AQ_SET;
    EPwm3Regs.AQCTLB.bit.CBU = AQ_CLEAR;

    EALLOW;
    EPwm3Regs.HRCNFG.all = 0x0;
    EPwm3Regs.HRCNFG.bit.EDGMODE = HR_FEP;       // MEP control on falling edge
    EPwm3Regs.HRCNFG.bit.CTLMODE = HR_CMP;
    EPwm3Regs.HRCNFG.bit.HRLOAD  = HR_CTR_ZERO;
    EDIS;
}

//
// HRPWM4_Config - 
//
void
HRPWM4_Config(Uint16 period)
{
    //
    // ePWM4 register configuration with HRPWM
    // ePWM4A toggle high/low with MEP control on falling edge
    //
    EPwm4Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;	  // set Immediate load
    EPwm4Regs.TBPRD = period-1;		              // PWM frequency = 1 / period
    EPwm4Regs.CMPA.half.CMPA = period / 2;        // set duty 50% initially
    EPwm4Regs.CMPA.half.CMPAHR = (1 << 8);        // initialize HRPWM extension
    EPwm4Regs.CMPB = period / 2;	              // set duty 50% initially
    EPwm4Regs.TBPHS.all = 0;
    EPwm4Regs.TBCTR = 0;

    EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
    EPwm4Regs.TBCTL.bit.PHSEN = TB_DISABLE;		  // EPwm4 is the Master
    EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
    EPwm4Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
    EPwm4Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    EPwm4Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm4Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
    EPwm4Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm4Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;

    EPwm4Regs.AQCTLA.bit.ZRO = AQ_SET;            // PWM toggle high/low
    EPwm4Regs.AQCTLA.bit.CAU = AQ_CLEAR;
    EPwm4Regs.AQCTLB.bit.ZRO = AQ_SET;
    EPwm4Regs.AQCTLB.bit.CBU = AQ_CLEAR;

    EALLOW;
    EPwm4Regs.HRCNFG.all = 0x0;
    EPwm4Regs.HRCNFG.bit.EDGMODE = HR_FEP;       // MEP control on falling edge
    EPwm4Regs.HRCNFG.bit.CTLMODE = HR_CMP;
    EPwm4Regs.HRCNFG.bit.HRLOAD  = HR_CTR_ZERO;
    EDIS;
}

//
// End of File
//

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Raymond、

    CMPAHR 寄存器为16位、可通过选择介于0-255之间的整数的 MEP 步长对其进行微调。 写入一个0.3的浮点值将把 CMPAHR 设定为零。 为了安全地写入 CMPAHR、我们建议按照示例向左移动8位、以便正确填充 HRPWM 寄存器。

    对于该器件、MEP 步长为150ps。 因此、在配置没有 HRPWM 的 ePWM 后、确定您希望占空比的精确度后、您可以选择0-255之间的任何整数值、并且该范围内的每个增量为+150ps。 (当 DutyFine = 1时、您的最终占空比将是您的当前占空比(无 HRPWM)+ 150ps)

    如果您希望占空比为0.55、并且 TBPRD 为30、EPWMCLK 为100Mhz、则可以将 MEP 步长设置为(DutyFine)=等于33。

    您可以使用该示例验证这一点。

    希望这对您有所帮助、

    Ryan Ma

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的解释。 我正在尝试构建一个数控降压转换器、因此我需要与 ADC 输入相比控制占空比。  

    您是否知道在这种情况下如何控制占空比? 我不确定如何通过移动位来管理它。  
    抱歉、我对数字设备不太熟悉。

    谢谢你

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您如何将占空比与 ADC 输入进行比较?  

    最棒的

    Ryan Ma

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ryan、

    我还没有设置 ADC 来读取输入。 我计划尝试在 PLECS 中实现 ADC 功能、并将其添加到控制占空比的代码中。 您会推荐这种方法吗? 我还没有查看过 ADC 示例代码。

    谢谢你

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Raymond、

    很遗憾、我不熟悉 PLECS、因此我无法告诉您是否推荐这种方法。

    我建议查看我们的 ADC 示例、培训视频和学院页面、并将其链接到此处。

    培训 视频

    2.学院 页面

    这些应有助于引导您向正确的方向前进。 如果您有任何与 ADC 相关的问题、则必须创建一个新的线程、以便我们可以提供专家来帮助您处理该外设。

    此致、

    Ryan Ma

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ryan、

    感谢您提供的资源、我将了解一下这些资源。  

    最后一个问题、您是否知道是否有其他方法可以在不移位位的情况下设置占空比?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您是否在谈论在没有 HRPWM 的情况下设置占空比?  

    如果是、那么是! 您只需写入 CMPA 寄存器即可。 下面是有关如何实现该目的的快速视频介绍。

    在视频中、它将讨论如何计算占空比并将其转换为可以写入 CMPA /B 寄存器的值。

    training.ti.com/c2000-enhanced-pulse-width-modulator-epwm-time-base-submodule

    最棒的

    Ryan Ma