This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280049C:刷写应用程序和引导加载程序的合并十六进制文件时、应用程序的.cINIT 未初始化。

Guru**** 2562120 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1196547/tms320f280049c-cinit-of-application-did-not-initialized-when-merged-hex-file-of-application-and-bootloader-was-flashed

器件型号:TMS320F280049C

我有2个 CCS 项目、应用程序和引导加载程序。

Booatloader 闪存存储器范围为0x080000至0x081FFF

应用程序闪存存储器的范围是0x082000到0x08FFFF

我使用-load_image 成功合并了它们、并为它们创建了一个十六进制文件。

但在我将其加载到控制卡中后、它可以从引导加载程序主循环跳转到应用程序主循环、但应用程序的.cinit 未初始化。

应用程序端无法读取应用程序.cinit 中的数据。  

I 监视器是 application.map 的.cinit.Cla1ToCpuMsgRam.load

请参阅随附的 bootloader 和应用程序的 link.cmd 和映射文件。

可以帮帮我吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    应用闪存 lnk cmd

    MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
       BEGIN            : origin = 0x082000, length = 0x00004
       RAMM0            : origin = 0x0000F3, length = 0x00030D
    
       RAMLS0           : origin = 0x008000, length = 0x000800
       RAMLS12          : origin = 0x008800, length = 0x001000
       RAMLS3           : origin = 0x009800, length = 0x000800
       RAMLS4           : origin = 0x00A000, length = 0x000800
       //RAMLS7           : origin = 0x00B800, length = 0x000800
       RESET            : origin = 0x3FFFC0, length = 0x000002
    
    /* Flash sectors */
       /* BANK 0 */
    //   FLASH_BANK0_BOOT  : origin = 0x080000, length = 0x002000    /* on-chip Flash */
    //   FLASH_BANK0_APP	 : origin = 0x082004, length = 0x00DFFB, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC0  : origin = 0x080000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK0_SEC2  : origin = 0x082004, length = 0x000FFC, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC78  : origin = 0x087000, length = 0x002000, fill = 0xFFFF    /* on-chip Flash */
    //   FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
    //   FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
       FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000, fill = 0xFFFF    /* on-chip Flash */
    
       /* BANK 1 */
       FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000    /* on-chip Flash */
       FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0    /* on-chip Flash */
    
    //   FLASH_BANK1_SEC15_RSVD : origin = 0x09FFF0, length = 0x000010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
    PAGE 1 :
    
       BOOT_RSVD       : origin = 0x000002, length = 0x0000F1     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       //RAMLS1           : origin = 0x008800, length = 0x000800
       //RAMLS2           : origin = 0x009000, length = 0x000800
       RAMLS5           : origin = 0x00A800, length = 0x000800
       RAMLS6           : origin = 0x00B000, length = 0x000800
       RAMLS7           : origin = 0x00B800, length = 0x000800
    
       RAMGS0           : origin = 0x00C000, length = 0x002000
       RAMGS1           : origin = 0x00E000, length = 0x002000
       RAMGS2           : origin = 0x010000, length = 0x002000
       RAMGS3           : origin = 0x012000, length = 0x001FF8
    //   RAMGS3_RSVD      : origin = 0x013FF8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       CLA1_MSGRAMLOW   : origin = 0x001480, length = 0x000080
       CLA1_MSGRAMHIGH  : origin = 0x001500, length = 0x000080
    }
    
    SECTIONS
    {
       codestart        : > BEGIN                   PAGE = 0, ALIGN(4)
       .text            : >>FLASH_BANK0_SEC2 | FLASH_BANK0_SEC6 | FLASH_BANK0_SEC78 | FLASH_BANK0_SEC9 | FLASH_BANK0_SEC10 | FLASH_BANK0_SEC11 | FLASH_BANK0_SEC12 | FLASH_BANK0_SEC13 | FLASH_BANK0_SEC14 | FLASH_BANK0_SEC15, PAGE = 0, ALIGN(4)
       .cinit           : > FLASH_BANK0_SEC4,       PAGE = 0, ALIGN(4)
    
       .stack           : > RAMM1                   PAGE = 1
       .switch          : > FLASH_BANK0_SEC4,       PAGE = 0, ALIGN(4)
    #if defined(__TI_EABI__)
       .init_array      : > FLASH_BANK0_SEC4,       PAGE = 0, ALIGN(4)
       .bss             : > RAMLS5,                 PAGE = 1
       .bss:output      : > RAMLS5,                 PAGE = 1
       .bss:cio         : > RAMLS5,                 PAGE = 1
       .data            : >>RAMLS6 | RAMLS7 | RAMLS5,        PAGE = 1
       .sysmem          : > RAMLS6,                 PAGE = 1
       .const           : > FLASH_BANK0_SEC4, PAGE = 0, ALIGN(4)
    #else
       .pinit           : > FLASH_BANK0_SEC4,       PAGE = 0, ALIGN(4)
       .ebss            : >>RAMLS5 | RAMLS6,        PAGE = 1
       .esysmem         : > RAMLS6,                 PAGE = 1
       .cio             : > RAMLS5,                 PAGE = 1
       .econst          : > FLASH_BANK0_SEC4,       PAGE = 0, ALIGN(4)
    #endif
    
       ramgs0           : > RAMGS2,                 PAGE = 1
       ramgs1           : > RAMGS3,                 PAGE = 1
        
       .reset           : > RESET,                  PAGE = 0, TYPE = DSECT /* not used, */
    
    /* Ram functions */
    
    
    #if defined(__TI_EABI__)
    	.TI.ramfunc		: LOAD = FLASH_BANK0_SEC4,
                          RUN  = RAMLS12
                          LOAD_START(RamfuncsLoadStart),
                          LOAD_SIZE( RamfuncsLoadSize ),
                          LOAD_END(  RamfuncsLoadEnd  ),
                          RUN_START( RamfuncsRunStart ),
                          RUN_SIZE(  RamfuncsRunSize  ),
                          RUN_END(   RamfuncsRunEnd   ),
                          PAGE = 0, ALIGN(4)
    #else
       .TI.ramfunc      : LOAD = FLASH_BANK0_SEC4,
                          RUN  = RAMLS12
                          LOAD_START(_RamfuncsLoadStart),
                          LOAD_SIZE( _RamfuncsLoadSize ),
                          LOAD_END(  _RamfuncsLoadEnd  ),
                          RUN_START( _RamfuncsRunStart ),
                          RUN_SIZE(  _RamfuncsRunSize  ),
                          RUN_END(   _RamfuncsRunEnd   ),
                          PAGE = 0, ALIGN(4)
    #endif
    
        /* Allocate fixed point Math - with Gen3 devices, IQMath is not required */
        IQmath          : > FLASH_BANK0_SEC6, PAGE = 0
        IQmathTables    : > FLASH_BANK0_SEC6, PAGE = 0  /* , TYPE = NOLOAD */
    
        /* Floating point Math */
    //    FPUmathTables   : > RAMGS3,           PAGE =1
        FPUmathTables   : > FLASH_BANK0_SEC4, PAGE = 0
    
    
    /* CLA linker */
    
        /* CLA specific sections */
    #if defined(__TI_EABI__)
        Cla1Prog        : LOAD = FLASH_BANK0_SEC5 | FLASH_BANK0_SEC6,
                          RUN  = RAMLS0,
                          LOAD_START(Cla1ProgLoadStart),
                          RUN_START( Cla1ProgRunStart ),
                          LOAD_SIZE( Cla1ProgLoadSize ),
                          PAGE = 0, ALIGN(4)
    #else
        Cla1Prog        : LOAD = FLASH_BANK0_SEC5,
                          RUN  = RAMLS0,
                          LOAD_START(_Cla1ProgLoadStart),
                          RUN_START( _Cla1ProgRunStart ),
                          LOAD_SIZE( _Cla1ProgLoadSize ),
                          PAGE = 0, ALIGN(4)
    #endif
    
        Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW,   PAGE = 1
        CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH,  PAGE = 1
    
    #if 0
        CLA1mathTables  :  LOAD = FLASH_BANK0_SEC5,
                           RUN = RAMLS7,
                           LOAD_START( Cla1mathTablesLoadStart),
                           LOAD_END(   Cla1mathTablesLoadEnd  ),
                           RUN_START(  Cla1mathTablesRunStart ),
                           LOAD_SIZE(  Cla1mathTablesLoadSize ),
                           PAGE = 0, ALIGN(4)
    #endif
    
       .scratchpad      : > RAMLS7,           PAGE = 1
       .bss_cla         : > RAMLS7,           PAGE = 1
       controlVariables : > RAMLS7,           PAGE = 1
    
       Cla1DataRam      : > RAMLS7,           PAGE = 1
       cla_shared       : > RAMLS7,           PAGE = 1
    
    #if defined(__TI_EABI__)
       .const_cla       : LOAD = FLASH_BANK0_SEC5,
                          RUN = RAMLS12,
                          RUN_START( Cla1ConstRunStart ),
                          LOAD_START(Cla1ConstLoadStart),
                          LOAD_SIZE( Cla1ConstLoadSize ),
                          PAGE = 0, ALIGN(4)
    #else
       .const_cla       : LOAD = FLASH_BANK0_SEC5,
                          RUN = RAMLS12,
                          RUN_START( _Cla1ConstRunStart ),
                          LOAD_START(_Cla1ConstLoadStart),
                          LOAD_SIZE( _Cla1ConstLoadSize ),
                          PAGE = 0, ALIGN(4)
    #endif
    }
    
    
    /*! @} */
    

    引导加载程序闪存 lnk cmd

    //
    // Keep the _bankSelect symbol
    //
    
    MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
    
       BEGIN            : origin = 0x080000, length = 0x000002
       RAMM0            : origin = 0x000008, length = 0x0003F8
    
       RAMLS0           : origin = 0x008000, length = 0x000800 /* 2kWord, for CLA code */
       RAMLS1           : origin = 0x008800, length = 0x000800
       //RAMLS3           : origin = 0x009800, length = 0x000800
       //RAMLS4           : origin = 0x00A000, length = 0x000800
       RAMLS34          : origin = 0x009800, length = 0x001000
       RESET            : origin = 0x3FFFC0, length = 0x000002
    
    
    /* Flash sectors */
       /* BANK 0 */
    //   FLASH_BANK0_SEC0  : origin = 0x080002, length = 0x000FFE	/* on-chip Flash */
    //   FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000	/* on-chip Flash */
       FLASH_BOOT        : origin = 0x080002, length = 0x001FFE	/* on-chip Flash */
       FLASH_BANK0_SEC2  : origin = 0x082000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000	/* on-chip Flash */
    
       /* BANK 1 */
       FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0	/* on-chip Flash */
    
    //   FLASH_BANK1_SEC15_RSVD : origin = 0x09FFF0, length = 0x000010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
    
    
    PAGE 1 :
    
       BOOT_RSVD       : origin = 0x000002, length = 0x0000F1     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
    //   RAMLS1           : origin = 0x008800, length = 0x000800
       RAMLS2           : origin = 0x009000, length = 0x000800
       RAMLS5           : origin = 0x00A800, length = 0x000800
       RAMLS6           : origin = 0x00B000, length = 0x000800
       RAMLS7           : origin = 0x00B800, length = 0x000800
    
       RAMGS0           : origin = 0x00C000, length = 0x002000
       RAMGS1           : origin = 0x00E000, length = 0x002000
       RAMGS2           : origin = 0x010000, length = 0x002000
       RAMGS3           : origin = 0x012000, length = 0x001FF8
    //   RAMGS3_RSVD      : origin = 0x013FF8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
    //   CLA1_MSGRAMLOW   : origin = 0x001480, length = 0x000080
    //   CLA1_MSGRAMHIGH  : origin = 0x001500, length = 0x000080
    }
    
    
    SECTIONS
    {
       codestart        : > BEGIN                   PAGE = 0, ALIGN(4)
       .text            : >> FLASH_BOOT,   PAGE = 0, ALIGN(4)
       .cinit           : > FLASH_BOOT,       PAGE = 0, ALIGN(4)
    
       .stack           : > RAMM0                   PAGE = 0
       .switch          : > FLASH_BOOT,       PAGE = 0, ALIGN(4)
    
    #if defined(__TI_EABI__)
       .init_array      : > FLASH_BOOT,       PAGE = 0, ALIGN(4)
       .bss             : > RAMLS34,                 PAGE = 0
       .bss:output      : > RAMLS34,                 PAGE = 0
       .bss:cio         : > RAMLS34,                 PAGE = 0
       .data            : >>RAMLS34,        		PAGE = 0
       .sysmem          : > RAMLS34,                PAGE = 0
       .const           : > FLASH_BOOT,       PAGE = 0, ALIGN(4)
    #else
       .pinit           : > FLASH_BOOT,       PAGE = 0, ALIGN(4)
       .ebss            : >>RAMLS34,       PAGE = 0
       .esysmem         : > RAMLS34,                PAGE = 0
       .cio             : > RAMLS34,                 PAGE = 0
       .econst          : > FLASH_BOOT,       PAGE = 0, ALIGN(4)
    #endif
    
       ramgs0           : > RAMGS0,                 PAGE = 1
       ramgs1           : > RAMGS1,                 PAGE = 1
        
       .reset           : > RESET,                  PAGE = 0, TYPE = DSECT /* not used, */
       
    
    /*
     * Ram functions
     * */
    #if defined(__TI_EABI__)
    	GROUP
    	{
    	   .TI.ramfunc
    	   {-l F021_API_F28004x_FPU32_EABI.lib}
    
       } LOAD = FLASH_BOOT,
                          RUN  = RAMLS34
                          LOAD_START(RamfuncsLoadStart),
                          LOAD_SIZE( RamfuncsLoadSize ),
                          LOAD_END(  RamfuncsLoadEnd  ),
                          RUN_START( RamfuncsRunStart ),
                          RUN_SIZE(  RamfuncsRunSize  ),
                          RUN_END(   RamfuncsRunEnd   ),
                          PAGE = 0, ALIGN(4)
    #endif
    
    }
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

    应用程序映射

    ******************************************************************************
                 TMS320C2000 Linker PC v21.6.0                     
    ******************************************************************************
    >> Linked Wed Feb 15 10:04:20 2023
    
    OUTPUT FILE NAME:   <application.out>
    ENTRY POINT SYMBOL: "code_start"  address: 00082000
    
    
    MEMORY CONFIGURATION
    
             name            origin    length      used     unused   attr    fill
    ----------------------  --------  ---------  --------  --------  ----  --------
    PAGE 0:
      RAMM0                 000000f3   0000030d  00000000  0000030d  RWIX
      RAMLS0                00008000   00000800  000007a0  00000060  RWIX
      RAMLS12               00008800   00001000  00000134  00000ecc  RWIX
      RAMLS3                00009800   00000800  00000000  00000800  RWIX
      RAMLS4                0000a000   00000800  00000000  00000800  RWIX
      DCSM_OTP_Z1_LINKPOINT 00078000   0000000c  00000000  0000000c  RWIX
      DCSM_OTP_Z1_GPREG     0007800c   00000004  00000002  00000002  RWIX
      DCSM_OTP_Z1_PSWDLOCK  00078010   00000004  00000004  00000000  RWIX
      DCSM_OTP_Z1_CRCLOCK   00078014   00000004  00000004  00000000  RWIX
      DCSM_OTP_Z1_BOOTCTRL  0007801c   00000004  00000002  00000002  RWIX
      DCSM_ZSEL_Z1_P0       00078020   00000010  00000000  00000010  RWIX
      DCSM_OTP_Z2_LINKPOINT 00078200   0000000c  00000000  0000000c  RWIX
      DCSM_OTP_Z2_GPREG     0007820c   00000004  00000000  00000004  RWIX
      DCSM_OTP_Z2_PSWDLOCK  00078210   00000004  00000000  00000004  RWIX
      DCSM_OTP_Z2_CRCLOCK   00078214   00000004  00000000  00000004  RWIX
      DCSM_OTP_Z2_BOOTCTRL  0007821c   00000004  00000000  00000004  RWIX
      DCSM_ZSEL_Z2_P0       00078220   00000010  00000000  00000010  RWIX
      B1_DCSM_OTP_Z1_LINKPO 00078400   0000000c  00000000  0000000c  RWIX
      B1_DCSM_ZSEL_Z1_P0    00078420   00000010  00000000  00000010  RWIX
      B1_DCSM_OTP_Z2_LINKPO 00078600   0000000c  00000000  0000000c  RWIX
      B1_DCSM_ZSEL_Z2_P0    00078620   00000010  00000000  00000010  RWIX
      FLASH_BANK0_SEC0      00080000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC1      00081000   00001000  00000000  00001000  RWIX
      BEGIN                 00082000   00000004  00000002  00000002  RWIX
      FLASH_BANK0_SEC2      00082004   00000ffc  00000ffc  00000000  RWIX  ffff 
      FLASH_BANK0_SEC3      00083000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC4      00084000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC5      00085000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC6      00086000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC78     00087000   00002000  00002000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC9      00089000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC10     0008a000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC11     0008b000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC12     0008c000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC13     0008d000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC14     0008e000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK0_SEC15     0008f000   00001000  00001000  00000000  RWIX  ffff 
      FLASH_BANK1_SEC0      00090000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC1      00091000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC2      00092000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC3      00093000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC4      00094000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC5      00095000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC6      00096000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC7      00097000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC8      00098000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC9      00099000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC10     0009a000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC11     0009b000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC12     0009c000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC13     0009d000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC14     0009e000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC15     0009f000   00000ff0  00000000  00000ff0  RWIX
      RESET                 003fffc0   00000002  00000000  00000002  RWIX
    
    PAGE 1:
      BOOT_RSVD             00000002   000000f1  00000001  000000f0  RWIX
      RAMM1                 00000400   000003f8  000003f8  00000000  RWIX
      ADCA_RESULT           00000b00   00000020  00000000  00000020  RWIX
      ADCB_RESULT           00000b20   00000020  00000000  00000020  RWIX
      ADCC_RESULT           00000b40   00000020  00000000  00000020  RWIX
      CPU_TIMER0            00000c00   00000008  00000000  00000008  RWIX
      CPU_TIMER1            00000c08   00000008  00000000  00000008  RWIX
      CPU_TIMER2            00000c10   00000008  00000000  00000008  RWIX
      PIE_CTRL              00000ce0   00000020  00000000  00000020  RWIX
      PIE_VECT              00000d00   00000200  00000000  00000200  RWIX
      DMA                   00001000   00000200  00000000  00000200  RWIX
      CLA1                  00001400   00000080  00000000  00000080  RWIX
      CLA1_MSGRAMLOW        00001480   00000080  00000014  0000006c  RWIX
      CLA1_MSGRAMHIGH       00001500   00000080  00000024  0000005c  RWIX
      EPWM1                 00004000   00000100  00000000  00000100  RWIX
      EPWM2                 00004100   00000100  00000000  00000100  RWIX
      EPWM3                 00004200   00000100  00000000  00000100  RWIX
      EPWM4                 00004300   00000100  00000000  00000100  RWIX
      EPWM5                 00004400   00000100  00000000  00000100  RWIX
      EPWM6                 00004500   00000100  00000000  00000100  RWIX
      EPWM7                 00004600   00000100  00000000  00000100  RWIX
      EPWM8                 00004700   00000100  00000000  00000100  RWIX
      EQEP1                 00005100   00000040  00000000  00000040  RWIX
      EQEP2                 00005140   00000040  00000000  00000040  RWIX
      ECAP1                 00005200   00000040  00000000  00000040  RWIX
      ECAP2                 00005240   00000040  00000000  00000040  RWIX
      ECAP3                 00005280   00000040  00000000  00000040  RWIX
      ECAP4                 000052c0   00000040  00000000  00000040  RWIX
      ECAP5                 00005300   00000040  00000000  00000040  RWIX
      ECAP6                 00005340   00000040  00000000  00000040  RWIX
      ECAP7                 00005380   00000040  00000000  00000040  RWIX
      PGA1                  00005b00   00000010  00000000  00000010  RWIX
      PGA2                  00005b10   00000010  00000000  00000010  RWIX
      PGA3                  00005b20   00000010  00000000  00000010  RWIX
      PGA4                  00005b30   00000010  00000000  00000010  RWIX
      PGA5                  00005b40   00000010  00000000  00000010  RWIX
      PGA6                  00005b50   00000010  00000000  00000010  RWIX
      PGA7                  00005b60   00000010  00000000  00000010  RWIX
      DACA                  00005c00   00000010  00000000  00000010  RWIX
      DACB                  00005c10   00000010  00000000  00000010  RWIX
      CMPSS1                00005c80   00000020  00000000  00000020  RWIX
      CMPSS2                00005ca0   00000020  00000000  00000020  RWIX
      CMPSS3                00005cc0   00000020  00000000  00000020  RWIX
      CMPSS4                00005ce0   00000020  00000000  00000020  RWIX
      CMPSS5                00005d00   00000020  00000000  00000020  RWIX
      CMPSS6                00005d20   00000020  00000000  00000020  RWIX
      CMPSS7                00005d40   00000020  00000000  00000020  RWIX
      SDFM1                 00005e00   00000080  00000000  00000080  RWIX
      SPIA                  00006100   00000010  00000000  00000010  RWIX
      SPIB                  00006110   00000010  00000000  00000010  RWIX
      CLAPROMCRC            000061c0   00000020  00000000  00000020  RWIX
      PMBUSA                00006400   00000020  00000000  00000020  RWIX
      FSITXA                00006600   00000080  00000000  00000080  RWIX
      FSIRXA                00006680   00000080  00000000  00000080  RWIX
      LINA                  00006a00   00000100  00000000  00000100  RWIX
      LINB                  00006b00   00000100  00000000  00000100  RWIX
      WD                    00007000   00000040  00000000  00000040  RWIX
      NMIINTRUPT            00007060   00000010  00000000  00000010  RWIX
      XINT                  00007070   00000010  00000000  00000010  RWIX
      SCIA                  00007200   00000010  00000000  00000010  RWIX
      SCIB                  00007210   00000010  00000000  00000010  RWIX
      I2CA                  00007300   00000040  00000000  00000040  RWIX
      ADCA                  00007400   00000080  00000000  00000080  RWIX
      ADCB                  00007480   00000080  00000000  00000080  RWIX
      ADCC                  00007500   00000080  00000000  00000080  RWIX
      INPUT_XBAR            00007900   00000020  00000000  00000020  RWIX
      XBAR                  00007920   00000020  00000000  00000020  RWIX
      SYNC_SOC              00007940   00000010  00000000  00000010  RWIX
      DMACLASRCSEL          00007980   00000040  00000000  00000040  RWIX
      EPWM_XBAR             00007a00   00000040  00000000  00000040  RWIX
      CLB_XBAR              00007a40   00000040  00000000  00000040  RWIX
      OUTPUT_XBAR           00007a80   00000040  00000000  00000040  RWIX
      GPIOCTRL              00007c00   00000200  00000000  00000200  RWIX
      GPIODAT               00007f00   00000040  00000000  00000040  RWIX
      RAMLS5                0000a800   00000800  0000035a  000004a6  RWIX
      RAMLS6                0000b000   00000800  0000078f  00000071  RWIX
      RAMLS7                0000b800   00000800  00000346  000004ba  RWIX
      RAMGS0                0000c000   00002000  00000000  00002000  RWIX
      RAMGS1                0000e000   00002000  00000000  00002000  RWIX
      RAMGS2                00010000   00002000  00000000  00002000  RWIX
      RAMGS3                00012000   00001ff8  00000000  00001ff8  RWIX
      CANA                  00048000   00000800  00000000  00000800  RWIX
      CANB                  0004a000   00000800  00000000  00000800  RWIX
      DEV_CFG               0005d000   00000180  00000000  00000180  RWIX
      CLK_CFG               0005d200   00000100  00000000  00000100  RWIX
      CPU_SYS               0005d300   00000100  00000000  00000100  RWIX
      PERIPH_AC             0005d500   00000200  00000000  00000200  RWIX
      ANALOG_SUBSYS         0005d700   00000100  00000000  00000100  RWIX
      DCC0                  0005e700   00000040  00000000  00000040  RWIX
      ERAD_GLOBAL           0005e800   00000013  00000000  00000013  RWIX
      ERAD_HWBP1            0005e900   00000008  00000000  00000008  RWIX
      ERAD_HWBP2            0005e908   00000008  00000000  00000008  RWIX
      ERAD_HWBP3            0005e910   00000008  00000000  00000008  RWIX
      ERAD_HWBP4            0005e918   00000008  00000000  00000008  RWIX
      ERAD_HWBP5            0005e920   00000008  00000000  00000008  RWIX
      ERAD_HWBP6            0005e928   00000008  00000000  00000008  RWIX
      ERAD_HWBP7            0005e930   00000008  00000000  00000008  RWIX
      ERAD_HWBP8            0005e938   00000008  00000000  00000008  RWIX
      ERAD_CTR1             0005e980   00000010  00000000  00000010  RWIX
      ERAD_CTR2             0005e990   00000010  00000000  00000010  RWIX
      ERAD_CTR3             0005e9a0   00000010  00000000  00000010  RWIX
      ERAD_CTR4             0005e9b0   00000010  00000000  00000010  RWIX
      DCSM_BANK0_Z1         0005f000   00000030  00000000  00000030  RWIX
      DCSM_BANK0_Z2         0005f040   00000030  00000000  00000030  RWIX
      DCSM_COMMON           0005f070   00000010  00000000  00000010  RWIX
      DCSM_BANK1_Z1         0005f100   00000030  00000000  00000030  RWIX
      DCSM_BANK1_Z2         0005f140   00000030  00000000  00000030  RWIX
      MEMCFG                0005f400   00000080  00000000  00000080  RWIX
      ACCESSPROTECTION      0005f4c0   00000040  00000000  00000040  RWIX
      MEMORYERROR           0005f500   00000040  00000000  00000040  RWIX
      FLASH0_CTRL           0005f800   00000300  00000000  00000300  RWIX
      FLASH0_ECC            0005fb00   00000040  00000000  00000040  RWIX
    
    
    SECTION ALLOCATION MAP
    
     output                                  attributes/
    section   page    origin      length       input sections
    --------  ----  ----------  ----------   ----------------
    codestart 
    *          0    00082000    00000002     
                      00082000    00000002     f28004x_codestartbranch.obj (codestart)
    
    .cinit     0    000844d4    0000023c     
                      000844d4    000000cb     (.cinit..data.1.load) [load image, compression = lzss]
                      0008459f    0000005d     (.cinit..data.2.load) [load image, compression = lzss]
                      000845fc    00000042     (.cinit..data.3.load) [load image, compression = lzss]
                      0008463e    00000035     (.cinit.controlVariables.load) [load image, compression = lzss]
                      00084673    0000002c     (.cinit..data.4.load) [load image, compression = lzss]
                      0008469f    00000029     (.cinit..data.5.load) [load image, compression = lzss]
                      000846c8    00000006     (__TI_handler_table)
                      000846ce    00000004     (.cinit..boot_data_sec.load) [load image, compression = zero_init]
                      000846d2    00000004     (.cinit..bss.load) [load image, compression = zero_init]
                      000846d6    00000004     (.cinit..scratchpad.load) [load image, compression = zero_init]
                      000846da    00000004     (.cinit.Cla1ToCpuMsgRAM.load) [load image, compression = zero_init]
                      000846de    00000004     (.cinit.CpuToCla1MsgRAM.load) [load image, compression = zero_init]
                      000846e2    00000002     --HOLE-- [fill = ffff]
                      000846e4    0000002c     (__TI_cinit_table)
    
    .stack     1    00000400    000003f8     UNINITIALIZED
                      00000400    000003f8     --HOLE--
    
    .init_array 
    *          0    00084000    00000000     UNINITIALIZED
    

    引导加载程序映射

    ******************************************************************************
                 TMS320C2000 Linker PC v21.6.0                     
    ******************************************************************************
    >> Linked Wed Feb 15 10:04:48 2023
    
    OUTPUT FILE NAME:   <bootloader.out>
    ENTRY POINT SYMBOL: "code_start"  address: 00080000
    
    
    MEMORY CONFIGURATION
    
             name            origin    length      used     unused   attr    fill
    ----------------------  --------  ---------  --------  --------  ----  --------
    PAGE 0:
      RAMM0                 00000008   000003f8  000003f8  00000000  RWIX
      RAMLS0                00008000   00000800  00000000  00000800  RWIX
      RAMLS1                00008800   00000800  00000000  00000800  RWIX
      RAMLS34               00009800   00001000  00000a59  000005a7  RWIX
      BEGIN                 00080000   00000002  00000002  00000000  RWIX
      FLASH_BOOT            00080002   00001ffe  00001553  00000aab  RWIX
      FLASH_BANK0_SEC2      00082000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC3      00083000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC4      00084000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC5      00085000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC6      00086000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC7      00087000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC8      00088000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC9      00089000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC10     0008a000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC11     0008b000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC12     0008c000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC13     0008d000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC14     0008e000   00001000  00000000  00001000  RWIX
      FLASH_BANK0_SEC15     0008f000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC0      00090000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC1      00091000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC2      00092000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC3      00093000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC4      00094000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC5      00095000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC6      00096000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC7      00097000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC8      00098000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC9      00099000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC10     0009a000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC11     0009b000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC12     0009c000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC13     0009d000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC14     0009e000   00001000  00000000  00001000  RWIX
      FLASH_BANK1_SEC15     0009f000   00000ff0  00000000  00000ff0  RWIX
      RESET                 003fffc0   00000002  00000000  00000002  RWIX
    
    PAGE 1:
      BOOT_RSVD             00000002   000000f1  00000001  000000f0  RWIX
      RAMM1                 00000400   000003f8  00000000  000003f8  RWIX
      RAMLS2                00009000   00000800  00000000  00000800  RWIX
      RAMLS5                0000a800   00000800  00000000  00000800  RWIX
      RAMLS6                0000b000   00000800  00000000  00000800  RWIX
      RAMLS7                0000b800   00000800  00000000  00000800  RWIX
      RAMGS0                0000c000   00002000  00000000  00002000  RWIX
      RAMGS1                0000e000   00002000  00000000  00002000  RWIX
      RAMGS2                00010000   00002000  00000000  00002000  RWIX
      RAMGS3                00012000   00001ff8  00000000  00001ff8  RWIX
    
    
    SECTION ALLOCATION MAP
    
     output                                  attributes/
    section   page    origin      length       input sections
    --------  ----  ----------  ----------   ----------------
    .stack     0    00000008    000003f8     UNINITIALIZED
                      00000008    000003f8     --HOLE--
    
    codestart 
    *          0    00080000    00000002     
                      00080000    00000002     f28004x_codestartbranch.obj (codestart)
    
    .cinit     0    00081530    0000002c     
                      00081530    0000000f     (.cinit..data.load) [load image, compression = lzss]
                      0008153f    00000001     --HOLE-- [fill = ffff]
                      00081540    00000006     (__TI_handler_table)
                      00081546    00000004     (.cinit..boot_data_sec.load) [load image, compression = zero_init]
                      0008154a    00000004     (.cinit..bss.load) [load image, compression = zero_init]
                      0008154e    00000002     --HOLE-- [fill = ffff]
                      00081550    0000000c     (__TI_cinit_table)
    
    .init_array 
    *          0    00080004    00000000     UNINITIALIZED
    
    .bss       0    0000a1d8    0000006e     UNINITIALIZED
                      0000a1d8    00000040     cfp_svcMngr.obj (.bss:service_table)
                      0000a218    00000020     sfa_update_manager.obj (.bss:buf)
                      0000a238    00000006     cfp_bls_tms32_f28004x.obj (.bss)
                      0000a23e    00000001     cfp_critical_section_f28004x.obj (.bss)
                      0000a23f    00000001     --HOLE--
                      0000a240    00000006     cfp_svcMngr.obj (.bss)
    
    .const     0    000813a8    00000186     
                      000813a8    0000009b     driverlib_eabi.lib : flash.obj (.const:.string)
                      00081443    00000001     --HOLE-- [fill = ffff]
                      00081444    0000009a                        : sysctl.obj (.const:.string)
                      000814de    00000050                        : cputimer.obj (.const:.string)
    
    .reset     0    003fffc0    00000000     DSECT

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Jan、

    我们的一位编译器工具专家将很快回答这个问题。

    谢谢、
    Ibukun

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Jan、

    为了获得更多背景信息、您能否准确地分享您如何从引导加载程序分支到应用程序?

    此致、
    Ibukun

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ibukun、

    很抱歉、我已经解决了问题、已延迟通知。  
    问题出在 f28004x_codestartbranch.asm 中、我直接调用 main 函数、而不是执行.cinit 的_c_int00。 请参阅以下代码。

    (三
    *函数:WD_DISABLE
    *
    *说明:禁用看门狗计时器
    (三
    如果 WD_DISABLE = 1

    .text
    WD_DISABLE:
    SETC OBJMODE;为28x 目标代码设置 OBJMODE
    EALLOW;启用 EALLOW 受保护寄存器访问
    MOVZ DP,#7029h>>>6;设置 WDCR 寄存器的数据页
    MOV @7029h、#0068h;将 WDCR 中的 WDDIS 位置位以禁用 WD
    EDIS;禁用 EALLOW 受保护寄存器访问
    ;LB _c_int00;分支到 RTS 库中启动。_asm
    LCR MAIN

    ;清理并退出。 此时、EntryAddr
    ;位于 ACC 寄存器中
    LB ExitBoot
    .endif

    ;结束 wd_disable

    我将其恢复为"LB _c_int00"

    然后、我通过以下代码更改从引导加载程序跳转到应用程序的实现。


    对于应用程序中的跳转:  
    asm (" lb 0x082000 ")

    对于引导加载程序中的跳转:
    asm (" lb 0x080000 ")

    此代码正常工作、也能够执行.cinit。  
    感谢您对我的问题的回答。
    我将把这个标记为已解决。


    此致、
    1月