This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28377D:cmd fille 为 err

Guru**** 2524550 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1218075/tms320f28377d-cmd-fille-is-err

器件型号:TMS320F28377D

大家好、

以下是客户可能需要您帮助的问题:

可以 理解为我在 RAM 中从 CPU 到 CLA 定义了一个变量。

 我有一个关于 CMD 文件的配置问题。

编译器的错误如下所示:

#10099-D 程序将无法放入可用内存中,或者该段包含的调用站点需要无法为该段生成 trampoline。 针对"Cla1Prog"大小0x84e page 0段运行对齐/分块失败。  可用存储器范围:

 我增加  FLASHD 空间,但它仍然有问题。

以下是我的 CMD 文件:

/*
* Copyright (c) 2015-2020, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/

/*
* ======== TMS320F28377D.cmd ========
* Define the memory block start/length for the F28377D
*/

// The user must define CLA_C in the project linker settings if using the
// CLA C compiler
// Project Properties -> C2000 Linker -> Advanced Options -> Command File
// Preprocessing -> --define
#ifdef CLA_C
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C

MEMORY
{
    PAGE 0 : /* Program Memory */
    /* BEGIN is used for the "boot to FLASH" bootloader mode */
    
    D01SARAM : origin = 0x00B000, length = 0x001000
    LS0SARAM : origin = 0x008000, length = 0x00800 /* on-chip RAM */
    LS5SARAM : origin = 0x00A800, length = 0x000800 /* on-chip RAM */
    
    /* Flash boot address */
    BEGIN : origin = 0x080000, length = 0x000002
    
    
    /* Flash sectors */
    FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
    FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
    FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
    #if 1
    FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
    FLASHEF : origin = 0x088000, length = 0x010000 /* on-chip Flash */
    #endif
    
    //FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
    FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
    FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
    FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
    FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
    FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
    FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
    FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
    FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
    RESET : origin = 0x3FFFC0, length = 0x000002
    
    PAGE 1 : /* Data Memory */
    
    BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom
    will use this for
    stack */
    
    M01SARAM : origin = 0x000122, length = 0x0006DE /* on-chip RAM */
    
    //LS0SARAM : origin = 0x008000, length = 0x00800 /* on-chip RAM */
    
    
    LS14SARAM : origin = 0x008800, length = 0x002000 /* on-chip RAM */
    
    /* on-chip Global shared RAMs */
    //RAMGS0 : origin = 0x00C000, length = 0x001000
    //RAMGS1 : origin = 0x00D000, length = 0x001000
    //RAMGS2 : origin = 0x00E000, length = 0x001000
    //RAMGS3 : origin = 0x00F000, length = 0x001000
    //RAMGS4 : origin = 0x010000, length = 0x001000
    //RAMGS5 : origin = 0x011000, length = 0x001000
    //RAMGS6 : origin = 0x012000, length = 0x001000
    //RAMGS7 : origin = 0x013000, length = 0x001000
    
    RAMGS07 : origin = 0x00C000, length = 0x008000
    RAMGS8 : origin = 0x014000, length = 0x001000
    RAMGS9 : origin = 0x015000, length = 0x001000
    RAMGS10 : origin = 0x016000, length = 0x001000
    RAMGS11 : origin = 0x017000, length = 0x001000
    RAMGS12 : origin = 0x018000, length = 0x001000
    RAMGS13 : origin = 0x019000, length = 0x001000
    RAMGS14 : origin = 0x01A000, length = 0x001000
    RAMGS15 : origin = 0x01B000, length = 0x001000
    
    /* Shared MessageRam */
    CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
    CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
    
    CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
    CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}


SECTIONS
{
    /* Allocate program areas: */
    .cinit : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    .binit : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    #ifdef __TI_EABI__
    .init_array : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    #else
    .pinit : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    #endif
    .text : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    
    
    codestart : > BEGIN PAGE = 0
    ramfuncs : LOAD = FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    
    RUN = RAMGS07 PAGE = 1
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    RUN_SIZE(_RamfuncsRunSize),
    RUN_END(_RamfuncsRunEnd)
    
    #ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 15009000
    .TI.ramfunc : {} LOAD = FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0,
    RUN = LS14SARAM PAGE = 1,
    table(BINIT)
    #endif
    #endif
    
    /* Allocate uninitalized data sections: */
    .stack : > M01SARAM | RAMGS07 PAGE = 1
    #ifdef __TI_EABI__
    .bss : > M01SARAM | LS14SARAM PAGE = 1
    .sysmem : > RAMGS07 | M01SARAM PAGE = 1
    #else
    .ebss : > M01SARAM | LS14SARAM PAGE = 1
    .esysmem : > RAMGS07 | M01SARAM PAGE = 1
    #endif
    .data : > M01SARAM | RAMGS07 PAGE = 1
    .cio : > RAMGS07 | M01SARAM PAGE = 1
    
    /* Initalized sections go in Flash */
    #ifdef __TI_EABI__
    .const : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    #else
    .econst : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    #endif
    .switch : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    .args : > FLASHA | FLASHB | FLASHC | FLASHD | FLASHEF |
    FLASHG | FLASHH | FLASHI | FLASHJ |
    FLASHK | FLASHL | FLASHM | FLASHN PAGE = 0
    
    Filter_RegsFile : > RAMGS07 | RAMGS8 | RAMGS9 |
    RAMGS10 | RAMGS11 | RAMGS12 | RAMGS13 | RAMGS14 |
    RAMGS15 PAGE = 1
    User_RegsFile : > RAMGS07 | RAMGS8 | RAMGS9 |
    RAMGS10 | RAMGS11 | RAMGS12 | RAMGS13 | RAMGS14 |
    RAMGS15 PAGE = 1
    .Bios_Stack : > RAMGS07 | RAMGS8 | RAMGS9 |
    RAMGS10 | RAMGS11 | RAMGS12 | RAMGS13 | RAMGS14 |
    RAMGS15 PAGE = 1
    
    /* CLA specific sections */
    #if defined(__TI_EABI__)
    Cla1Prog : LOAD = FLASHD,
    RUN = LS5SARAM,
    LOAD_START(Cla1funcsLoadStart),
    LOAD_END(Cla1funcsLoadEnd),
    RUN_START(Cla1funcsRunStart),
    LOAD_SIZE(Cla1funcsLoadSize),
    PAGE = 0, ALIGN(8)
    #else
    Cla1Prog : LOAD = FLASHD,
    RUN = LS5SARAM,
    LOAD_START(_Cla1funcsLoadStart),
    LOAD_END(_Cla1funcsLoadEnd),
    RUN_START(_Cla1funcsRunStart),
    LOAD_SIZE(_Cla1funcsLoadSize),
    PAGE = 0, ALIGN(8)
    #endif
    
    CLADataLS0 : > LS0SARAM, PAGE = 0
    CLADataLS1 : > LS0SARAM, PAGE = 0
    
    Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
    CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
    /* CLA C compiler sections */
    //
    // Must be allocated to memory the CLA has write access to
    //
    CLAscratch :
    { *.obj(CLAscratch)
    . += CLA_SCRATCHPAD_SIZE;
    *.obj(CLAscratch_end) } > LS0SARAM, PAGE = 0
    
    .scratchpad : > LS0SARAM, PAGE = 0
    .bss_cla : > LS0SARAM, PAGE = 0
    .const_cla : LOAD = FLASHB,
    RUN = LS0SARAM, PAGE = 0
    RUN_START(Cla1ConstRunStart),
    LOAD_START(Cla1ConstLoadStart),
    LOAD_SIZE(Cla1ConstLoadSize)
    /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }
    
    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        GETBUFFER : TYPE = DSECT
        GETWRITEIDX : TYPE = DSECT
        PUTREADIDX : TYPE = DSECT
    }
}

--

谢谢、此致

耶鲁

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    耶鲁大学  

    您可以请求客户尝试使用区域 FLASHEF 而不是 FLASHD。  由于出现错误、看起来 FLASHD 没有足够的空间来容纳 Cla1Prog 代码。 已注意到 FLASHD 也在链接器命令的其他段中使用、因此可能没有所需的空间(0x84e)。

    此致

    Siddharth