This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280025:在 CCS V12中将十六进制转换为二进制失败

Guru**** 2933120 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1212018/tms320f280025-converting-hex-to-bin-fails-in-ccs-v12

器件型号:TMS320F280025

post_Build:

"${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/ofd2000" "${CG_TOOL_ROOT}/bin/hex2000" "${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin"

日志:

Finished building target: "led_ex1_blinky.out"       

Building secondary target: "led_ex1_blinky.hex"
Invoking: C2000 Hex Utility
"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/hex2000" --romwidth=16 --diag_wrap=off -o "led_ex1_blinky.hex" "led_ex1_blinky.out"
Translating to Extended Tektronix format...
"led_ex1_blinky.out" codestart ==> codestart
"led_ex1_blinky.out" .text ==> .text
"led_ex1_blinky.out" .const ==> .const
"led_ex1_blinky.out" .TI.ramfunc ==> .TI.ramfunc
"led_ex1_blinky.out" .cinit ==> .cinit
Finished building secondary target: "led_ex1_blinky.hex"       

"C:/ti/ccs1220/ccs/utils/tiobj2bin/tiobj2bin" "led_ex1_blinky.out" "led_ex1_blinky.bin" "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/ofd2000" "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/hex2000" "C:/ti/ccs1220/ccs/utils/tiobj2bin/mkhex4bin"
makefile:225: recipe for target 'post-build' failed
'C:' 不是内部或外部命令,也不是可运行的程序            /*'C:' is not recognized as an internal or external command, operable program or batch file.*/
或批处理文件。
gmake[2]: [post-build] Error 255 (ignored)

--

谢谢、此致

耶鲁