This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280049C:ePWM 示例代码

Guru**** 2524460 points
Other Parts Discussed in Thread: C2000WARE, TMS320F280049C

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1204028/tms320f280049c-epwm-example-code

器件型号:TMS320F280049C
主题中讨论的其他器件:C2000WARE

有人能否生成一个非常基本的示例、说明如何使用位域编码在 TMS320f280049C Launch Pad 上启用2个互补的 ePWM 信号。 我在挣扎着,无法找到我的错误的根源。 我曾尝试遵循 c2000ware 中的示例代码、但这些示例只有少数位域示例、并且这些示例非常复杂、我无法理解。 感谢任何帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Kody

    我们大多数示例都使用 driverlib、因为它们对客户更流行、我们的工具基于这些示例构建而成。

    您看了看 driverlib 重复该过程 ePWM 的基本示例?

    您可以通过查看 driverlib 函数的定义并了解它们如何使用 HWREG (base +寄存器偏移)=寄存器值来访问寄存器、将 driverlib 示例转换为位域。

    我们有很多 driverlib 示例(大约20个)您可以查看这些示例吗?  

    如果您尝试编写位域代码但无法正常工作、请随时在此处分享您的 EPWM 配置、我们可以帮助您找到问题的根本原因。

    NIMA

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢 Nima 的帮助。 我能够找出我的问题并运行我的代码。 我现在遇到了与 HRPWM 周期控制有关的问题。 我希望它在 HRPWM 模式下运行、这样我就可以对我的周期进行高分辨率控制、并得到 PWM 恰好是155kHz 的频率。 但是、当我将周期设置为数字来实现这一点时、我没有获得准确的信息、也没有获得相应的人力资源控制。 我会在一封单独的邮件中共享我的代码、所以您或许可以帮助我找到我遇到的问题。

    感谢您的帮助、Kody

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    //#############################################################################
    //
    // FILE:   empty_bitfield_main.c
    //
    // TITLE:  Empty Example
    //
    // Empty Bit-Field Example
    //
    // This example is an empty project setup for Bit-Field development.
    //
    //#############################################################################
    //
    //
    // $Copyright:
    // Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //#############################################################################
    
    //
    // Included Files
    //
    #include "F28x_Project.h"
    
    
    void InitEpwm1Gpio(void);
    void InitEpwm2Gpio(void);
    void InitEpwm4Gpio(void);
    void InitEpwm5Gpio(void);
    void ConfigureEPWM(void);
    void InitEpwm1(void);
    void InitEpwm2(void);
    void InitEpwm4(void);
    void InitEpwm5(void);
    void InitEpwm1Gpio(void);
    
    Uint16 period = 304;//6.45us/2*10ns for 155kHz
    Uint16 dtCountTx = 10; // dead time on both edges
    Uint16 dtCountRx = 14;
    
    
    //
    // Main
    //
    void main(void)
    {
        // 1) Initilize System Control
        // PLL, WatchDog, enable Peripheral Clocks
        InitSysCtrl();
    
        // 2) Initilize GPIOs
        // enable PWM1, PWM2, PWM4, PWM5
        // then init Gpio for same PWMs
        InitGpio(); //May need later if code does not work
    
        InitEpwm1Gpio();
        InitEpwm2Gpio();
        InitEpwm4Gpio();
        InitEpwm5Gpio();
    
        // 3) Clear all interrupts and initilize PIE vector table
        // Disaple CPU interrupts
        DINT;
        InitPieCtrl();
        IER = 0x0000;
        IFR = 0x0000;
        InitPieVectTable();
    
    
    
    
        // Enable Global Interrupt (INTM) and high priority real-time debug events
        EINT; // Enable INTM
        ERTM; // Enable global realtime interrupt DBGM, may or may not be needed.
    
        InitEpwm1();
        InitEpwm2();
        InitEpwm4();
        InitEpwm5();
    }
    
    //
    // ConfigureEPWM - Configure EPWM SOC and compare values confused skip for now
    //
    
    
    
    //
    // EPWM 1 Set up
    //
    void InitEpwm1(void)
    {
    
        EALLOW;
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
        EDIS;
    
    
        //EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;  // set Shadow load
        EPwm1Regs.TBPRD = period;               // PWM frequency = 1/(2*TBPRD)
        EPwm1Regs.CMPA.bit.CMPA = period / 2;   // set duty 50% initially
        EPwm1Regs.CMPA.bit.CMPAHR = (1 << 8);   // initialize HRPWM extension
        EPwm1Regs.CMPB.bit.CMPB = period / 2;   // set duty 50% initially
        EPwm1Regs.CMPB.all |= 1;
        EPwm1Regs.TBPHS.all = 0;
        EPwm1Regs.TBCTR = 0;
    
        EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Select up-down
                                                        // count mode
        EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;
        EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
        EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;// TBCLK = SYSCLKOUT
        EPwm1Regs.TBCTL.bit.PHSEN = TB_ENABLE;
        //EPwm1Regs.TBCTL.bit.FREE_SOFT = 11;
    
        EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;  // LOAD CMPA on CTR = 0
        EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
        EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    
        EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;             // PWM toggle high/low
        EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;
        EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR;             // PWM toggle high/low
        EPwm1Regs.AQCTLB.bit.CBD = AQ_SET;
    
        EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL;
        EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // set rising and falling edge delay
        EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
        EPwm1Regs.DBRED.bit.DBRED = dtCountRx; //rising edge delay
        EPwm1Regs.DBFED.bit.DBFED = dtCountRx; //falling edge delay
    
        EALLOW;
        EPwm1Regs.HRCNFG.all = 0x0;
        EPwm1Regs.HRCNFG.bit.EDGMODE = HR_BEP;          // MEP control on
                                                        // both edges.
        EPwm1Regs.HRCNFG.bit.CTLMODE = HR_CMP;          // CMPAHR and TBPRDHR
                                                         // HR control.
        EPwm1Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO_PRD;  // load on CTR = 0
                                                         // and CTR = TBPRD
        EPwm1Regs.HRCNFG.bit.EDGMODEB = HR_BEP;         // MEP control on
                                                         // both edges
        EPwm1Regs.HRCNFG.bit.CTLMODEB = HR_CMP;         // CMPBHR and TBPRDHR
                                                         // HR control
        EPwm1Regs.HRCNFG.bit.HRLOADB = HR_CTR_ZERO_PRD; // load on CTR = 0
                                                         // and CTR = TBPRD
        EPwm1Regs.HRCNFG.bit.AUTOCONV = 1;        // Enable autoconversion for
                                                   // HR period
    
        EPwm1Regs.HRPCTL.bit.TBPHSHRLOADE = 1;    // Enable TBPHSHR sync
                                                   // (required for updwn
                                                   //  count HR control)
        EPwm1Regs.HRPCTL.bit.HRPE = 1;            // Turn on high-resolution
                                                   // period control.
    
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;      // Enable TBCLK within
                                                   // the EPWM
        CpuSysRegs.PCLKCR2.bit.EPWM1 = 1;
        EPwm1Regs.TBCTL.bit.SWFSYNC = 1;
        EDIS;
    
    
    }
    
    //
    // EPWM 2 Set up
    //
    void InitEpwm2(void)
    {
    
        EALLOW;
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
        EDIS;
    
    
       // EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;  // set Shadow load
        EPwm2Regs.TBPRD = period;               // PWM frequency = 1/(2*TBPRD)
        EPwm2Regs.CMPA.bit.CMPA = period / 2;   // set duty 50% initially
        EPwm2Regs.CMPA.bit.CMPAHR = (1 << 8);   // initialize HRPWM extension
        EPwm2Regs.CMPB.bit.CMPB = period / 2;   // set duty 50% initially
        EPwm2Regs.CMPB.all |= 1;
        EPwm2Regs.TBPHS.all = 0;
        EPwm2Regs.TBCTR = 0;
    
        EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Select up-down
                                                        // count mode
        EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
        EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
        EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;          // TBCLK = SYSCLKOUT
        EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;
       // EPwm2Regs.TBCTL.bit.FREE_SOFT = 11;
    
        EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;  // LOAD CMPA on CTR = 0
        EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
        EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    
        EPwm2Regs.AQCTLA.bit.CAU = AQ_SET;             // PWM toggle high/low
        EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;
        EPwm2Regs.AQCTLB.bit.CBU = AQ_CLEAR;             // PWM toggle high/low
        EPwm2Regs.AQCTLB.bit.CBD = AQ_SET;
    
        EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;
        EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // set rising and falling edge delay
        EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
        EPwm2Regs.DBRED.bit.DBRED = dtCountRx; //rising edge delay
        EPwm2Regs.DBFED.bit.DBFED = dtCountRx; //falling edge delay
    
    
    
    
        EALLOW;
        EPwm2Regs.HRCNFG.all = 0x0;
        EPwm2Regs.HRCNFG.bit.EDGMODE = HR_BEP;          // MEP control on
                                                        // both edges.
        EPwm2Regs.HRCNFG.bit.CTLMODE = HR_CMP;          // CMPAHR and TBPRDHR
                                                        // HR control.
        EPwm2Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO_PRD;  // load on CTR = 0
                                                         // and CTR = TBPRD
        EPwm2Regs.HRCNFG.bit.EDGMODEB = HR_BEP;         // MEP control on
                                                         // both edges
        EPwm2Regs.HRCNFG.bit.CTLMODEB = HR_CMP;         // CMPBHR and TBPRDHR
                                                         // HR control
        EPwm2Regs.HRCNFG.bit.HRLOADB = HR_CTR_ZERO_PRD; // load on CTR = 0
                                                         // and CTR = TBPRD
        EPwm2Regs.HRCNFG.bit.AUTOCONV = 1;        // Enable autoconversion for
                                                   // HR period
        EPwm2Regs.HRPCTL.bit.TBPHSHRLOADE = 1;    // Enable TBPHSHR sync
                                                   // (required for updwn
                                                   //  count HR control)
        EPwm2Regs.HRPCTL.bit.HRPE = 1;            // Turn on high-resolution
                                                   // period control.
    
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;      // Enable TBCLK within
                                                   // the EPWM
        EPwm2Regs.TBCTL.bit.SWFSYNC = 1;
        EDIS;
    
    
    }
    
    //
    // EPWM 4 Set up
    //
    void InitEpwm4(void)
    {
    
        EALLOW;
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
        EDIS;
    
    
       // EPwm4Regs.TBCTL.bit.PRDLD = TB_SHADOW;  // set Shadow load
        EPwm4Regs.TBPRD = period;               // PWM frequency = 1/(2*TBPRD)
        EPwm4Regs.CMPA.bit.CMPA = period / 2;   // set duty 50% initially
        EPwm4Regs.CMPA.bit.CMPAHR = (1 << 8);   // initialize HRPWM extension
        EPwm4Regs.CMPB.bit.CMPB = period / 2;   // set duty 50% initially
        EPwm4Regs.CMPB.all |= 1;
        EPwm4Regs.TBPHS.all = 0;
        EPwm4Regs.TBCTR = 0;
    
        EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Select up-down
                                                        // count mode
        EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;
        EPwm4Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
        EPwm4Regs.TBCTL.bit.CLKDIV = TB_DIV1;          // TBCLK = SYSCLKOUT
        EPwm4Regs.TBCTL.bit.PHSEN = TB_ENABLE;
        EPwm4Regs.TBPHS.bit.TBPHS = period/4;
       // EPwm4Regs.TBCTL.bit.FREE_SOFT = 11;
    
        EPwm4Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;  // LOAD CMPA on CTR = 0
        EPwm4Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
        EPwm4Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        EPwm4Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    
        EPwm4Regs.AQCTLA.bit.CAU = AQ_SET;             // PWM toggle high/low
        EPwm4Regs.AQCTLA.bit.CAD = AQ_CLEAR;
        EPwm4Regs.AQCTLB.bit.CBU = AQ_CLEAR;             // PWM toggle high/low
        EPwm4Regs.AQCTLB.bit.CBD = AQ_SET;
    
        EPwm4Regs.DBCTL.bit.IN_MODE = DBA_ALL;
        EPwm4Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // set rising and falling edge delay
        EPwm4Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
        EPwm4Regs.DBRED.bit.DBRED = dtCountTx; //rising edge delay
        EPwm4Regs.DBFED.bit.DBFED = dtCountTx; //falling edge delay
    
        EALLOW;
    
        SyncSocRegs.SYNCSELECT.bit.EPWM4SYNCIN =0;
        EDIS;
        EALLOW;
        EPwm4Regs.HRCNFG.all = 0x0;
        EPwm4Regs.HRCNFG.bit.EDGMODE = HR_BEP;          // MEP control on
                                                        // both edges.
        EPwm4Regs.HRCNFG.bit.CTLMODE = HR_CMP;          // CMPAHR and TBPRDHR
                                                         // HR control.
        EPwm4Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO_PRD;  // load on CTR = 0
                                                         // and CTR = TBPRD
        EPwm4Regs.HRCNFG.bit.EDGMODEB = HR_BEP;         // MEP control on
                                                         // both edges
        EPwm4Regs.HRCNFG.bit.CTLMODEB = HR_CMP;         // CMPBHR and TBPRDHR
                                                         // HR control
        EPwm4Regs.HRCNFG.bit.HRLOADB = HR_CTR_ZERO_PRD; // load on CTR = 0
                                                         // and CTR = TBPRD
        EPwm4Regs.HRCNFG.bit.AUTOCONV = 1;        // Enable autoconversion for
                                                   // HR period
    
        EPwm4Regs.HRPCTL.bit.TBPHSHRLOADE = 1;    // Enable TBPHSHR sync
                                                   // (required for updwn
                                                   //  count HR control)
        EPwm4Regs.HRPCTL.bit.HRPE = 1;            // Turn on high-resolution
                                                   // period control.
    
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;      // Enable TBCLK within
                                                   // the EPWM
        CpuSysRegs.PCLKCR2.bit.EPWM4 = 1;
        EPwm4Regs.TBCTL.bit.SWFSYNC = 1;
        EDIS;
    
    
    }
    
    //
    // EPWM 5 Set up
    //
    void InitEpwm5(void)
    {
    
        EALLOW;
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
        EDIS;
    
    
        //EPwm5Regs.TBCTL.bit.PRDLD = TB_SHADOW;  // set Shadow load
        EPwm5Regs.TBPRD = period;               // PWM frequency = 1/(2*TBPRD)
        EPwm5Regs.CMPA.bit.CMPA = period / 2;   // set duty 50% initially
        EPwm5Regs.CMPA.bit.CMPAHR = (1 << 8);   // initialize HRPWM extension
        EPwm5Regs.CMPB.bit.CMPB = period / 2;   // set duty 50% initially
        EPwm5Regs.CMPB.all |= 1;
        EPwm5Regs.TBPHS.all = 0;
        EPwm5Regs.TBCTR = 0;
    
        EPwm5Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Select up-down
                                                        // count mode
        EPwm5Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
        EPwm5Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
        EPwm5Regs.TBCTL.bit.CLKDIV = TB_DIV1;          // TBCLK = SYSCLKOUT
        EPwm5Regs.TBCTL.bit.PHSEN = TB_ENABLE;
        //EPwm5Regs.TBPHS.bit.TBPHS = period/4;
        //EPwm5Regs.TBCTL.bit.FREE_SOFT = 11;
    
        EPwm5Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;  // LOAD CMPA on CTR = 0
        EPwm5Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
        EPwm5Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        EPwm5Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    
        EPwm5Regs.AQCTLA.bit.CAU = AQ_CLEAR;             // PWM toggle high/low
        EPwm5Regs.AQCTLA.bit.CAD = AQ_SET;
        EPwm5Regs.AQCTLB.bit.CBU = AQ_SET;             // PWM toggle high/low
        EPwm5Regs.AQCTLB.bit.CBD = AQ_CLEAR;
    
        EPwm5Regs.DBCTL.bit.IN_MODE = DBA_ALL;
        EPwm5Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // set rising and falling edge delay
        EPwm5Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
        EPwm5Regs.DBRED.bit.DBRED = dtCountTx; //rising edge delay
        EPwm5Regs.DBFED.bit.DBFED = dtCountTx; //falling edge delay
    
    
        EALLOW;
        EPwm5Regs.HRCNFG.all = 0x0;
        EPwm5Regs.HRCNFG.bit.EDGMODE = HR_BEP;          // MEP control on
                                                       // both edges.
        EPwm5Regs.HRCNFG.bit.CTLMODE = HR_CMP;          // CMPAHR and TBPRDHR
                                                         // HR control.
        EPwm5Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO_PRD;  // load on CTR = 0
                                                         // and CTR = TBPRD
        EPwm5Regs.HRCNFG.bit.EDGMODEB = HR_BEP;         // MEP control on
                                                         // both edges
        EPwm5Regs.HRCNFG.bit.CTLMODEB = HR_CMP;         // CMPBHR and TBPRDHR
                                                        // HR control
        EPwm5Regs.HRCNFG.bit.HRLOADB = HR_CTR_ZERO_PRD; // load on CTR = 0
                                                         // and CTR = TBPRD
        EPwm5Regs.HRCNFG.bit.AUTOCONV = 1;        // Enable autoconversion for
                                                   // HR period
        EPwm5Regs.HRPCTL.bit.TBPHSHRLOADE = 1;    // Enable TBPHSHR sync
                                                   // (required for updwn
                                                   //  count HR control)
        EPwm5Regs.HRPCTL.bit.HRPE = 1;            // Turn on high-resolution
                                                   // period control.
    
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;  // Enable TBCLK within
                                                   // the EPWM
    
        EPwm5Regs.TBCTL.bit.SWFSYNC = 1;
        EDIS;
    
    
    }
    
    
    
    
    
    //
    // End of File
    //
    
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    "对不起,我不小心给弄丢了。" 您还有问题吗?或者问题是否已解决?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    不用担心 Nima、我还没有想出我的 HR PWM 控制的问题。 即使设置的周期数正确、高分辨率周期控制也不能正常工作。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    不用担心 Nima、我还没有想出我的 HR PWM 控制的问题。 即使设置的周期数正确、高分辨率周期控制也不能正常工作。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Kody,

    要使用高分辨率周期控制、您必须将周期写入 TBPRDHR 寄存器而不是正常的 TBPRD 寄存器。 请告诉我、这是否可以解决您的问题。