This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28035:C2000十六进制实用程序,如何使用"--fill"和"--image"

Guru**** 2538930 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1208992/tms320f28035-c2000-hex-utility-how-to-use---fill-and---image

器件型号:TMS320F28035

****项目 OBC_F28032****的配置调试构建

"D:\\ti\\ccs1220\\ccs\\utils\\bin\\gmake"-k -j 16 all -O

生成文件:"../SOURCE/KADD008U1_SciBoot.c
调用:C2000编译器
"d:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000 -v28 -ml -mt --include_path="E:/0.MCU_Code/00.CCS12/OBC_F28032/OBC_F28032"- include_path="D:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include --include_path="E:/0.MCU_Code/00.CC /SOURCE/KADD008U1_SciBoot.c
已完成建设:"../SOURCE/KADD008U1_SciBoot.c "

构建目标:"OBC_F28032.out"
调用:C2000链接器
"d:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000 -v28 -ml -mt --advice:performance=all -g - diag_warning=225 --diag_wrap =off /ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include --display_error_number --abi=coffabi -z -m"obc_F28032.map"--stack_size=0x200 --warn_sections -i"D:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib -display_error_number - rom_model -o "obc_f28032.out".TI"/INCLUDE/KADD008U1_IsrVariableDefs.obj /SOURCE/DSP280x_CSMPasswords.obj /SOURCE/DSP280x_DBGIER.obj /SOURCE/DSP280x_ECan.obj /SOURCE/DSP280x_Gpio.obj /SOURCE/DSP280x_MemCopy.obj /SOURCE/DSP280x_Sci.obj /SOURCE/GBB_EntryVect.obj /SOURCE/KADD008U1_Isr.obj /SOURCE/KADD008U1_cal.obj /SOURCE/KADD008U1_vAdcTreatment.obj ".k"/SOURCE/DSP280x_CpuTimers.obj /SOURCE/DSP280x_DisInt.obj /SOURCE/DSP280x_GlobalVariableDefs.obj /SOURCE/DSP280x_InitPeripherals.obj /SOURCE/DSP280x_PieVect.obj /SOURCE/DSP280x_usDelay.obj /SOURCE/GBB_main.obj /SOURCE/KADD008U1_SciBoot.obj /SOURCE/KADD008U1_start.obj ".k"/SOURCE/DSP280x_EPwm.obj /SOURCE/DSP280x_I2C.obj /SOURCE/DSP280x_PieCtrl.obj /SOURCE/DSP280x_SysCtrl.obj /SOURCE/GBB_epromdata.obj /SOURCE/KADD008U1_SciApp.obj /SOURCE/KADD008U1_initial.obj /SOURCE/KADD008U1_warnctrl.obj ".k".k"/SOURCE/DSP280x_DefaultIsr.obj ".k"/SOURCE/DSP280x_CodeStartBranch.obj ".k"/SOURCE/DSP280x_Adc.obj ".k"/SOURCE/DSP2803x_Comp.obj

"../F28032.cmd",第157行:警告#10068-D:没有匹配的段
"../F28032.cmd",第161行:警告#10068-D:没有匹配的部分
警告#10063-D:指定"_c_int00"以外的入口点符号:"_B1_Rst_Entry"
完成构建目标:"OBC_F28032.out"

生成辅助目标:"OBC_F28032.hex"
调用:C2000十六进制实用程序
"d:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/hex2000 "--fill=0xFFFF --image --memwidth=16 --romwidth=16 --diag_wrap=off --Intel -o "OBC_F28032.hex""OBC_F28032.out"
Makefile:189:目标'OBC_F28032.hex'的食谱失败
错误:-image 需要 ROMS 指令
gmake[1]:***[OBC_F28032.hex]错误1.
gmake[1]:目标"辅助输出"由于错误而没有重新生成。
Makefile: 178:食谱的目标'all'失败
gmake:***[全部]错误2.

****构建完成****