This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28035:F28035 ADC

Guru**** 2538950 points
Other Parts Discussed in Thread: C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1230339/tms320f28035-f28035-adc

器件型号:TMS320F28035
主题中讨论的其他器件:C2000WARE

大家好

我使用 AdcoffsetSelfCal 函数、但代码 在 AdcConversion 函数中(AdcRegs.ADCINTFLG.bit.ADCINT1 = 0)停止在线路上。

这是怎么了?

Uint16 AdcConversion(void)
{
    Uint16 index, SampleSize, Mean, ACQPS_Value;
    Uint32 Sum;

    index       = 0;            //initialize index to 0
    SampleSize  = 256;          //set sample size to 256 (**NOTE: Sample size must be multiples of 2^x where is an integer >= 4)
    Sum         = 0;            //set sum to 0
    Mean        = 999;          //initialize mean to known value

    //Set the ADC sample window to the desired value (Sample window = ACQPS + 1)
    ACQPS_Value = 8;
    AdcRegs.ADCSOC0CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC1CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC2CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC3CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC4CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC5CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC6CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC7CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC8CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC9CTL.bit.ACQPS  = ACQPS_Value;
    AdcRegs.ADCSOC10CTL.bit.ACQPS = ACQPS_Value;
    AdcRegs.ADCSOC11CTL.bit.ACQPS = ACQPS_Value;
    AdcRegs.ADCSOC12CTL.bit.ACQPS = ACQPS_Value;
    AdcRegs.ADCSOC13CTL.bit.ACQPS = ACQPS_Value;
    AdcRegs.ADCSOC14CTL.bit.ACQPS = ACQPS_Value;
    AdcRegs.ADCSOC15CTL.bit.ACQPS = ACQPS_Value;


    //Enable ping-pong sampling

    // Enabled ADCINT1 and ADCINT2
    AdcRegs.INTSEL1N2.bit.INT1E = 1;
    AdcRegs.INTSEL1N2.bit.INT2E = 1;

    // Disable continuous sampling for ADCINT1 and ADCINT2
    AdcRegs.INTSEL1N2.bit.INT1CONT = 0;
    AdcRegs.INTSEL1N2.bit.INT2CONT = 0;

    AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1;    //ADCINTs trigger at end of conversion

    // Setup ADCINT1 and ADCINT2 trigger source
    AdcRegs.INTSEL1N2.bit.INT1SEL = 6;      //EOC6 triggers ADCINT1
    AdcRegs.INTSEL1N2.bit.INT2SEL = 14;     //EOC14 triggers ADCINT2

    // Setup each SOC's ADCINT trigger source
    AdcRegs.ADCINTSOCSEL1.bit.SOC0  = 2;    //ADCINT2 starts SOC0-7
    AdcRegs.ADCINTSOCSEL1.bit.SOC1  = 2;
    AdcRegs.ADCINTSOCSEL1.bit.SOC2  = 2;
    AdcRegs.ADCINTSOCSEL1.bit.SOC3  = 2;
    AdcRegs.ADCINTSOCSEL1.bit.SOC4  = 2;
    AdcRegs.ADCINTSOCSEL1.bit.SOC5  = 2;
    AdcRegs.ADCINTSOCSEL1.bit.SOC6  = 2;
    AdcRegs.ADCINTSOCSEL1.bit.SOC7  = 2;
    AdcRegs.ADCINTSOCSEL2.bit.SOC8  = 1;    //ADCINT1 starts SOC8-15
    AdcRegs.ADCINTSOCSEL2.bit.SOC9  = 1;
    AdcRegs.ADCINTSOCSEL2.bit.SOC10 = 1;
    AdcRegs.ADCINTSOCSEL2.bit.SOC11 = 1;
    AdcRegs.ADCINTSOCSEL2.bit.SOC12 = 1;
    AdcRegs.ADCINTSOCSEL2.bit.SOC13 = 1;
    AdcRegs.ADCINTSOCSEL2.bit.SOC14 = 1;
    AdcRegs.ADCINTSOCSEL2.bit.SOC15 = 1;

   // DELAY_US(ADC_usDELAY);                  // Delay before converting ADC channels
    int i;
    for ( i= 0 ; i<10000; i++);

    //ADC Conversion

    AdcRegs.ADCSOCFRC1.all = 0x00FF;  // Force Start SOC0-7 to begin ping-pong sampling

    while( index < SampleSize ){

        //Wait for ADCINT1 to trigger, then add ADCRESULT0-7 registers to sum
        while (AdcRegs.ADCINTFLG.bit.ADCINT1 == 0){}
        AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;   //Must clear ADCINT1 flag since INT1CONT = 0
        Sum += AdcResult.ADCRESULT0;
        Sum += AdcResult.ADCRESULT1;
        Sum += AdcResult.ADCRESULT2;
        Sum += AdcResult.ADCRESULT3;
        Sum += AdcResult.ADCRESULT4;
        Sum += AdcResult.ADCRESULT5;
        Sum += AdcResult.ADCRESULT6;
        // Wait for SOC9 conversion to start, which gives time for SOC7 conversion result
        while( AdcRegs.ADCSOCFLG1.bit.SOC9 == 1 ){}
        Sum += AdcResult.ADCRESULT7;

        //Wait for ADCINT2 to trigger, then add ADCRESULT8-15 registers to sum
        while (AdcRegs.ADCINTFLG.bit.ADCINT2 == 0){}
        AdcRegs.ADCINTFLGCLR.bit.ADCINT2 = 1;   //Must clear ADCINT2 flag since INT2CONT = 0
        Sum += AdcResult.ADCRESULT8;
        Sum += AdcResult.ADCRESULT9;
        Sum += AdcResult.ADCRESULT10;
        Sum += AdcResult.ADCRESULT11;
        Sum += AdcResult.ADCRESULT12;
        Sum += AdcResult.ADCRESULT13;
        Sum += AdcResult.ADCRESULT14;
        // Wait for SOC1 conversion to start, which gives time for SOC15 conversion result
        while( AdcRegs.ADCSOCFLG1.bit.SOC1 == 1 ){}
        Sum += AdcResult.ADCRESULT15;

        index+=16;

    } // end data collection

    //Disable ADCINT1 and ADCINT2 to STOP the ping-pong sampling
    AdcRegs.INTSEL1N2.bit.INT1E = 0;
    AdcRegs.INTSEL1N2.bit.INT2E = 0;

    while(AdcRegs.ADCSOCFLG1.all != 0){} // Wait for any pending SOCs to complete

    // Clear any pending interrupts
    AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
    AdcRegs.ADCINTFLGCLR.bit.ADCINT2 = 1;
    AdcRegs.ADCINTOVFCLR.bit.ADCINT1 = 1;
    AdcRegs.ADCINTOVFCLR.bit.ADCINT2 = 1;

    //reset RR pointer to 32, so that next SOC is SOC0
    AdcRegs.SOCPRICTL.bit.SOCPRIORITY = 1;
    while( AdcRegs.SOCPRICTL.bit.SOCPRIORITY != 1 );
    AdcRegs.SOCPRICTL.bit.SOCPRIORITY = 0;
    while( AdcRegs.SOCPRICTL.bit.SOCPRIORITY != 0 );

    Mean = Sum / SampleSize;    //Calculate average ADC sample value

    return Mean;                //return the average

}//end AdcConversion

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您能否尝试从 C2000WARE 导入此示例、并查看您是否有同样的问题?  

    此示例位于[Your_C2000Ware]\device_support\f2803x\examples\c28\  

    此致、

    Ben Collier

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的回答、但 这没有解决 我的问题。

    当我使用 DELAY_US 宏时,我的代码项非法 ISR , 当我更改延迟代码(使用 for loop)时,代码 在行  (AdcRegs.ADCINTFLG.bit.ADCINTT1 ==0)停止。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您是否从闪存运行程序? 我注意到了示例中的这条注释。

     

    此致、

    Ben Collier

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我使用 F28035连接器

    /*
    // TI File $Revision: /main/4 $
    // Checkin $Date: November 9, 2009   15:09:12 $
    //###########################################################################
    //
    // FILE:	F2808.cmd
    //
    // TITLE:	Linker Command File For F2808 Device
    //
    //###########################################################################
    // $TI Release: 2803x C/C++ Header Files and Peripheral Examples V1.24 $
    // $Release Date: January 11, 2011 $
    // $Copyright:
    // Copyright (C) 2009-2023 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2803x_Headers\cmd
    //
    // For BIOS applications add:      DSP2803x_Headers_BIOS.cmd
    // For nonBIOS applications add:   DSP2803x_Headers_nonBIOS.cmd
    ========================================================= */
    
    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper
    // locations within the memory map                                    */
    
    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2803x_Headers_nonBIOS.cmd */
    
    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2803x_Headers_BIOS.cmd */
    
    /* 2) In your project add the path to <base>\DSP2803x_headers\cmd to the
       library search path under project->build options, linker tab,
       library search path (-i).
    /*========================================================= */
    
    /* Define the memory block start/length for the F28035
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
       Notes:
             Memory blocks on F2803x are uniform (ie same
             physical memory) in both PAGE 0 and PAGE 1.
             That is the same memory region should not be
             defined for both PAGE 0 and PAGE 1.
             Doing so will result in corruption of program
             and/or data.
    
             L0 memory block is mirrored - that is
             it can be accessed in high memory or low memory.
             For simplicity only one instance is used in this
             linker file.
    
             Contiguous SARAM memory blocks or flash sectors can be
             be combined if required to create a larger memory block.
    */
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
       RAML0       : origin = 0x008000, length = 0x000800     /* on-chip RAM block L0 */
       RAML1       : origin = 0x008800, length = 0x000400     /* on-chip RAM block L1 */
       OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
       FLASHH      : origin = 0x3E8000, length = 0x002000     /* on-chip FLASH */
       FLASHG      : origin = 0x3EA000, length = 0x002000     /* on-chip FLASH */
       FLASHF      : origin = 0x3EC000, length = 0x002000     /* on-chip FLASH */
       FLASHE      : origin = 0x3EE000, length = 0x002000     /* on-chip FLASH */
       FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASH */
       FLASHC      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASH */
       FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
    
       IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
       IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA	  /* IQ Math Tables in Boot ROM */
    
       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
    
    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */
       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       RAML2       : origin = 0x008C00, length = 0x000400     /* on-chip RAM block L2 */
       RAML3       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L3 */
       FLASHB      : origin = 0x3F4000, length = 0x002000     /* on-chip FLASH */
    
    }
    
    /* Allocate sections to memory blocks.
       Note:
             codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                       execution when booting to flash
             ramfuncs  user defined section to store functions that will be copied from Flash into RAM
    */
    
    SECTIONS
    {
    
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0
       .pinit              : > FLASHA,     PAGE = 0
       .text               : > FLASHA      PAGE = 0
       codestart           : > BEGIN       PAGE = 0
       ramfuncs            : LOAD = FLASHD,
                             RUN = RAML0,
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_SIZE(_RamfuncsLoadSize),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0
    
       csmpasswds          : > CSM_PWL_P0  PAGE = 0
       csm_rsvd            : > CSM_RSVD    PAGE = 0
    
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM0       PAGE = 1
       .ebss               : > RAML2       PAGE = 1
       .esysmem            : > RAML2       PAGE = 1
    
       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHA      PAGE = 0
       .switch             : > FLASHA      PAGE = 0
    
       /* Allocate IQ math areas: */
       IQmath              : > FLASHA      PAGE = 0            /* Math Code */
       IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD
    
      /* Uncomment the section below if calling the IQNexp() or IQexp()
          functions from the IQMath.lib library in order to utilize the
          relevant IQ Math table in Boot ROM (This saves space and Boot ROM
          is 1 wait-state). If this section is not uncommented, IQmathTables2
          will be loaded into other memory (SARAM, Flash, etc.) and will take
          up space, but 0 wait-state is possible.
       */
       /*
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
       {
    
                  IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
    
       }
       */
        /* Uncomment the section below if calling the IQNasin() or IQasin()
           functions from the IQMath.lib library in order to utilize the
           relevant IQ Math table in Boot ROM (This saves space and Boot ROM
           is 1 wait-state). If this section is not uncommented, IQmathTables2
           will be loaded into other memory (SARAM, Flash, etc.) and will take
           up space, but 0 wait-state is possible.
        */
        /*
        IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
        {
    
                   IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
    
        }
        */
    
       /* .reset is a standard section used by the compiler.  It contains the */
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
    
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    好的、看起来您的程序从闪存运行、因此您的问题可能是由于需要将 ramfuncs 从闪存复制到 RAM 所致。

    在尝试运行我之前提到的示例时、您是否看到过同样的错误?  

    此致、

    Ben Collier