This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28027:使用28027的 SCI 通信

Guru**** 2756805 points

Other Parts Discussed in Thread: TMS320F28027

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1270102/tms320f28027-sci-communication-using-28027

器件型号:TMS320F28027

大家好!

我需要使用串行通信在 C20000 (TMS320F28027)和 ESP32之间传输数据。 显示的数据将显示在连接到 ESP32的 LCD 中。 我修改了 SCI 环回示例以传输单个整数值。 但是、LCD 中没有显示任何内容。  我正在附加主代码。 我已禁用回送。 在示例代码中是否还有其他事情要做。 谢谢

// TI File $Revision: /main/4 $
// Checkin $Date: October 6, 2010   14:43:12 $
//###########################################################################
//
// FILE:   Example_2802xSci_FFDLB_int.c
//
// TITLE:  DSP2802x Device SCI Digital Loop Back porgram.
//
//
// ASSUMPTIONS:
//
//    This program requires the DSP2802x header files.
//
//    This program uses the internal loop back test mode of the peripheral.
//    Other then boot mode pin configuration, no other hardware configuration
//    is required.
//
//    As supplied, this project is configured for "boot to SARAM"
//    operation.  The 2802x Boot Mode table is shown below.
//    For information on configuring the boot mode of an eZdsp,
//    please refer to the documentation included with the eZdsp,
//
//    $Boot_Table
//    While an emulator is connected to your device, the TRSTn pin = 1,
//    which sets the device into EMU_BOOT boot mode. In this mode, the
//    peripheral boot modes are as follows:
//
//      Boot Mode:   EMU_KEY        EMU_BMODE
//                   (0xD00)	     (0xD01)
//      ---------------------------------------
//      Wait		 !=0x55AA        X
//      I/O		     0x55AA	         0x0000
//      SCI		     0x55AA	         0x0001
//      Wait 	     0x55AA	         0x0002
//      Get_Mode	 0x55AA	         0x0003
//      SPI		     0x55AA	         0x0004
//      I2C		     0x55AA	         0x0005
//      OTP		     0x55AA	         0x0006
//      Wait		 0x55AA	         0x0007
//      Wait		 0x55AA	         0x0008
//      SARAM		 0x55AA	         0x000A	  <-- "Boot to SARAM"
//      Flash		 0x55AA	         0x000B
//	    Wait		 0x55AA          Other
//
//   Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger
//   according to the Boot Mode Table above. Build/Load project,
//   Reset the device, and Run example
//
//   $End_Boot_Table
//
//   Assumes the device has both SCI-A and SCI-B peripherals.
//
// DESCRIPTION:
//
//    This program is a SCI example that uses the internal loopback of
//    the peripheral.  Both interrupts and the SCI FIFOs are used.
//
//    A stream of data is sent and then compared to the recieved stream.
//
//    The SCI-A sent data looks like this:
//    00 01
//    01 02
//    02 03
//    ....
//    FE FF
//    FF 00
//    etc..
//
//
//
//    The pattern is repeated forever.
//
//    Watch Variables:
//       sdataA             Data being sent
//       rdataA             Data received
//       rdata_pointA       Keep track of where we are in the datastream
//                          This is used to check the incoming data
//###########################################################################
// Original Source by S.D.
//
// $TI Release: 2802x C/C++ Header Files and Peripheral Examples V1.29 $
// $Release Date: January 11, 2011 $
//###########################################################################

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

#define CPU_FREQ 	40E6        // Default = 40 MHz. Change to 60E6 for 60 MHz devices
#define LSPCLK_FREQ CPU_FREQ/4
#define SCI_FREQ 	100E3
#define SCI_PRD 	(LSPCLK_FREQ/(SCI_FREQ*8))-1

// Prototype statements for functions found within this file.
interrupt void sciaTxFifoIsr(void);
//interrupt void sciaRxFifoIsr(void);
interrupt void scibTxFifoIsr(void);
//interrupt void scibRxFifoIsr(void);
void scia_fifo_init(void);
void scib_fifo_init(void);
void error(void);

// Global variables
Uint16 sdataA[2];    // Send data for SCI-A
Uint16 rdataA[2];    // Received data for SCI-A
Uint16 rdata_pointA; // Used for checking the received data

void main(void)
{
   Uint16 i;

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2802x_SysCtrl.c file.
   InitSysCtrl();

// Step 2. Initalize GPIO:
// This example function is found in the DSP2802x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();
// Setup only the GP I/O only for SCI-A and SCI-B functionality
// This function is found in DSP2802x_Sci.c
   InitSciGpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2802x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in DSP2802x_DefaultIsr.c.
// This function is found in DSP2802x_PieVect.c.
   InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
   EALLOW;	// This is needed to write to EALLOW protected registers
 //  PieVectTable.SCIRXINTA = &sciaRxFifoIsr;
   PieVectTable.SCITXINTA = &sciaTxFifoIsr;
   EDIS;   // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2802x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
   scia_fifo_init();  // Init SCI-A

// Step 5. User specific code, enable interrupts:

// Init send data.  After each transmission this data
// will be updated for the next transmission
   for(i = 0; i<2; i++)
   {
      sdataA[i] = i;
   }

   rdata_pointA = sdataA[0];
// Enable interrupts required for this example
   PieCtrlRegs.PIECTRL.bit.ENPIE = 1;   // Enable the PIE block
   PieCtrlRegs.PIEIER9.bit.INTx1=1;     // PIE Group 9, INT1
   PieCtrlRegs.PIEIER9.bit.INTx2=1;     // PIE Group 9, INT2
   IER = 0x100;	// Enable CPU INT
   EINT;

// Step 6. IDLE loop. Just sit and loop forever (optional):
	for(;;);

}

void error(void)
{
    asm("     ESTOP0"); // Test failed!! Stop!
    for (;;);
}

interrupt void sciaTxFifoIsr(void)
{
    Uint16 i=3108;

    SciaRegs.SCITXBUF=i;     // Send data
	SciaRegs.SCIFFTX.bit.TXFFINTCLR=1;	// Clear SCI Interrupt flag
	PieCtrlRegs.PIEACK.all|=0x100;      // Issue PIE ACK
}

//interrupt void sciaRxFifoIsr(void)
//{
//    Uint16 i;
//	for(i=0;i<2;i++)
//	{
//	   rdataA[i]=SciaRegs.SCIRXBUF.all;	 // Read data
//	}
//	for(i=0;i<2;i++)                     // Check received data
//	{
//	   if(rdataA[i] != ( (rdata_pointA+i) & 0x00FF) ) error();
//	}
//	rdata_pointA = (rdata_pointA+1) & 0x00FF;
//
//	SciaRegs.SCIFFRX.bit.RXFFOVRCLR=1;   // Clear Overflow flag
//	SciaRegs.SCIFFRX.bit.RXFFINTCLR=1;   // Clear Interrupt flag
//
//	PieCtrlRegs.PIEACK.all|=0x100;       // Issue PIE ack
//}

void scia_fifo_init()
{
   SciaRegs.SCICCR.all =0x0007;   // 1 stop bit,  No loopback
                                  // No parity,8 char bits,
                                  // async mode, idle-line protocol
   SciaRegs.SCICTL1.all =0x0003;  // enable TX, RX, internal SCICLK,
                                  // Disable RX ERR, SLEEP, TXWAKE
   SciaRegs.SCICTL2.bit.TXINTENA =1;
   SciaRegs.SCICTL2.bit.RXBKINTENA =1;

  // SciaRegs.SCIHBAUD = 0x0000;This is the default value in the programme
   SciaRegs.SCILBAUD = SCI_PRD;// This defines the baud rate for 100k.This is the default value in the programme

   
   SciaRegs.SCIHBAUD    =0x0000;  // 9600 baud @LSPCLK = 15MHz (60 MHz SYSCLK).
   SciaRegs.SCILBAUD    =0x00C2;


   //SciaRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back

   SciaRegs.SCICCR.bit.LOOPBKENA =0; // Disable loopback

   SciaRegs.SCIFFTX.all=0xC022;
   SciaRegs.SCIFFRX.all=0x0022;
   SciaRegs.SCIFFCT.all=0x00;

   SciaRegs.SCICTL1.all =0x0023;     // Relinquish SCI from Reset
   SciaRegs.SCIFFTX.bit.TXFIFOXRESET=1;
   SciaRegs.SCIFFRX.bit.RXFIFORESET=1;

}

//===========================================================================
// No more.
//===========================================================================

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Sachin:

    您能否使用默认示例和电路板进行测试、看看它是否起作用?

    此致、

    文斯

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Vince,

    我运行了 带中断的 SCI 环回的默认示例。 手表寄存器正确显示了 sdataA 和 rdataA 的值。 我使用 GPIO 28 29和 GND 进行连接。 不过、在 ESP32中未收到任何信息。 我正在附加代码。 波特率为9600。 我使用的是 TMS320F28027的 Lauchpad。 还有没有其他事情要做

    // TI File $Revision: /main/4 $
    // Checkin $Date: October 6, 2010   14:43:12 $
    //###########################################################################
    //
    // FILE:   Example_2802xSci_FFDLB_int.c
    //
    // TITLE:  DSP2802x Device SCI Digital Loop Back porgram.
    //
    //
    // ASSUMPTIONS:
    //
    //    This program requires the DSP2802x header files.
    //
    //    This program uses the internal loop back test mode of the peripheral.
    //    Other then boot mode pin configuration, no other hardware configuration
    //    is required.
    //
    //    As supplied, this project is configured for "boot to SARAM"
    //    operation.  The 2802x Boot Mode table is shown below.
    //    For information on configuring the boot mode of an eZdsp,
    //    please refer to the documentation included with the eZdsp,
    //
    //    $Boot_Table
    //    While an emulator is connected to your device, the TRSTn pin = 1,
    //    which sets the device into EMU_BOOT boot mode. In this mode, the
    //    peripheral boot modes are as follows:
    //
    //      Boot Mode:   EMU_KEY        EMU_BMODE
    //                   (0xD00)	     (0xD01)
    //      ---------------------------------------
    //      Wait		 !=0x55AA        X
    //      I/O		     0x55AA	         0x0000
    //      SCI		     0x55AA	         0x0001
    //      Wait 	     0x55AA	         0x0002
    //      Get_Mode	 0x55AA	         0x0003
    //      SPI		     0x55AA	         0x0004
    //      I2C		     0x55AA	         0x0005
    //      OTP		     0x55AA	         0x0006
    //      Wait		 0x55AA	         0x0007
    //      Wait		 0x55AA	         0x0008
    //      SARAM		 0x55AA	         0x000A	  <-- "Boot to SARAM"
    //      Flash		 0x55AA	         0x000B
    //	    Wait		 0x55AA          Other
    //
    //   Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger
    //   according to the Boot Mode Table above. Build/Load project,
    //   Reset the device, and Run example
    //
    //   $End_Boot_Table
    //
    //   Assumes the device has both SCI-A and SCI-B peripherals.
    //
    // DESCRIPTION:
    //
    //    This program is a SCI example that uses the internal loopback of
    //    the peripheral.  Both interrupts and the SCI FIFOs are used.
    //
    //    A stream of data is sent and then compared to the recieved stream.
    //
    //    The SCI-A sent data looks like this:
    //    00 01
    //    01 02
    //    02 03
    //    ....
    //    FE FF
    //    FF 00
    //    etc..
    //
    //
    //
    //    The pattern is repeated forever.
    //
    //    Watch Variables:
    //       sdataA             Data being sent
    //       rdataA             Data received
    //       rdata_pointA       Keep track of where we are in the datastream
    //                         This is used to check the incoming data
    //###########################################################################
    // Original Source by S.D.
    //
    // $TI Release: 2802x C/C++ Header Files and Peripheral Examples V1.29 $
    // $Release Date: January 11, 2011 $
    //###########################################################################
    
    #include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
    
    #define CPU_FREQ 	40E6        // Default = 40 MHz. Change to 60E6 for 60 MHz devices
    #define LSPCLK_FREQ CPU_FREQ/4
    #define SCI_FREQ 	100E3
    #define SCI_PRD 	(LSPCLK_FREQ/(SCI_FREQ*8))-1
    
    // Prototype statements for functions found within this file.
    interrupt void sciaTxFifoIsr(void);
    interrupt void sciaRxFifoIsr(void);
    interrupt void scibTxFifoIsr(void);
    interrupt void scibRxFifoIsr(void);
    void scia_fifo_init(void);
    void scib_fifo_init(void);
    void error(void);
    
    // Global variables
    Uint16 sdataA[2];    // Send data for SCI-A
    Uint16 rdataA[2];    // Received data for SCI-A
    Uint16 rdata_pointA; // Used for checking the received data
    
    void main(void)
    {
       Uint16 i;
    
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the DSP2802x_SysCtrl.c file.
       InitSysCtrl();
    
    // Step 2. Initalize GPIO:
    // This example function is found in the DSP2802x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    // InitGpio();
    // Setup only the GP I/O only for SCI-A and SCI-B functionality
    // This function is found in DSP2802x_Sci.c
       InitSciGpio();
    
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
       DINT;
    
    // Initialize PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the DSP2802x_PieCtrl.c file.
       InitPieCtrl();
    
    // Disable CPU interrupts and clear all CPU interrupt flags:
       IER = 0x0000;
       IFR = 0x0000;
    
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in DSP2802x_DefaultIsr.c.
    // This function is found in DSP2802x_PieVect.c.
       InitPieVectTable();
    
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
       EALLOW;	// This is needed to write to EALLOW protected registers
       PieVectTable.SCIRXINTA = &sciaRxFifoIsr;
       PieVectTable.SCITXINTA = &sciaTxFifoIsr;
       EDIS;   // This is needed to disable write to EALLOW protected registers
    
    // Step 4. Initialize all the Device Peripherals:
    // This function is found in DSP2802x_InitPeripherals.c
    // InitPeripherals(); // Not required for this example
       scia_fifo_init();  // Init SCI-A
    
    // Step 5. User specific code, enable interrupts:
    
    // Init send data.  After each transmission this data
    // will be updated for the next transmission
       for(i = 0; i<2; i++)
       {
          sdataA[i] = i;
       }
    
       rdata_pointA = sdataA[0];
    // Enable interrupts required for this example
       PieCtrlRegs.PIECTRL.bit.ENPIE = 1;   // Enable the PIE block
       PieCtrlRegs.PIEIER9.bit.INTx1=1;     // PIE Group 9, INT1
       PieCtrlRegs.PIEIER9.bit.INTx2=1;     // PIE Group 9, INT2
       IER = 0x100;	// Enable CPU INT
       EINT;
    
    // Step 6. IDLE loop. Just sit and loop forever (optional):
    	for(;;);
    
    }
    
    void error(void)
    {
        asm("     ESTOP0"); // Test failed!! Stop!
        for (;;);
    }
    
    interrupt void sciaTxFifoIsr(void)
    {
        Uint16 i;
        for(i=0; i< 2; i++)
        {
     	   //SciaRegs.SCITXBUF=sdataA[i];     // Send data
            SciaRegs.SCITXBUF=100;
    	}
    
        for(i=0; i< 2; i++)                 //Increment send data for next cycle
        {
     	   //sdataA[i] = (sdataA[i]+1) & 0x00FF;
            sdataA[i] = 100;
    	}
    
    	SciaRegs.SCIFFTX.bit.TXFFINTCLR=1;	// Clear SCI Interrupt flag
    	PieCtrlRegs.PIEACK.all|=0x100;      // Issue PIE ACK
    }
    
    interrupt void sciaRxFifoIsr(void)
    {
        Uint16 i;
    	for(i=0;i<2;i++)
    	{
    	   rdataA[i]=SciaRegs.SCIRXBUF.all;	 // Read data
    	}
    	for(i=0;i<2;i++)                     // Check received data
    	{
    	   if(rdataA[i] != ( (rdata_pointA+i) & 0x00FF) ) error();
    	}
    	rdata_pointA = (rdata_pointA+1) & 0x00FF;
    
    	SciaRegs.SCIFFRX.bit.RXFFOVRCLR=1;   // Clear Overflow flag
    	SciaRegs.SCIFFRX.bit.RXFFINTCLR=1;   // Clear Interrupt flag
    
    	PieCtrlRegs.PIEACK.all|=0x100;       // Issue PIE ack
    }
    
    void scia_fifo_init()
    {
       SciaRegs.SCICCR.all =0x0007;   // 1 stop bit,  No loopback
                                      // No parity,8 char bits,
                                      // async mode, idle-line protocol
       SciaRegs.SCICTL1.all =0x0003;  // enable TX, RX, internal SCICLK,
                                      // Disable RX ERR, SLEEP, TXWAKE
       SciaRegs.SCICTL2.bit.TXINTENA =1;
       SciaRegs.SCICTL2.bit.RXBKINTENA =1;
       SciaRegs.SCIHBAUD    =0x0000;  // 9600 baud @LSPCLK = 15MHz (60 MHz SYSCLK).
       SciaRegs.SCILBAUD    =0x00C2;
       SciaRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back
       SciaRegs.SCIFFTX.all=0xC022;
       SciaRegs.SCIFFRX.all=0x0022;
       SciaRegs.SCIFFCT.all=0x00;
    
       SciaRegs.SCICTL1.all =0x0023;     // Relinquish SCI from Reset
       SciaRegs.SCIFFTX.bit.TXFIFOXRESET=1;
       SciaRegs.SCIFFRX.bit.RXFIFORESET=1;
    
    }
    
    //===========================================================================
    // No more.
    //===========================================================================
    
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在继续中、如果我使用 SCI_Echoback programm 示例、并将28027的 GPIO 28 29连接到 ESP32 Rx TX 引脚以及两个控制器的接地端。

    并将行修改为  

     SciaRegs.SCITXBUF=200;

    以传输值200。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Sachin:

    您能否提供 C2000 TX 引脚的示波器捕获? 想知道这是否可能是硬件问题。

    此致、

    文斯