This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28069:测量 ADC 值

Guru**** 2540720 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1270864/tms320f28069-measure-adc-value

器件型号:TMS320F28069

大家好! 我正在尝试检查 MCU 的 ADC 输出。 我使用了 AdcGTO 的可用 C2000示例。 我所做的就是为我的设置提供3.3V 和0V、并测量输出 ADC 值。 对于0V、它显示635数字输出、而对于3.3V、它显示3025值。 我使用万用表测量引脚上的电压、它会提供准确的值。 我想知道我为什么得到这个偏差值。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Bhashini,

    请参阅 ADC:初始转换公告在 F2806x 勘误表中、此注释介绍了如何进行初始转换。 您是在 序列中的每一次/多次转换、还是仅在序列中的第一次转换上看到此问题? 这 很可能就是原因。

    此致、

    阿米尔·奥马尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我每次都遇到这个错误。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Bhashini,

    您是否验证了 ADC 的 VREFHI 和 VREFLO 是正确的? 您使用的是内部还是外部基准? 您是否在使用中断、如果是、您是否已验证有足够的采样/保持时间对 ADC 进行采样?

    此致、

    阿米尔·奥马尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    //###########################################################################
    //
    // FILE:   Example_2806xAdcSoc.c
    //
    // TITLE:  ADC Start of Conversion Example
    //
    //! \addtogroup f2806x_example_list
    //! <h1> ADC Start of Conversion (adc_soc)</h1>
    //! 
    //! This ADC example uses ePWM1 to generate a periodic ADC SOC - ADCINT1.
    //! Two channels are converted, ADCINA4 and ADCINA2.
    //! 
    //! \b Watch \b Variables \n
    //! - Voltage1[10]    - Last 10 ADCRESULT0 values
    //! - Voltage2[10]    - Last 10 ADCRESULT1 values
    //! - ConversionCount - Current result number 0-9
    //! - LoopCount       - Idle loop counter
    //
    //###########################################################################
    // $TI Release: $
    // $Release Date: $
    // $Copyright:
    // Copyright (C) 2009-2023 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    
    //
    // Included Files
    //
    #include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
    
    //
    // Function Prototypes
    //
    __interrupt void adc_isr(void);
    void Adc_Config(void);
    
    //
    // Globals
    //
    Uint16 LoopCount;
    Uint16 ConversionCount;
    Uint16 Voltage1[10];
    Uint16 Voltage2[10];
    
    //
    // Main
    // 
    void main(void)
    {
        //
        // Step 1. Initialize System Control:
        // PLL, WatchDog, enable Peripheral Clocks
        // This example function is found in the F2806x_SysCtrl.c file.
        //
        InitSysCtrl();
    
        //
        // Step 2. Initialize GPIO:
        // This example function is found in the F2806x_Gpio.c file and
        // illustrates how to set the GPIO to it's default state.
        //
        // InitGpio();  // Skipped for this example
    
        //
        // Step 3. Clear all interrupts and initialize PIE vector table:
        // Disable CPU interrupts
        //
        DINT;
    
        //
        // Initialize the PIE control registers to their default state.
        // The default state is all PIE interrupts disabled and flags
        // are cleared.
        // This function is found in the F2806x_PieCtrl.c file.
        //
        InitPieCtrl();
    
        //
        // Disable CPU interrupts and clear all CPU interrupt flags:
        //
        IER = 0x0000;
        IFR = 0x0000;
    
        //
        // Initialize the PIE vector table with pointers to the shell Interrupt
        // Service Routines (ISR).
        // This will populate the entire table, even if the interrupt
        // is not used in this example.  This is useful for debug purposes.
        // The shell ISR routines are found in F2806x_DefaultIsr.c.
        // This function is found in F2806x_PieVect.c.
        //
        InitPieVectTable();
    
        //
        // Interrupts that are used in this example are re-mapped to
        // ISR functions found within this file.
        //
        EALLOW;  // This is needed to write to EALLOW protected register
        PieVectTable.ADCINT1 = &adc_isr; //interrupt service request
        EDIS;    // This is needed to disable write to EALLOW protected registers
    
        //
        // Step 4. Initialize all the Device Peripherals:
        // This function is found in F2806x_InitPeripherals.c
        // InitPeripherals(); // Not required for this example
        //
        InitAdc();  // For this example, init the ADC
        AdcOffsetSelfCal();//ADC Zero Offset Calibration
    
        //
        // Step 5. User specific code, enable interrupts:
        //
    
        //
        // Enable ADCINT1 in PIE
        //
        PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
        IER |= M_INT1; 					   // Enable CPU Interrupt 1
        EINT;          					   // Enable Global interrupt INTM
        ERTM;          					   // Enable Global realtime interrupt DBGM
    
        LoopCount = 0;
        ConversionCount = 0;
    
        //
        // Configure ADC
        //
        EALLOW;
        AdcRegs.ADCCTL2.bit.ADCNONOVERLAP = 1; // Enable non-overlap mode - overlap sample is not allowed
        
        //
        // ADCINT1 trips after AdcResults latch
        //
        AdcRegs.ADCCTL1.bit.INTPULSEPOS	= 1; // INt Pulse generation occurs 1 cycle prior to ADC result latching into its result register
        
        AdcRegs.INTSEL1N2.bit.INT1E     = 1;  // Enabled ADCINT1
        AdcRegs.INTSEL1N2.bit.INT1CONT  = 0;  // Disable ADCINT1 Continuous mode
        
        //
        // setup EOC1 to trigger ADCINT1 to fire
        //
        AdcRegs.INTSEL1N2.bit.INT1SEL 	= 1;
        
        AdcRegs.ADCSOC0CTL.bit.CHSEL 	= 4;  // set SOC0 channel select to ADCINA4
        AdcRegs.ADCSOC1CTL.bit.CHSEL 	= 2;  // set SOC1 channel select to ADCINA2
        
        //
        // set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts
        // first then SOC1
        //
        AdcRegs.ADCSOC0CTL.bit.TRIGSEL 	= 5;
        
        //
        // set SOC1 start trigger on EPWM1A, due to round-robin SOC0 converts 
        // first then SOC1
        //
        AdcRegs.ADCSOC1CTL.bit.TRIGSEL 	= 5;
        
        //
        // set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
        //
        AdcRegs.ADCSOC0CTL.bit.ACQPS 	= 6;
        
        //
        // set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
        //    
        AdcRegs.ADCSOC1CTL.bit.ACQPS 	= 6;
        EDIS;
    
        //
        // Assumes ePWM1 clock is already enabled in InitSysCtrl();
        //
        EPwm1Regs.ETSEL.bit.SOCAEN	= 1;		// Enable SOC on A group
        EPwm1Regs.ETSEL.bit.SOCASEL	= 4;		// Select SOC from CMPA on upcount
        EPwm1Regs.ETPS.bit.SOCAPRD 	= 1;		// Generate pulse on 1st event
        EPwm1Regs.CMPA.half.CMPA 	= 0x0080;	// Set compare A value
        EPwm1Regs.TBPRD 			= 0xFFFF;	// Set period for ePWM1
        EPwm1Regs.TBCTL.bit.CTRMODE	= 0;		// count up and start
    
        //
        // Wait for ADC interrupt
        //
        for(;;)
        {
            LoopCount++;
        }
    }
    
    //
    // adc_isr - 
    //
    __interrupt void
    adc_isr(void)
    {
        Voltage1[ConversionCount] = AdcResult.ADCRESULT0;
        Voltage2[ConversionCount] = AdcResult.ADCRESULT1;
        
        //
        // If 20 conversions have been logged, start over
        //
        if(ConversionCount == 9)
        {
            ConversionCount = 0;
        }
        else
        {
            ConversionCount++;
        }
    
        //
        // Clear ADCINT1 flag reinitialize for next SOC
        //
        AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
        
        PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;   // Acknowledge interrupt to PIE
    
        return;
    }
    
    //
    // End of File
    //
    
    

    1.您好。 上面是我用于测试的代码。 我使用了 TMS320F28069 开发板、并为 ADCINA4和 ADCINA2引脚提供3.3V 和0V 电压。 我使用开发板中的3.3V 引脚提供3.3V 电压、并通过接地端提供0V 电压。 我使用跳线连接了这些引脚。 然后构建和调试上述示例、并使用实时表达式查看 Voltage1和 Voltage2的值。 但根据计算、0V 的预期值为0、3.3V 的预期值为4095。 但我没有在实时表达式中观察到这些值。 我需要首先解决该误差。

    2.然后我需要更改上述代码以显示 ADCINB1的输出,即上述 MCU 中的29个引脚。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Bhashini,

    您是否已经 验证 ACQPS 足以用于连接到引脚的信号? 该值根据提供该电压的电路的阻抗进行设置、 有关详细信息、请参阅第8.2.1节"ADC 采集(采样保持)窗口"。

    您使用的器件是哪种类型的器件、它是 controlCARD 吗? 此外、您能否向我展示0V 和3.3V 信号范围的图像? 您是否还看过了器件的电源轨范围、以确保 它们处于预期的范围内?

    此致、

    阿米尔·奥马尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Omer,感谢你的支持。 当我将 ACQPS 更改为25时、它会按预期工作。 非常感谢。