This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28388D:无法编程和引导至 SSBL

Guru**** 2771175 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1270866/tms320f28388d-unable-to-program-and-boot-to-ssbl

器件型号:TMS320F28388D

这是以下主题的后续问题

e2e.ti.com/.../4708780

因此、正如以上线程的最后一个注释所述、

1.我们尝试了启用 ECC 和编程、但失败了、因为数据块尚未写入、引导失败、所有扇区都按8对齐、请在下面找到链接器文件

MEMORY
{
/* Flash sectors */
CMBANK0_RESETISR : origin = 0x00200000, length = 0x00000064 /* Boot to Flash Entry Point */
CMBANK0_SECTOR0 : origin = 0x00200064, length = 0x00003F93
CMBANK0_SECTOR1 : origin = 0x00204000, length = 0x00004000
CMBANK0_SECTOR2 : origin = 0x00208000, length = 0x00004000
CMBANK0_SECTOR3 : origin = 0x0020C000, length = 0x00004000
CMBANK0_SECTOR4 : origin = 0x00210000, length = 0x00010000
CMBANK0_SECTOR5 : origin = 0x00220000, length = 0x00010000
CMBANK0_SECTOR6 : origin = 0x00230000, length = 0x00010000
CMBANK0_SECTOR7 : origin = 0x00240000, length = 0x00010000
CMBANK0_SECTOR8 : origin = 0x00250000, length = 0x00010000
CMBANK0_SECTOR9 : origin = 0x00260000, length = 0x00010000
CMBANK0_SECTOR10 : origin = 0x00270000, length = 0x00004000
CMBANK0_SECTOR11 : origin = 0x00274000, length = 0x00004000
CMBANK0_SECTOR12 : origin = 0x00278000, length = 0x00004000
CMBANK0_SECTOR13 : origin = 0x0027C000, length = 0x00004000

C1RAM : origin = 0x1FFFC000, length = 0x00001FFF
C0RAM : origin = 0x1FFFE000, length = 0x00001FFF

BOOT_RSVD : origin = 0x20000000, length = 0x00000800 /* Part of S0, BOOT rom will use this for stack */
SRAM : origin = 0x20000800, length = 0x0000F7FF
E0RAM : origin = 0x20010000, length = 0x00003FFF

CPU1TOCMMSGRAM0 : origin = 0x20080000, length = 0x00000800
CPU1TOCMMSGRAM1 : origin = 0x20080800, length = 0x00000800
CMTOCPU1MSGRAM0 : origin = 0x20082000, length = 0x00000800
CMTOCPU1MSGRAM1 : origin = 0x20082800, length = 0x00000800
CPU2TOCMMSGRAM0 : origin = 0x20084000, length = 0x00000800
CPU2TOCMMSGRAM1 : origin = 0x20084800, length = 0x00000800
CMTOCPU2MSGRAM0 : origin = 0x20086000, length = 0x00000800
CMTOCPU2MSGRAM1 : origin = 0x20086800, length = 0x00000800
}

SECTIONS
{
.resetisr : > CMBANK0_RESETISR,FILL=0
.vftable : > CMBANK0_SECTOR3,ALIGN(16) /* Application placed vector table in Flash, this shall not be collided with any other flash sectors*/
.vtable : > E0RAM /* Application placed vector table in RAM*/


.text : >> CMBANK0_SECTOR2,ALIGN(16)
.cinit : > CMBANK0_SECTOR1,ALIGN(16)
.pinit : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1,ALIGN(16)
.switch : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1,ALIGN(16)
.text : > CMBANK0_SECTOR3, PAGE= 0, ALIGN(16) /* Here ALIGN(8) makes sure that .text section starts on a 128-bit aligned memory address*/
//.text : > CMBANK0_SECTOR3, PAGE= 0, ALIGN(8)
.sysmem : > E0RAM
.binit : > CMBANK0_SECTOR1

.stack : > C0RAM
.ebss : > C0RAM
.econst : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1 ,ALIGN(16)
.esysmem : > C0RAM
.data : > E0RAM
.bss : > E0RAM
.const : {} LOAD = CMBANK0_SECTOR0 | CMBANK0_SECTOR1 |CMBANK0_SECTOR2 ,ALIGN(16)
RUN = E0RAM,
LOAD_START(constLoadStart),
LOAD_SIZE(constLoadSize),
LOAD_END(constLoadEnd),
RUN_START(constRunStart),
RUN_SIZE(constRunSize),
RUN_END(constRunEnd)

MSGRAM_CM_TO_CPU1 : > CMTOCPU1MSGRAM0, type=NOINIT
MSGRAM_CM_TO_CPU2 : > CMTOCPU2MSGRAM0, type=NOINIT
MSGRAM_CPU1_TO_CM : > CPU1TOCMMSGRAM0, type=NOINIT
MSGRAM_CPU2_TO_CM : > CPU2TOCMMSGRAM0, type=NOINIT

.TI.ramfunc : {} LOAD = CMBANK0_SECTOR0 | CMBANK0_SECTOR1 | CMBANK0_SECTOR2 ,
RUN = E0RAM,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

2.您可以复查代码 并指出我需要在启用 ECC 方法中对闪存成功进行更改的地方

数据将来自 CPU1 IPC 1024个块用于复制数据函数、其中8个字节的数据将通过 Flash_data_program_8函数传递并写入闪存

//Main //
int main(void)
{
    Fapi_FlashStatusWordType oFlashStatusWord;

    //  ///////////////////////////////////////
    // Initializing the CM. Loading the required functions to SRAM.
    //
    CM_init();

    isWD_Reset();

    //
    // Enable processor interrupts.
    //
    Interrupt_enableInProcessor();

    //CM- CPU1
    IPC_clearFlagLtoR(IPC_CM_L_CPU1_R, IPC_FLAG_ALL);
    IPC_registerInterrupt(IPC_CM_L_CPU1_R, IPC_INT0, IPC_CPU1_CM_ISR0);

    //falsh module initialization//
    Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, 2);
    initFlashSectors();
    Flash_enableECC(FLASH0ECC_BASE);
//    Flash_disableECC(FLASH0ECC_BASE);

    Flash_claimPumpSemaphore(FLASH_CM_WRAPPER);

    while(1)
    {
        Fapi_doBlankCheck((uint32_t *)0x0027C000, 1, &oFlashStatusWord);

          if((oFlashStatusWord.au32StatusWord[1] & 0x0000FFFF) == BOOT_MODE_CD_WORD)
          {

              if( (!gis_WD_Reset) )
              {
                  IPC_sync(IPC_CM_L_CPU1_R, IPC_FLAG28);
                  IPC_sync(IPC_CM_L_CPU2_R, IPC_FLAG29);
              }
              Flash_releasePumpSemaphore();
              entryAddress = 0x210001;
              ( (void (*)(void))entryAddress)();

          }
          else
          {
              ;
          }

    }
}

//Flash Sector initialization//
void initFlashSectors(void){
    Fapi_StatusType  oReturnCheck;

   //
   // Initialize the Flash API by providing the Flash register base address
   // and operating frequency(in MHz).
   // This function is required to initialize the Flash API based on CM
   // operating frequency before any other Flash API operation can be performed.
   // This function must also be called whenever System frequency or RWAIT is
   // changed.
   //
   oReturnCheck = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS,
                                     CM_CLK_FREQ/1000000U);

   if(oReturnCheck != Fapi_Status_Success)
   {
       //
       // Check Flash API documentation for possible errors
       //
//       exampleError(oReturnCheck);
   }

   //
   // Initialize the Flash banks and FMC for erase and program operations.
   // Fapi_setActiveFlashBank() function sets the Flash banks and FMC for
   // further Flash operations to be performed on the banks.
   //
   oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);

   if(oReturnCheck != Fapi_Status_Success)
   {
       //
       // Check Flash API documentation for possible errors
       //
//       exampleError(oReturnCheck);
   }

}

bool Flash_data_program_8(uint32 Flash_sector, uint8 *Buffer, uint8 words)
{
//    uint16 i = 0;
    uint32 u32Index = 0;
    //  uint16 i = 0;
    uint32 *Buffer32 = (uint32 *) Buffer;
    Fapi_StatusType oReturnCheck;
    volatile Fapi_FlashStatusType oFlashStatus;
    Fapi_FlashStatusWordType oFlashStatusWord;


    if((Flash_sector >= 0x00210000) && (Flash_sector <= 0x00278000) )
    {
    oReturnCheck = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS,
                                      200);

    if(oReturnCheck != Fapi_Status_Success)
    {
        //
        // Check Flash API documentation for possible errors
        //
//        return false;

//        Example_Error(oReturnCheck);
    }

    //
    // Initialize the Flash banks and FMC for erase and program operations.
    // Fapi_setActiveFlashBank() function sets the Flash banks and FMC for
    // further Flash operations to be performed on the banks.
    //
    oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);

    if(oReturnCheck != Fapi_Status_Success)
    {
//        return false;

        //
        // Check Flash API documentation for possible errors
        //
//        Example_Error(oReturnCheck);
    }
    oReturnCheck = Fapi_issueProgrammingCommand((uint32 *)Flash_sector,Buffer,
                                                words, 0, 0, Fapi_DataOnly);

    //
    // Wait until the Flash program operation is over
    //
    while(Fapi_checkFsmForReady() == Fapi_Status_FsmBusy);

    if(oReturnCheck != Fapi_Status_Success)
    {
//        return false;

        //
        // Check Flash API documentation for possible errors
        //
//        Example_Error(oReturnCheck);
    }

    //
    // Read FMSTAT register contents to know the status of FSM after
    // program command to see if there are any program operation related
    // errors
    //
    oFlashStatus = Fapi_getFsmStatus();
    if(oFlashStatus != 0)
    {
//        return false;

        //
        // Check FMSTAT and debug accordingly
        //
//        FMSTAT_Fail();
    }


    //
    // Verify the values programmed.  The Program step itself does a verify
    // as it goes.  This verify is a 2nd verification that can be done.
    //
//    oReturnCheck = Fapi_doVerify((uint32 *) Flash_sector, words / 4,
//                                     Buffer, &oFlashStatusWord);
//
//    if (oReturnCheck != Fapi_Status_Success)
//    {
//        return FALSE;
//        //   Example_Error(oReturnCheck);
//    }
    oReturnCheck = Fapi_doVerifyByByte((uint32_t *)Flash_sector, words, Buffer, &oFlashStatusWord);
        if (oReturnCheck != Fapi_Status_Success)
        {
            write_status[2]=1;
            write_status[5] =iteration_cnt;
                return false;
        }

    return true;
    }
    write_status[4] = iteration_cnt;
    return false;

}

/**
 * @brief: this function it will handle the given hex data as per boot structure of TI controller
 *         it will validate key value and then write hex data as given block size and block address.
 * @author <19 FEB 2021 ; Basweshwar >
 * @return after successful completion return TRUE otherwise FALSE.
 */
#ifdef __cplusplus
#pragma CODE_SECTION(".TI.ramfunc");
#else
#pragma CODE_SECTION(copy_data, ".TI.ramfunc");
#endif
bool copy_data(uint8_t * aBuffer)
{
/* this function it will handle the given hex data as per boot structure of TI controller
 * it will validate key value and then write hex data as given block size and block address by
 * calling Flash_data_program_8 function*/
}

谢谢。此致、

普拉奈

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Pranay:

    您是否可以在代码中添加一个检查、以确保传递给编程命令的每个地址都是对齐的地址(64位对齐、因为您说过 一次编程为64位)?

    您是否尝试一次编程128位(16字节)?

    谢谢。此致、
    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vamsi:

    您能否在代码中加入一个检查,以确保传递给 program 命令的每个地址都是对齐的地址(64位对齐,因为您说是 一次编程64位)?

    在复制数据函数中,我们将检查并传递与64位对齐的地址到程序命令。

    您是否尝试一次编程128位(16字节)?

    否,我们还没有尝试一次编程128位。

    谢谢。此致、

    普拉奈

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Pranay:

    正如离线讨论的那样、将请求的文件发送给我、我们可以根据需要在会议中进行进一步分析。

    谢谢。此致、

    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Pranay:

    由于我没有收到您的反馈、我现在将关闭此帖子。

    您可以根据需要打开新帖子。

    谢谢。此致、
    瓦姆西