This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28035:带有闪存的 EEPROM 仿真不能可靠地工作

Guru**** 1858750 points
Other Parts Discussed in Thread: TMS320F28035
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1274603/tms320f28035-eeprom-emulation-with-flash-not-working-reliably

器件型号:TMS320F28035

在基于 TMS320F28035的项目中、我将尝试在片上闪存中模拟 EEPROM。   我遵循了应用手册- 应用报告
 《用于第2代 C2000实时 MCU 的 EEPROM 仿真》(SPRab69a1)。  我修改了以下 文件以与我的代码集成

DSP280x_Memcopy.c
F280xx_EEPROM.c
F280xx_EEPROM.h

F28035.cmd

我正在使用扇区 H ( FLASHH   : origin = 0x3E8000, length = 0x002000 )

在运行代码时、EEPROM 写入操作前3到6次、然后在状态代码为30或31时失败、此外代码也会崩溃和控制器复位。

附加文件。  如果您能帮助我找到崩溃的原因、请表示感谢。  

此致、

Rameshe2e.ti.com/.../0636.F280xx_5F00_EEPROM.ce2e.ti.com/.../4341.F280xx_5F00_EEPROM.he2e.ti.com/.../DSP280x_5F00_MemCopy.c

*
// TI File $Revision: /main/4 $
// Checkin $Date: November 9, 2009   15:09:12 $
//###########################################################################
//
// FILE:	F2808.cmd
//
// TITLE:	Linker Command File For F2808 Device
//
//###########################################################################
// $TI Release: F2803x Support Library v2.01.00.00 $
// $Release Date: Sun Sep 29 07:32:51 CDT 2019 $
// $Copyright:
// Copyright (C) 2009-2019 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
*/

/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in <base>\DSP2803x_Headers\cmd
//
// For BIOS applications add:      DSP2803x_Headers_BIOS.cmd
// For nonBIOS applications add:   DSP2803x_Headers_nonBIOS.cmd
========================================================= */

/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map                                    */

/* Uncomment this line to include file only for non-BIOS applications */
/* -l DSP2803x_Headers_nonBIOS.cmd */

/* Uncomment this line to include file only for BIOS applications */
/* -l DSP2803x_Headers_BIOS.cmd */

/* 2) In your project add the path to <base>\DSP2803x_headers\cmd to the
   library search path under project->build options, linker tab,
   library search path (-i).
/*========================================================= */

/* Define the memory block start/length for the F28035
   PAGE 0 will be used to organize program sections
   PAGE 1 will be used to organize data sections

   Notes:
         Memory blocks on F2803x are uniform (ie same
         physical memory) in both PAGE 0 and PAGE 1.
         That is the same memory region should not be
         defined for both PAGE 0 and PAGE 1.
         Doing so will result in corruption of program
         and/or data.

         L0 memory block is mirrored - that is
         it can be accessed in high memory or low memory.
         For simplicity only one instance is used in this
         linker file.

         Contiguous SARAM memory blocks or flash sectors can be
         be combined if required to create a larger memory block.
*/

MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
   RAML0       : origin = 0x008000, length = 0x000800     /* on-chip RAM block L0 */
   RAML1       : origin = 0x008800, length = 0x000400     /* on-chip RAM block L1 */
   OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
   FLASHH      : origin = 0x3E8000, length = 0x002000     /* on-chip FLASH */
   FLASHG      : origin = 0x3EA000, length = 0x002000     /* on-chip FLASH */
   FLASHF      : origin = 0x3EC000, length = 0x002000     /* on-chip FLASH */
   FLASHE      : origin = 0x3EE000, length = 0x002000     /* on-chip FLASH */
   FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASH */
   FLASHC      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASH */
   FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
   CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */

   IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA	  /* IQ Math Tables in Boot ROM */

   ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */

PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */
   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
   RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
   RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAML2       : origin = 0x008C00, length = 0x000400     /* on-chip RAM block L2 */
   RAML3       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L3 */
   FLASHB      : origin = 0x3F4000, length = 0x002000     /* on-chip FLASH */

}

/* Allocate sections to memory blocks.
   Note:
         codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                   execution when booting to flash
         ramfuncs  user defined section to store functions that will be copied from Flash into RAM
*/

SECTIONS
{

   /* Allocate program areas: */
   .cinit              : > FLASHA      PAGE = 0
   .pinit              : > FLASHA,     PAGE = 0
 /*  .text               : > FLASHA      PAGE = 0 */
   .text             : >> FLASHD | FLASHC | FLASHA,     PAGE = 0
   codestart           : > BEGIN       PAGE = 0
       Flash28_API:
   {
        -lFlash2803x_API_V100.lib(.econst)
        -lFlash2803x_API_V100.lib(.text)
   }                   LOAD = FLASHA,
                       RUN = RAML0,
                       LOAD_START(_Flash28_API_LoadStart),
                       LOAD_END(_Flash28_API_LoadEnd),
                       RUN_START(_Flash28_API_RunStart),
                       PAGE = 0

   ramfuncs            : LOAD = FLASHD,
                         RUN = RAML0,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0

   csmpasswds          : > CSM_PWL_P0  PAGE = 0
   csm_rsvd            : > CSM_RSVD    PAGE = 0

   /* Allocate uninitalized data sections: */
 /* .stack              : > RAMM1    PAGE = 1 */  /* change this to Raml3 */
    .stack              : > RAML3    PAGE = 1
 /*     .stack              : >> RAMM1 | RAMM0,   PAGE = 1 8/
 /*     .stack              : > RAMM0       PAGE = 1  */
   .ebss               : > RAML2       PAGE = 1
   .esysmem            : > RAML2       PAGE = 1

   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHA      PAGE = 0
   .switch             : > FLASHA      PAGE = 0

   /* Allocate IQ math areas: */
   IQmath              : > FLASHA      PAGE = 0            /* Math Code */
   IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD

  /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {

              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

   }
   */
    /* Uncomment the section below if calling the IQNasin() or IQasin()
       functions from the IQMath.lib library in order to utilize the
       relevant IQ Math table in Boot ROM (This saves space and Boot ROM
       is 1 wait-state). If this section is not uncommented, IQmathTables2
       will be loaded into other memory (SARAM, Flash, etc.) and will take
       up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {

               IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

    }
    */

   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Ramesh、

    我假设根据状态代码30和31、您指的是闪存 API 的返回状态:

    当您运行程序时、您是否验证了闪存已被擦除? 您在上面的代码的哪一行看到错误状态?

    运行代码时、EEPROM 写入操作前3到6次、然后失败、状态代码为30或31、代码也会崩溃和控制器重置。

    状态代码和崩溃/复位问题是否不存在?或者在出现错误状态时、代码会崩溃并复位? 您如何检测器件是否复位?

    此致、

    阿米尔·奥马尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Omer Amir:

    感谢您的快速响应。   

    "我假设根据状态代码30和31、您是指闪存 API 的返回状态:"

    可以。  我指的是闪存 API 的返回状态。

    实际上、我假定每次 从 CCS "运行"时、所有闪存存储器都被擦除(不确定我是否正确)。  我没有显式擦除该扇区。

    崩溃和错误状态一致。  只要闪存 API 返回错误状态、代码就会崩溃并复位。  我在代码中启用了看门狗。  不过、根据 API 文档、当调用 API 时会禁用看门狗。  复位后、我还可以看到 WDCR 寄存器中设置了 WDFLAG。

    此致、

    拉梅什

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我浏览了该位置的闪存、全部显示0xFFFF。

    在成功写入期间 、我可以看到如下所示的存储器

    0x003E8042
    00FF 0000 0000
    0000 0000 0000 8A08 FFFF
    0020 493E 0003 FFFF 8A0B
    0034 0100 001F FFFF FFFF
    FFFF FFFF FFFF FFFF FFFF FFFF
    FFFF FFFF FFFF FFFF FFFF

    失败后,每一页都填充了以下数据(不仅仅是我正在写的页面)。

    0000 0000 0000 0000 0000
    0000 0000 0000 8A08 FFFF
    0020 493E 0003 FFFF 8A0B
    0034 0100 001F FFFF FFFF
    FFFF FFFF FFFF FFFF FFFF FFFF
    FFFF FFFF FFFF FFFF FFFF

    附加监视窗口屏幕截图以跟踪组指针和页指针

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Ramesh、

    如果您单步执行代码、您能找出 闪存存储器在什么位置被擦除/编程吗? 闪存 擦除发生在扇区级别、因此看起来该程序在被擦除后未按预期发生。 如果我的理解不正确、请告诉我。

    此致、

    阿米尔·奥马尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Omer Amir:

    在 CCS 中下载代码期间、闪存存储器被擦除。  之后、它不会被擦除。  根据代码、擦除将在使用3个存储体且尚未达到该级别之后发生。  在第一个银行第3页或第二个银行第2页后出现该问题。  如果 我注释  EEPROM_Write(),代码不会崩溃。  所以我假设  EEPROM_Write ()存在一些问题;  

    此致、

    拉梅什  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Ramesh、

    您在最初的帖子中提到、您遵循了一份应用报告、然后根据您的程序进行了一些修改;在 阅读该文档时、您是否确认该项目运行良好? 您能否逐个测试您所做的更改(如果适用)?

    如果 我注释  eeprom_Write(),代码不会崩溃。  所以我的假设是  EEPROM_Write ()的一些问题; 

    您是否可以通过逐步执行函数并逐行运行来进一步缩小问题的范围? 理想情况下、我们应该找到导致问题的指令或指令集、然后在存储器中缩小问题的范围。

    此致、

    阿米尔·奥马尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Omer Amir:

    抱歉、 我是在度假。  我通过在调用    EEPROM_Write ();函数之前禁用中断来解决了问题。  就表示工作正常。

    此致、

    拉梅什