This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280049C:闪存 EEPROM 仿真配置

Guru**** 2568565 points
Other Parts Discussed in Thread: C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1276858/tms320f280049c-flash-eeprom-emulation-configuration

器件型号:TMS320F280049C
主题中讨论的其他器件:C2000WARE

您好!

我目前正在尝试将 C2000器件中闪存存储体的一个未使用扇区用于 EEPROM 仿真。 在研究这一点时、我收到了一个文档(SPRAB69A)、其中概述了对较旧的第2代器件的类似实现。

我打算使用最新的闪存 API 来修改该框架。 但是、在应用程序中运行此代码时遇到了持久的问题。 我一直收到错误消息"无法在此地址找到源文件。"

此外、当我尝试在代码中包含"Fapi_setActiveFlashBank"函数时、我遇到另一个错误:"#10099-D 程序将无法装入可用内存中、或者该段包含一个需要 trampoline 但无法为此段生成的调用站点。 对"Group_1"大小为0x933的段0进行对齐/分块运行放置失败。 可用内存范围:"

我附上了我的代码供您参考。

感谢您的帮助。

链接器代码:

MEMORY
{
PAGE 0 :

   RAMM0           	: origin = 0x0000F5, length = 0x00030B

   RAMLS0          	: origin = 0x008000, length = 0x000800
   RAMLS1          	: origin = 0x008800, length = 0x000800
   RAMLS2      		: origin = 0x009000, length = 0x000800
   RAMLS3      		: origin = 0x009800, length = 0x000800
   RAMLS4      		: origin = 0x00A000, length = 0x000800
   RESET           	: origin = 0x3FFFC0, length = 0x000002

#ifdef __TI_COMPILER_VERSION__
   #if __TI_COMPILER_VERSION__ >= 20012000
GROUP {      /* GROUP memory ranges for crc/checksum of entire flash */
   #endif
#endif
  /* BEGIN is used for the "boot to Flash" bootloader mode   */

   BEGIN           	: origin = 0x080000, length = 0x000002

   /* Flash sectors */
   /* BANK 0 */
   FLASH_BANK0_SEC0  : origin = 0x080002, length = 0x000FFE	/* on-chip Flash */
   FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC2  : origin = 0x082000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000	/* on-chip Flash */

   /* BANK 1 */
   FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0	/* on-chip Flash */
   FLASH_BANK1_SEC15_DO_NOT_USE     : origin = 0x09FFF0, length = 0x000010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

#ifdef __TI_COMPILER_VERSION__
  #if __TI_COMPILER_VERSION__ >= 20012000
}  crc(_ccs_flash_checksum, algorithm=C28_CHECKSUM_16)
  #endif
#endif

PAGE 1 :

   BOOT_RSVD       : origin = 0x000002, length = 0x0000F3     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */

   RAMLS5      : origin = 0x00A800, length = 0x000800
   RAMLS6      : origin = 0x00B000, length = 0x000800
   RAMLS7      : origin = 0x00B800, length = 0x000800

   RAMGS0      : origin = 0x00C000, length = 0x002000
   RAMGS1      : origin = 0x00E000, length = 0x002000
   RAMGS2      : origin = 0x010000, length = 0x002000
   RAMGS3      : origin = 0x012000, length = 0x002000
}


SECTIONS
{
   codestart        : > BEGIN,     PAGE = 0, ALIGN(4)
   .text            : >>FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3,   PAGE = 0, ALIGN(4)
   .cinit           : > FLASH_BANK0_SEC1,     PAGE = 0, ALIGN(4)
   .pinit           : > FLASH_BANK0_SEC1,     PAGE = 0, ALIGN(4)
   .switch          : > FLASH_BANK0_SEC1,     PAGE = 0, ALIGN(4)
   .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */

   .stack           : > RAMM1,     PAGE = 1
   .ebss            : > RAMLS5,    PAGE = 1
   .esysmem         : > RAMLS5,    PAGE = 1
   .econst          : > FLASH_BANK0_SEC4,    PAGE = 0, ALIGN(4)

   ramgs0           : > RAMGS0,    PAGE = 1
   ramgs1           : > RAMGS1,    PAGE = 1

   GROUP
   {
	.TI.ramfunc
	{ -l F021_API_F28004x_FPU32.lib}
	}
						 LOAD = FLASH_BANK0_SEC9 | FLASH_BANK0_SEC10 | FLASH_BANK0_SEC13,
                         RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(4)

   /* crc/checksum section configured as COPY section to avoid including in executable */
   .TI.memcrc          : type = COPY

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

头文件:

//############################################################################
//
// FILE:   F280xx_EEPROM.h
//
// TITLE:  Function Prototypes, Global Variables, Pointer Initialization
//		   and, Bank/Page Status Definitions  
//
//############################################################################
// Authors: Tim Love / Pradeep Shinde
// Release Date: Sep 2009 
//############################################################################


#include <F021_F28004x_C28x.h>

// Project specific defines
//#define SINGLE_BYTE 1
#define MULTI_BYTE  1

//Just for flash
#define FLASH_SECTOR    0x090000
#define RESET_BANK_POINTER Bank_Pointer = (uint16 *)FLASH_SECTOR	// Sector H
#define RESET_PAGE_POINTER Page_Pointer = (uint16 *)(FLASH_SECTOR+1)
#define END_OF_SECTOR 0x8FFFF;

//Only for ECC
#define ECC_BANK_BUFFER  (uint16*)0x0
#define ECC_PAGE_BUFFER  (uint16*)0x0

//#endif

// Bank/Page Status Definitions
#define EMPTY_BANK   0xFFFF
#define CURRENT_BANK 0xA00A
#define USED_BANK 	 0x0000
#define BLANK_PAGE 	 0xFFFF
#define CURRENT_PAGE 0x00FF
#define USED_PAGE    0x0000		

// Function Prototypes
extern void EEPROM_GetValidBank();
extern void EEPROM_Erase();
extern void EEPROM_Read();
extern void EEPROM_Write();
extern void EEPROM_UpdateBankStatus();
extern void EEPROM_UpdatePageStatus();
extern void EEPROM_GetSinglePointer(uint16 First_Call);
extern void EEPROM_ProgramSingleByte(uint16 data);

// Global Variables
extern uint16 *Bank_Pointer;
extern uint16 *Page_Pointer;
extern uint16 *Sector_End;
extern uint16 Read_Buffer[64];
extern uint16 Write_Buffer[64];

源文件:

//############################################################################
//
// FILE:   F280xx_EEPROM.c
//
// TITLE:  EEPROM Read, Write, and Erase Functions
//
//############################################################################
// Authors: Tim Love / Pradeep Shinde
// Release Date: Sep 2009
//############################################################################


#include "F280xx_EEPROM.h"						// EEPROM Include File

// Global Variables
uint16 Read_Buffer[64];
uint16 Write_Buffer[64];
uint16 Bank_Counter = 0;
uint16 Page_Counter = 0;
uint16 Bank_Status[1] = {0};
uint16 Page_Status[1] = {0};
uint16 *Bank_Pointer;
uint16 *Page_Pointer;
uint16 *Sector_End;

//Fapi_FlashStatusType FlashStatus;
Fapi_FlashStatusType ProgStatus;

// All Flash API functions need to be ran from internal RAM. Place all functions
// that contain Flash API calls in .TI.ramfunc to allow copy from Flash to RAM.
#pragma CODE_SECTION(EEPROM_Erase,".TI.ramfunc");
#pragma CODE_SECTION(EEPROM_Write,".TI.ramfunc");
#pragma CODE_SECTION(EEPROM_UpdateBankStatus,".TI.ramfunc");
#pragma CODE_SECTION(EEPROM_UpdatePageStatus,".TI.ramfunc");
#pragma CODE_SECTION(EEPROM_ProgramSingleByte,".TI.ramfunc");


//######################### EEPROM_GET_VALID_BANK ############################
void EEPROM_GetValidBank()
{
//Each page holds 64 data words
//Page size = Page_status word + 64W = 65W
//Bank Size = Bank_status word + 8 * Page size = 1 + 8*65 = 521W

	uint16 i;

   	RESET_BANK_POINTER;		// Reset Bank Pointer to enable search for current Bank
   	RESET_PAGE_POINTER;		// Reset Page Pointer to enable search for current Page

	// Find Current Bank 
	for(i=0;i<8;i++)
	{
		Bank_Status[0] = *(Bank_Pointer);		// Read contents of Bank Pointer
		
		if(Bank_Status[0] == EMPTY_BANK)		// Check for Unused Bank  
		{
			Bank_Counter = i;					// Set Bank Counter to number of current page								 	
			return;								// If Bank is Unused, return as EEPROM is empty
		}
	
		if(Bank_Status[0] == CURRENT_BANK)		// Check for In Use Bank 
		{
			Bank_Counter = i;					// Set Bank Counter to number of current bank
			Page_Pointer = Bank_Pointer + 1;	// Set Page Pointer to first page in current bank
			break;								// Break from loop as current bank has been found
		}

		if(Bank_Status[0] == USED_BANK)   		// Check for Used Bank											
			Bank_Pointer += 521; 				// If Bank has been used, set pointer to next bank		
	}

	// Find Current Page
	for(i=0;i<8;i++)
	{
		Page_Status[0] = *(Page_Pointer);		// Read contents of Page Pointer
		
		// Check for Blank Page or Current Page	
		if(Page_Status[0] == BLANK_PAGE || Page_Status[0] == CURRENT_PAGE)
		{
			Page_Counter = i;					// Set Page Counter to number of current page		
			break;								// Break from loop as current page has been found
		}

		if(Page_Status[0] == USED_PAGE)			// Check for Used Page
			Page_Pointer += 65;					// If page has been used, set pointer to next page
	}

	if (Bank_Counter==7 && Page_Counter==7)		// Check for full EEPROM
	{
		EEPROM_Erase();							// Erase flash sector being used as EEPROM
  		RESET_BANK_POINTER; 					// Reset Bank Pointer as EEPROM is empty
   		RESET_PAGE_POINTER;						// Reset Pank Pointer as EEPROM is empty
		asm(" ESTOP0");
	}
}
//######################### EEPROM_GET_VALID_BANK ############################


//############################# EEPROM_ERASE #################################
void EEPROM_Erase()
{
    Fapi_StatusType Status;

	Status = Fapi_issueAsyncCommandWithAddress((Fapi_EraseSector),(uint32 *)FLASH_SECTOR);

	while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){}

   	if(Status != Fapi_Status_Success) 		// If Erase fails halt program or handle error
   	{
      	asm(" ESTOP0");
   	} 
}
//############################# EEPROM_ERASE #################################


//############################# EEPROM_READ ##################################
void EEPROM_Read()
{
	uint16 i;

	EEPROM_GetValidBank();					// Find In Use Bank and Current Page

	// Transfer contents of Current Page to Read Buffer
	for(i=0;i<64;i++)
		Read_Buffer[i] = *(++Page_Pointer); 	
}
//############################# EEPROM_READ ##################################


//############################ EEPROM_WRITE ##################################
void EEPROM_Write()
{
	// Variables need for Flash API Functions
    Fapi_StatusType Status;
	uint32 Length;
//	Fapi_FlashStatusType ProgStatus;
	//Fapi_setActiveFlashBank(Fapi_FlashBank0);

	EEPROM_GetValidBank();					// Find In Use Bank and Current Page

    EEPROM_UpdatePageStatus();				// Update Page Status of previous page 
	EEPROM_UpdateBankStatus();				// Updage Bank Status of current and previous bank

	// Program data located in Write_Buffer to current page
	Length = 64;							// Set Length for programming
	Status = Fapi_issueProgrammingCommand((uint32 *)(Page_Pointer+1),Write_Buffer,Length,ECC_BANK_BUFFER,Length, Fapi_DataOnly);
	
	// Modify Page Status from Blank Page to Current Page if flash programming was successful
	if (Status == Fapi_Status_Success)
	{
		Page_Status[0] = CURRENT_PAGE;  	// Set Page Status to Current Page
		Length = 1;							// Set Length for programming status
		Status = Fapi_issueProgrammingCommand((uint32 *)Page_Pointer,Page_Status,Length,ECC_PAGE_BUFFER,Length, Fapi_DataOnly);
	}
}
//############################ EEPROM_WRITE ##################################


//###################### EEPROM_UPDATE_BANK_STATUS ###########################
void EEPROM_UpdateBankStatus()
{
	// Variables needed for Flash API Functions
	uint32 Length;

	Length = 1;								// Set Length for programming

	Bank_Status[0] = *(Bank_Pointer);		// Read Bank Status from Bank Pointer
	Page_Status[0] = *(Page_Pointer);		// Read Page Status from Page Pointer

	// Program Bank Status for Empty EEPROM
	if (Bank_Status[0] == EMPTY_BANK)		
	{	
		Bank_Status[0] = CURRENT_BANK;  	// Set Bank Status to In Use Bank
		
		// Program Bank Status to current bank
		Fapi_issueProgrammingCommand((uint32 *)Bank_Pointer,Bank_Status,Length,ECC_BANK_BUFFER,Length, Fapi_DataOnly);
		Page_Counter =0;
		Page_Pointer = Bank_Pointer + 1;	// Set Page Pointer to first page of current bank
	}	

	// Program Bank Status of full bank and following bank
	if (Bank_Status[0] == CURRENT_BANK && Page_Counter == 7)	
	{	
		Bank_Status[0] = USED_BANK;			// Set Bank Status to Used Bank
		
		// Program Bank Status to full bank			
		Fapi_issueProgrammingCommand((uint32 *)Bank_Pointer,Bank_Status,Length,ECC_BANK_BUFFER,Length, Fapi_DataOnly);
		
		Bank_Pointer +=521;					// Increment Bank Pointer to next bank
	
		Bank_Status[0] = CURRENT_BANK;		// Set Bank Status to In Use Bank
	
		// Program Bank Status to current bank		
		Fapi_issueProgrammingCommand((uint32 *)Bank_Pointer,Bank_Status,Length,ECC_BANK_BUFFER,Length, Fapi_DataOnly);

		Page_Counter = 0;
		Page_Pointer = Bank_Pointer +1;		// Set Page Pointer to first page of current bank
	}
}
//###################### EEPROM_UPDATE_BANK_STATUS ###########################


//###################### EEPROM_UPDATE_PAGE_STATUS ###########################
void EEPROM_UpdatePageStatus()
{
	// Variables needed for Flash API Functions
	uint16 Length;

	Bank_Status[0] = *(Bank_Pointer);		// Read Bank Status from Bank Pointer			
	Page_Status[0] = *(Page_Pointer);		// Read Page Status from Page Pointer

	// Check if Page Status is blank. If so return to EEPROM_WRITE.
	if(Page_Status[0] == BLANK_PAGE)
		return;
	
	// Program previous page's status to Used Page
	else
	{			
		Page_Status[0] = USED_PAGE; 		// Set Page Status to Used Page 	
		Length = 1;							// Set Length for programming 
		Fapi_issueProgrammingCommand((uint32 *)Page_Pointer,Page_Status,Length,ECC_BANK_BUFFER,Length, Fapi_DataOnly);
		Page_Pointer +=65;					// Increment Page Pointer to next page
	}
}
//###################### EEPROM_UPDATE_PAGE_STATUS ###########################


//###################### EEPROM_GET_SINGLE_POINTER ###########################
void EEPROM_GetSinglePointer(uint16 First_Call)
{
	uint16 *End_Address;

	End_Address = (uint16 *)END_OF_SECTOR;	// Set End_Address for sector

	if(First_Call == 1)						// If this is first call to function, find valid pointer
	{	
		RESET_BANK_POINTER;					// Reset Bank Pointer to beginning of sector
		while(*(Bank_Pointer) != 0xFFFF)	// Test each location for data
			Bank_Pointer++;					// Increment to next location
	}
		
	if(Bank_Pointer >= End_Address)			// Test if sector is full 
	{    
		EEPROM_Erase();						// Erase flash sector being used as EEPROM
  		RESET_BANK_POINTER; 				// Reset Bank Pointer as EEPROM is empty
   		asm(" ESTOP0");
	}
	
}
//###################### EEPROM_GET_SINGLE_POINTER ###########################


//##################### EEPROM_PROGRAM_SINGLE_BYTE ###########################
void EEPROM_ProgramSingleByte(uint16 data)
{
	// Variables needed for Flash API Functions
	uint32 Length;

	Write_Buffer[0] = data;					// Prepare data to be programmed
		
	Length = 1;								// Set Length for programming
	Fapi_issueProgrammingCommand((uint32 *)Bank_Pointer++,Write_Buffer,Length,ECC_BANK_BUFFER,Length, Fapi_DataOnly);
	EEPROM_GetSinglePointer(0);				// Test for full sector	
}
//##################### EEPROM_PROGRAM_SINGLE_BYTE ###########################

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    每当您进入闪存 API 库函数时、CCS 都会向您显示 "无法在此地址找到源文件"。 消息、因为闪存 API 源不可供其显示-这不是问题。  您可以忽略此警告。

    关于链接器错误: 只是说、为该输出段分配的存储器是不够的。  尝试合并几个存储器范围(以便适合该段)并将该段映射到新的大存储器范围。   

    另请注意、我们计划在即将发布的 C2000Ware 版本中发布 EEPROM 示例(针对 F28P65x 器件-但您应该能够针对 F28004x 轻松对其进行编辑)。

    谢谢。此致、

    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vamsi:

    以下是我立即尝试运行代码时收到的提示消息:C:/Users\...\Debug\project.out:{3}0x3fbd92{4}中没有"_system_post_cinit ()"的源可用  

    0x3fbd92{4}地址恰好位于引导 ROM 中。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此外、该代码会在没有 "Fapi_setActiveFlashBank"函数的情况下构建、但在图片中、它将生成所描述的错误消息。

    谢谢。此致、

    阿洛巴。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    有关引导 ROM 中登录执行错误的说明:如 TRM 的表 4-15所示。 等待点地址、地址0x3fbd92属于 ITRAP ISR。  

    这意味着 CPU 执行了一个非法指令。  在调用映射到.TI.ramfunc 段的任何函数之前、请检查是否执行了 memcpy ()。

    对于链接器错误、请遵循我之前提供的建议。

    谢谢。此致、

    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vamsi:

    感谢您的答复。 我已经尝试实施您的建议来解决链接器错误、但遗憾的是、仍然存在。

    关于`memcpy ()`函数,它不会在我的代码中的任何点执行,因为我不确定源或目的。

    请看一下我共享的命令文件吗? 您的建议将会非常有帮助。

    谢谢、此致、

    阿洛巴

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Atoba,

    请查看此常见问题解答一次:  

    如何将应用程序从 RAM 配置修改为闪存配置?: https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/878674 

    此外、您可以看看任何 C2000Ware 示例-它们应该具有闪存构建配置(如上面的常见问题解答中所述)。 您可以单步执行并了解常见问题解答中介绍的过程。

    谢谢。此致、

    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    至于链接器命令文件:您能展示您在链接器命令文件中所做的操作(您说的此操作无助于消除错误)吗?

    谢谢。此致、

    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vamsi:

    以下是我对链接器命令文件所做的修改:

    从这里:

     

       GROUP
       {
    	.TI.ramfunc
    	{ -l F021_API_F28004x_FPU32.lib}
    	}
    						 LOAD = FLASH_BANK0_SEC9 | FLASH_BANK0_SEC10 | FLASH_BANK0_SEC13,
                             RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,

    为此、请执行以下操作:  

       GROUP
       {
    	.TI.ramfunc
    	{ -l F021_API_F28004x_FPU32.lib}
    	}
    						 LOAD = FLASH_BANK0_SEC7 | FLASH_BANK0_SEC8 | FLASH_BANK0_SEC9 | FLASH_BANK0_SEC10 | FLASH_BANK0_SEC13,
                             RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,

    谢谢。

    阿洛巴。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您可以将几个存储器合并到一个存储器范围中并尝试、而不是使用存储器?

    示例:

    从这里:

    FLASH_A:origin = 0x90000、length = 0x1000

    FLASH_B:origin = 0xA0000、length = 0x1000

    为此、请执行以下操作:

    FLASH_AB:origin = 0x90000、length = 0x2000

    并使用合并的存储器范围。

    请告诉我们这是否有帮助。

    谢谢。此致、

    瓦姆西  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    由于我没有收到您的回复、因此我将关闭此帖子、前提是我的最后一次回复帮助您解决了此问题。

    如果您仍有其他问题、可以根据需要打开新帖子。

    谢谢。此致、

    瓦姆西