主题中讨论的其他器件:C2000WARE
主设备和从属设备:F28377S
波特率: 500kHz
主器件每1ms 向从器件发送一帧数据、长度为5字节。
从机使用中断 方式从主机处接收数据。 起初、从器件正常接收。 经过一段时间后、从机无法从主机接收数据(仅指定的 ID)。 时间间隔不是固定的、从器件有时会正常工作很长时间。
主器件和从器件之间的连接正常。
发生错误后、使用 CAN 工具将其他帧 ID 的数据发送到从机、从机可以正常接收。
它还可以检测主器件使用这个指定的帧 ID 发送的数据是否输出。
使用 CAN 工具发送具有这个指定 ID 的数据、而从器件无法接收该 ID。
// ==================================================================== // === 1. 主函数初始化部分 ============================================ // ==================================================================== void main(void) { // // Initialize the CAN controllers // CANInit(CANA_BASE); // // Setup CAN to be clocked off the PLL output clock // CANClkSourceSelect(CANA_BASE, 0); // // Set up the CAN bus bit rate to 500kHz for each module // This function sets up the CAN bus timing for a nominal configuration. // You can achieve more control over the CAN bus timing by using the // function CANBitTimingSet() instead of this one, if needed. // Additionally, consult the device data sheet for more information about // the CAN module clocking. // CANBitRateSet(CANA_BASE, 200000000, 500000); // CANBitRateSet(CANA_BASE, 200000000, 1000000); // // Enable interrupts on the CAN A peripheral. // // CANIntEnable(CANA_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS); CANIntEnable(CANA_BASE, CAN_INT_MASTER | CAN_INT_ERROR); // Enable AutoBusOn CAN_enableAutoBusOn(CANA_BASE); CAN_setAutoBusOnTime(CANA_BASE, 100000); CAN_disableRetry(CANA_BASE); // // Enable the CAN-A interrupt signal // CANGlobalIntEnable(CANA_BASE, CAN_GLB_INT_CANINT0); CanObjInit(); // // Start CAN module A operations // CANEnable(CANA_BASE); } // ==================================================================== // === 2. 主机DSP CanObjInit()初始化配置邮箱,及发送程序 ============= // ==================================================================== void CanObjInit() { // 两DSP CAN通信,发送 sTXCANMsgDspComm01.ui32MsgID = 0x0C100201; sTXCANMsgDspComm01.ui32MsgIDMask = 0; sTXCANMsgDspComm01.ui32Flags = 0; sTXCANMsgDspComm01.ui32MsgLen = 5; sTXCANMsgDspComm01.pucMsgData = TxMsgDspCommData01; } // ====== 发送部分程序,1ms发送1次 ===================================== // 发送给从机电流设定值 TxMsgDspCommData01[0] = ((int)(onGridCloseLoopIdref * 100) & 0x00FF); TxMsgDspCommData01[1] = ((int)(onGridCloseLoopIdref * 100) & 0xFF00) >> 8; TxMsgDspCommData01[2] = ((int)(onGridCloseLoopIqref * 100) & 0x00FF); TxMsgDspCommData01[3] = ((int)(onGridCloseLoopIqref * 100) & 0xFF00) >> 8; TxMsgDspCommData01[4] = 0; CANMessageSet(CANA_BASE, 4, &sTXCANMsgDspComm01, MSG_OBJ_TYPE_TX); // ==================================================================== // === 3. 从机DSP CanObjInit()初始化配置邮箱,及接收程序 ============= // ==================================================================== void CanObjInit() { // 两DSP CAN通信,接收 sRXCANMsgDspComm01.ui32MsgID = 0x0C100201; sRXCANMsgDspComm01.ui32MsgIDMask = 0; sRXCANMsgDspComm01.ui32Flags = MSG_OBJ_RX_INT_ENABLE; sRXCANMsgDspComm01.ui32MsgLen = 5; sRXCANMsgDspComm01.pucMsgData = RxMsgDspCommData01; CANMessageSet(CANA_BASE, 15, &sRXCANMsgDspComm01, MSG_OBJ_TYPE_RX); } // ======== 在中断中接收主机发送过来的数据(status = 15时接收该帧 ) ============================ #if (G9_5PL != 0) __interrupt void CANA0_ISR(void) // CAN-A { // Set interrupt priority: volatile Uint16 TempPIEIER = PieCtrlRegs.PIEIER9.all; IER |= M_INT9; IER &= MINT9; // Set "global" priority PieCtrlRegs.PIEIER9.all &= MG9_5; // Set "group" priority PieCtrlRegs.PIEACK.all = 0xFFFF; // Enable PIE interrupts __asm(" NOP"); EINT; uint32_t status; // // Read the CAN-A interrupt status to find the cause of the interrupt // status = CANIntStatus(CANA_BASE, CAN_INT_STS_CAUSE); // // If the cause is a controller status interrupt, then get the status // if(status == CAN_INT_INT0ID_STATUS) { // DSP_OUT1_TOGGLE; // // Read the controller status. This will return a field of status // error bits that can indicate various errors. Error processing // is not done in this example for simplicity. Refer to the // API documentation for details about the error status bits. // The act of reading this status will clear the interrupt. // status = CANStatusGet(CANA_BASE, CAN_STS_CONTROL); // // Check to see if an error occurred. // // if(((status & ~(CAN_ES_RXOK)) != 7) && // ((status & ~(CAN_ES_RXOK)) != 0)) // if(((status & ~(CAN_ES_RXOK | CAN_ES_TXOK | CAN_ES_BOFF)) != 7) && // ((status & ~(CAN_ES_RXOK | CAN_ES_TXOK | CAN_ES_BOFF)) != 0)) if(((status & ~(CAN_ES_RXOK | CAN_ES_TXOK)) != 7) && ((status & ~(CAN_ES_RXOK | CAN_ES_TXOK)) != 0)) { // // Set a flag to indicate some errors may have occurred. // errorFlag = 1; // 调试 CanConfigInit(); // DSP_OUT1_TOGGLE; // 调试 } } else if(status == 15) { DSP_OUT1_TOGGLE; errorFlag = 0; CanReceiveDsp01(); CANIntClear(CANA_BASE, 15); } else if(status == 16) { CanReceiveDsp02(); CANIntClear(CANA_BASE, 16); } else if(status == 17) { // DSP_OUT1_TOGGLE; // 调试 CanReceiveDsp03(); CANIntClear(CANA_BASE, 17); } // // Check if the cause is the CAN-A receive message object 1 // else if(status == 25) { // // Get the received message // // CANMessageGet(CANA_BASE, 2, &sRXCANMsgChkInfo, true); CanReceiveSrhInfo(); // // Getting to this point means that the RX interrupt occurred on // message object 1, and the message RX is complete. Clear the // message object interrupt. // CANIntClear(CANA_BASE, 25); // // Increment a counter to keep track of how many messages have been // received. In a real application this could be used to set flags to // indicate when a message is received. // // rxMsgCount++; // // Since the message was received, clear any error flags. // // errorFlag = 0; } else if(status == 26) { CanReceiveRdSet(); CANIntClear(CANA_BASE, 26); } else if(status == 27) { CanReceiveCtlSet(); CANIntClear(CANA_BASE, 27); } else if(status == 28) { CanReceiveParaSet(); CANIntClear(CANA_BASE, 28); } // // If something unexpected caused the interrupt, this would handle it. // else { // // Spurious interrupt handling can go here. // // errorFlag = 2; // 调试 } // // Clear the global interrupt flag for the CAN interrupt line // CANGlobalIntClear(CANA_BASE, CAN_GLB_INT_CANINT0); // // Restore registers saved: // DINT; PieCtrlRegs.PIEIER9.all = TempPIEIER; } #endif
--
谢谢、此致