请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMS320F2810 尊敬的 TI 团队:
我很长时间以来就收到这个警告、想知道是不是问题、还是可以忽略它。
我在 CCS 文件夹中查看了 cmd 文件、它应该没问题、CodeStartBranch.asm 看起来也没什么问题。
请建议、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的 TI 团队:
我很长时间以来就收到这个警告、想知道是不是问题、还是可以忽略它。
我在 CCS 文件夹中查看了 cmd 文件、它应该没问题、CodeStartBranch.asm 看起来也没什么问题。
请建议、
../../../../Cpu/TMS320F2810/softfloat/softfloat.obj
MEMORY
{
PAGE 0 :
BOOT(R) : origin = 0x3E8000, length = 0x000080 /* */
FLASHE : origin = 0x3E8080, length = 0x007F7F /* on-chip FLASH Program */
FLASHC : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH Program */
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH Program */
FLASHA : origin = 0x3F6000, length = 0x001F7F /* on-chip FLASH Bootloader*/
PROG(RWX) : origin = 0x3F8000, length = 0x001FFF /* RAM Bereich für Code (ramfuncs) */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Area for CSM enable */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008
PAGE 1 :
/* SARAM */
M0RAM(RW) : origin = 0x000000, length = 0x400
M1RAM(RW) : origin = 0x000400, length = 0x400
L0L1RAM(RW) : origin = 0x008000, length = 0x2000
/* Peripheral Frame 0: */
DEV_EMU : origin = 0x000880, length = 0x000180
FLASH_REGS : origin = 0x000A80, length = 0x000060
CSM_REGS : origin = 0x000AE0, length = 0x000010
XINTF : origin = 0x000B20, length = 0x000020
CPU_TIMER0 : origin = 0x000C00, length = 0x000008
CPU_TIMER1 : origin = 0x000C08, length = 0x000008
CPU_TIMER2 : origin = 0x000C10, length = 0x000008
PIE_CTRL : origin = 0x000CE0, length = 0x000020
PIE_VECT : origin = 0x000D00, length = 0x000100
/* Peripheral Frame 1: */
ECAN_A : origin = 0x006000, length = 0x000100
ECAN_AMBOX : origin = 0x006100, length = 0x000100
/* Peripheral Frame 2: */
SYSTEM : origin = 0x007010, length = 0x000020
SPI_A : origin = 0x007040, length = 0x000010
SCI_A : origin = 0x007050, length = 0x000010
XINTRUPT : origin = 0x007070, length = 0x000010
GPIOMUX : origin = 0x0070C0, length = 0x000020
GPIODAT : origin = 0x0070E0, length = 0x000020
ADC : origin = 0x007100, length = 0x000020
EV_A : origin = 0x007400, length = 0x000040
EV_B : origin = 0x007500, length = 0x000040
SPI_B : origin = 0x007740, length = 0x000010
SCI_B : origin = 0x007750, length = 0x000010
MCBSP_A : origin = 0x007800, length = 0x000040
}
SECTIONS
{
/* Allocate Peripheral Frame 0 Register Structures: */
DevEmuRegsFile : > DEV_EMU, PAGE = 1
FlashRegsFile : > FLASH_REGS, PAGE = 1
CsmRegsFile : > CSM_REGS, PAGE = 1
XintfRegsFile : > XINTF, PAGE = 1
CpuTimer0RegsFile : > CPU_TIMER0, PAGE = 1
CpuTimer1RegsFile : > CPU_TIMER1, PAGE = 1
CpuTimer2RegsFile : > CPU_TIMER2, PAGE = 1
PieCtrlRegsFile : > PIE_CTRL, PAGE = 1
PieVectTable : > PIE_VECT, PAGE = 1
/* Allocate Peripheral Frame 2 Register Structures: */
ECanaRegsFile : > ECAN_A, PAGE = 1
ECanaMboxesFile : > ECAN_AMBOX PAGE = 1
/* Allocate Peripheral Frame 1 Register Structures: */
SysCtrlRegsFile : > SYSTEM, PAGE = 1
SpiaRegsFile : > SPI_A, PAGE = 1
SciaRegsFile : > SCI_A, PAGE = 1
XIntruptRegsFile : > XINTRUPT, PAGE = 1
GpioMuxRegsFile : > GPIOMUX, PAGE = 1
GpioDataRegsFile : > GPIODAT PAGE = 1
AdcRegsFile : > ADC, PAGE = 1
EvaRegsFile : > EV_A, PAGE = 1
EvbRegsFile : > EV_B, PAGE = 1
ScibRegsFile : > SCI_B, PAGE = 1
McbspaRegsFile : > MCBSP_A, PAGE = 1
/* 22-bit program sections */
.reset : > RESET, PAGE = 0, TYPE = DSECT
.pinit : > FLASHE, PAGE = 0
.cinit : > FLASHE, PAGE = 0
.text : > FLASHE, PAGE = 0
csm_enable : > CSM_RSVD, PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHB, RUN = PROG, PAGE = 0
secValid : LOAD = 0x3F5FFA, PAGE = 0
/* 16-Bit data sections */
.const : > FLASHE, PAGE = 0
.bss : > M0RAM, PAGE = 1
.stack : > M1RAM, PAGE = 1
.sysmem : > M0RAM, PAGE = 1
/* 32-bit data sections */
.ebss : > L0L1RAM, PAGE = 1
.econst : > FLASHE, PAGE = 0
.switch : > FLASHE PAGE = 0
.esysmem : > L0L1RAM, PAGE = 1
CsmPwlFile : > CSM_PWL, PAGE = 0 /* CSM Password Locations */
.boot > BOOT
{
-l../../../../Cpu\TMS320F2810\rts2800_ml.lib <boot.obj> (.text)
}
support LOAD = FLASHB, RUN = PROG, PAGE = 0
{
-l../../../../Cpu\TMS320F2810\Bootloader\Flash2810_API_V210.lib (.text)
-l../../../../Cpu\TMS320F2810\Bootloader\Flash2810_API_V210.lib (.econst)
}
}