This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28377D:cmd DATA_SECTION 地址偏移问题

Guru**** 2522770 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1297580/tms320f28377d-cmd-data_section-address-offset-issue

器件型号:TMS320F28377D

大家好、

CPU2和 CPU1具有共享的数据。 客户将把所有数据放入0x03F810。 并且已定义段名称。 详细信息如下:

#pragma DATA_SECTION(SetDataMap,"CPU2TOCPU1DATA");
stSetVale SetDataMap;

编译后、发现映射文件中的地址位置相对于预期值偏移了0x40:

MEMORY
{
    PAGE 0 :
    /* BEGIN is used for the "boot to SARAM" bootloader mode */

    BEGIN : origin = 0x080000, length = 0x000002
    RAMM0 : origin = 0x0000A2, length = 0x00035E
    RAMD0 : origin = 0x00B000, length = 0x000800
    RAMLS0 : origin = 0x008000, length = 0x000800
    RAMLS1 : origin = 0x008800, length = 0x000800
    RAMLS2 : origin = 0x009000, length = 0x000800
    RAMLS3 : origin = 0x009800, length = 0x000800
    RAMLS4 : origin = 0x00A000, length = 0x000800
    RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
    RAMGS15 : origin = 0x01B000, length = 0x000FF8 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */

    // RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

    RESET : origin = 0x3FFFC0, length = 0x000002

    /* Flash sectors */
    FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
    FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
    FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
    FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
    FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
    FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
    FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
    FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
    FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
    FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
    FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
    FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
    FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
    FLASHN : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */

    // FLASHN_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

    PAGE 1 :

    BOOT_RSVD : origin = 0x000002, length = 0x0000A0 /* Part of M0, BOOT rom will use this for stack */
    RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
    // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    RAMD1 : origin = 0x00B800, length = 0x000800

    RAMLS5 : origin = 0x00A800, length = 0x000800

    RAMGS0 : origin = 0x00C000, length = 0x001000
    RAMGS1 : origin = 0x00D000, length = 0x001000
    RAMGS2 : origin = 0x00E000, length = 0x001000

    CPU2TOCPU1FLAG : origin = 0x03F800, length = 0x000010
    CPU2TOCPU1RAM : origin = 0x03F810, length = 0x0003E0

    CPU1TOCPU2FLAG : origin = 0x03FC00, length = 0x000010
    CPU1TOCPU2RAM : origin = 0x03FC10, length = 0x0003E0
}

SECTIONS
{
    /* Allocate program areas: */
    .cinit : > FLASHB PAGE = 0, ALIGN(8)
    .text : > FLASHB PAGE = 0, ALIGN(8)
    codestart : > BEGIN PAGE = 0, ALIGN(8)

    /* Allocate uninitalized data sections: */
    .stack : > RAMM1 PAGE = 1

    /* Initalized sections go in Flash */
    .switch : > FLASHB PAGE = 0, ALIGN(8)
    .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

    #if defined(__TI_EABI__)
    .init_array : > FLASHB, PAGE = 0, ALIGN(8)
    .bss : > RAMLS5, PAGE = 1
    .bss:output : > RAMLS3, PAGE = 0
    .bss:cio : > RAMLS5, PAGE = 1
    .data : > RAMLS5, PAGE = 1
    .sysmem : > RAMLS5, PAGE = 1
    /* Initalized sections go in Flash */
    .const : > FLASHF, PAGE = 0, ALIGN(8)
    #else
    .pinit : > FLASHB, PAGE = 0, ALIGN(8)
    .ebss : >> RAMLS5 | RAMGS0 | RAMGS1, PAGE = 1
    .esysmem : > RAMLS5, PAGE = 1
    .cio : > RAMLS5, PAGE = 1
    /* Initalized sections go in Flash */
    .econst : >> FLASHF PAGE = 0, ALIGN(8)
    #endif

    SHARERAMGS0 : > RAMGS0, PAGE = 1
    SHARERAMGS1 : > RAMGS1, PAGE = 1
    SHARERAMGS2 : > RAMGS2, PAGE = 1

    CPU1TOCPU2CMDFLAG : > CPU1TOCPU2FLAG, PAGE = 1
    CPU1TOCPU2DATA : > CPU1TOCPU2RAM, PAGE = 1

    CPU2TOCPU1CMDFLAG : > CPU2TOCPU1FLAG, PAGE = 1,ALIGN(8)
    CPU2TOCPU1DATA : > CPU2TOCPU1RAM, PAGE = 1 ,ALIGN(8)

    #ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 15009000
    #if defined(__TI_EABI__)
    .TI.ramfunc : {} LOAD = FLASHD,
    RUN = RAMLS0,
    LOAD_START(RamfuncsLoadStart),
    LOAD_SIZE(RamfuncsLoadSize),
    LOAD_END(RamfuncsLoadEnd),
    RUN_START(RamfuncsRunStart),
    RUN_SIZE(RamfuncsRunSize),
    RUN_END(RamfuncsRunEnd),
    PAGE = 0, ALIGN(8)
    #else
    .TI.ramfunc : {} LOAD = FLASHD,
    RUN = RAMLS0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    RUN_SIZE(_RamfuncsRunSize),
    RUN_END(_RamfuncsRunEnd),
    PAGE = 0, ALIGN(8)
    #endif
    #else
    ramfuncs : LOAD = FLASHD,
    RUN = RAMLS0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    RUN_SIZE(_RamfuncsRunSize),
    RUN_END(_RamfuncsRunEnd),
    PAGE = 0, ALIGN(8)
    #endif
    #endif

    /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }

    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        GETBUFFER : TYPE = DSECT
        GETWRITEIDX : TYPE = DSECT
        PUTREADIDX : TYPE = DSECT
    }
}

--

谢谢、此致

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    您可以共享映射文件吗?  是否有任何其他段分配给 CPU2TOCPU1RAM 存储器?

    此致

    西达尔特