This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280037C:CPU 在 SYSTEM_POST_cinit ()中堆栈

Guru**** 2673945 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1292737/tms320f280037c-cpu-gets-stacked-in-system_post_cinit

器件型号:TMS320F280037C

您好、团队成员:  

我在调试器件时遇到了问题。  

项目构建正确、处理器可能也进行了正确编程、但当我单击"play"按钮时、CPU 会堆栈在引导 ROM 中:

问题随机出现。 当我编辑代码时、即使只是删除或添加一行代码项目、也会正确编译、并且 CPU 可以正常运行、正如我预期的那样。  

您知道什么可能触发此故障行为吗?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Mateusz:

    Unknown 说:
    项目构建正确、处理器可能也编程正确、但当我点击"play"按钮时、CPU 会堆叠在引导 ROM 中

    您能否尝试单步执行代码以查看问题发生在哪一行? 根据您的屏幕截图、看起来这可能是 ITRAP (指令陷阱、当运行无效指令时会发生)。 在执行此操作时、请确保查看反汇编以验证正在执行有效指令。

    Unknown 说:
    当我编辑代码时、即使只是删除或添加一行代码项目时、CPU 也能正确编译、CPU 也能正常运行。  [/报价]

    您能详细说明一下您正在编辑什么内容吗? 是您要删除的某一行还是仅某些行? 请进行全面测试、以便我们缩小问题根源。

    此致、

    阿米尔·奥马尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Omer:  

    我找到了什么触发了 ITRAP、但我不知道为什么这个函数一次触发了非法操作 INT、但一次不会触发。  

    该函数是 Fapi_setActiveFlashBank (Fapi_Flash 1)、我在器件初始化过程结束时执行该函数:

    void Device_init(void)
    {
        //
        // Disable the watchdog
        //
        SysCtl_disableWatchdog();
    #ifdef CMDTOOL
        CMD_init();
    #endif
    
    #ifdef _FLASH
    #ifndef CMDTOOL
        //
        // Copy time critical code and flash setup code to RAM. This includes the
        // following functions: InitFlash();
        //
        // The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart symbols
        // are created by the linker. Refer to the device .cmd file.
        //
        memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
    #endif
        //
        // Call Flash Initialization to setup flash waitstates. This function must
        // reside in RAM.
        //
        Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, DEVICE_FLASH_WAITSTATES);
    #endif
    
        //
        // Set up PLL control and clock dividers
        //
        SysCtl_setClock(DEVICE_SETCLOCK_CFG);
    
        //
        // Make sure the LSPCLK divider is set to the default (divide by 4)
        //
        SysCtl_setLowSpeedClock(SYSCTL_LSPCLK_PRESCALE_1);
    
        //
        // These asserts will check that the #defines for the clock rates in
        // device.h match the actual rates that have been configured. If they do
        // not match, check that the calculations of DEVICE_SYSCLK_FREQ and
        // DEVICE_LSPCLK_FREQ are accurate. Some examples will not perform as
        // expected if these are not correct.
        //
        ASSERT(SysCtl_getClock(DEVICE_OSCSRC_FREQ) == DEVICE_SYSCLK_FREQ);
        ASSERT(SysCtl_getLowSpeedClock(DEVICE_OSCSRC_FREQ) == DEVICE_LSPCLK_FREQ);
    
    #ifndef _FLASH
        //
        // Call Device_cal function when run using debugger
        // This function is called as part of the Boot code. The function is called
        // in the Device_init function since during debug time resets, the boot code
        // will not be executed and the gel script will reinitialize all the
        // registers and the calibrated values will be lost.
    	// Sysctl_deviceCal is a wrapper function for Device_Cal
        //
        SysCtl_deviceCal();
    #endif
    
        //
        // Turn on all peripherals
        //
        Device_enableAllPeripherals();
    
        //
        // Lock VREGCTL Register
        // The register VREGCTL is not supported in this device. It is locked to
        // prevent any writes to this register
        //
        ASysCtl_lockVREG();
    
        //
        // Configure GPIO20 and GPIO21 as digital pins
        //
        GPIO_setAnalogMode(20U, GPIO_ANALOG_DISABLED);
        GPIO_setAnalogMode(21U, GPIO_ANALOG_DISABLED);
        /*
         * SET MCAN CLOCK PRESCALER
         */
        SysCtl_setMCANClk(SYSCTL_MCANCLK_DIV_1);
        //
        // Jump to RAM and call the Flash API functions
        //
        CallFlashAPI();
    }
    
    
    #pragma CODE_SECTION(CallFlashAPI, ".TI.ramfunc");
    void CallFlashAPI(void)
    {
    
        //
        // This function is required to initialize the Flash API based on
        // System frequency before any other Flash API operation can be performed
        // Note that the FMC register base address and system frequency are passed as the parameters
        //
        // This function must also be called whenever System frequency or RWAIT is changed.
        //
        oReturnCheck = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS, CPUCLK_FREQUENCY);
        if(oReturnCheck != Fapi_Status_Success)
        {
            Example_Error(oReturnCheck);
        }
    
        //
        // Fapi_setActiveFlashBank function initializes Flash bank
        // and FMC for erase and program operations.
        //
    #warning triggers post C init
        oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank1);
    
        if(oReturnCheck != Fapi_Status_Success)
        {
            Example_Error(oReturnCheck);
        }
    
    }
    
    

    此处检测到非法操作。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在执行擦除和编程操作之前、我的整个代码可以正常工作、闪存 API 可以正常工作、而没有设置闪存存储体。  

    在本例中进行 FAPI 初始化就足够了、但我确信必须设置 bank1、因为我正在对 bank1扇区进行操作。 也许在这个 MCU 中、 没有必要设置适当的闪存存储体?

    另一个问题未解决。 例如、当我编辑代码时、即使它是一行的重复、也可以为变量分配新值。  

                        (*data[1]).module1.modulesID.all = 0x0;
                        (*data[1]).module2.modulesID.all = 0x0;
                        (*data[1]).module3.modulesID.all = 0x0;
                        (*data[1]).module4.modulesID.all = 0x0;

     使用函数 Fapi_setActiveFlashBank(event1) Fapi_Flash 的项目工作正常。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    我找到了什么触发了 ITRAP,但我不知道为什么这个函数一旦触发了非法操作 INT 而不是一次。  [/报价]

    您是否确保闪存 API 函数未从正在运行的闪存组中运行? 这在闪存 API 用户指南中进行了说明:

    此外、请确保不会修改您调用函数的位置(也就是说、如果函数所在的位置为 RAM 未初始化或闪存未被擦除)。

    当我编辑代码时,例如,即使它重复了一行,为变量分配一个新值。  [/报价]

    请您重新写下该问题/陈述吗? 我不确定我是否理解这意味着什么、或者下面的代码中涉及的内容。 您是说您无法为变量分配值吗?

    [/quote]
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您是否确定闪存 API 函数未从正在运行的闪存组运行? 这是闪存 API 用户指南中描述的内容:

    我确信 flashAPI 位于 RAM 中、因此我假定从 RAM 运行。  

    FlashAPIlib 位于闪存组0中、然后传输到 RAM。 我正在闪存存储体1上运行、这是我在调用函数  Fapi setActiveFlashBank (Fapi_Flash 1)时希望设置的存储体。

    还要确保没有任何内容正在修改您调用函数的位置(例如,如果函数所在的位置是 RAM 未初始化或闪存未被擦除)。

    RAM 和闪存在 CallFlashAPI ()之前初始化,我确信在调用闪存 API 之后启用了中断。

    您能改写此问题/陈述吗? 我不确定我是否理解这意味着什么、或者下面的代码中涉及的内容。 您是否说无法为变量分配值?

    我想说的是、对代码和输出文件进行的一些修改使 函数 Fapi_setActiveFlashBank(Fapi_Flash 52 1)的项目能够正常工作。 这一点我还不清楚、因为一旦项目正常运行、而在修改前未使用该功能。  

    现在、我每次使用闪存 API 时都添加了 EALLOW 和 EDIS 指令、这似乎可以解决问题。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [报价 userid="444961" url="~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1292737/tms320f280037c-cpu-gets-stacked-in-system_post_cinit/4910620 #4910620"]现在,我每次使用闪存 API 时都添加了 EALLOW 和 EDIS 指令,似乎解决了问题。  [/报价]

    我不知道为什么这对于代码功能是必要的、我会将这篇文章转发给闪存专家、以确认为什么这使您的程序正常工作。 由于他们目前因节假日不在办公室、敬请期待下周三左右的回复。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Mateusz:

    您能否附加您正在使用的设备的图像?   

    谢谢。此致、
    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此外、请从调试器内存窗口中共享 TI-OTP 内存转储。

    谢谢。此致、

    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Mateusz:

    您能否提供请求的信息?

    谢谢。此致、

    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vamis:  

    很抱歉这么晚才回答。 以下是请求提供的信息。  

    您能否附上您正在使用的设备的图像?  [/报价]

    此外,请从调试器内存窗口共享 TI-OTP 内存转储。

    e2e.ti.com/.../TI_5F00_OTP_5F00_0x70000_5F00_0x703FF.txt

    谢谢。此致、

    M·斯塔西亚克

    [/quote]
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Mateusz:

    感谢您的评分  将在12月4日查看并返回给您。

    谢谢。此致、
    瓦姆西  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Mateusz:

    您能否共享链接器命令文件和映射文件?  您可以从其中删除任何专有信息。

    从您共享的快照中、我看到闪存 driverlib 被复制到 RAM 中。  我想确认是否将闪存 API 本身复制到 RAM 中。 谢谢你。  

    此 致、

    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vamsi:

    您能否共享链接器命令文件和映射文件?  您可以从其中删除任何专有信息。

    从您共享的快照中、我看到闪存 driverlib 被复制到 RAM 中。  我想确认是否将闪存 API 本身复制到 RAM 中。 谢谢你。  

    [/报价]

    在源文件中、我使用#pragma code_section 指令将 FlashAPI 函数添加到 ".TI.ramfunc"程序块。  

    例如:

    #pragma CODE_SECTION(CallFlashAPI, ".TI.ramfunc");
    void CallFlashAPI(void)
    {
        EALLOW;
        //
        // This function is required to initialize the Flash API based on
        // System frequency before any other Flash API operation can be performed
        // Note that the FMC register base address and system frequency are passed as the parameters
        //
        // This function must also be called whenever System frequency or RWAIT is changed.
        //
        oReturnCheck = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS, CPUCLK_FREQUENCY);
        if(oReturnCheck != Fapi_Status_Success)
        {
            Example_Error(oReturnCheck);
        }
        //
        // Fapi_setActiveFlashBank function initializes Flash bank
        // and FMC for erase and program operations.
        //
        oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank1);
    
        if(oReturnCheck != Fapi_Status_Success)
        {
            Example_Error(oReturnCheck);
        }
        EDIS;
    }

    该指令从我的定制闪存 API 源文件中分配我的所有函数。  

    在我的函数内的每个 flashAPI 驱动程序库函数都在 FLASH_BANK_0中分配。

    这是项目中的.map 文件的一部分。

    .TI.ramfunc 
    *          0    00081000    000001c5     RUN ADDR = 00008000
                      00081000    00000049     driverlib.lib : flash.obj (.TI.ramfunc:Flash_initModule)
                      00081049    0000003c     Fapi_UserDefinedFunctions.obj (.TI.ramfunc:writeVector)
                      00081085    00000031     Fapi_UserDefinedFunctions.obj (.TI.ramfunc:FlashAPIEraseSectorIDVector)
                      000810b6    0000002c     driverlib.lib : flash.obj (.TI.ramfunc:Flash_setBankPowerMode)
                      000810e2    00000023                   : flash.obj (.TI.ramfunc:Flash_setWaitstates)
                      00081105    0000001d                   : flash.obj (.TI.ramfunc:Flash_setPumpPowerMode)
                      00081122    00000019     Fapi_UserDefinedFunctions.obj (.TI.ramfunc:CallFlashAPI)
                      0008113b    00000018     driverlib.lib : flash.obj (.TI.ramfunc:Flash_disableCache)
                      00081153    00000018                   : flash.obj (.TI.ramfunc:Flash_disablePrefetch)
                      0008116b    00000017                   : flash.obj (.TI.ramfunc:Flash_enableCache)
                      00081182    00000017                   : flash.obj (.TI.ramfunc:Flash_enablePrefetch)
                      00081199    00000016                   : flash.obj (.TI.ramfunc:Flash_enableECC)
    
                      000811b7    00000006     Fapi_UserDefinedFunctions.obj (.TI.ramfunc:Example_Error)
                      000811bd    00000004     driverlib.lib : sysctl.obj (.TI.ramfunc)
                      000811c1    00000004     f28003x_usdelay.obj (.TI.ramfunc)
    
    ########################################################################################                  
    ######################   The rest of the Fapi functions                  
    ########################################################################################                  
    0     0000f9b8  Fapi_GlobalInit                  
    0     0008bffe  Fapi_WriteReadBack               
    0     0008b9cf  Fapi_calculateFletcherChecksum   
    0     0008c6ac  Fapi_calculateOtpChecksum        
    0     0008c630  Fapi_checkFsmForReady            
    0     0008a86c  Fapi_checkRegionForValueBy16bits 
    0     0008af85  Fapi_configureFMAC               
    0     0008b9fb  Fapi_divideUnsignedLong          
    0     0008a7f0  Fapi_doBlankCheck                
    0     0008c5d6  Fapi_doVerifyBy16bits            
    0     0008be78  Fapi_flushPipeline               
    0     0008c99a  Fapi_getFsmStatus                
    0     0008b7ec  Fapi_initializeAPI               
    0     0008bca9  Fapi_isAddressEcc                
    0     0008b526  Fapi_isAddressValid              
    0     0008a770  Fapi_issueAsyncCommandWithAddress
    0     0008b047  Fapi_issueFsmCommand             
    0     00087b56  Fapi_issueProgrammingCommand     
    0     0008a8e7  Fapi_loopRegionForValue          
    0     0008b784  Fapi_loopRegionForValueBy16bits  
    0     0008c81b  Fapi_scaleCycleValues            
    0     0008b59b  Fapi_setActiveFlashBank          
    0     0008b8b3  Fapi_setupBankSectorEnable       
    0     0008bf07  Fapi_setupSectorsForWrite        
    0     00008085  FlashAPIEraseSectorIDVector      
    0     00008000  Flash_initModule                          
                      

    我不知道这是否会是个问题。 我没有在 FLASH_BANK_0上操作、而是在 没有闪存 API 函数的 Bank_1上操作。

    此致、  

    马特乌斯

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Mateusz:

    我们发现此用例存在问题。

    您是否可以向我发送友谊请求(将鼠标悬停在我的名字上并单击"请求友谊")?

    我会向您发送一个您可以使用的权变措施。  

    谢谢。此致、
    瓦姆西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vamsi:  

    我已经给您发送了一个请求。  

    感谢您的快速重播。  

    此致、

    马特乌斯  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Mateusz:

    我为您提供了一个简单的权变措施。

    让我知道情况如何。   

    您的实施已关闭并通过验证后、我们可以在此处进行更新。

    谢谢。此致、  
    瓦姆西  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Mateusz:

    我将关闭此帖子、因为我们已对齐该修复离线。

    供参考:我们建议客户在调用 Fapi_setActiveFlashBank ()之前禁用预取机制。  可以在执行 Fapi_setActiveFlashBank()后启用预取。  禁用和启用预取机制的代码应从 RAM 执行。   

    我们将在下一个版本中相应地更新文档。

    谢谢。此致、
    瓦姆西