您好、TI 社区:
我在开发板上遇到了一个关于 MAX1978的问题、它无法响应来自 C2000 MCU 的 SPI 传输。 我将 MAX5144 DAC 用于 SPI-DAC 转换。 我发送了一个固定测试值计算为uint16_t fixedData = (uint16_t)(0.3 * 16383),考虑 MAX5144的14位分辨率。
//############################################################################# // // FILE: spi_ex3_external_loopback_fifo_interrupt.c // // TITLE: SPI Digital Loopback with FIFO Interrupts // //! \addtogroup driver_example_list //! <h1>SPI Digital External Loopback with FIFO Interrupts</h1> //! //! This program uses the external loopback between two SPI modules. Both //! the SPI FIFOs and their interrupts are used. SPIA is configured as a slave //! and receives data from SPI B which is configured as a master. //! //! A stream of data is sent and then compared to the received stream. //! The sent data looks like this: \n //! 0000 0001 \n //! 0001 0002 \n //! 0002 0003 \n //! .... \n //! FFFE FFFF \n //! FFFF 0000 \n //! etc.. \n //! This pattern is repeated forever. //! //! \b External \b Connections \n //! -GPIO25 and GPIO17 - SPISOMI //! -GPIO24 and GPIO16 - SPISIMO //! -GPIO27 and GPIO19 - SPISTE //! -GPIO26 and GPIO18 - SPICLK //! //! \b Watch \b Variables \n //! - \b sData - Data to send //! - \b rData - Received data //! - \b rDataPoint - Used to keep track of the last position in the receive //! stream for error checking //! // //############################################################################# // // $Release Date: $ // $Copyright: // Copyright (C) 2013-2023 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // Included Files // #include "driverlib.h" #include "device.h" // // Globals // volatile uint16_t sData[2]; // Send data buffer volatile uint16_t rData[2]; // Receive data buffer volatile uint16_t rDataPoint = 0; // To keep track of where we are in the // data stream to check received data // // Function Prototypes // void initSPIBMaster(void); void initSPIASlave(void); void configGPIOs(void); __interrupt void spibTxFIFOISR(void); __interrupt void spiaRxFIFOISR(void); // // Main // void main(void) { uint16_t i; // // Initialize device clock and peripherals // Device_init(); // // Disable pin locks and enable internal pullups. // Device_initGPIO(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); // // Interrupts that are used in this example are re-mapped to ISR functions // found within this file. // Interrupt_register(INT_SPIB_TX, &spibTxFIFOISR); Interrupt_register(INT_SPIA_RX, &spiaRxFIFOISR); // // Configure GPIOs for external loopback. // configGPIOs(); // // Set up SPI B as master, initializing it for FIFO mode // initSPIBMaster(); // // Set up SPI A as slave, initializing it for FIFO mode // initSPIASlave(); // // Initialize the data buffers // for(i = 0; i < 2; i++) { sData[i] = i; rData[i]= 0; } // // Enable interrupts required for this example // Interrupt_enable(INT_SPIA_RX); Interrupt_enable(INT_SPIB_TX); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; // // Loop forever. Suspend or place breakpoints to observe the buffers. // while(1) { ; } } // // Function to configure SPI B as master with FIFO enabled. // void initSPIBMaster(void) { // // Must put SPI into reset before configuring it // SPI_disableModule(SPIB_BASE); // // SPI configuration. Use a 500kHz SPICLK and 16-bit word size. // SPI_setConfig(SPIB_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0, SPI_MODE_MASTER, 500000, 16); SPI_disableLoopback(SPIB_BASE); SPI_setEmulationMode(SPIB_BASE, SPI_EMULATION_FREE_RUN); // // FIFO and interrupt configuration // SPI_enableFIFO(SPIB_BASE); SPI_clearInterruptStatus(SPIB_BASE, SPI_INT_TXFF); SPI_setFIFOInterruptLevel(SPIB_BASE, SPI_FIFO_TX2, SPI_FIFO_RX2); SPI_enableInterrupt(SPIB_BASE, SPI_INT_TXFF); // // Configuration complete. Enable the module. // SPI_enableModule(SPIB_BASE); } // // Function to configure SPI A as slave with FIFO enabled. // void initSPIASlave(void) { // // Must put SPI into reset before configuring it // SPI_disableModule(SPIA_BASE); // // SPI configuration. Use a 500kHz SPICLK and 16-bit word size. // SPI_setConfig(SPIA_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0, SPI_MODE_SLAVE, 500000, 16); SPI_disableLoopback(SPIA_BASE); SPI_setEmulationMode(SPIA_BASE, SPI_EMULATION_FREE_RUN); // // FIFO and interrupt configuration // SPI_enableFIFO(SPIA_BASE); SPI_clearInterruptStatus(SPIA_BASE, SPI_INT_RXFF); SPI_setFIFOInterruptLevel(SPIA_BASE, SPI_FIFO_TX2, SPI_FIFO_RX2); SPI_enableInterrupt(SPIA_BASE, SPI_INT_RXFF); // // Configuration complete. Enable the module. // SPI_enableModule(SPIA_BASE); } // // Configure GPIOs for external loopback. // void configGPIOs(void) { // // This test is designed for an external loopback between SPIA // and SPIB. // External Connections: // -GPIO25 and GPIO17 - SPISOMI // -GPIO24 and GPIO16 - SPISIMO // -GPIO27 and GPIO19 - SPISTE // -GPIO26 and GPIO18 - SPICLK // // // GPIO17 is the SPISOMIA. // GPIO_setMasterCore(17, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_17_SPISOMIA); GPIO_setPadConfig(17, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(17, GPIO_QUAL_ASYNC); // // GPIO16 is the SPISIMOA clock pin. // GPIO_setMasterCore(16, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_16_SPISIMOA); GPIO_setPadConfig(16, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(16, GPIO_QUAL_ASYNC); // // GPIO19 is the SPISTEA. // GPIO_setMasterCore(19, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_19_SPISTEA); GPIO_setPadConfig(19, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(19, GPIO_QUAL_ASYNC); // // GPIO18 is the SPICLKA. // GPIO_setMasterCore(18, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_18_SPICLKA); GPIO_setPadConfig(18, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(18, GPIO_QUAL_ASYNC); // // GPIO25 is the SPISOMIB. // GPIO_setMasterCore(25, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_25_SPISOMIB); GPIO_setPadConfig(25, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(25, GPIO_QUAL_ASYNC); // // GPIO24 is the SPISIMOB clock pin. // GPIO_setMasterCore(24, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_24_SPISIMOB); GPIO_setPadConfig(24, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(24, GPIO_QUAL_ASYNC); // // GPIO27 is the SPISTEB. // GPIO_setMasterCore(27, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_27_SPISTEB); GPIO_setPadConfig(27, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(27, GPIO_QUAL_ASYNC); // // GPIO26 is the SPICLKB. // GPIO_setMasterCore(26, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_26_SPICLKB); GPIO_setPadConfig(26, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(26, GPIO_QUAL_ASYNC); } // // SPI A Transmit FIFO ISR // /*__interrupt void spibTxFIFOISR(void) { uint16_t i; // // Send data // for(i = 0; i < 2; i++) { SPI_writeDataNonBlocking(SPIB_BASE, sData[i]); } // // Increment data for next cycle // for(i = 0; i < 2; i++) { sData[i] = sData[i] + 1; } // // Clear interrupt flag and issue ACK // SPI_clearInterruptStatus(SPIB_BASE, SPI_INT_TXFF); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP6); }*/ __interrupt void spibTxFIFOISR(void) { uint16_t i; // 计算DAC的固定值,例如0.3的比例 uint16_t fixedData = (uint16_t)(0.3 * 16383); // 16383 = 2^14 - 1 uint8_t highByte, lowByte; // 从16位数据中提取两个8位字节 highByte = (fixedData >> 8) & 0xFF; // 高8位 lowByte = fixedData & 0xFF; // 低8位 // 发送数据 for(i = 0; i < 2; i++) { // 发送高8位 SPI_writeDataNonBlocking(SPIB_BASE, highByte); // 发送低8位 SPI_writeDataNonBlocking(SPIB_BASE, lowByte); } // Increment data for next cycle - 但在这里我们不修改数据,因为我们发送固定的值 for(i = 0; i < 2; i++) { // 在这里不需要修改sData,因为我们总是发送相同的固定值 } // 清除中断标志并确认 SPI_clearInterruptStatus(SPIB_BASE, SPI_INT_TXFF); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP6); } // // SPI B Receive FIFO ISR // __interrupt void spiaRxFIFOISR(void) { uint16_t i; // // Read data // for(i = 0; i < 2; i++) { rData[i] = SPI_readDataNonBlocking(SPIA_BASE); } // // Check received data // for(i = 0; i < 2; i++) { if(rData[i] != (rDataPoint + i)) { // Something went wrong. rData doesn't contain expected data. Example_Fail = 1; ESTOP0; } } rDataPoint++; // // Clear interrupt flag and issue ACK // SPI_clearInterruptStatus(SPIA_BASE, SPI_INT_RXFF); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP6); Example_PassCount++; } // // End of File //e2e.ti.com/.../MAX5141_2D00_MAX5144.pdfe2e.ti.com/.../8422.max1978evkit.pdf 删除了 MAX1978和 MAX5144的数据表
SPI 输出看上去正确、但 MAX1978未按预期作出响应、尤其是在 TEC 温度控制方面。 我预计 TEC 会因对应于0.3 DAC 值而升温。 是否有人可以就此问题提供见解或故障排除建议?
提前感谢!
内罗






我做了这个,在改变了它之后,现在没有更多的信号哈哈