This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280049C:运行 F280049 CAN 示例、CAN 接收器无法捕获任何消息框

Guru**** 1168960 points
Other Parts Discussed in Thread: C2000WARE
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1310376/tms320f280049c-run-f280049-can-example-can-receiver-cannot-catch-any-message-boxes

器件型号:TMS320F280049C
主题中讨论的其他器件:C2000WARE

我使用 C2000 ware 中的一个 CAN 示例、该示例工程的名称为 can_ex3_external_transmit。

因为我只想测试 CAN 传输、所以删除了错误检查、并永久地将邮箱发送出去。

我使用 F280049C LaunchPad、 在 CCS 中设置一个预定义的宏_LAUNCHXL_F280049C、源文件

更改如下:

//#############################################################################
//
// FILE:   can_ex3_external_transmit.c
//
// TITLE:   CAN External Transmit Example
//
//! \addtogroup driver_example_list
//! <h1> CAN-A to CAN-B External Transmit </h1>
//!
//! This example initializes CAN module A and CAN module B for external
//! communication. CAN-A module is setup to transmit incrementing data for "n"
//! number of times to the CAN-B module, where "n" is the value of TXCOUNT.
//! CAN-B module is setup to trigger an interrupt service routine (ISR) when
//! data is received. An error flag will be set if the transmitted data doesn't
//! match the received data. 
//! 
//! \note Both CAN modules on the device need to be connected to each other
//!       via CAN transceivers.
//!
//! \b Hardware \b Required \n
//!  - A C2000 board with two CAN transceivers
//!
//! \b External \b Connections \n
//!  - ControlCARD CANA is on DEVICE_GPIO_PIN_CANTXA (CANTXA)
//!  - and DEVICE_GPIO_PIN_CANRXA (CANRXA)
//!  - ControlCARD CANB is on DEVICE_GPIO_PIN_CANTXB (CANTXB)
//!  - and DEVICE_GPIO_PIN_CANRXB (CANRXB)
//!
//! \b Watch \b Variables \n
//!  - TXCOUNT - Adjust to set the number of messages to be transmitted
//!  - txMsgCount - A counter for the number of messages sent
//!  - rxMsgCount - A counter for the number of messages received
//!  - txMsgData - An array with the data being sent
//!  - rxMsgData - An array with the data that was received
//!  - errorFlag - A flag that indicates an error has occurred
//!
//
//#############################################################################
//
//
// $Copyright:
// Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################

//
// Included Files
//
#include "driverlib.h"
#include "device.h"

//
// Defines
//
#define TXCOUNT  100
#define MSG_DATA_LENGTH    4
#define TX_MSG_OBJ_ID    1
#define RX_MSG_OBJ_ID    1

//
// Globals
//
volatile unsigned long i;
volatile uint32_t txMsgCount = 0;
volatile uint32_t rxMsgCount = 0;
volatile uint32_t errorFlag = 0;
uint16_t txMsgData[4];
uint16_t rxMsgData[4];

//
// Function Prototypes
//
__interrupt void canbISR(void);

//
// Main
//
void main(void)
{
    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Initialize GPIO and configure GPIO pins for CANTX/CANRX
    // on module A and B
    //
    Device_initGPIO();
    GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXA);
    GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXA);
    GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXB);
    GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXB);

    //
    // Initialize the CAN controllers
    //
    CAN_initModule(CANA_BASE);
    CAN_initModule(CANB_BASE);

    //
    // Set up the CAN bus bit rate to 500kHz for each module
    // Refer to the Driver Library User Guide for information on how to set
    // tighter timing control. Additionally, consult the device data sheet
    // for more information about the CAN module clocking.
    //
    CAN_setBitRate(CANA_BASE, DEVICE_SYSCLK_FREQ, 500000, 20);
    CAN_setBitRate(CANB_BASE, DEVICE_SYSCLK_FREQ, 500000, 20);

    //
    // Enable interrupts on the CAN B peripheral.
    //
    CAN_enableInterrupt(CANB_BASE, CAN_INT_IE0 | CAN_INT_ERROR |
                        CAN_INT_STATUS);

    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts.
    //
    Interrupt_initModule();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    Interrupt_initVectorTable();

    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    // This registers the interrupt handler in PIE vector table.
    //
    Interrupt_register(INT_CANB0, &canbISR);

    //
    // Enable the CAN-B interrupt signal
    //
    Interrupt_enable(INT_CANB0);
    CAN_enableGlobalInterrupt(CANB_BASE, CAN_GLOBAL_INT_CANINT0);

    //
    // Initialize the transmit message object used for sending CAN messages.
    // Message Object Parameters:
    //      CAN Module: A
    //      Message Object ID Number: 1
    //      Message Identifier: 0x15555555
    //      Message Frame: Extended
    //      Message Type: Transmit
    //      Message ID Mask: 0x0
    //      Message Object Flags: None
    //      Message Data Length: 4 Bytes (Note that DLC field is a "don't care"
    //      for a Receive mailbox
    //
    CAN_setupMessageObject(CANA_BASE, TX_MSG_OBJ_ID, 0x15555555,
                           CAN_MSG_FRAME_EXT, CAN_MSG_OBJ_TYPE_TX, 0,
                           CAN_MSG_OBJ_NO_FLAGS, MSG_DATA_LENGTH);

    //
    // Initialize the receive message object used for receiving CAN messages.
    // Message Object Parameters:
    //      CAN Module: B
    //      Message Object ID Number: 1
    //      Message Identifier: 0x15555555
    //      Message Frame: Extended
    //      Message Type: Receive
    //      Message ID Mask: 0x0
    //      Message Object Flags: Receive Interrupt
    //      Message Data Length: 4 Bytes
    //
    CAN_setupMessageObject(CANB_BASE, RX_MSG_OBJ_ID, 0x15555555,
                           CAN_MSG_FRAME_EXT, CAN_MSG_OBJ_TYPE_RX, 0,
                           CAN_MSG_OBJ_RX_INT_ENABLE, MSG_DATA_LENGTH);

    //
    // Initialize the transmit message object data buffer to be sent
    //
    txMsgData[0] = 0x12;
    txMsgData[1] = 0x34;
    txMsgData[2] = 0x56;
    txMsgData[3] = 0x78;

    //
    // Start CAN module A and B operations
    //
    CAN_startModule(CANA_BASE);
    CAN_startModule(CANB_BASE);

    //
    // Transmit messages from CAN-A to CAN-B
    //
//    for(i = 0; i < TXCOUNT; i++)
    while (1)
    {
        //
        // Check the error flag to see if errors occurred
        //
        if(errorFlag)
        {
//            asm("   ESTOP0");
        }

        //
        // Verify that the number of transmitted messages equal the number of
        // messages received before sending a new message
        //
//        if(txMsgCount == rxMsgCount)
        {
            CAN_sendMessage(CANA_BASE, TX_MSG_OBJ_ID, MSG_DATA_LENGTH,
                            txMsgData);
            txMsgCount++;
        }
//        else
//        {
//            errorFlag = 1;
//        }

        //
        // Delay 0.25 second before continuing
        //
        DEVICE_DELAY_US(250000);

        //
        // Increment the value in the transmitted message data.
        //
        txMsgData[0] += 0x01;
        txMsgData[1] += 0x01;
        txMsgData[2] += 0x01;
        txMsgData[3] += 0x01;
        
        //
        // Reset data if exceeds a byte
        //
        if(txMsgData[0] > 0xFF)
        {
            txMsgData[0] = 0;
        }
        if(txMsgData[1] > 0xFF)
        {
            txMsgData[1] = 0;
        }
        if(txMsgData[2] > 0xFF)
        {
            txMsgData[2] = 0;
        }
        if(txMsgData[3] > 0xFF)
        {
            txMsgData[3] = 0;
        }        
    }

    //
    // Stop application
    //
    asm("   ESTOP0");
}

//
// CAN B ISR - The interrupt service routine called when a CAN interrupt is
//             triggered on CAN module B.
//
__interrupt void
canbISR(void)
{
    uint32_t status;

    //
    // Read the CAN-B interrupt status to find the cause of the interrupt
    //
    status = CAN_getInterruptCause(CANB_BASE);

    //
    // If the cause is a controller status interrupt, then get the status
    //
    if(status == CAN_INT_INT0ID_STATUS)
    {
        //
        // Read the controller status.  This will return a field of status
        // error bits that can indicate various errors.  Error processing
        // is not done in this example for simplicity.  Refer to the
        // API documentation for details about the error status bits.
        // The act of reading this status will clear the interrupt.
        //
        status = CAN_getStatus(CANB_BASE);

        //
        // Check to see if an error occurred.
        //
        if(((status  & ~(CAN_STATUS_RXOK)) != CAN_STATUS_LEC_MSK) &&
           ((status  & ~(CAN_STATUS_RXOK)) != CAN_STATUS_LEC_NONE))
        {
            //
            // Set a flag to indicate some errors may have occurred.
            //
            errorFlag = 1;
        }
    }
    //
    // Check if the cause is the CAN-B receive message object 1
    //
    else if(status == RX_MSG_OBJ_ID)
    {
        //
        // Get the received message
        //
        CAN_readMessage(CANB_BASE, RX_MSG_OBJ_ID, rxMsgData);

        //
        // Getting to this point means that the RX interrupt occurred on
        // message object 1, and the message RX is complete.  Clear the
        // message object interrupt.
        //
        CAN_clearInterruptStatus(CANB_BASE, RX_MSG_OBJ_ID);

        //
        // Increment a counter to keep track of how many messages have been
        // received. In a real application this could be used to set flags to
        // indicate when a message is received.
        //
        rxMsgCount++;

        //
        // Since the message was received, clear any error flags.
        //
        errorFlag = 0;
    }
    //
    // If something unexpected caused the interrupt, this would handle it.
    //
    else
    {
        //
        // Spurious interrupt handling can go here.
        //
    }

    //
    // Clear the global interrupt flag for the CAN interrupt line
    //
    CAN_clearGlobalInterruptStatus(CANB_BASE, CAN_GLOBAL_INT_CANINT0);

    //
    // Acknowledge this interrupt located in group 9
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}

//
// End of File
//

顺便说一下、LaunchPad 上的 S9位于 CAN 侧。  

在 F28379D LaunchPad 上运行 CAN 通信程序时、我的 CAN 接收器正常工作。

谢谢。

家开市

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Jiakai,

             如果您"按原样"运行 c2000ware 示例、它是否起作用? 请下载我的应用报告 http://www.ti.com/lit/SPRACE5 并查看提供的调试提示。 通过查看此检查清单、可以解决大多数 CAN 问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Hareesh。

    我 在 LaunchPad 上运行原始代码、不起作用、因此我添加了一个预定义的宏 _LAUNCHXL_F280049C、以便将 GPIO32/33用作 CAN 端口。

    我再次运行该程序、仍然不起作用、我想我可能必须将 CANA 链接到 CANB、 但 LaunchPad 只有一组用于 CANA 的 CAN 驱动程序、我不能直接连接 CANA 和 CANB、所以我删除了错误校验码(检查接收的数据是否与发送的数据相同)、让程序连续发送消息框。

    我再次检查了 SPRACE5、没有找到任何可以帮助我的东西。

    谢谢。

    家开市

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    我想我可能必须将 CANA 链接至 CANB

    是的。

    但 launchpad 只有一组用于 CANA 的 CAN 驱动程序,

    某个操作。

    所以我删除了错误检查代码(检查接收到的数据是否与发送的数据相同)并让程序连续发送消息框。

    它不以这种方式工作。 我在 SPRACE5中解释了为何需要第二个节点。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Hareesh。

    我不将 CANA 连接到 CANB、因此 CANB 无法接收任何消息框、我删除了错误校验代码、以便 CANA 可以连续传输该消息框。

    您能指出更新后的代码中有什么错误吗?

    顺便说一下、您是否有仅传输 CAM 消息框的示例? 例如 F2837x 中的 can_ex4_simple_transmit?

    谢谢。

    家开市

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    我没有将 CANA 连接至 CANB,所以 CANB 无法收到任何消息框,我删除了错误检查代码,以便 CANA 可以连续传输消息框[/报价]

    再说一次、CAN 不能以这种方式工作。 您需要在网络上有一个正确配置的节点来提供 ACK。 我已经在中清楚地解释了这一点 3.1所需的最小节点数 在 SPRACE5中。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我 使用一个 CAN 接收器作为我的 PC 上的另一个节点、它可以显示从此程序发送的每个位。

    顺便说一下、我在 F28379D 上编写了一个具有相同功能的程序、我可以通过 CAN 接收器检查输出。

    谢谢。

    家开市

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Jiakai,

             我不知道你需要我提供什么帮助。 我已经为您提供了足够的指导来找到解决方案。 请完成 SPRACE5中的每个调试步骤并报告您找到的内容。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢您、Hareesh。

    作为程序员、我 希望专家 能够通过他的知识或经验直接指出我的代码中存在的问题、我通常对 TI 社区专家感到满意。

    再次感谢您、

    家开市