This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [常见问题解答] TMS320F28003x、TMS320F28004x:闪存 API 使用通报/勘误表

Guru**** 1133960 points
Other Parts Discussed in Thread: C2000WARE
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1320238/faq-tms320f28003x-tms320f28004x-flash-api-usage-advisory-errata

主题中讨论的其他器件:C2000WARE

以下勘误通报适用于 具有多个闪存组的 TMS320F28003x、TMS320F28004x 器件。  我们很快会将此公告添加到相应的器件勘误表文档中。  此外、我们将更新 C2000Ware_5_02_00_00 (目标发布日期为2024年4月)中的闪存编程示例、以包含以下讨论的软件权变措施。   

闪存勘误咨询:在不禁用闪存预取的情况下执行 Fapi_setActiveFlashBank()可能会导致 ITRAP。

详细信息:仅当没有任何对闪存的活动提取存取时、才应通过从 RAM 执行的代码禁用闪存预取机制。  Fapi_setActiveFlashBank()禁用预取机制。  当预取-禁用进程正在进行时、任何闪存执行都会导致 ITRAP。 因此,应在执行 Fapi_setActiveFlashBank()之前禁用预取。

解决方法:在调用 Fapi_setActiveFlashBank()之前禁用预取机制。  可以在执行 Fapi_setActiveFlashBank()后启用预取。  禁用和启用预取机制的代码应从 RAM 执行。  当这个变通办法被执行时,请注意 Fapi_setActiveFlashBank()可以从闪存执行(不是从擦除/编程操作所针对的存储体执行),因为预取已经被禁用。  

C2000Ware_5_02_00_00 (及更高版本)中提供的闪存 API 使用示例描述了此变通办法的用法。

TMS320F28003x 示例的路径:

C2000Ware_5_02_00_00\driverlib\f28003x\examples\flash\flashapi_ex1_programming.c

TMS320F28004x 示例路径:

C2000Ware_5_02_00_00\driverlib\f28004x\examples\flash\flashapi_ex1_program_autoecc.c

在这些示例中 ,从 RAM 执行 Flash_Disable fetch_sw_Workaround()以禁用预取,然后调用  Fapi_setActiveFlashBank()。   Flash_Enable fetch_sw_Workaround()从 RAM 执行以在调用  Fapi_setActiveFlashBank()后启用预取。

注: 由于 C2000Ware_5_02_00_00尚未发布、我在下面提供了软件权变措施实现详细信息:

/* Implementation details: */

// As shown in below code snippet:
// Call Flash_DisablePrefetch_SW_Workaround() before Fapi_setActiveFlashBank().
// Call Flash_EnablePrefetch_SW_Workaround() after Fapi_setActiveFlashBank().


    //
    // Disable Flash prefetch before Fapi_setActiveFlashBank()
    //
    Flash_DisablePrefetch_SW_Workaround(FLASH0CTRL_BASE);

    //
    // Initialize the Flash banks and FMC for erase and program operations.
    // Fapi_setActiveFlashBank() function sets the Flash banks and FMC for
    // further Flash operations to be performed on the banks.
    //
    oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);

    if(oReturnCheck != Fapi_Status_Success)
    {
        //
        // Check Flash API documentation for possible errors
        //
        Example_Error(oReturnCheck);
    }

    //
    // Enable Flash prefetch after Fapi_setActiveFlashBank()
    //
    Flash_EnablePrefetch_SW_Workaround(FLASH0CTRL_BASE);
    
/* Below is the code for Flash_DisablePrefetch_SW_Workaround().  */

//*****************************************************************************
//
//! Disables flash prefetch mechanism and adds 7 cycle delay
//!
//! \param ctrlBase is the base address of the flash wrapper control registers.
//!
//! \return None.
//
//*****************************************************************************

#ifdef __cplusplus
#pragma CODE_SECTION(".TI.ramfunc");
#else
#pragma CODE_SECTION(Flash_DisablePrefetch_SW_Workaround, ".TI.ramfunc");
#endif
void Flash_DisablePrefetch_SW_Workaround(uint32_t ctrlBase)
{
    //
    // Check the arguments.
    //
    ASSERT(Flash_isCtrlBaseValid(ctrlBase));

    //
    // Disable flash prefetch
    //
    Flash_disablePrefetch(ctrlBase);

    //
    // Force a pipeline flush to ensure that the write to the last register
    // configured occurs before returning.
    //
    FLASH_DELAY_CONFIG;
}

/* Below is the code for Flash_EnablePrefetch_SW_Workaround()  */

//*****************************************************************************
//
//! Enables flash prefetch mechanism and adds 7 cycle delay
//!
//! \param ctrlBase is the base address of the flash wrapper control registers.
//!
//! \return None.
//
//*****************************************************************************

#ifdef __cplusplus
#pragma CODE_SECTION(".TI.ramfunc");
#else
#pragma CODE_SECTION(Flash_EnablePrefetch_SW_Workaround, ".TI.ramfunc");
#endif
void Flash_EnablePrefetch_SW_Workaround(uint32_t ctrlBase)
{
    //
    // Check the arguments.
    //
    ASSERT(Flash_isCtrlBaseValid(ctrlBase));

    //
    // Disable flash prefetch
    //
    Flash_enablePrefetch(ctrlBase);

    //
    // Force a pipeline flush to ensure that the write to the last register
    // configured occurs before returning.
    //
    FLASH_DELAY_CONFIG;
}