This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28388D:从闪存加载代码、但在电源复位后不工作(LED 停止闪烁)

Guru**** 2796425 points

Other Parts Discussed in Thread: TMS320F28388D, C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1317210/tms320f28388d-code-loading-from-flash-memory-but-it-is-not-working-after-power-reset-led-stopped-blinking

器件型号:TMS320F28388D
主题中讨论的其他器件: C2000WARE

我正在使用控制卡(TMS320F28388D)将代码加载到 FLASH_CPU1存储器、代码正在运行(即我可以看到 LED 在闪烁)、但当我重新启动电路板的 LED 时、它不闪烁、这意味着
MCU 无法从闪存引导、但我为闪存设置了开关(S2->Position (1、1))。


我从 f2838X 系列导入了一个示例程序并使用 FLASH_CPU1存储器进行了刷写、并在目标侧观察 LED 闪烁程序、配置的 LED 在闪烁、但当我复位(断电/上电)时
LED 停止工作

请告诉我如何解决该问题?

此致

班迪

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    请检查闪存中的入口点是否正确、此外您还在 代码中包含了 f2838x_codestartbranch.asm 文件。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Vivek、

    由于我不熟悉 CCS 和 TI 电路板、您能详细说明如何在 代码中的闪存和 f2838x_codestartbranch.asm 文件中设置切入点

    如果您可以为上述设置提供任何设置或参考图像

    此致

    班迪  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    C2000Ware 中的所有示例都应具有这些设置。 只需检查您 的项目中是否包含 f2838x_codestartbranch.asm 文件。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Vivek、

    是的、我可以看到 f2838x_codestartbranch.asm 文件包含在我的项目中、共享以供您参考。

    仍然无法通过组合(1、1)从闪存启动代码、有什么建议吗?

     

    ;//###########################################################################
    ;//
    ;// FILE:  f2838x_codestartbranch.asm
    ;//
    ;// TITLE: Branch for redirecting code execution after boot.
    ;//
    ;// For these examples, code_start is the first code that is executed after
    ;// exiting the boot ROM code.
    ;//
    ;// The codestart section in the linker cmd file is used to physically place
    ;// this code at the correct memory location.  This section should be placed
    ;// at the location the BOOT ROM will re-direct the code to.  For example,
    ;// for boot to FLASH this code will be located at 0x3f7ff6.
    ;//
    ;// In addition, the example F2838x projects are setup such that the codegen
    ;// entry point is also set to the code_start label.  This is done by linker
    ;// option -e in the project build options.  When the debugger loads the code,
    ;// it will automatically set the PC to the "entry point" address indicated by
    ;// the -e linker option.  In this case the debugger is simply assigning the PC,
    ;// it is not the same as a full reset of the device.
    ;//
    ;// The compiler may warn that the entry point for the project is other then
    ;//  _c_init00.  _c_init00 is the C environment setup and is run before
    ;// main() is entered. The code_start code will re-direct the execution
    ;// to _c_init00 and thus there is no worry and this warning can be ignored.
    ;//
    ;//###########################################################################
    ;//
    ;//
    ;// $Copyright:
    ;// Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com
    ;//
    ;// Redistribution and use in source and binary forms, with or without 
    ;// modification, are permitted provided that the following conditions 
    ;// are met:
    ;// 
    ;//   Redistributions of source code must retain the above copyright 
    ;//   notice, this list of conditions and the following disclaimer.
    ;// 
    ;//   Redistributions in binary form must reproduce the above copyright
    ;//   notice, this list of conditions and the following disclaimer in the 
    ;//   documentation and/or other materials provided with the   
    ;//   distribution.
    ;// 
    ;//   Neither the name of Texas Instruments Incorporated nor the names of
    ;//   its contributors may be used to endorse or promote products derived
    ;//   from this software without specific prior written permission.
    ;// 
    ;// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    ;// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    ;// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    ;// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    ;// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    ;// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    ;// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    ;// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    ;// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    ;// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    ;// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    ;// $
    ;//###########################################################################
    
    ***********************************************************************
    
    WD_DISABLE  .set  1    ;set to 1 to disable WD, else set to 0
    
        .ref _c_int00
        .global code_start
    
    ***********************************************************************
    * Function: codestart section
    *
    * Description: Branch to code starting point
    ***********************************************************************
    
        .sect "codestart"
        .retain
    
    code_start:
        .if WD_DISABLE == 1
            LB wd_disable       ;Branch to watchdog disable code
        .else
            LB _c_int00         ;Branch to start of boot._asm in RTS library
        .endif
    
    ;end codestart section
    
    ***********************************************************************
    * Function: wd_disable
    *
    * Description: Disables the watchdog timer
    ***********************************************************************
        .if WD_DISABLE == 1
    
        .text
    wd_disable:
        SETC OBJMODE        ;Set OBJMODE for 28x object code
        EALLOW              ;Enable EALLOW protected register access
        MOVZ DP, #7029h>>6  ;Set data page for WDCR register
        MOV @7029h, #0068h  ;Set WDDIS bit in WDCR to disable WD
        EDIS                ;Disable EALLOW protected register access
        LB _c_int00         ;Branch to start of boot._asm in RTS library
    
        .endif
    
    ;end wd_disable
    
        .end
    
    ;//
    ;// End of file.
    ;//
    

    谢谢、此致

    班迪  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您是否使用闪存构建配置?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    PFA、是的、我使用的是闪存构建配置

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    由于一切看起来都正常、您可能需要重新检查引导引脚上的值。 通过 CCS 寄存器视图检查 GPIO 寄存器中引导引脚的值、看看这些值是否正确读取。

    维维克·辛格