This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28035:TMS320F28035

Guru**** 1119300 points
Other Parts Discussed in Thread: CONTROLSUITE
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1321791/tms320f28035-tms320f28035

器件型号:TMS320F28035
主题中讨论的其他器件:controlSUITE

大家好!

当我尝试在我的代码中使用 PI 控制器时、不断出现链接错误。 有人能在这里提问吗?

下面是代码:

#include "DSP28x_Project.h" // Device Headerfile and Examples Include File

#include <math.h>

#include "Solar_F.h"




__interrupt void cpu_timer0_isr(void);
__interrupt void cpu_timer1_isr(void);

void Adc_Config(void);
void EPwm1(void);
void EPwm2(void);
void EPwm3(void);
void gpiosetup (void);


CNTL_PI_F cntl_pi1;




// Global variables
//
Uint16 LoopCount;
Uint16 ConversionCount;
Uint16 Vin[10];
Uint16 Vo[10];
Uint16 Iin[10];
Uint16 Io[10];
float duty1=0.4;
float duty2=0.4;
float duty3=0.5;
float Vin_act,Vo_act, Iin_act,Io_act;
float Gv = 155;
float Gi = 2.5;
Uint16 i;

int16 period = 600;
int16 phase = 300;

void main(void)
{

InitSysCtrl();


DINT;


InitPieCtrl();


IER = 0x0000;
IFR = 0x0000;


InitPieVectTable();


EALLOW; 
PieVectTable.TINT0 = &cpu_timer0_isr;
PieVectTable.TINT1 = &cpu_timer1_isr;
// PieVectTable.ADCINT1 = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers

//
// Step 4. Initialize all the Device Peripherals:
//
InitAdc(); // For this example, init the ADC
InitCpuTimers();

ConfigCpuTimer(&CpuTimer0, 60, 100);
ConfigCpuTimer(&CpuTimer1, 60, 8.33);

CpuTimer0Regs.TCR.all = 0x4000;
CpuTimer1Regs.TCR.all = 0x4000;
IER |= M_INT1;
IER |= M_INT13;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
PieCtrlRegs.PIEIER1.bit.INTx6 =1;

gpiosetup ();
EPwm1();
EPwm2();
EPwm3();

CNTL_PI_F_init(&cntl_pi1);
cntl_pi1.Ki = (0.1);
cntl_pi1.Kp = (0.2);
cntl_pi1.Umax = (0.25);
cntl_pi1.Umin = (0.025);





EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;

EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;


EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM

LoopCount = 0;
ConversionCount = 0;

//
// Configure ADC
// Note: Channel ADCINA4 will be double sampled to workaround the
// ADC 1st sample issue for rev0 silicon errata
//
EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch
AdcRegs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; // Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 2; // setup EOC2 to trigger
// ADCINT1 to fire

//
// set SOC0 channel select to ADCINA0 and SOC 1 -A1, SOC 2 -A2, SOC 3 -A3, SOC 4 -A4
// (dummy sample for rev0 errata workaround)
//
AdcRegs.ADCSOC0CTL.bit.CHSEL = 0;
AdcRegs.ADCSOC1CTL.bit.CHSEL = 1; //set SOC1 channel select to ADCINA1
AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2
AdcRegs.ADCSOC3CTL.bit.CHSEL = 3;
AdcRegs.ADCSOC4CTL.bit.CHSEL = 4;
//
// set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts
// first then SOC1, SOC1,2, 3 then SOC3
//
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5;
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 5;
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 5;
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 5;
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 5;
//
// set SOC0.SOC1,2, 3,4 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
//
AdcRegs.ADCSOC0CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC1CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC2CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC3CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC4CTL.bit.ACQPS = 6;
EDIS;

for(;;);
// {
// LoopCount++;
// }
}


__interrupt void cpu_timer0_isr(void)
{

Vin[ConversionCount] = AdcResult.ADCRESULT0;
Vo[ConversionCount] = AdcResult.ADCRESULT1;
Iin[ConversionCount] = AdcResult.ADCRESULT2;
Io[ConversionCount] = AdcResult.ADCRESULT4;
Vin_act=(Vin[ConversionCount]*Gv*3.3)/4095;
Vo_act=(Vo[ConversionCount]*Gv*3.3)/4095;
Iin_act=(Iin[ConversionCount]*Gi*3.3)/4095;
Io_act=(Io[ConversionCount]*Gi*3.3)/4095;




cntl_pi1.Ref = (1.0);
cntl_pi1.Fbk = (0.1);
CNTL_PI_F_FUNC(&cntl_pi1);


// EPwm1Regs.CMPA.half.CMPA = (EPwm1Regs.TBPRD)*duty;
EPwm1Regs.CMPA.half.CMPA = (EPwm1Regs.TBPRD)*duty1;
EPwm2Regs.CMPA.half.CMPA = (EPwm2Regs.TBPRD)*duty2;
// EPwm3Regs.CMPA.half.CMPA = (EPwm3Regs.TBPRD)*duty3;

//
// If 20 conversions have been logged, start over
//
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else
{
ConversionCount++;
}

//
// Clear ADCINT1 flag reinitialize for next SOC
//
if(i==9)
{
i=0;
}
else
{
i++;
}
// AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
CpuTimer0.InterruptCount++;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE

return;
}

__interrupt void cpu_timer1_isr(void)
{

EPwm3Regs.CMPA.half.CMPA = (EPwm3Regs.TBPRD)*duty3;
CpuTimer1.InterruptCount++;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE

return;
}

void EPwm1()
{
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event

// actual*****


EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE; // set Immediate load
EPwm1Regs.TBPRD = period/2; // PWM frequency = 1 / period
EPwm1Regs.TBPHS.half.TBPHS = 0;
EPwm1Regs.TBCTR = 0;
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;

EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // sync "down-stream"

// Counter Compare Submodule Registers
EPwm1Regs.CMPA.half.CMPA = 0; // set duty 0% initially
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;

// Action Qualifier SubModule Registers
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm1Regs.AQCTLA.bit.CAD = AQ_SET;

}

void EPwm2()
{
EPwm2Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;
// EPwm2Regs.CMPA.half.CMPA = 300; // Set compare A value
EPwm2Regs.TBPRD = period/2; // Set period for ePWM1


EPwm2Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm2Regs.TBCTR = 0x0000; // Clear counter

EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
// EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;

EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // sync "down-stream"

//code for phase shift start
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;

if ((0 <= phase)&&(phase <= 2))
{
EPwm2Regs.TBPHS.half.TBPHS = (2-phase);
EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP; // set to count up after sync
}
else if ((2 < phase)&&(phase <= period/2))
{
EPwm2Regs.TBPHS.half.TBPHS = (phase-2);
EPwm2Regs.TBCTL.bit.PHSDIR = TB_DOWN; // set to count down after sync
}
else if ((period/2 < phase)&&(phase <= period))
{
EPwm2Regs.TBPHS.half.TBPHS = (period-phase+2);
EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP; // set to count up after sync
}
EPwm2Regs.CMPA.half.CMPA = 0;
//code for phase shift end

EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO
// EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;

EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set PWM1A on CAU
EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; // Clear PWM1A on CAD


}

void EPwm3()
{
//
EPwm3Regs.TBCTL.bit.CLKDIV = 0x000;
EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0x001;
EPwm3Regs.TBCTL.bit.CTRMODE = 2;

EPwm3Regs.AQCTLA.all = 0x0060;
EPwm3Regs.AQCTLB.all = 0x0090;
EPwm3Regs.CMPA.half.CMPA = 67; // Set compare A value
EPwm3Regs.TBPRD = 125;

EPwm3Regs.DBFED = 10;
EPwm3Regs.DBRED = 10;

EPwm3Regs.DBCTL.bit.OUT_MODE = 3;
EPwm3Regs.DBCTL.bit.POLSEL = 2;
EPwm3Regs.DBCTL.bit.IN_MODE = 0;



}
void gpiosetup(void)
{
EALLOW;

GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1; // Disable pull-up on GPIO0 (EPWM1A)
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 1; // Disable pull-up on GPIO1 (EPWM1B)
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // Configure GPIO0 as EPWM1A
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1;

GpioCtrlRegs.GPAPUD.bit.GPIO2 = 1; // Disable pull-up on GPIO2 (EPWM2A)
GpioCtrlRegs.GPAPUD.bit.GPIO3 = 1; // Disable pull-up on GPIO3 (EPWM2B)
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // Configure GPIO2 as EPWM2A
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1;

GpioCtrlRegs.GPAPUD.bit.GPIO4 = 1; // Disable pull-up on GPIO4 (EPWM3A)
GpioCtrlRegs.GPAPUD.bit.GPIO5 = 1; // Disable pull-up on GPIO5 (EPWM3B)
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // Configure GPIO4 as EPWM3A
GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1;

EDIS;
}

错误:

error: errors encountered during linking; "Example_2803xAdcSoc.out" not built
gmake: *** [Example_2803xAdcSoc.out] Error 1
gmake: Target 'all' not remade because of errors.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Prasanth,

    您能否 使用 Insert > Code 为您的帖子设置代码块(或者我可以为您执行此操作、因为滚动浏览该主题很困难)? 此外、您能否提供错误的完整控制台输出?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、 Omer:

    非常感谢您的答复。 请找到必需的。

    #include "DSP28x_Project.h" // Device Headerfile and Examples Include File
    
    #include <math.h>
    
    #include "Solar_F.h"
    
    
    __interrupt void cpu_timer0_isr(void);
    __interrupt void cpu_timer1_isr(void);
    
    void Adc_Config(void);
    void EPwm1(void);
    void EPwm2(void);
    void EPwm3(void);
    void gpiosetup (void);
    
    
    CNTL_PI_F cntl_pi1;
    
    
    // Global variables
    //
    Uint16 LoopCount;
    Uint16 ConversionCount;
    Uint16 Vin[10];
    Uint16 Vo[10];
    Uint16 Iin[10];
    Uint16 Io[10];
    float duty1=0.4;
    float duty2=0.4;
    float duty3=0.5;
    float Vin_act,Vo_act, Iin_act,Io_act;
    float Gv = 155;
    float Gi = 2.5;
    Uint16 i;
    
    int16 period = 600;
    int16 phase = 300;
    
    void main(void)
    {
    
    InitSysCtrl();
    
    
    DINT;
    
    
    InitPieCtrl();
    
    
    IER = 0x0000;
    IFR = 0x0000;
    
    
    InitPieVectTable();
    
    
    EALLOW; 
    PieVectTable.TINT0 = &cpu_timer0_isr;
    PieVectTable.TINT1 = &cpu_timer1_isr;
    // PieVectTable.ADCINT1 = &adc_isr;
    EDIS; // This is needed to disable write to EALLOW protected registers
    
    //
    // Step 4. Initialize all the Device Peripherals:
    //
    InitAdc(); // For this example, init the ADC
    InitCpuTimers();
    
    ConfigCpuTimer(&CpuTimer0, 60, 100);
    ConfigCpuTimer(&CpuTimer1, 60, 8.33);
    
    CpuTimer0Regs.TCR.all = 0x4000;
    CpuTimer1Regs.TCR.all = 0x4000;
    IER |= M_INT1;
    IER |= M_INT13;
    PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
    PieCtrlRegs.PIEIER1.bit.INTx6 =1;
    
    gpiosetup ();
    EPwm1();
    EPwm2();
    EPwm3();
    
    CNTL_PI_F_init(&cntl_pi1);
    cntl_pi1.Ki = (0.1);
    cntl_pi1.Kp = (0.2);
    cntl_pi1.Umax = (0.25);
    cntl_pi1.Umin = (0.025);
    
    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
    EDIS;
    
    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
    EDIS;
    
    
    EINT; // Enable Global interrupt INTM
    ERTM; // Enable Global realtime interrupt DBGM
    
    LoopCount = 0;
    ConversionCount = 0;
    
    //
    // Configure ADC
    // Note: Channel ADCINA4 will be double sampled to workaround the
    // ADC 1st sample issue for rev0 silicon errata
    //
    EALLOW;
    AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch
    AdcRegs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
    AdcRegs.INTSEL1N2.bit.INT1CONT = 0; // Disable ADCINT1 Continuous mode
    AdcRegs.INTSEL1N2.bit.INT1SEL = 2; // setup EOC2 to trigger
    // ADCINT1 to fire
    
    //
    // set SOC0 channel select to ADCINA0 and SOC 1 -A1, SOC 2 -A2, SOC 3 -A3, SOC 4 -A4
    // (dummy sample for rev0 errata workaround)
    //
    AdcRegs.ADCSOC0CTL.bit.CHSEL = 0;
    AdcRegs.ADCSOC1CTL.bit.CHSEL = 1; //set SOC1 channel select to ADCINA1
    AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2
    AdcRegs.ADCSOC3CTL.bit.CHSEL = 3;
    AdcRegs.ADCSOC4CTL.bit.CHSEL = 4;
    //
    // set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts
    // first then SOC1, SOC1,2, 3 then SOC3
    //
    AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 5;
    //
    // set SOC0.SOC1,2, 3,4 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
    //
    AdcRegs.ADCSOC0CTL.bit.ACQPS = 6;
    AdcRegs.ADCSOC1CTL.bit.ACQPS = 6;
    AdcRegs.ADCSOC2CTL.bit.ACQPS = 6;
    AdcRegs.ADCSOC3CTL.bit.ACQPS = 6;
    AdcRegs.ADCSOC4CTL.bit.ACQPS = 6;
    EDIS;
    
    for(;;);
    // {
    // LoopCount++;
    // }
    }
    
    
    __interrupt void cpu_timer0_isr(void)
    {
    
    Vin[ConversionCount] = AdcResult.ADCRESULT0;
    Vo[ConversionCount] = AdcResult.ADCRESULT1;
    Iin[ConversionCount] = AdcResult.ADCRESULT2;
    Io[ConversionCount] = AdcResult.ADCRESULT4;
    Vin_act=(Vin[ConversionCount]*Gv*3.3)/4095;
    Vo_act=(Vo[ConversionCount]*Gv*3.3)/4095;
    Iin_act=(Iin[ConversionCount]*Gi*3.3)/4095;
    Io_act=(Io[ConversionCount]*Gi*3.3)/4095;
    
    
    cntl_pi1.Ref = (1.0);
    cntl_pi1.Fbk = (0.1);
    CNTL_PI_F_FUNC(&cntl_pi1);
    
    
    // EPwm1Regs.CMPA.half.CMPA = (EPwm1Regs.TBPRD)*duty;
    EPwm1Regs.CMPA.half.CMPA = (EPwm1Regs.TBPRD)*duty1;
    EPwm2Regs.CMPA.half.CMPA = (EPwm2Regs.TBPRD)*duty2;
    // EPwm3Regs.CMPA.half.CMPA = (EPwm3Regs.TBPRD)*duty3;
    
    //
    // If 20 conversions have been logged, start over
    //
    if(ConversionCount == 9)
    {
    ConversionCount = 0;
    }
    else
    {
    ConversionCount++;
    }
    
    //
    // Clear ADCINT1 flag reinitialize for next SOC
    //
    if(i==9)
    {
    i=0;
    }
    else
    {
    i++;
    }
    // AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
    CpuTimer0.InterruptCount++;
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
    
    return;
    }
    
    __interrupt void cpu_timer1_isr(void)
    {
    
    EPwm3Regs.CMPA.half.CMPA = (EPwm3Regs.TBPRD)*duty3;
    CpuTimer1.InterruptCount++;
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
    
    return;
    }
    
    void EPwm1()
    {
    EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
    EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
    EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
    
    // actual*****
    
    
    EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE; // set Immediate load
    EPwm1Regs.TBPRD = period/2; // PWM frequency = 1 / period
    EPwm1Regs.TBPHS.half.TBPHS = 0;
    EPwm1Regs.TBCTR = 0;
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    
    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;
    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // sync "down-stream"
    
    // Counter Compare Submodule Registers
    EPwm1Regs.CMPA.half.CMPA = 0; // set duty 0% initially
    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;
    
    // Action Qualifier SubModule Registers
    EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
    EPwm1Regs.AQCTLA.bit.CAD = AQ_SET;
    
    }
    
    void EPwm2()
    {
    EPwm2Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;
    // EPwm2Regs.CMPA.half.CMPA = 300; // Set compare A value
    EPwm2Regs.TBPRD = period/2; // Set period for ePWM1
    
    
    EPwm2Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
    EPwm2Regs.TBCTR = 0x0000; // Clear counter
    
    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
    // EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    
    EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;
    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // sync "down-stream"
    
    //code for phase shift start
    EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;
    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
    
    if ((0 <= phase)&&(phase <= 2))
    {
    EPwm2Regs.TBPHS.half.TBPHS = (2-phase);
    EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP; // set to count up after sync
    }
    else if ((2 < phase)&&(phase <= period/2))
    {
    EPwm2Regs.TBPHS.half.TBPHS = (phase-2);
    EPwm2Regs.TBCTL.bit.PHSDIR = TB_DOWN; // set to count down after sync
    }
    else if ((period/2 < phase)&&(phase <= period))
    {
    EPwm2Regs.TBPHS.half.TBPHS = (period-phase+2);
    EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP; // set to count up after sync
    }
    EPwm2Regs.CMPA.half.CMPA = 0;
    //code for phase shift end
    
    EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO
    // EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;
    
    EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set PWM1A on CAU
    EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; // Clear PWM1A on CAD
    
    
    }
    
    void EPwm3()
    {
    //
    EPwm3Regs.TBCTL.bit.CLKDIV = 0x000;
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0x001;
    EPwm3Regs.TBCTL.bit.CTRMODE = 2;
    
    EPwm3Regs.AQCTLA.all = 0x0060;
    EPwm3Regs.AQCTLB.all = 0x0090;
    EPwm3Regs.CMPA.half.CMPA = 67; // Set compare A value
    EPwm3Regs.TBPRD = 125;
    
    EPwm3Regs.DBFED = 10;
    EPwm3Regs.DBRED = 10;
    
    EPwm3Regs.DBCTL.bit.OUT_MODE = 3;
    EPwm3Regs.DBCTL.bit.POLSEL = 2;
    EPwm3Regs.DBCTL.bit.IN_MODE = 0;
    
    }
    void gpiosetup(void)
    {
    EALLOW;
    
    GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1; // Disable pull-up on GPIO0 (EPWM1A)
    GpioCtrlRegs.GPAPUD.bit.GPIO1 = 1; // Disable pull-up on GPIO1 (EPWM1B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // Configure GPIO0 as EPWM1A
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1;
    
    GpioCtrlRegs.GPAPUD.bit.GPIO2 = 1; // Disable pull-up on GPIO2 (EPWM2A)
    GpioCtrlRegs.GPAPUD.bit.GPIO3 = 1; // Disable pull-up on GPIO3 (EPWM2B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // Configure GPIO2 as EPWM2A
    GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1;
    
    GpioCtrlRegs.GPAPUD.bit.GPIO4 = 1; // Disable pull-up on GPIO4 (EPWM3A)
    GpioCtrlRegs.GPAPUD.bit.GPIO5 = 1; // Disable pull-up on GPIO5 (EPWM3B)
    GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // Configure GPIO4 as EPWM3A
    GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1;
    
    EDIS;

    这是控制台文件。

    **** Build of configuration Debug for project ADCinterleaved2 ****
    
    "C:\\ti\\ccs1220\\ccs\\utils\\bin\\gmake" -k all
    
    Building target: "Example_2803xAdcSoc.out"
    Invoking: C2000 Linker
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla0 --define=_DEBUG --define=LARGE_MODEL -g --diag_suppress=10063 --diag_warning=225 --issue_remarks --verbose_diagnostics --quiet -z -m"Example_2803xAdcSoc.map" --stack_size=0x300 --warn_sections -i"C:/ti/controlSUITE/libs/app_libs/solar/v1.2/float/include" -i"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib" -i"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" -i"C:/Users/drjppram/workspace_v12/ADCinterleaved2" -i"C:/ti/controlSUITE/libs/app_libs/solar/v1.2/float/source" -i"C:/ti/C2000Ware_5_01_00_00/device_support/f2803x/common/lib" -i"C:/ti/C2000Ware_5_01_00_00/libraries/math/IQmath/c28/lib" --reread_libs --issue_remarks --verbose_diagnostics --xml_link_info="Example_2803xAdcSoc_linkInfo.xml" --entry_point=code_start --rom_model -o "Example_2803xAdcSoc.out" "./ADCinterleaved2.obj" "./DSP2803x_Adc.obj" "./DSP2803x_CodeStartBranch.obj" "./DSP2803x_CpuTimers.obj" "./DSP2803x_DefaultIsr.obj" "./DSP2803x_EPwm.obj" "./DSP2803x_GlobalVariableDefs.obj" "./DSP2803x_PieCtrl.obj" "./DSP2803x_PieVect.obj" "./DSP2803x_SysCtrl.obj" "./DSP2803x_usDelay.obj" "C:/ti/C2000Ware_5_01_00_00/device_support/f2803x/common/cmd/28035_RAM_lnk.cmd" "C:/ti/C2000Ware_5_01_00_00/device_support/f2803x/headers/cmd/DSP2803x_Headers_nonBIOS.cmd" "C:/ti/controlSUITE/libs/math/IQmath/v160/lib/IQmath.lib" "C:/ti/controlSUITE/device_support/f2803x/v126/DSP2803x_common/lib/SFO_TI_Build_V6b.lib" "../Solar_Lib_Float.lib" "C:/ti/controlSUITE/libs/app_libs/solar/v1.2/IQ/lib/Solar_Lib_IQ.lib" -l"C:/ti/controlSUITE/libs/app_libs/solar/v1.2/float/lib/Solar_Lib_Float.lib" -lrts2800_ml.lib -lIQmath.lib
    
    >> Compilation failure
    makefile:151: recipe for target 'Example_2803xAdcSoc.out' failed
    error: file "../Solar_Lib_Float.lib<CNTL_PI_F.obj>" specifies ISA revision
    "C28FPU32", which is not compatible with ISA revision "C2800" specified in a
    previous file or on the command line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <boot28.asm.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <fs_div28.asm.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <fs_mpy28.asm.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <fs_tol28.asm.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <fs_tou28.asm.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <u_tofs28.asm.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <cpy_tbl.c.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <memcpy.c.obj>" specifies ISA revision "C2800", which is not compatible with
    ISA revision "C2700" specified in a previous file or on the command line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <pre_init.c.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <startup.c.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <exit.c.obj>" specifies ISA revision "C2800", which is not compatible with
    ISA revision "C2700" specified in a previous file or on the command line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <_lock.c.obj>" specifies ISA revision "C2800", which is not compatible with
    ISA revision "C2700" specified in a previous file or on the command line
    error: file
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib/rts2800_ml.lib
    <args_main.c.obj>" specifies ISA revision "C2800", which is not compatible
    with ISA revision "C2700" specified in a previous file or on the command
    line
    warning: could not resolve index library "IQmath.lib" to a compatible library
    error: errors encountered during linking; "Example_2803xAdcSoc.out" not built
    gmake: *** [Example_2803xAdcSoc.out] Error 1
    gmake: Target 'all' not remade because of errors.
    
    **** Build Finished ****

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Prasanth,

    我已修改了在您的帖子中插入的代码、以便我查看(如果您希望我还原它、请告诉我)。

    编译控制台输出中对这些错误进行了更清楚的描述、实际上、有些库并非使用与工程相同的"ISA 修订版"编译。 您需要重新构建 C2800.lib 等库以及您的主工程、以便使用与 rts2800_ml.lib 相同的版本(即 Solar_Lib_Float)。 很遗憾、我无法用我所看到的来仿真器件上的这些误差、所以请告诉我您能否这样做。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Omar:  

    非常感谢您对 我的问题的亲切回应。 我解决了链接中的错误。 但是、我无法解决 PI 控制器问题。 我在 CCS 中看到如下控制台、 我很快就 在代码中使用太阳能(浮点)头文件。 我很抱歉有很多错误、您能建议我在这里解决这个问题吗?  

     

    **** Build of configuration Debug for project ADCinterleaved2 ****
    
    "C:\\ti\\ccs1220\\ccs\\utils\\bin\\gmake" -k all 
     
    Building file: "../ADCinterleaved2.c"
    Invoking: C2000 Compiler
    "C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla0 --include_path="C:/ti/controlSUITE/libs/app_libs/solar/v1.2/float/include" --include_path="C:/ti/controlSUITE/libs/app_libs/solar/v1.2/float/source" --include_path="C:/ti/controlSUITE/libs/math/IQmath/v160/include" --include_path="C:/ti/controlSUITE/libs/math/IQmath/v160/lib" --include_path="C:/ti/controlSUITE/libs/control/DCL/v1_00_00_00/include" --include_path="C:/ti/controlSUITE/libs/control/DCL/v1_00_00_00/source" --include_path="C:/ti/controlSUITE/libs/app_libs/solar/v1.2/IQ/include" --include_path="C:/ti/controlSUITE/libs/app_libs/solar/v1.2/IQ/source" --include_path="C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --include_path="C:/ti/C2000Ware_5_01_00_00/device_support/f2803x/headers/include" --include_path="C:/ti/controlSUITE/libs/math/FPUfastRTS/V100/include" --include_path="C:/ti/C2000Ware_5_01_00_00/device_support/f2803x/common/include" --include_path="C:/ti/C2000Ware_5_01_00_00/libraries/math/IQmath/c28/include" --define=_DEBUG --define=LARGE_MODEL -g --diag_suppress=10063 --diag_warning=225 --issue_remarks --verbose_diagnostics --quiet --preproc_with_compile --preproc_dependency="ADCinterleaved2.d_raw"  "../ADCinterleaved2.c"
     
    >> Compilation failure
    subdir_rules.mk:9: recipe for target 'ADCinterleaved2.obj' failed
    "C:\ti\controlSUITE\libs\app_libs\solar\v1.2\float\include\MPPT_INCC_I_F.h",
              line 28: error: invalid redeclaration of type name
              "MPPT_INCC_I_handle" (declared at line 28 of
              "C:\ti\controlSUITE\libs\app_libs\solar\v1.2\IQ\include\MPPT_INCC_I_I
              Q.h")
      typedef MPPT_INCC_I_F *MPPT_INCC_I_handle;
                             ^
     
    "C:\ti\controlSUITE\libs\app_libs\solar\v1.2\float\include\PID_GRANDO_F.h",
              line 41: error: invalid redeclaration of type name "PID_handle"
              (declared at line 41 of
              "C:\ti\controlSUITE\libs\app_libs\solar\v1.2\IQ\include\PID_GRANDO_IQ
              .h")
      typedef PID_GRANDO_F_CONTROLLER	*PID_handle;
                                     	 ^
     
    2 errors detected in the compilation of "../ADCinterleaved2.c".
    gmake: *** [ADCinterleaved2.obj] Error 1
    gmake: Target 'all' not remade because of errors.
    
    **** Build Finished ****

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Omar:

    很抱歉在这方面有很多错误、虽然我无法运行 Solar_F   库、但是代码成功建立在 Solar_IQ 库中;然而、PI 控制器不工作。 当我使用断点检查控制器时、我被打开了包含消息的对话框(尽管代码已编译)

    在"C:\Git\development\libs\app_libs\solar\v1.2\IQ\source\Debug/../CNTL_PI_IQ.c"中找不到源文件
    找到文件或编辑源查找路径以包括其位置。"

    我请求你看看我在下面附上的图片,我明白 PI 控制器已被宣布,但未被发挥作用。 请更正我的错误。 关于 SOLAR_F 库的访问、我还在 C2000编译器中尝试了更改浮点执行(FPU32);然而、未成功访问它们。 请建议(帮助)我一些替代的方式,以太阳能浮点库和 Solar_IQ 库。 如果我有办法来执行它们、那将会很感激。  

    非常感谢。

    Prasanth Ram

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Prasanth,

    ""Can't find a source file at "C:\Git\development\libs\app_libs\solar\v1.2\IQ\Source\Debug/./CNTL_PI_IQ.c"
    找到文件或编辑源查找路径以包括其位置。"

    您可以参阅 此 E2E 文章、 了解同一问题。

    关于对 SOLAR_F 库的访问,我还尝试了在 C2000编译器中更改浮点执行(FPU32);然而,我没有成功访问它们。 请建议(帮助)我一些替代的方式,以太阳能浮点库和 Solar_IQ 库。 如果我有某种方式来执行它们,我会很感激。

    我不是完全了解这个库以及可以对它进行哪些更改/如何进行更改、因此我会将问题转发给相应的专家。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    当您下载 controlSUITE 时、PI 控制器位于以下方向:

    C:\TI\controlSUITE\libs\app_libs\solar\v1.2\IQ\source

    因此、请在您的 PC 中检查该文件、并将路径更改为与该文件相匹配、