Other Parts Discussed in Thread: LAUNCHXL-F280039C, TMS320F280025C
主题中讨论的其他器件:TMS320F280025C、LAUNCHXL-F280039C
您好!
我有一个项目、其中 F280025C 已替换为 F280039C、相关迁移文档: www.ti.com/.../spruiw4.pdf
尝试在 F280039C 工程(通用电机控制库)的电机控制 SDK 5.1中验证与 XDS110 (来自 TMS320F280025C 评估套件)的连接时、出现以下错误:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\SEBAST~1\AppData\Local\TEXASI~1\
CCS\ccs1210\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Jun 2 2023'.
The library build time was '12:47:07'.
The library package version is '9.12.0.00150'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End]
有趣的是、当我在电机控制 SDK 4.0中执行同样的操作(目标是 F280025C、但硬件是 F280039C)时、验证会成功。
哪里出了问题?