This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28379D:#10247-D 创建输出段".data"无 SECTIONS 规范

Guru**** 2532070 points
Other Parts Discussed in Thread: SYSBIOS, C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1326127/tms320f28379d-10247-d-creating-output-section-data-without-a-sections-specification

器件型号:TMS320F28379D
Thread 中讨论的其他器件:SYSBIOSC2000WARE

当我编译我的项目时、我收到以下警告:

#10247-D 在没有段规范 C/C++问题的情况下创建输出段".data"

在映射文件中、我可以了解此部分中存储了哪些变量:

.data 1 00000002 000000d2未初始化
00000002 00000020 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:ti_sysbios_KNL_KNL_STATE__V Task_Module_)
00000022 00000016 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:ti_sysbios_KNL_KNL_STATE___V Clock_Module_)
00000038 00000008 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:ti_sysbios_family_c28_sys_state__V Timer_Module_)
00000040 0000004c DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:ti_sysbios_utils_sys_state__V Load_Module_)
0000008c 00000012 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:ti_sysBIOS_BIOS_Module__STATE_V)
0000009e 00000010 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:ti_sysBIOS_family_c28_sys_state__V Hwi_Module_)
000000ae 0000000c DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:ti_sysbios_KNL_KNL_STATE__V Swi_Module_)
000000ba 00000004 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:xdc_runtime_runtime_state_state__V Registry_Module_)
000000be 00000002 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:xdc_runtime_runtime_state_state__V Memory_Module_)
000000c0 00000004 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:xdc_runtime_runtime_state_state__V Startup_Module_)
000000c4 00000004 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:XDC_RUNTIME_SYSSD_STATE__V Min_Module_)
000000c8 00000004 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:xdc_runtime_runtime_state_state__V System_Module_)
000000cc 00000004 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:xdc_runtime_runtime_state_state__V Text_Module_)
000000d0 00000003 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:xdc_runtime_Logcion_state_V Buf_Module_)
000000d3 00000001 DEV_FLASH_CONFIG_cpu01_p28fp.o28FP (.data:xdc_runtime_runtime_state_state__V Error_Module_)

此区域似乎由 Sys/BIOS 和 XDC_runtime 使用。 在我的 cmd 文件中、我获得了.data 段的以下定义:

	/* Allocate data memory at RAM
	 * - .stack: Stack space | Volatile memory (SRAM). The C28x Stack Pointer (SP) is 16 bits. .stack must be in the low 64k words.
	 * - .bss and ebss: Global and static variables | Volatile memory (SRAM)
	 * - .sysmem and .esysmem: Memory for malloc type functions | Volatile memory (SRAM)
	 * - .data: Initialized data
	 * - .cio: Debugger section | Buffer for stdio functions
	 */

    /*
	 * .stack section cannot be split and must be in the low 64k words
	 * This section is only used for HWIs and SWIs. SYS/BIOS Thread stacks are allocated in .ebss
	 */
    .stack           	: > RAMM0,  PAGE = 1
#ifdef __TI_EABI__
    .bss             	: >> RAMGS0 | RAMGS1 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1
    .bss:output      	: >> RAMGS0 | RAMGS1 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1
    .sysmem          	: > RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1
    .data            	: > RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1
#else
	.ebss            	: >> RAMGS0 | RAMGS1 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1
	.esysmem         	: >  RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1
#endif
    .cio    	 		: >> RAMM1 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1

我是否应该担心该警告? 如何解决呢?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Clecio:

    您能否共享完整的链接器 cmd 文件以进行进一步分析。  

    您正在使用输出格式作为 EABI right 吗?

    谢谢

    阿斯温

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Aswin。

    我使用传统 COFF。 我将使用 C2000Ware 附带的 F2837xD_Headers_BIOS_cpu1.cmd 和以下 cmd:

    /* File Header
     * - TODO
     */
    
    /* CLA_SCRATCHPAD
     * Define a size for the CLA scratchpad area that will be used
     * by the CLA compiler for local symbols and temps
     * Also force references to the special symbols that mark the
     * scratchpad are.
     */
    CLA_SCRATCHPAD_SIZE = 0x100;
    --undef_sym=__cla_scratchpad_end
    --undef_sym=__cla_scratchpad_start
    
    /* Physical memory allocation */
    MEMORY
    {
    PAGE 0 :
    	/* Program Memory */
    
       /*
    	* Application entry point.
    	* Whenever the bootloader receives a command to jump to
    	* application firmware it jumps here
    	*/
        BEGIN : origin = 0x086000, length = 0x000002
    
    	/* Reset */
        RESET : origin = 0x3FFFC0, length = 0x000002
    
       /*
    	* CLA Program memory.
    	* Use to execute CLA Tasks and functions.
    	*/
    	//RAMLS4 : origin = 0x00A000, length = 0x000800
    	//RAMLS5 : origin = 0x00A800, length = 0x000800
    	CLA_PROG_RAM : origin = 0x00A000, length = 0x001000
    
       /*
    	* CPU Program memory.
    	* Use to execute CPU functions from RAM.
    	*/
    	//RAMGS4 : origin = 0x010000, length = 0x001000
        //RAMGS5 : origin = 0x011000, length = 0x001000
    	RAM_PROGRAM : origin = 0x010000, length = 0x002000
    
       /*
    	* Bootloader code.
    	* Bootloader firmware code goes here
    	* thus FLASHA and FLASHB must not be used by application code!
    	*/
        //FLASHA  : origin = 0x080002, length = 0x001FFE
    	//FLASHB : origin = 0x082000, length = 0x002000
    
       /*
    	* Application code.
    	* Application firmware code goes here.
    	*/
        FLASHD : origin = 0x086002, length = 0x001FFE
        FLASHE : origin = 0x088000, length = 0x008000
        FLASHF : origin = 0x090000, length = 0x008000
    	FLASHG : origin = 0x098000, length = 0x008000
    
       /*
    	* Reserved for future use.
    	* Could be used to store factory default application firmware
    	* or used to store persistant data.
    	*/
    	//FLASHI : origin = 0x0A8000, length = 0x008000
    	//FLASHJ : origin = 0x0B0000, length = 0x008000
    	//FLASHK : origin = 0x0B8000, length = 0x002000
    	//FLASHL : origin = 0x0BA000, length = 0x002000
    
    PAGE 1 :
    	/* Data Memory */
    
    	/* BOOT ROM Stack
    	 * - ECC, Hibernate retention and Access protection
    	 */
        BOOT_RSVD : origin = 0x000002, length = 0x000121
    
       /*
    	* Small nonsecure blocks that are tightly coupled with the CPU
    	* (that is, only the CPU has access to them).
    	* Has Hibernate Retention.
    	* May be used as general purpose RAM.
    	*/
    	RAMM0 : origin = 0x000123, length = 0x0002DD
    	RAMM1 : origin = 0x000400, length = 0x0003F8
    
       /*
    	* Secure RAM.
    	* General purpose RAM with ECC, Security and Access protection features.
    	*/
    	RAMD0 : origin = 0x00B000, length = 0x000800
    	RAMD1 : origin = 0x00B800, length = 0x000800
    
       /*
    	* CLA data memory.
    	* Has Parity, Security and Access protection features
    	*/
    	//RAMLS0 : origin = 0x008000, length = 0x000800
    	//RAMLS1 : origin = 0x008800, length = 0x000800
    	//RAMLS2 : origin = 0x009000, length = 0x000800
    	//RAMLS3 : origin = 0x009800, length = 0x000800
    	CLA_DATA_RAM : origin = 0x008000, length = 0x002000
    
       /*
    	* CPU data memory.
    	* RAMGS0 and RAMGS1 must always be used as data memory
    	* because, since they are within the lower 64k words,
    	* they can be used for SYS/BIOS Thread Stacks. Usually one would
    	* use the RAMLSx for thrad stack, however we have dedicated all
    	* local shared RAMs to the CLA.
    	*/
    	RAMGS0 : origin = 0x00C000, length = 0x001000
    	RAMGS1 : origin = 0x00D000, length = 0x001000
    
       /*
    	* The remaining RAMGSx blocks can be allocated
    	* for anything.
    	*/
    	RAMGS6 : origin = 0x012000, length = 0x001000
    	RAMGS7 : origin = 0x013000, length = 0x001000
    	RAMGS8 : origin = 0x014000, length = 0x001000
    	RAMGS9 : origin = 0x015000, length = 0x000F00
    
        /*
    	* This regions are exclusively used by CpuxSharedIO section
    	* and must be equal in the linker command files of both CPUs
    	*/
    	CPU1_SHARED_IO : origin = 0x015F00, length = 0x000FC
    	CPU2_SHARED_IO : origin = 0x01BF00, length = 0x00100
    
    
    	TEMP_SENSOR_OFFSET : origin = 0x015FFC, length = 0x000002
    	TEMP_SENSOR_SLOPE  : origin = 0x015FFE, length = 0x000002
    
       /*
    	* Bootloader data.
    	* Bootloader const data goes here
    	* thus FLASHC must not be used by application code!
    	*/
        //FLASHC : origin = 0x084000, length = 0x002000
    
       /*
    	* Application firmware const data.
    	*/
    	FLASHH : origin = 0x0A0000, length = 0x008000
    
       /*
    	* Reserved for future use.
    	* Could be used to store factory default application firmware
    	* or used to store persistent data.
    	*/
    	//FLASHM : origin = 0x0BC000, length = 0x002000
    
    	/* App and Boot Shared Consts
    	 * The following regions: APP_METADATA, APP_SHARED_CONST
    	 * and BOOTLOADER_SHARED_CONST are all located at Flash
    	 * Sector 13, aka FLASH N.
    	 */
    
    	/* Application Metadata
    	 * This flash region is used to store
    	 * information about the application firmware
    	 */
    	APP_METADATA : origin = 0x0BE000, length = 0x000080 //128 words
    
    	/* Application shared consts
    	 * This flash region can be used freely to share consts data and functions between
    	 * application firmware and bootloader. This region must be
    	 * Read Only for Bootloader but Read/Write for the Application firmware.
    	 */
    	APP_SHARED_CONST : origin = 0x0BE080, length = 0x000FC0 //4032 words
    
    	/* Bootloader shared consts
    	 * This flash region can be used freely to share consts data and functions between
    	 * application firmware and bootloader. This region must be
    	 * Read/Write for Bootloader but Read Only for the Application firmware
    	 */
    	BOOTLOADER_SHARED_CONST : origin = 0x0BF040, length = 0x000FC0 //4032 words
    
       /*
    	* CPU and CLA message RAM.
    	* Has Parity, Security and Access protection features
    	*/
    	CLATOCPU : origin = 0x001480, length = 0x000080
    	CPUTOCLA : origin = 0x001500, length = 0x000080
    
       /*
    	* CPU1 and CPU2 message RAM.
    	*/
        CPU2TOCPU1 : origin = 0x03F800, length = 0x000400
        CPU1TOCPU2 : origin = 0x03FC00, length = 0x000400
    
       /*
    	* External SDRAM accessed by EMIF
    	*/
        SDRAM : origin = 0x80000000, length = 0x00800000
    }
    
    /* Sections allocation into physical memory */
    SECTIONS
    {
    	/* Allocate program memory
    	 * - codestart: Jump address after boot rom
    	 * - .reset: Reset vector | This section is not typically used by C28x devices and should be set to type=DSECT.
    	 * - .cinit: Initalized global and static variables | Non volatile memory (flash)
    	 * - .binit: Copy tables for boot time initialization
    	 * - .init_array and .pinit: Contains the list of global constructors for C++ programs
    	 * - .text: Executable code and constants | Load into non-volatile memory (flash). Run time-critical code in SARAM.
    	 * - ramfuncs and .TI.ramfunc: TI section to store functions that must run from RAM (see --ramfunc=on/off linker command)
    	 */
    
    	codestart           : > BEGIN PAGE = 0, ALIGN(8)
    	.reset           	: > RESET, PAGE = 0, TYPE = DSECT
    
    	.switch             : > FLASHD | FLASHE | FLASHF | FLASHG, PAGE = 0, ALIGN(8)
        .cinit              : > FLASHD | FLASHE | FLASHF | FLASHG, PAGE = 0, ALIGN(8)
        .binit              : > FLASHD | FLASHE | FLASHF | FLASHG, PAGE = 0, ALIGN(8)
    #ifdef __TI_EABI__
        .init_array         : > FLASHD | FLASHE | FLASHF | FLASHG, PAGE = 0, ALIGN(8)
    #else
        .pinit              : > FLASHD | FLASHE | FLASHF | FLASHG, PAGE = 0, ALIGN(8)
    #endif
        .text               : >> FLASHD | FLASHE | FLASHF | FLASHG, PAGE = 0, ALIGN(8)
    
    #ifdef __TI_COMPILER_VERSION__
    	#if __TI_COMPILER_VERSION__ >= 15009000
    		#if defined(__TI_EABI__)
    			.TI.ramfunc : {} LOAD = FLASHD | FLASHE | FLASHF | FLASHG,
    			                 RUN = RAM_PROGRAM,
    			                 LOAD_START(RamfuncsLoadStart),
    			                 LOAD_SIZE(RamfuncsLoadSize),
    			                 LOAD_END(RamfuncsLoadEnd),
    			                 RUN_START(RamfuncsRunStart),
    			                 RUN_SIZE(RamfuncsRunSize),
    			                 RUN_END(RamfuncsRunEnd),
    			                 PAGE = 0, ALIGN(8)
    		#else
    			.TI.ramfunc : {} LOAD = FLASHD | FLASHE | FLASHF | FLASHG,
    			                 RUN = RAM_PROGRAM,
    			                 LOAD_START(_RamfuncsLoadStart),
    			                 LOAD_SIZE(_RamfuncsLoadSize),
    			                 LOAD_END(_RamfuncsLoadEnd),
    			                 RUN_START(_RamfuncsRunStart),
    			                 RUN_SIZE(_RamfuncsRunSize),
    			                 RUN_END(_RamfuncsRunEnd),
    			                 PAGE = 0, ALIGN(8)
    		#endif
    	#else
    		ramfuncs : LOAD = FLASHD | FLASHE | FLASHF | FLASHG,
    		           RUN = RAM_PROGRAM,
    		           LOAD_START(_RamfuncsLoadStart),
    		           LOAD_SIZE(_RamfuncsLoadSize),
    		           LOAD_END(_RamfuncsLoadEnd),
    		           RUN_START(_RamfuncsRunStart),
    		           RUN_SIZE(_RamfuncsRunSize),
    		           RUN_END(_RamfuncsRunEnd),
    		           PAGE = 0, ALIGN(8)
    	#endif
    #endif
    
    	/* Allocate data memory at RAM
    	 * - .stack: Stack space | Volatile memory (SRAM). The C28x Stack Pointer (SP) is 16 bits. .stack must be in the low 64k words.
    	 * - .bss and ebss: Global and static variables | Volatile memory (SRAM)
    	 * - .sysmem and .esysmem: Memory for malloc type functions | Volatile memory (SRAM)
    	 * - .data: Initialized data
    	 * - .cio: Debugger section | Buffer for stdio functions
    	 */
    
        /*
    	 * .stack section cannot be split and must be in the low 64k words
    	 * This section is only used for HWIs and SWIs. SYS/BIOS Thread stacks are allocated in .ebss
    	 */
        .stack           	: > RAMM0,  PAGE = 1, ALIGN(8)
    #ifdef __TI_EABI__
        .bss             	: >> RAMGS0 | RAMGS1 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1, ALIGN(8)
        .bss:output      	: >> RAMGS0 | RAMGS1 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1, ALIGN(8)
        .sysmem          	: > RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1, ALIGN(8)
        .data            	: > RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1, ALIGN(8)
    #else
    	.ebss            	: >> RAMGS0 | RAMGS1 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1, ALIGN(8)
    	.esysmem         	: > RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1, ALIGN(8)
    #endif
        .cio    	 		: >> RAMM1 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9,  PAGE = 1, ALIGN(8)
    
    	/* Allocate data memory at FLASH
    	 * - .const and econst: Constant data | Non volatile memory (flash)
    	 * - .switch: Tables for switch statements | Non volatile memory (flash)
    	 * - .args: Section used to pass arguments via argc and argv
    	 */
    
    #ifdef __TI_EABI__
        .const              : > FLASHH, PAGE = 1, ALIGN(8)
    #else
        .econst             : > FLASHH, PAGE = 1, ALIGN(8)
    #endif
        .args               : > FLASHH, PAGE = 1, ALIGN(8)
    
       /*
    	* All variables declared with __attribute__((far))
    	* will be allocated here
    	*/
    	.farbss 			: > SDRAM, PAGE = 1, ALIGN(8)
    
    	/* Application Metadata Section */
    	AppMetadata : > APP_METADATA, PAGE = 1
    
       /*
    	* This section must be made up of only Global Shared RAM.
    	*/
        CpuRamData : >> RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9, PAGE = 1
    
        /*
    	* This section is dedicated to allocate objects shared between CPUs.
    	*/
        Cpu1SharedIO : > CPU1_SHARED_IO, PAGE = 1
        Cpu2SharedIO : > CPU2_SHARED_IO, PAGE = 1
    
    
       /*
    	* This section is not shared with CLA or DMA.
    	* It is exclusively for CPU usage.
    	*/
        CpuDedicatedRAM : >> RAMM0 | RAMM1 | RAMD0 | RAMD1, PAGE = 1
    
    	TempSensOffset : > TEMP_SENSOR_OFFSET, PAGE = 1
    	TempSensSlope  : > TEMP_SENSOR_SLOPE, PAGE = 1
    
    
    	/* Allocation sections needed for IPC API Drivers
    	 * - CPU1TOCPU2: Message RAM to pass data from CPU01 to CPU02 | IPC Driver
    	 * - CPU2TOCPU1: Message RAM to pass data from CPU02 to CPU01 | IPC Driver
    	 */
    
        GROUP : > CPU1TOCPU2, PAGE = 1
        {
            PUTBUFFER
            PUTWRITEIDX
            GETREADIDX
        }
    
        GROUP : > CPU2TOCPU1, PAGE = 1
        {
            GETBUFFER :    TYPE = DSECT
            GETWRITEIDX :  TYPE = DSECT
            PUTREADIDX :   TYPE = DSECT
        }
    
    	/* Allocation CLA specific sections
    	 * - cla_to_cpu_ram: Message RAM to pass data from CLA to CPU
    	 * - cpu_to_cla_ram: Message RAM to pass data from CPU to CLA
    	 * - Cla1Prog: CLA program ram section
    	 * - CLAscratch: CLA_SCRATCHPAD_SIZE cla section size
    	 * - .scratchpad: Local variables and compiler temps are placed into a scratchpad memory area, which acts as the CLA C software stack.
    	 *			      It is expected that the scratchpad memory area is defined and managed in the application's linker command file.
    	 * - .bss_cla: Uninitialized global data
    	 * - .const_cla: Initialized constant data
    	 */
    
    	cla_to_cpu_ram		: > CLATOCPU, PAGE = 1
    	cpu_to_cla_ram  	: > CPUTOCLA, PAGE = 1
    
        Cla1Prog : LOAD = FLASHD | FLASHE | FLASHF | FLASHG,
                   RUN = CLA_PROG_RAM,
                   LOAD_START(_Cla1funcsLoadStart),
                   LOAD_END(_Cla1funcsLoadEnd),
                   RUN_START(_Cla1funcsRunStart),
                   LOAD_SIZE(_Cla1funcsLoadSize),
                   PAGE = 0, ALIGN(8)
    
       Cla1Data : > CLA_DATA_RAM, PAGE = 1
    
       CLAscratch :
                   { *.obj(CLAscratch)
                   . += CLA_SCRATCHPAD_SIZE;
                   *.obj(CLAscratch_end) } >  CLA_DATA_RAM, PAGE = 1
    
       .scratchpad : > CLA_DATA_RAM, PAGE = 1
       .bss_cla	   : > CLA_DATA_RAM, PAGE = 1
       .const_cla  :  LOAD = FLASHH,
                      RUN = CLA_DATA_RAM,
                      RUN_START(_Cla1ConstRunStart),
                      LOAD_START(_Cla1ConstLoadStart),
                      LOAD_SIZE(_Cla1ConstLoadSize),
                      PAGE = 1, ALIGN(8)
    }
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Clecio:

    您是否可以尝试使用 EABI 并检查您是否仍面临此问题(将项目属性中的 C2000编译器标记更新为--abi=eabi )

    谢谢

    阿斯温

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Aswin。

    我尝试了 EABI 格式,警告消失了(项目的转换不是那么简单)。

    谢谢您的建议。

    EABI 与 COFF 相比有哪些优势? 将项目转换为这种新格式是否有任何风险?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Clecio:

    请查看此处了解有关 COFF 到 EABI 迁移的更多信息- 从 COFF 到 EABI 的 C2000迁移

    谢谢

    阿斯温

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的。 谢谢!