This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28378S:连接到目标时出错:(错误-1156 @ 0x0)器件在编程 CSM 密码后可能正在低功耗模式下运行

Guru**** 2931100 points

Other Parts Discussed in Thread: UNIFLASH

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1342704/tms320f28378s-error-connecting-to-the-target-error--1156-0x0-device-may-be-operating-in-low-power-mode-after-programming-csm-password

器件型号:TMS320F28378S
主题中讨论的其他器件:UNIFLASH

我将测试 DCSM 和编程的 CSM 密码。 然后、我无法再连接控制器。 尝试解锁控制器时(使用 CCS 或 Uniflash)、始终得到:

 [ERROR] C28xx_CPU1: Error connecting to the target: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 9.9.0.00040)

CCS JTAG 连接测试成功。