Other Parts Discussed in Thread: UNIFLASH
主题中讨论的其他器件:UNIFLASH
您好、我用过它
Proj_lab10a / 2802 x0_flashapi_bootromsymbols_v2。 01.库
这个闪存库、发现第一次通电时遇到普通存储故障、也可以存储几次、但是一旦发生存储故障、又发现回电的芯片好像死了、这就是为什么
初始如下所示:用于更改正式代码的配置/。
void InitFlash(void)
{
EALLOW;
//
// Enable Flash Pipeline mode to improve performance of code executed from
// Flash.
//
FlashRegs.FOPT.bit.ENPIPE = 1;
//
// CAUTION
// Minimum waitstates required for the flash operating
// at a given CPU rate must be characterized by TI.
// Refer to the datasheet for the latest information.
//
#if (CPU_FRQ_60MHZ)
//
// Set the Paged Waitstate for the Flash
//
FlashRegs.FBANKWAIT.bit.PAGEWAIT = 2;
//
// Set the Random Waitstate for the Flash
//
FlashRegs.FBANKWAIT.bit.RANDWAIT = 2;
//
// Set the Waitstate for the OTP
//
FlashRegs.FOTPWAIT.bit.OTPWAIT = 2;
#elif (CPU_FRQ_40MHZ)
//
// Set the Paged Waitstate for the Flash
//
FlashRegs.FBANKWAIT.bit.PAGEWAIT = 1;
//
// Set the Random Waitstate for the Flash
//
FlashRegs.FBANKWAIT.bit.RANDWAIT = 1;
//
// Set the Waitstate for the OTP
//
FlashRegs.FOTPWAIT.bit.OTPWAIT = 1;
#endif
//
// CAUTION: ONLY THE DEFAULT VALUE FOR THESE 2 REGISTERS SHOULD BE USED
//
FlashRegs.FSTDBYWAIT.bit.STDBYWAIT = 0x01FF;
FlashRegs.FACTIVEWAIT.bit.ACTIVEWAIT = 0x01FF;
EDIS;
//
// Force a pipeline flush to ensure that the write to the last register
// configured occurs before returning.
//
asm(" RPT #7 || NOP");
}
void usermain_flash( void )
{
/*------------------------------------------------------------------
To use the Flash API, the following steps
must be followed:
1. Modify Flash2802x_API_Config.h for your targets operating
conditions.
2. Include Flash2802x_API_Library.h in the application.
3. Add the approparite Flash API library to the project.
The user's code is responsible for the following:
4. Initalize the PLL to the proper CPU operating frequency.
5. If required, copy the flash API functions into on-chip zero waitstate
RAM.
6. Initalize the Flash_CPUScaleFactor variable to SCALE_FACTOR
7. Initalize the callback function pointer or set it to NULL
8. Optional: Run the Toggle test to confirm proper frequency configuration
of the API.
9. Optional: Unlock the CSM.
10. Make sure the PLL is not running in limp mode
11. Call the API functions: Flash_Erase(), Flash_Program(), Flash_Verify()
The API functions will:
Disable the watchdog
Check the device PARTID.
Disable interrupts during time critical code.
Perform the desired operation and return status
------------------------------------------------------------------*/
Uint16 Status;
/*------------------------------------------------------------------
Initalize the PLLCR value before calling any of the F2802x Flash API
functions.
Check to see if the PLL needs to changed
PLLCR_VALUE is defined in Example_Flash2802x_API.h
1) Make sure PLL is not in limp mode
2) Disable missing clock detect logic
3) Make the change
4) Wait for the DSP to switch to the PLL clock
This wait is performed to ensure that the flash API functions
will be executed at the correct frequency.
5) While waiting, feed the watchdog so it will not reset.
6) Re-enable the missing clock detect logic
------------------------------------------------------------------*/
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2802x_SysCtrl.c file.
//InitSysCtrl();
/*------------------------------------------------------------------
Unlock the CSM.
If the API functions are going to run in unsecured RAM
then the CSM must be unlocked in order for the flash
API functions to access the flash.
If the flash API functions are executed from secure memory
(L0-L3) then this step is not required.
------------------------------------------------------------------*/
Status = Example_CsmUnlock();
if(Status != STATUS_SUCCESS)
{
Example_Error(Status);
}
/*------------------------------------------------------------------
Copy API Functions into SARAM
The flash API functions MUST be run out of internal
zero-waitstate SARAM memory. This is required for
the algos to execute at the proper CPU frequency.
If the algos are already in SARAM then this step
can be skipped.
DO NOT run the algos from Flash
DO NOT run the algos from external memory
------------------------------------------------------------------*/
// If the build links in the 2802x_FlashAPI_BootROMSymbols.lib, then
// The API is in boot ROM and we do not need to copy it from flash.
//
// If the build links in the software API library:
// i.e. Flash2802x_API_<version>.lib
// then we need to copy the flash API from the flash memory to RAM.
#if (BOOT_ROM_API == 0)
// Example_MemCopy(&Flash28_API_LoadStart, &Flash28_API_LoadEnd, &Flash28_API_RunStart);
#endif
// We must also copy required user interface functions to RAM.
// Example_MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
/*------------------------------------------------------------------
Initalize Flash_CPUScaleFactor.
Flash_CPUScaleFactor is a 32-bit global variable that the flash
API functions use to scale software delays. This scale factor
must be initalized to SCALE_FACTOR by the user's code prior
to calling any of the Flash API functions. This initalization
is VITAL to the proper operation of the flash API functions.
SCALE_FACTOR is defined in Example_Flash2802x_API.h as
#define SCALE_FACTOR 1048576.0L*( (200L/CPU_RATE) )
This value is calculated during the compile based on the CPU
rate, in nanoseconds, at which the algorithums will be run.
------------------------------------------------------------------*/
EALLOW;
Flash_CPUScaleFactor = SCALE_FACTOR;
EDIS;
/*------------------------------------------------------------------
Initalize Flash_CallbackPtr.
Flash_CallbackPtr is a pointer to a function. The API uses
this pointer to invoke a callback function during the API operations.
If this function is not going to be used, set the pointer to NULL
NULL is defined in <stdio.h>.
------------------------------------------------------------------*/
EALLOW;
Flash_CallbackPtr = &MyCallbackFunction;
EDIS;
MyCallbackCounter = 0; // Increment this counter in the callback function
// Jump to SARAM and call the Flash API functions
// Example_CallFlashAPI();
}