Other Parts Discussed in Thread: C2000WARE, TMS320F28388D, SYSCONFIG, TMDSCNCD28388D
主题中讨论的其他器件:TMS320F28388D、 SysConfig、C2000WARE、
工具与软件:
您好
我正在尝试通过 SPI 获得 LS7366R iC 的寄存器值,然而,我有一些问题,我需要一些帮助,因为我不能解决这些问题大约3周...
这是我想在 LS7366R (SPI 从器件)和 TMS320F28388D (SPI 主器件)之间制作的 SPI 协议图。
(这是 LS7366R 数据表中的图表。 LS7366R 数据表链接: https://lsicsi.com/datasheets/LS7366R.pdf
我设置了 SysConfig 设置、写入代码、并将 SPI 线路连接到示波器。 这些图片是我的 SysConfig 设置、代码和 示波器 信号截屏。
//############################################################################# // // FILE: spi_ex1_loopback.c // // TITLE: SPI Digital Loopback // //! \addtogroup driver_example_list //! <h1>SPI Digital Loopback</h1> //! //! This program uses the internal loopback test mode of the SPI module. This //! is a very basic loopback that does not use the FIFOs or interrupts. A //! stream of data is sent and then compared to the received stream. //! The pinmux and SPI modules are configure through the sysconfig file. //! //! The sent data looks like this: \n //! 0000 0001 0002 0003 0004 0005 0006 0007 .... FFFE FFFF 0000 //! //! This pattern is repeated forever. //! //! \note This example project has support for migration across our C2000 //! device families. If you are wanting to build this project from launchpad //! or controlCARD, please specify in the .syscfg file the board you're using. //! At any time you can select another device to migrate this example. //! //! \b External \b Connections \n //! - None //! //! \b Watch \b Variables \n //! - \b sData - Data to send //! - \b rData - Received data //! // //############################################################################# // // // $Copyright: // Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# /*Included Files*/ #include "driverlib.h" #include "device.h" #include "board.h" #include <stdio.h> /*IR REG*/ //OP CODE #define CLR_REG 0x00 #define RD_REG 0x40 #define WR_REG 0x80 #define LOAD_REG 0xC0 //SEL REG #define MDR0 0x00 | (0b001 << 3) #define MDR1 0x00 | (0b010 << 3) /*MDR0 SETTING*/ #define MDR0_4QUAD_MODE 0x00 | 0b11 /*MDR1 SETTING*/ #define MDR1_4BYTE_MODE 0x00 | 0b00 #define STE_HIGH GPIO_writePin(SPISTE, 1) #define STE_LOW GPIO_writePin(SPISTE, 0) #define STE_STATE GPIO_readPin(SPISTE) /*private code*/ #define nData 2 uint16_t TxData[nData] = {0,}; uint16_t RxData[nData] = {0,}; /*Main*/ void main(void) { /*start settings*/ // Initialize device clock and peripherals Device_init(); // Disable pin locks and enable internal pullups. Device_initGPIO(); // Initialize PIE and clear PIE registers. Disables CPU interrupts. Interrupt_initModule(); // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). Interrupt_initVectorTable(); // Board initialization Board_init(); // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) EINT; ERTM; /*USER CODE*/ STE_HIGH; while(1) { STE_LOW; TxData[0] = (WR_REG | MDR0); TxData[1] = (MDR0_4QUAD_MODE); SPI_writeDataBlockingNonFIFO(mySPI0_BASE, (TxData[0] << 8U)); SPI_writeDataBlockingNonFIFO(mySPI0_BASE, (TxData[1] << 8U)); // DEVICE_DELAY_US(200); STE_HIGH; DEVICE_DELAY_US(20); // DEVICE_DELAY_US(1000); // // STE_LOW; // SPI_writeDataBlockingNonFIFO(mySPI0_BASE, (RD_REG | MDR0) << 8U); // RxData[0] = SPI_readDataBlockingNonFIFO(mySPI0_BASE); // DEVICE_DELAY_US(20); // STE_HIGH; // // DEVICE_DELAY_US(1000); } } // // End File //
CLK 只能在 STE ==低电平时工作、CLK 也能在 STE ==高电平时工作。
如果您看看主代码的逻辑、绝对没有理由使 CLK 工作、因为它在数据传输后将 STE 升高到高电平、但我不知道它为什么如此。
查看示波器波形、SPI_writeDataBlockingNonFIFO 和 STE 似乎独立运行。
这是因为 STE 和 GPIO 的操作吗? 我不知道为什么。。。
为了解决数据传输函数处于 STE==LOW 状态时不工作的问题、在 SPI_writeDataBlockingNonFIFO 和 STE_HIGH 之间任意指定了 DEVICE_DELAY_US (200)、并获取以下波形。
此时、观察 STE (=SS)波形时、低电平状态恰好保持在200us 左右。
我是按代码顺序编写的、但 GPIO 和 SPI 是独立移动的吗? 我该如何看待这个现象?
如果这是使用 GPIO 进行控制引起的问题、我应如何在 SysConfig 的 SPI 中设置该问题以连续发送两个8位数据?