主题中讨论的其他器件:SysConfig、 C2000WARE
工具与软件:
硬件:控制卡 F28379D
产品:C2000Ware 5.1.0.00和 SysConfig 1.18.0
问题:
一个 包含 SysConfig 文件的闪烁项目、用于设置外设。
SysConfig 会生成在将构建配置用作 CPU1_RAM 时编译和正常运行的代码、但在设置活动配置 CPU1_FLASH 时、SysConfig 会在构建中显示错误:
Building file: "../config.syscfg"
Invoking: SysConfig
"C:/ti/ccs1250/ccs/utils/sysconfig_1.18.0/sysconfig_cli.bat" -s "C:/ti/C2000Ware_5_01_00_00/.metadata/sdk.json" -d "F2837xD" --script "C:/git/firmware/f28379d_dev/sysconfig/project/config.syscfg" -o "syscfg" --compiler ccs
Running script...
subdir_rules.mk:16: recipe for target 'build-427106431' failed
Error: cannot set '$assign' to 'hsecDigital.69': No option named hsecDigital.69 defined, valid options are
Any
GPIO18
ball.9
GPIO62
ball.57
GPIO70
ball.76
GPIO10
ball.100
GPIO13
ball.4
GPIO17
ball.8
GPIO21
ball.13
GPIO73
ball.81
at setHelper (C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\src\pinmux\services\objectManagers\proxyHandlers\managedObjectProxyHandler.ts:162:10)
at Object.set (C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\src\pinmux\services\objectManagers\proxyHandlers\managedObjectProxyHandler.ts:29:10)
at scriptFunc (C:\git\firmware\f28379d_dev\sysconfig\sysconfig-base-perphase\config.syscfg:200:27)
at cb (C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\src\pinmux\services\scripting\runScript.ts:112:7)
at Object.withDeprecatedAccess (C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\src\pinmux\services\deprecatedAccessGuard.ts:14:10)
at Object.runAsUserScript (C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\src\pinmux\services\scripting\scriptingGuard.ts:61:3)
at iteratee (C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\src\pinmux\services\scripting\runScript.ts:110:5)
at baseEach (C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\node_modules\lodash\lodash.js:530:11)
at Function.each (C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\node_modules\lodash\lodash.js:9409:52)
at C:\ti\ccs1250\ccs\utils\sysconfig_1.18.0\dist\webpack:\src\pinmux\services\scripting\runScript.ts:108:6
gmake[1]: *** [build-427106431] Error 1
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
makefile:140: recipe for target 'all' failed
**** Build Finished ****
SysConfig 文件的内容如下:
/**
* These arguments were used when this file was generated. They will be automatically applied on subsequent loads
* via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
* @cliArgs --board "/boards/TMDSCNCD28379D" --context "CPU1" --product "C2000WARE@5.01.00.00"
* @versions {"tool":"1.18.0+3266"}
*/
/**
* Import the modules used in this configuration.
*/
const can = scripting.addModule("/driverlib/can.js", {}, false);
const can1 = can.addInstance();
const sci = scripting.addModule("/driverlib/sci.js", {}, false);
const sci1 = sci.addInstance();
const sci2 = sci.addInstance();
const spi = scripting.addModule("/driverlib/spi.js", {}, false);
const spi1 = spi.addInstance();
/**
* Write custom configuration values to the imported modules.
*/
can1.useCase = "CUSTOM";
can1.useInterfacePins = ["CANRX@","CANTX@"];
can1.startModule = false;
can1.$name = "CANDSP";
can1.can.canrxPin.$assign = "hsecDigital.69";
can1.can.cantxPin.$assign = "hsecDigital.67";
scripting.suppress("Connected to hardware,@@@.+?@@@ is connected to SPIA on the Control Card F28379D\\. Consider selecting it in 'use hardware' above\\. @@@.+?@@@", can1.can, "canrxPin");
scripting.suppress("Connected to hardware,@@@.+?@@@ is connected to SPIA on the Control Card F28379D\\. Consider selecting it in 'use hardware' above\\. @@@.+?@@@", can1.can, "cantxPin");
sci1.$name = "UART";
sci1.sci.scirxdPin.$assign = "hsecDigital.73";
sci1.sci.scitxdPin.$assign = "hsecDigital.71";
scripting.suppress("Connected to hardware,@@@.+?@@@ is connected to SPIA on the Control Card F28379D\\. Consider selecting it in 'use hardware' above\\. @@@.+?@@@", sci1.sci, "scirxdPin");
scripting.suppress("Connected to hardware,@@@.+?@@@ is connected to SPIA on the Control Card F28379D\\. Consider selecting it in 'use hardware' above\\. @@@.+?@@@", sci1.sci, "scitxdPin");
sci2.$name = "UART_POCKETBEAGLE";
sci2.sci.$assign = "SCIA";
sci2.sci.scirxdPin.$assign = "hsecDigital.121";
sci2.sci.scitxdPin.$assign = "hsecDigital.122";
spi1.$name = "SPI_DAC1";
spi1.mode = "SPI_MODE_CONTROLLER";
spi1.useCase = "3-WIRE MASTER";
spi1.spi.spi_picoPin.$assign = "hsecDigital.125";
spi1.spi.spi_clkPin.$assign = "hsecDigital.108";
spi1.spi.spi_ptePin.$assign = "hsecDigital.110";
/**
* Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
* version of the tool will not impact the pinmux you originally saw. These lines can be completely deleted in order to
* re-solve from scratch.
*/
can1.can.$suggestSolution = "CANB";
sci1.sci.$suggestSolution = "SCIB";
spi1.spi.$suggestSolution = "SPIB";
这是 SysConfig 的错误吗、还是遗漏了什么?
谢谢!