Other Parts Discussed in Thread: TMS320F280025C
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMS320F280025C 工具与软件:
您好!
具有 TMS320F280025C 控制器的16 x 2 LCD 显示屏。 我附上了一个电路供您参考。 给出给 LCD 的电源电压为+5VDC。 但 LCD 完全空白、第一行显示黑盒。 背光工作正常。 用于调节对比度的电位计为1k。 请提供任何帮助。 我在这里编写代码供您参考。
#include "F28x_Project.h" #include "common.h" #include "extern.h" #include "math.h" void main(void) { // // Initialize device clock and peripherals // InitSysCtrl(); // // Initialize GPIO // InitGpio(); // // Disable CPU interrupts // DINT; // // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // InitPieCtrl(); // // Disable CPU interrupts and clear all CPU interrupt flags: // IER = 0x0000; IFR = 0x0000; // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // InitPieVectTable(); lcd_init(); EALLOW; // // Enable PIE interrupt // PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // // Enable global Interrupts and higher priority real-time debug events: // IER |= M_INT1; // Enable group 1 interrupts EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM while(1) { send_string("Hello, LCD!"); DELAY_US(1000); // Delay for 1 second } } void lcd_init(void) { GpioCtrlRegs.GPBMUX1.bit.GPIO40 = 0; GpioCtrlRegs.GPBDIR.bit.GPIO40 = 1; GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 0; GpioCtrlRegs.GPBDIR.bit.GPIO41 = 1; GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 0; GpioCtrlRegs.GPADIR.bit.GPIO23 = 1; GpioCtrlRegs.GPAMUX2.bit.GPIO22 = 0; GpioCtrlRegs.GPADIR.bit.GPIO22 = 1; // Configure LCD control pins as outputs GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 0; // RS GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; // EN GpioCtrlRegs.GPADIR.bit.GPIO1 = 1; // RS GpioCtrlRegs.GPADIR.bit.GPIO0 = 1; // EN DELAY_US(15000); // 15000us...0.015 seconds DELAY_US(4100); // 4100us DELAY_US(100); send_command(0x33); // 4 bit mode send_command(0x32); // 4 bit mode DELAY_US(4100); send_command(0x28); // 4 bit mode DELAY_US(40); send_command(0x0E); // display on cursor on DELAY_US(40); send_command(0x01); // clear the screen DELAY_US(40); send_command(0x06); // increment cursor DELAY_US(1640); send_command(0x80); // row 1 column 1 DELAY_US(4100); } void send_command(unsigned char cmd) { GpioDataRegs.GPACLEAR.bit.GPIO1 = 1; // RS = 0 (command mode) GpioDataRegs.GPASET.bit.GPIO0 = 1; // EN = 1 (enable high) GpioDataRegs.GPBDAT.bit.GPIO40 = (cmd >> 4) & 0x01; GpioDataRegs.GPADAT.bit.GPIO23 = (cmd >> 5) & 0x01; GpioDataRegs.GPBDAT.bit.GPIO41 = (cmd >> 6) & 0x01; GpioDataRegs.GPADAT.bit.GPIO22 = (cmd >> 7) & 0x01; GpioDataRegs.GPACLEAR.bit.GPIO0 = 1; // EN = 0 (enable low) DELAY_US(2000); // Delay required for command execution GpioDataRegs.GPASET.bit.GPIO0 = 1; // EN = 1 (enable high) GpioDataRegs.GPBDAT.bit.GPIO40 = cmd & 0x01; GpioDataRegs.GPADAT.bit.GPIO23 = (cmd >> 1) & 0x01; GpioDataRegs.GPBDAT.bit.GPIO41 = (cmd >> 2) & 0x01; GpioDataRegs.GPADAT.bit.GPIO22 = (cmd >> 3) & 0x01; GpioDataRegs.GPACLEAR.bit.GPIO0 = 1; // EN = 0 (enable low) DELAY_US(2000); } void send_string(char *s) { while(*s) { send_data(*s); s++; } } void send_data(unsigned char data) { GpioDataRegs.GPASET.bit.GPIO1 = 1; // RS = 1 (Data mode) GpioDataRegs.GPASET.bit.GPIO0 = 1; // EN = 1 (enable high) GpioDataRegs.GPBDAT.bit.GPIO40 = (data >> 4) & 0x01; GpioDataRegs.GPADAT.bit.GPIO23 = (data >> 5) & 0x01; GpioDataRegs.GPBDAT.bit.GPIO41 = (data >> 6) & 0x01; GpioDataRegs.GPADAT.bit.GPIO22 = (data >> 7) & 0x01; GpioDataRegs.GPACLEAR.bit.GPIO0 = 1; // EN = 0 (enable low) DELAY_US(2000); // Delay required for command execution GpioDataRegs.GPASET.bit.GPIO0 = 1; // EN = 1 (enable high) GpioDataRegs.GPBDAT.bit.GPIO40 = data & 0x01; GpioDataRegs.GPADAT.bit.GPIO23 = (data >> 1) & 0x01; GpioDataRegs.GPBDAT.bit.GPIO41 = (data >> 2) & 0x01; GpioDataRegs.GPADAT.bit.GPIO22 = (data >> 3) & 0x01; GpioDataRegs.GPACLEAR.bit.GPIO0 = 1; // EN = 0 (enable low) DELAY_US(2000);
}