This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280038C-Q1:与链接器命令文件相关的 UNIFLASH 编程错误(存储器映射)

Guru**** 2558250 points
Other Parts Discussed in Thread: UNIFLASH, TIDM-02009

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1385707/tms320f280038c-q1-uniflash-programming-error-related-to-linkercommand-file-memory-mapping

器件型号:TMS320F280038C-Q1
主题中讨论的其他器件:UNIFLASHTIDM-02009

工具与软件:

您好!

我有一个非常好的项目。 我需要派一个不在办公室的人将程序加载到闪存中。 我将尝试使用 UNIFLASH 程序。

当我尝试使用 CCS 加载程序时、没有错误、我很好地使用了项目。

当我尝试使用加载相同的程序时。 UNIFLASH 导出文件中看到以下错误。

      [错误] C28xx_CPU1:文件加载程序:验证失败:地址0x080001的值@程序不匹配请验证目标存储器和存储器映射。]

我使用 TI DCL 函数、需要更改链接器命令文件。 这个问题可能会引起。 但是、在 CCS 上我没有这个问题。

这是我的连接器命令文件。

/*
//###########################################################################
//
// FILE:	F280038_flash_lnk.cmd
//
// TITLE:	Linker Command File For F280038 Device
//
//###########################################################################
*/
MEMORY
{

   BOOT_RSVD		: origin = 0x00000002, length = 0x00000126

   RAMM0           	: origin = 0x00000128, length = 0x000002D8
   RAMM1            : origin = 0x00000400, length = 0x000003F8     /* on-chip RAM block M1 */
// RAMM1_RSVD       : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   RAMLS0           : origin = 0x00008000, length = 0x00000800
   RAMLS1LS2        : origin = 0x00008800, length = 0x00001000
   RAMLS3           : origin = 0x00009800, length = 0x00000800
//   RAMLS4           : origin = 0x0000A000, length = 0x00000800
//   RAMLS5LS6LS7        : origin = 0x0000A800, length = 0x00001800
   RAMLS4LS5LS6LS7        : origin = 0x0000A000, length = 0x00002000
//   RAMLS6           : origin = 0x0000B000, length = 0x00000800
//   RAMLS7           : origin = 0x0000B800, length = 0x00000800

   /* Combining all the LS RAMs */
   //RAMLS            : origin = 0x00008000, length = 0x00004000

   RAMGS0GS1        : origin = 0x0000C000, length = 0x00002000
//   RAMGS1           : origin = 0x0000D000, length = 0x00001000
   RAMGS2           : origin = 0x0000E000, length = 0x00001000
   RAMGS3           : origin = 0x0000F000, length = 0x00000FF8
// RAMGS3_RSVD       : origin = 0x000FFF8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   BOOTROM          : origin = 0x003F8000, length = 0x00007FC0
   SECURE_ROM       : origin = 0x003F2000, length = 0x00006000

   RESET            : origin = 0x003FFFC0, length = 0x00000002

#ifdef __TI_COMPILER_VERSION__
   #if __TI_COMPILER_VERSION__ >= 20012000
GROUP {      /* GROUP memory ranges for crc/checksum of entire flash */
   #endif
#endif
   BEGIN           	: origin = 0x00080000, length = 0x00000002
   /* Flash sectors */
   /* BANK 0 */
   FLASH_BANK0_SEC0  		: origin = 0x080002, length = 0x000FFE
   FLASH_BANK0_SEC1			: origin = 0x081000, length = 0x001000
   FLASH_BANK0_SEC2  		: origin = 0x082000, length = 0x001000
   FLASH_BANK0_SEC3  		: origin = 0x083000, length = 0x001000
   FLASH_BANK0_SEC4  		: origin = 0x084000, length = 0x001000
   FLASH_BANK0_SEC5  		: origin = 0x085000, length = 0x001000
   FLASH_BANK0_SEC6  		: origin = 0x086000, length = 0x001000
   FLASH_BANK0_SEC7  		: origin = 0x087000, length = 0x001000
   FLASH_BANK0_SEC8  		: origin = 0x088000, length = 0x001000
   FLASH_BANK0_SEC9  		: origin = 0x089000, length = 0x001000
   FLASH_BANK0_SEC10 		: origin = 0x08A000, length = 0x001000
   FLASH_BANK0_SEC11_12_13 	: origin = 0x08B000, length = 0x003000
   FLASH_BANK0_SEC14 		: origin = 0x08E000, length = 0x001000
   FLASH_BANK0_SEC15 		: origin = 0x08F000, length = 0x001000

   /* BANK 1 */
   FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000
   FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000
   FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000
   FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000
   FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000
   FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000
   FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000
   FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000
   FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000
   FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000
   FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000
   FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000
   FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000
   FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000
   FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000
   FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000

  /* BANK 2 */
   FLASH_BANK2_SEC0  : origin = 0x0A0000, length = 0x001000
   FLASH_BANK2_SEC1  : origin = 0x0A1000, length = 0x001000
   FLASH_BANK2_SEC2  : origin = 0x0A2000, length = 0x001000
   FLASH_BANK2_SEC3  : origin = 0x0A3000, length = 0x001000
   FLASH_BANK2_SEC4  : origin = 0x0A4000, length = 0x001000
   FLASH_BANK2_SEC5  : origin = 0x0A5000, length = 0x001000
   FLASH_BANK2_SEC6  : origin = 0x0A6000, length = 0x001000
   FLASH_BANK2_SEC7  : origin = 0x0A7000, length = 0x001000
   FLASH_BANK2_SEC8  : origin = 0x0A8000, length = 0x001000
   FLASH_BANK2_SEC9  : origin = 0x0A9000, length = 0x001000
   FLASH_BANK2_SEC10 : origin = 0x0AA000, length = 0x001000
   FLASH_BANK2_SEC11 : origin = 0x0AB000, length = 0x001000
   FLASH_BANK2_SEC12 : origin = 0x0AC000, length = 0x001000
   FLASH_BANK2_SEC13 : origin = 0x0AD000, length = 0x001000
   FLASH_BANK2_SEC14 : origin = 0x0AE000, length = 0x001000
   FLASH_BANK2_SEC15 : origin = 0x0AF000, length = 0x000FF0
   FLASH_BANK2_SEC15_DO_NOT_USE : origin = 0x0AFFF0, length = 0x000010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

#ifdef __TI_COMPILER_VERSION__
  #if __TI_COMPILER_VERSION__ >= 20012000
}  crc(_ccs_flash_checksum, algorithm=C28_CHECKSUM_16)
  #endif
#endif

}


SECTIONS
{
   codestart        : > BEGIN, ALIGN(8)
   .text            : >> FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3 | FLASH_BANK0_SEC4 | FLASH_BANK0_SEC5 | FLASH_BANK0_SEC6 | FLASH_BANK0_SEC7 ,   ALIGN(8)
   .cinit           : > FLASH_BANK0_SEC1,  ALIGN(8)
   .switch          : > FLASH_BANK0_SEC1,  ALIGN(8)
   .reset           : > RESET,                  TYPE = DSECT /* not used, */

   .stack           : > RAMM1

#if defined(__TI_EABI__)
   .init_array      : > FLASH_BANK0_SEC1,  ALIGN(8)
   .bss             : >> RAMLS4LS5LS6LS7,  ALIGN(8)
   .bss:output      : > RAMLS3
   .bss:cio         : > RAMLS0
   .data            : > RAMLS5
   .sysmem          : > RAMLS4LS5LS6LS7
   .const           : > FLASH_BANK0_SEC4,  ALIGN(8)
#else
   .pinit           : > FLASH_BANK0_SEC1,  ALIGN(8)
   .ebss            : >> RAMLS4LS5LS6LS7,  ALIGN(8)
   .esysmem         : > RAMLS4LS5LS6LS7
   .cio             : > RAMLS0
   .econst          : > FLASH_BANK0_SEC4,  ALIGN(8)
#endif

//    ramgs0 : > RAMGS0, PAGE = 1
//    ramgs1 : > RAMGS1, PAGE = 1

    /*  Allocate IQ math areas: */
   IQmath           : > FLASH_BANK0_SEC1, ALIGN(8)
   IQmathTables     : > FLASH_BANK0_SEC2, ALIGN(8)

   .TI.ramfunc      : LOAD = FLASH_BANK0_SEC1,
                      RUN = RAMGS0GS1,
                      LOAD_START(_RamfuncsLoadStart),
                      LOAD_SIZE(_RamfuncsLoadSize),
                      LOAD_END(_RamfuncsLoadEnd),
                      RUN_START(_RamfuncsRunStart),
                      RUN_SIZE(_RamfuncsRunSize),
                      RUN_END(_RamfuncsRunEnd),
                      ALIGN(8)

   /* crc/checksum section configured as COPY section to avoid including in executable */
   .TI.memcrc          : type = COPY


     GROUP
    {
        isrcodefuncs
        dclfuncs
    }    LOAD = FLASH_BANK0_SEC11_12_13,
		 RUN =  RAMLS4LS5LS6LS7,
         LOAD_START(_isrcodefuncsLoadStart),
         LOAD_SIZE(_isrcodefuncsLoadSize),
         LOAD_END(_isrcodefuncsLoadEnd),
         RUN_START(_isrcodefuncsRunStart),
         RUN_SIZE(_isrcodefuncsRunSize),
         RUN_END(_isrcodefuncsRunEnd),
         PAGE = 0, ALIGN(4)
}
/*
//###########################################################################
// End of file.
//###########################################################################
*/

1)问题的原因是什么?

2)如何解决?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    当我尝试使用编程时,我也遇到了以下错误。 通过 UNIFLASH 生成十六进制文件。
    第7行错误:校验和不匹配(校验和:11、计算:0)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这与之前的内容无关、但我有一个问题要问您。 我有一些关于 TIDM-02009 DC to DC 的问题、我没有您的电子邮件地址、所以我会离开我的电子邮件地址。 请与我分享您的电子邮件吗?   op2020@daum.net

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Gokhan:

    我现在被分配到这个职位。

    关于验证错误:它不是来自闪存擦除/编程。  它来自根据您提供的文件对存储器进行独立验证。  您确定之前在器件上编程了同一个文件吗?

    关于 Checksun 不匹配:是否可以启用 Verbose 输出模式并发送完整的控制台窗口错误消息?

    谢谢。此致、

    Vamsi  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    崔熙燮

    请为您的查询打开单独的 E2E 帖子。

    谢谢。此致、

    Vamsi

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vamsi:

    关于验证错误:并非来自闪存擦除/编程。  它来自根据您提供的文件对存储器进行独立验证。  您确定之前在器件上编程了同一个文件吗?[/QUOT]

    实际上、我无法加载程序。 后来,我尝试了验证。 因此、它导致了此类错误。 我现在了解到、我需要首先加载程序才能验证。

    [报价 userid="16728" url="~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1385707/tms320f280038c-q1-uniflash-programming-error-related-to-linkercommand-file-memory-mapping/5298968 #5298968"]

    关于 Checksun 不匹配:是否可以启用 Verbose 输出模式并发送完整的控制台窗口错误消息?

    [报价]

    您能否指导我如何启用详细输出模式?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Gokhan:

    好的、感谢您澄清由于未加载代码、因此验证失败。  这样可以确认我的评估。

    关于控制台输出和调试日志:请搜索"为了分析刷写故障、我们应该向 TI 发送什么调试信息?" 在本常见问题解答中: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1096194/faq-c2000-ccs-flash-plugin-and-uniflash 

    谢谢。此致、

    Vamsi