This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28335:C2000微控制器论坛

Guru**** 2533780 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1385194/tms320f28335-c2000-microcontrollers-forum

器件型号:TMS320F28335

工具与软件:

您好、

我是学习 DSP 的初学者。 在针对 eCAN 的 A 到 B 输出使用示例程序时、我遇到了一个问题、在这个问题上、无论怎样、波形都不会改变。 即使我修改数据或 ID、此问题仍然存在。

有人可以帮我吗?

此波形是通过示波器上的触发器获得的。

//###########################################################################
//
// FILE:   Example_2833xEcanA_to_B_Xmit.c
//
// TITLE:  eCAN-A to eCAN-B Transmit Loop Example
//
//! \addtogroup f2833x_example_list
//! <h1>eCAN-A to eCAN-B Transmit Loop (ecan_a_to_b_xmit)</h1>
//!
//! This example TRANSMITS data to another CAN module using MAILBOX5
//! This program could either loop forever or transmit "n" # of times,
//! where "n" is the TXCOUNT value. \n
//!
//! This example can be used to check CAN-A and CAN-B. Since CAN-B is
//! initialized in DSP2833x_ECan.c, it will acknowledge all frames
//! transmitted by the node on which this code runs. Both CAN ports of
//! the 2833x DSP need to be connected to each other (via CAN transceivers)
//!
//! \b External \b Connections \n
//! - eCANA is on GPIO31 (CANTXA) and GPIO30 (CANRXA)
//! - eCANB is on GPIO8 (CANTXB) and GPIO10 (CANRXB)
//! - Connect eCANA  to eCANB via CAN transceivers
//
//###########################################################################
// $TI Release: $
// $Release Date: $
// $Copyright:
// Copyright (C) 2009-2024 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

//
// Defines
//
#define TXCOUNT  100            // Transmission will take place (TXCOUNT) times

//
// Globals
//
long      i;
long 	  loopcount = 0;

//
// Main
//
void main(void)
{
    //
    // Create a shadow register structure for the CAN control registers. 
    // This is needed, since only 32-bit access is allowed to these registers. 
    // 16-bit access to these registers could potentially corrupt the register 
    // contents or return false data.
    //
    struct ECAN_REGS ECanaShadow;

    //
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the DSP2833x_SysCtrl.c file.
    //
    InitSysCtrl();

    //
    // Step 2. Initialize GPIO:
    // This example function is found in the DSP2833x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    //
    // InitGpio();  // Skipped for this example

    //
    // Just initialize eCAN pins for this example
    // This function is in DSP2833x_ECan.c
    //
    InitECanGpio();

    //
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    //
    DINT;

    //
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the DSP2833x_PieCtrl.c file.
    //
    InitPieCtrl();

    //
    // Disable CPU interrupts and clear all CPU interrupt flags
    //
    IER = 0x0000;
    IFR = 0x0000;

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in DSP2833x_DefaultIsr.c.
    // This function is found in DSP2833x_PieVect.c.
    //
    InitPieVectTable();

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    //

    //
    // No interrupts used in this example.
    //

    //
    // Step 4. Initialize all the Device Peripherals:
    // This function is found in DSP2833x_InitPeripherals.c
    //
    // InitPeripherals(); // Not required for this example

    //
    // In this case just initialize eCAN-A and eCAN-B
    // This function is in DSP2833x_ECan.c
    //
    InitECan();

    //
    // Step 5. User specific code
    //

    //
    // Write to the MSGID field
    //
    ECanaMboxes.MBOX25.MSGID.all = 0x95555555;          // Extended Identifier

    //
    // Configure Mailbox under test as a Transmit mailbox
    //
    ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
    ECanaShadow.CANMD.bit.MD25 = 0;
    ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;

    //
    // Enable Mailbox under test
    //
    ECanaShadow.CANME.all = ECanaRegs.CANME.all;
    ECanaShadow.CANME.bit.ME25 = 1;
    ECanaRegs.CANME.all = ECanaShadow.CANME.all;

    //
    // Write to DLC field in Master Control reg
    //
    ECanaMboxes.MBOX25.MSGCTRL.bit.DLC = 8;

    //
    // Write to the mailbox RAM field
    //
    ECanaMboxes.MBOX25.MDL.all = 0x55555555;
    ECanaMboxes.MBOX25.MDH.all = 0x55555555;

    //
    // Begin transmitting
    //
    for(i=0; i < TXCOUNT; i++)
    {
        ECanaShadow.CANTRS.all = 0;
        ECanaShadow.CANTRS.bit.TRS25 = 1;     // Set TRS for mailbox under test
        ECanaRegs.CANTRS.all = ECanaShadow.CANTRS.all;

        do
        {
            ECanaShadow.CANTA.all = ECanaRegs.CANTA.all;
        } while(ECanaShadow.CANTA.bit.TA25 == 0 );// Wait for TA5 bit to be set

        ECanaShadow.CANTA.all = 0;
        ECanaShadow.CANTA.bit.TA25 = 1;     	         // Clear TA5
        ECanaRegs.CANTA.all = ECanaShadow.CANTA.all;

        loopcount ++;
    }
    __asm(" ESTOP0");  // Stop here
}

//
// End of File
//

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    波形看起来不像 CAN 信号。 Launchpad 或实验套件是否具有用于 eCAN-A 和 eCAN-B 的收发器? CAN 总线上是否有120欧姆终端电阻器?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这是 DSP 上 Tx 和 Rx 的输出、未连接到任何收发器。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    CAN 总线信号如下所示:

    您的消息 ID 为0x15555555。 位28为1、位27为0、等等 我在您的波形中看不到消息 ID。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、我了解了这部分。 我也清楚地知道这个波形是错误的。 我曾尝试更改 ID 和数据内容、但波形仍未改变。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    示波器的"黑色探头"是否已连接到 GND? 从图中可以看出、您的黑色探头已连接到 GPIO18。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    首先、黑色探针 连接到 GPIO 32。 之后、将其更改为连接到 GND、但波形仍然没有变化。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    很抱歉、由于这个角度、布线位置不是很清楚、但是 图中的红色探针连接到了 GPIO 31、黑色探针连接到了 GPIO 30。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    请将"黑色探头"连接到 GND

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我已经尝试将黑色探针连接 到 GND、但波形仍然没有变化。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    CAN-A 是否连接到 CAN-B? 扩展坞卡上的线缆有什么用? 如果没有 CAN 收发器、则无法将 CAN-A 直接连接到 CAN-B。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在此阶段、我只 检查 DSP 的 Tx 输出状态、未连接任何器件。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我没有 F28335控制卡、但我会探测另一个 F28x LaunchPad 上的 CAN_TX 引脚。 在 TX 引脚上获取信号波形没有问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我正在使用示例程序进行测试、但没有设置任何配置;关于输出设置、是否有任何特定的配置?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    请确保在测试中将 GPIO31和 GPIO30用于 eCAN-A。 eCAN-A 也可以使用 GPIO18和 GPIO19。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    "对不起,我不明白你的意思。"

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您可以配置 eCAN-A 以使用 GPIO18和 GPIO19。

    GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3;//为 CANRXA 配置 GPIO18
    GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 3;// Configure GPIO19 for CANTXA

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我已经尝试过,但它仍然是错误的。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我怀疑 CAN 信号是否正确路由至坞站卡。 您是否可以将  GPIO18/GPIO19或 GPIO30/GPIO31配置为 GPIO 信号、使用 GPIO API 切换这些 GPIO 信号以及检查 GPIO 引脚是否可以切换?

    您可以使用以下示例:

    示例_2833xGpioToggle

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢。 我会尝试它。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的、谢谢