请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMS320F2800157-Q1 工具与软件:
大家好、专家:
客户反馈、他尝试 显式将 float 变量转换为整数、如果 float 的值为负、则转换后的整数的值为0。 但根据他对 C 编程语言中的数据类型的理解、应将其解析为负有符号整数(如果转换为有符号整数)或大无符号整数(如果转换为无符号整数)。
我做了一个简单的测试并得到了类似的结果。 请帮助阐明 C2000器件上将负浮点型转换为整数型时的预期行为。 如果有一些相关文档可以指导客户、那将是完美的。
谢谢。
下面是我的测试代码、以及每个变量的值的屏幕截图。
//############################################################################# // // FILE: empty_driverlib_main.c // //! \addtogroup driver_example_list //! <h1>Empty Project Example</h1> //! //! This example is an empty project setup for Driverlib development. //! // //############################################################################# // // // $Copyright: // Copyright (C) 2024 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // Included Files // #include "driverlib.h" #include "device.h" #include "board.h" #include "c2000ware_libraries.h" float f1 = 1.2345; float f2 = -6.789; unsigned int u1 = 0; unsigned int u2 = 0; signed int s1 = 0; signed int s2 = 0; // // Main // void main(void) { // // Initialize device clock and peripherals // Device_init(); // // Disable pin locks and enable internal pull-ups. // Device_initGPIO(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); // // PinMux and Peripheral Initialization // Board_init(); // // C2000Ware Library initialization // C2000Ware_libraries_init(); // // Enable Global Interrupt (INTM) and real time interrupt (DBGM) // EINT; ERTM; while(1) { u1 = (unsigned int)f1; u2 = (unsigned int)f2; s1 = (unsigned int)f1; s2 = (unsigned int)f2; } } // // End of File //