This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28P650DK:SPI 外部环回示例仅在调试期间有效。

Guru**** 2540720 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1406722/tms320f28p650dk-spi-external-loopback-example-only-works-during-debugging

器件型号:TMS320F28P650DK

工具与软件:

大家好
我想设置 SPI 通信、因此我首先上传了 spi_ex4_external_loopback_fifo_interrupt 示例。 不幸的是、根据我是否设置了断点、它的运行方式有所不同。

没有断点:
如果我让它正常运行、除了芯片选择之外、我可以测量示波器上的所有信号。 这会始终保持低电平、即使它也是低电平有效信号、这就是为什么我实际上会期望至少是高电平的原因。 此外、该参数不变。 因此它会一直保持低电平。

使用断点:
如果我设置一个断点、例如在 SPI_writeDataNonBlocking (SPIB_BASE、sData[i])处;电平始终如预期的高、除非它发送数据、否则它短暂地处于低电平。

有人知道导致这种情况的原因吗? 如果能有任何帮助、我将不胜感激。

//#############################################################################
//
// FILE:   spi_ex4_external_loopback_fifo_interrupt.c
//
// TITLE:  SPI Digital Loopback with FIFO Interrupts
//
//! \addtogroup driver_example_list
//! <h1>SPI Digital External Loopback with FIFO Interrupts</h1>
//!
//! This program uses the external loopback between two SPI modules. Both
//! the SPI FIFOs and their interrupts are used. SPIA is configured as a peripheral
//! and receives data from SPI B which is configured as a controller.
//!
//! A stream of data is sent and then compared to the received stream.
//! The sent data looks like this: \n
//!  0000 0001 \n
//!  0001 0002 \n
//!  0002 0003 \n
//!  .... \n
//!  FFFE FFFF \n
//!  FFFF 0000 \n
//!  etc.. \n
//! This pattern is repeated forever.
//!
//!  \note This example project has support for migration across our C2000
//!  device families. If you are wanting to build this project from launchpad
//!  or controlCARD, please specify in the .syscfg file the board you're using.
//!  At any time you can select another device to migrate this example.
//!
//! \b External \b Connections \n
//! Refer to SysConfig for external connections (GPIO pin numbers) specific to each device
//!
//! \b Watch \b Variables \n
//!  - \b sData - Data to send
//!  - \b rData - Received data
//!  - \b rDataPoint - Used to keep track of the last position in the receive
//!    stream for error checking
//!
//
//#############################################################################
//
// C2000Ware v5.03.00.00
//
// Copyright (C) 2024 Texas Instruments Incorporated - http://www.ti.com
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
//   Redistributions of source code must retain the above copyright
//   notice, this list of conditions and the following disclaimer.
//
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the
//   documentation and/or other materials provided with the
//   distribution.
//
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "board.h"

//
// Globals
//
volatile uint16_t sData[2];                  // Send data buffer
volatile uint16_t rData[2];                  // Receive data buffer
volatile uint16_t rDataPoint = 0;            // To keep track of where we are in the
                                    // data stream to check received data


//
// Function Prototypes
//
__interrupt void spibTxFIFOISR(void);
__interrupt void spiaRxFIFOISR(void);

//
// Main
//
void main(void)
{
    uint16_t i;

    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Disable pin locks and enable internal pullups.
    //
    Device_initGPIO();

    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts.
    //
    Interrupt_initModule();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    Interrupt_initVectorTable();

    //
    // Board initialization
    //
    Board_init();

    //
    // Initialize the data buffers
    //
    for(i = 0; i < 2; i++)
    {
        sData[i] = i;
        rData[i]= 0;
    }

    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

    //
    // Loop forever. Suspend or place breakpoints to observe the buffers.
    //
    while(1)
    {
        ;
    }
}

//
// SPI B Transmit FIFO ISR
//
__interrupt void spibTxFIFOISR(void)
{
    uint16_t i;

    //
    // Send data
    //
    for(i = 0; i < 2; i++)
    {
       SPI_writeDataNonBlocking(SPIB_BASE, sData[i]);
    }

    //
    // Increment data for next cycle
    //
    for(i = 0; i < 2; i++)
    {
       sData[i] = sData[i] + 1;
    }

    //
    // Clear interrupt flag and issue ACK
    //
    SPI_clearInterruptStatus(SPIB_BASE, SPI_INT_TXFF);
    Interrupt_clearACKGroup(INT_SPIB_controller_TX_INTERRUPT_ACK_GROUP);
}

//
// SPI A Receive FIFO ISR
//
 __interrupt void spiaRxFIFOISR(void)
{
    uint16_t i;

    //
    // Read data
    //
    for(i = 0; i < 2; i++)
    {
        rData[i] = SPI_readDataNonBlocking(SPIA_BASE);
    }

    //
    // Check received data
    //
    for(i = 0; i < 2; i++)
    {
        if(rData[i] != (rDataPoint + i))
        {
            // Something went wrong. rData doesn't contain expected data.
//            ESTOP0;
        }
    }

    rDataPoint++;

    //
    // Clear interrupt flag and issue ACK
    //
    SPI_clearInterruptStatus(SPIA_BASE, SPI_INT_RXFF);
    Interrupt_clearACKGroup(INT_SPIA_peripheral_RX_INTERRUPT_ACK_GROUP);
}

 //
 // Enabled only for SysConfig functionality
 //
__interrupt void INT_SPIA_peripheral_TX_ISR(void) {
    //
    // Issue ACK
    //
    Interrupt_clearACKGroup(INT_SPIA_peripheral_TX_INTERRUPT_ACK_GROUP);
}

//
// Enabled only for SysConfig functionality
//
__interrupt void INT_SPIB_controller_RX_ISR(void) {
    //
    // Issue ACK
    //
    Interrupt_clearACKGroup(INT_SPIB_controller_RX_INTERRUPT_ACK_GROUP);

}

//
// End of file
//

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    关于这一主题的专家目前不在办公室,直到星期二9/3,所以请期待一个延迟的答复。 对此造成的不便、我深表歉意。

    此致、
    Delaney

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常好、非常感谢。


  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    在使用硬件断点时也会观察到相同的行为吗? 示例似乎按预期工作、但您会看到不同的结果、具体取决于 BP 的设置方式、这也是预期结果。 您是否也在"Expressions"窗口中观察变量? 正如数据表中指定的、除了在 FIFO 和非 FIFO 模式下的背对背传输字之间的情况外、在字的尾端、SPIPTE 将变为无效。  

    此致、

    Aishwarya.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常感谢。 我还没有尝试过、因为我在两天前安装了一个小的等待环路、就开始工作了。
    当然、我不知道这是否是最佳解决方案、实际上很高兴知道问题是什么、但我现在不能在这上面投入太多时间。

    __interrupt void spibTxFIFOISR(void)
    {
        uint16_t i;
    
        //
        // Send data
        //
        for(i = 0; i < 2; i++)
        {
        
        while(temp < 10000){
                temp++;
            }
    
           SPI_writeDataNonBlocking(SPIB_BASE, sData[i]);
        }
    
        //
        // Increment data for next cycle
        //
        for(i = 0; i < 2; i++)
        {
           sData[i] = sData[i] + 1;
        }
    
        //
        // Clear interrupt flag and issue ACK
        //
        SPI_clearInterruptStatus(SPIB_BASE, SPI_INT_TXFF);
        Interrupt_clearACKGroup(INT_SPIB_controller_TX_INTERRUPT_ACK_GROUP);
    }


  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我认为这里没有任何问题。 由于您将考虑项目、函数调用等的优化而设定的 SWBP、输出会有所不同

    添加该等待环路 绝对是一种可接受的方法、您还可以使用器件延迟功能来帮助确保每次点击 BP 时都会出现在所需的相同位置。

    此致、

    Aishwarya.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您也可以使用设备延迟功能

    不幸的是、我无法做到这一点。 实际上、我想使用 DELAY_US、但我收到以下错误:



  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您还可以尝试使用 SYSCTL.c 中的以下函数: SYSCTL_DELAY (t)。  

    此致、

    Aishwarya.
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常感谢:)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果没有其他问题、我将继续、关闭该主题。

    此致、

    Aishwarya.