This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28P650DK:双核程序中出现 XDS200调试器错误

Guru**** 1800230 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1407106/tms320f28p650dk-xds200-debugger-error-in-dual-core-programs

器件型号:TMS320F28P650DK

工具与软件:

您好!

我正在尝试将我的应用的调试器从 XDS110更改为 XDS200。 该程序涉及双核、并且从两个内核进行擦除和闪存操作、XDS110调试探针没有任何错误。 但是、当我使用 XDS200 USB 调试探针时、程序显示以下错误:

C28xx_CPU1: GEL Output: 
Memory Map Initialization Complete
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ... 
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: 
 CPU2 is out of reset and configured to wait boot.
 (If you connected previously, may have to resume CPU2 to reach wait boot loop.)
C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. User code execution from SR could commence after the selected CPU1/CPU2 flash banks executable are programmed.
C28xx_CPU1: Only CPU1 on-chip Flash Plugin can configure clock for CPU1, and CPU2 Flash operations. Plugin automatically configures PLL when CPU1 Flash operations are invoked. However, if users want to do only CPU2 Flash operations without doing a prior CPU1 operation in the current session, they should click on 'Configure Clock' button in CPU1's on-chip Flash Plugin before invoking CPU2 Flash operations. When this button is used, Flash Plugin will configure the clock for CPU1/CPU2 at 200MHz using INTOSC as the clock source. Plugin will leave PLL config like this and user application should configure the PLL as required by application.
C28xx_CPU1: Before doing any flash operations using the flash plugin, (a) Please select which flash banks should be mapped to which CPU (CPU1 vs CPU2) - This selection should be done in CPU1 flash plugin GUI. (b) Please select the flash banks that the user would like the flash plugin to erase (in the CPU1 flash plugin GUI and the CPU2 flash plugin GUI)
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ... 
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: 
 CPU2 is out of reset and configured to wait boot.
 (If you connected previously, may have to resume CPU2 to reach wait boot loop.)
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ... 
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: 
 CPU2 is out of reset and configured to wait boot.
 (If you connected previously, may have to resume CPU2 to reach wait boot loop.)
C28xx_CPU1: GSxMSEL register configured correctly
C28xx_CPU1: BankMuxSel register configured correctly
C28xx_CPU2: GEL Output: 

RAM initialization done

C28xx_CPU2: GEL Output: 
Memory Map Initialization Complete
C28xx_CPU2: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. User code execution from SR could commence after the selected CPU1/CPU2 flash banks executable are programmed.
C28xx_CPU2: Only CPU1 on-chip Flash Plugin can configure clock for CPU1, and CPU2 Flash operations. Plugin automatically configures PLL when CPU1 Flash operations are invoked. However, if users want to do only CPU2 Flash operations without doing a prior CPU1 operation in the current session, they should click on 'Configure Clock' button in CPU1's on-chip Flash Plugin before invoking CPU2 Flash operations. When this button is used, Flash Plugin will configure the clock for CPU1/CPU2 at 200MHz using INTOSC as the clock source. Plugin will leave PLL config like this and user application should configure the PLL as required by application.
C28xx_CPU2: Before doing any flash operations using the flash plugin, (a) Please select which flash banks should be mapped to which CPU (CPU1 vs CPU2) - This selection should be done in CPU1 flash plugin GUI. (b) Please select the flash banks that the user would like the flash plugin to erase (in the CPU1 flash plugin GUI and the CPU2 flash plugin GUI)
C28xx_CPU2: GSxMSEL register configured correctly
C28xx_CPU2: Error occurred during flash operation: Timed out waiting for target to halt while executing init.alg
C28xx_CPU2: Error during initialization (Flash algorithm timed out). Operation cancelled.
C28xx_CPU2: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash.  If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
C28xx_CPU2: File Loader: Memory write failed: Unknown error
C28xx_CPU2: GEL: File: C:\<path to folder>\CPU2_FLASH_RAM\filename.out: Load failed.

组0、1和2分配给 CPU1、组3和4分配给 CPU2。 目标配置中.ccxml 中的测试连接成功。 针对类似帖子的建议解决方案涉及在调试器模式下访问某些设置、但在调试器模式打开之前、加载失败并退出(本例中介绍了这种情况)。 如何解决此问题?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    请按照说明手动启动调试会话: https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_debug-main.html#launching-a-debug-session

    然后连接到每个 CPU、并相应地修改片上闪存工具、以便将正确的闪存存储体分配给 CPU1和 CPU2。 我认为您的错误是由片上闪存工具错误地分配了闪存组引起的。  

    此致、

    Ben Collier  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    感谢您的答复。 我使用片上闪存工具分配了正确的闪存组。 现在、我可以手动加载程序并成功运行它们。

    但是、自动调试会话仍会出现与之前相同的错误。 我每次都必须启动手动调试会话、在两个内核上手动加载程序、然后运行它们。 我如何使自动调试正常工作?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我认为您应该能够编辑调试配置中的设置、可在"运行">"调试配置"下进行访问。

    此致、

    Ben Collier